powered by CADENAS

Social Share

Moustache (9525 views - Human)

A moustache (UK: ; American English: mustache, ) is facial hair grown on the upper lip. Moustaches can be groomed by trimming and styling with a type of pomade called moustache wax.
Go to Article

Explanation by Hotspot Model

Moustache

Moustache

Moustache

A moustache (UK: /məˈstɑːʃ/; American English: mustache, /ˈmʌstæʃ/)[1] is facial hair grown on the upper lip. Moustaches can be groomed by trimming and styling with a type of pomade called moustache wax.

Etymology

The word "moustache" is French, and is derived from the Italian moustacio (fourteenth century), dialectal mostaccio (16th century), from Medieval Latin moustaccium (eighth century), Medieval Greek μοστάκιον (moustakion), attested in the ninth century, which ultimately originates as a diminutive of Hellenistic Greek μύσταξ (mustax, mustak-), meaning "upper lip" or "facial hair",[2] probably derived from Hellenistic Greek μύλλον (mullon), "lip".[3][4]

History

Shaving with stone razors was technologically possible from Neolithic times, but the oldest portrait showing a shaved man with a moustache is an ancient Iranian (Scythian) horseman from 300 BC.

Various cultures have developed different associations with moustaches. For example, in many 20th-century Arab countries, moustaches are associated with power, beards with Islamic traditionalism, and lack of facial hair with more liberal, secular tendencies.[5] In Islam, trimming the moustache is considered to be a sunnah and mustahabb, that is, a way of life that is recommended, especially among Sunni Muslims. The moustache is also a religious symbol for the male followers of the Yarsan religion.[6]

A traditional Indian belief is that a man's facial hair is a sign of his virility. This caused a problem during the time of British Raj in the 19th Century and, as a result, Indian moustaches had a profound effect on British facial hair. The British Army, who had up until that time were clean shaven, had difficulty maintaining authority among the Indian soldiers, who saw their officers' lack of a moustache, beard and sideburns as a lack of manliness. Eventually British officers began to cultivate moustaches and other facial hair to gain the respect of their troops. The trend of sporting a moustache spread quickly through the army and then back home amongst the general British civilian population.[7][8]

Development and care

The moustache forms its own stage in the development of facial hair in adolescent males.[9]

As with most human biological processes, this specific order may vary among some individuals depending on one's genetic heritage or environment.[10][11]

Moustaches can be tended through shaving the hair of the chin and cheeks, preventing it from becoming a full beard. A variety of tools have been developed for the care of moustaches, including safety razors, moustache wax, moustache nets, moustache brushes, moustache combs and moustache scissors.

In the Middle East, there is a growing trend for moustache transplants, which involves undergoing a procedure called follicular unit extraction in order to attain fuller, and more impressive facial hair.[12]

The longest moustache measures 4.29 m (14 ft) and belongs to Ram Singh Chauhan (India). It was measured on the set of the Italian TV show "Lo Show dei Record" in Rome, Italy, on 4 March 2010.[13]

Styles

The World Beard and Moustache Championships 2007 had six sub-categories for moustaches:[14]

  • Dalí – narrow, long points bent or curved steeply upward; areas past the corner of the mouth must be shaved. Artificial styling aids needed. Named after Salvador Dalí.
  • English moustache – narrow, beginning at the middle of the upper lip the whiskers are very long and pulled to the side, slightly curled; the ends are pointed slightly upward; areas past the corner of the mouth usually shaved. Artificial styling may be needed.
  • Freestyle – All moustaches that do not match other classes. The hairs are allowed to start growing from up to a maximum of 1.5 cm beyond the end of the upper lip. Aids are allowed.
  • Hungarian – Big and bushy, beginning from the middle of the upper lip and pulled to the side. The hairs are allowed to start growing from up to a maximum of 1.5 cm beyond the end of the upper lip.
  • Imperial – whiskers growing from both the upper lip and cheeks, curled upward (distinct from the royale, or impériale)
  • Natural – Moustache may be styled without aids.

Other types of moustache include:

Occurrence and perceptions

Like many other fashion trends, the moustache is subject to shifting popularity through time. Though modern culture often associates moustaches with men of the Victorian Era, Susan Walton shows that at the start of the Victorian Era facial hair was "viewed with distaste" and that the moustache was considered the mark of an artist or revolutionary, both of which remained on the social fringe at the time.[15] This is supported by the fact that only one member of parliament sported facial hair from the years 1841-1847.[15] However, by the 1860s, this changes and moustaches become wildly popular even among distinguished men but by the end of the century facial hair became passé once more.[15] Though one cannot be entirely sure as to the cause of such changes, Walton speculates that the rise of the facial hair trend was due largely in part because the impending war against Russia, and the belief that moustaches and beards projected a more 'manly' image, which was brought about by the so-called 'rebranding' of the British military and the rehabilitation of military virtues.[15] Moustaches became a defining trait of the British soldier, as even late as 1908 no enlisted soldier was permitted to shave his upper lip.[16] However, the next generation of men perceived facial hair, such as moustaches, to be an outdated emblem of masculinity and therefore there was a dramatic decline in the moustache trend and a clean-shaven face became the mark of a modern man.[15]

Marriage

According to a study performed by Nigel Barber, results have shown a strong correlation between a good marriage market for women and an increased number of moustaches worn by the male population.[17] By comparing the number of males pictured in Illustrated London News sporting a moustache against the ratio of single women to single men, the similar trends in the two over the years would suggest that these two factors are correlated.[17] Barber suggests that this correlation may be due to the fact the men with moustaches are perceived to be more attractive, industrious, creative, masculine, dominant and mature by both men and women,[17] as supported by the research conducted by Hellström and Tekle.[18] Barber suggests that these perceived traits would influence a woman's choice of husband as they would suggest a high reproductive and biological qualities, and a capacity to invest in children, so when males must compete heavily for marriage they are more likely to grow a moustache in an attempt to project these qualities.[17] This theory is also supported by the correlation between beard fashion and women wearing long dresses, as shown by Robinson's study,[19] which then relates to the correlation between dress fashion and the marriage market, as shown in Barber's 1999 study.[20]

Illegitimacy ratio

Barber's studies also show that when the illegitimacy ratio, that is, the ratio of illegitimate births in comparison to the number of total births, is high the number of moustaches within the population drops.[17] This negative correlation between moustaches and the illegitimacy ratio would suggest that the illegitimacy ratio may also be a factor in the moustache trend within the population. Barber suggested that as facial expressions are heavily reliant on the mouth, being clean-shaven may give the impression that one's expressions are more readable and therefore more trustworthy, therefore those with no facial hair are perceived as being more trustworthy, which in a time where men outnumber available women, women tend to look for men who appear trustworthy.[17]

Age perception

The moustache and other forms of facial hair are globally understood to be signs of the post-pubescent male,[21] however those with moustaches are perceived to be older than those who are clean-shaven of the same age.[21] This was determined by manipulating a photo of six male subjects, with varying levels of baldness, to have moustaches and beards and then asking undergraduate college students to rate both the photos of the men with facial hair and without facial hair in terms of social maturity, aggression, age, appeasement, and attractiveness. Regardless of how bald the subject was, the results found in relation to the perception of moustaches remained constant. Although males with facial hair were perceived, in general, to be older than the same subject pictured without facial hair,[22] the moustached subjects were also perceived to be far less socially mature.[21] The decreased perception of social maturity of the moustached men may partially be due to the increase in the perception of aggression in the moustached men,[21] as aggression is incompatible with social maturity.[21]

Workplace

In a study performed by J.A. Reed and E.M. Blunk, persons in management positions were shown to positively perceive, and therefore be more likely to hire, men with facial hair.[23] Although men with beards over all scored better than men with only moustaches, the moustached men scored much higher than those men who were clean-shaven.[23] In this experiment 228 persons, both male and female, who held management positions that made hiring decisions were shown ink sketches of six male job applicants. The men in these ink sketches ranged from clean-shaven, to moustached, to bearded. A positive correlation between perception and facial hair. The men with facial hair were rated higher by the employers on aspects of masculinity, maturity, physical attractiveness, dominance, self-confidence, nonconformity, courage, industriousness, enthusiasm, intelligence, sincerity, and general competency.[23] The results were found to be fairly similar for both female and male employers, which Reed and Blunk suggest would imply that gender does not factor into one's perceptions of a moustache on a male applicant.[23] However, Blunk and Reed also stipulate that the meaning and acceptability of facial hair does change depending on the time period. However, the studies performed by Hellström & Tekle[18] and also the studies performed by Klapprott[24] would suggest that moustaches are not favourable to all professions as it has been shown that clean-shaven men are seen as more reliable in roles such as salesmen and professors. Other studies have suggested that acceptability of facial hair may vary depending on culture and location, as in a study conducted in Brazil, clean-shaven men were preferred by personnel managers over applicants who were bearded, goateed, or moustached.[25]

Race

Black men tend to have a higher percentage wearing a mustache than white men in the United States: "A far greater percentage of African- American males than white males wear mustaches today and have always worn mustaches."[26]

Cultures

In Western culture, it has been shown that women dislike men who displayed a visible moustache or beard, but preferred men who had a visible hint of a beard such as stubble (often known as a five-o-clock shadow) over those who were clean-shaven.[27] This supports the idea that in Western culture, females prefer men who have the capability to cultivate facial hair, such as a moustache, but choose not to. However some researchers have suggested that it is possible that in ecologies in which physical aggressiveness is more adaptive than cooperation, bearded men might be preferred by women.[21] However, varying opinion on moustaches is not reserved to international cultural differences as even within the US, there have been discrepancies observed on female preference of male facial hair as Freedman's study suggested that women studying at the University of Chicago preferred men with facial hair because they perceived them to be more masculine, sophisticated and mature than clean-shaven men.[28] Similarly, a study performed by Kenny and Fletcher at Memphis State University, which is largely a commuter school and usually is regarded as more conventional than the University of Chicago, suggested that men with facial hair such as moustaches and beards, were perceived as stronger and more masculine by female students.[29] However, the study performed by Feinman and Gill would suggest that this reaction to facial hair is not nationwide, as women studying in the state of Wyoming showed a marked preference for clean-shaven men over men with facial hair.[30] Some accredit this difference to the difference between region, rurality, and political and social conservatism between the various studies.[30] Thus it can be seen that even within the US, there are slight variations in the perceptions of moustaches.

Religions

In addition to various cultures, the perception of the moustache is also altered by religion as some religions support the growth of a moustache or facial hair in general, whereas others tend to reject those with moustaches, while many churches remain somewhat ambivalent on the subject.

Amish

While Amish men grow beards when married and never trim them, they eschew moustaches and continue shaving their upper lips. This is rooted in a rejection of the German military fashion of sporting moustaches, which was prevalent at the time of the Amish community's formation in Europe, hence serving as a symbol of their commitment to pacifism.

Mormon

Though it is never explicitly stated by The Church of Jesus Christ of Latter-day Saints that all male members must be clean-shaven, within Mormon circles it is often considered "taboo" for men to have moustaches as the missionaries of the church are required to be clean-shaven, and this has become somewhat of a social norm within the church itself.[31] This often leads those members who do choose to wear moustaches feel somewhat like they do not quite fit the norm, and yet in the studies shown done by Nielsen and White, these men reportedly do not mind this feeling and that is why they continue to grow their facial hair.[31]

Islam

Even though facial grooming is not specifically mentioned within the Qur'an, numerous narrations of hadith (sayings of Muhammad) address personal hygiene, including facial hair maintenance.[32] In one such example, Muhammad advised that men must grow beards, and as to moustaches, cut the longer hairs as to not let them cover the upper lips (as this is the Fitra—the origin).[33] Thus, growing a beard while keeping the moustache short and trimmed is a well-established tradition in many Muslim societies.[32]

Notable moustaches

Individuals

The longest moustache measures 4.29 m (14 ft) and belongs to Ram Singh Chauhan of India. It was measured on the set of Lo Show dei Record in Rome, Italy, on 4 March 2010.[34]

In some cases, the moustache is so prominently identified with a single individual that it could identify him without any further identifying traits, as in the cases of Adolf Hitler[quantify] or Joseph Stalin. For example, Kaiser Wilhelm II's moustache, grossly exaggerated, featured prominently in Triple Entente propaganda. In other cases, such as those of Charlie Chaplin and Groucho Marx, the moustache in question was artificial for most of the wearer's life.

In art, entertainment, and media

Alias

  • Moustache was the alias name of a French comic actor, François-Alexandre Galipedes (b. February 14, 1929 in Paris, France - d. March 25, 1987 in Arpajon, Essonne, France), known for his roles in Paris Blues (1961), How to Steal a Million (1966), and Zorro (1975)[35]

Fictional characters

  • Moustaches have long been used by artists to make characters distinctive, as with Charlie Chan, the video game character Mario, Hercule Poirot, or Snidely Whiplash.
  • Sharabi movie from Bollywood had a character Natthulal whose moustache became a legend. Munchhen hon to Natthulal jaisi, warna na hon (Mostaches should be like Natthulal's or shouldn't be at all) became one of the most quoted dialogue.
  • At least one fictional moustache has been so notable that a whole style has been named after it: the Fu Manchu moustache.

Literature

Visual art

They have also been used to make a social or political point as with:

In the military

  • In the Indian Army, most senior rifle Rajputana regiment soldiers have moustaches,[37][38][39] and the Rajputana Moustache is a symbol of dignity, caste status, and the spirit of Rajput soldiers.[40]
  • Moustaches are also noted among U.S. Army armour and cavalry soldiers.[41]

In sport

Gallery

Moustache examples
Satirist Michael "Atters" Attree sporting his Handlebar Club tie 
Venceslau Brás, former President of Brazil, with handlebar or imperial moustache 
General George Campbell of Inverneill with an imperial moustache 
Adolf Hitler with toothbrush moustache 
Surrealist Salvador Dalí with the flamboyant moustache he popularized 
Richard Petty with a chevron moustache (side view) 
Emiliano Zapata sporting a wide "Mexican" moustache 
Moustachioed members of the Pakistani Frontier Corps with US DEA agent Karen P. Tandy. 

See also



This article uses material from the Wikipedia article "", which is released under the Creative Commons Attribution-Share-Alike License 3.0. There is a list of all authors in Wikipedia

Human

3D