powered by CADENAS

Social Share

Architectural engineering (8203 views - Architecure & BIM & MEP)

Architectural engineering, also known as building engineering, is the application of engineering principles and technology to building design and construction. Definitions of an architectural engineer may refer to: An engineer in the structural, mechanical, electrical, construction or other engineering fields of building design and construction. A licensed engineering professional in parts of the United States. Architectural engineers are those who work with other engineers and architects for the designing and construction of buildings.
Go to Article

Explanation by Hotspot Model

Architectural engineering

Architectural engineering

Architectural engineering

Licensed under Creative Commons Attribution 2.0 (Bryan Chang).

Architectural engineering, also known as building engineering, is the application of engineering principles and technology to building design and construction. Definitions of an architectural engineer may refer to:

Engineering for designer

Structural engineering

Structural engineering involves the analysis and design of physical objects (buildings, bridges, equipment supports, towers and walls). Those concentrating on buildings are responsible for the structural performance of a large part of the built environment and are, sometimes, informally referred to as "building engineers". Structural engineers require expertise in strength of materials and in the seismic design of structures covered by earthquake engineering. Architectural Engineers sometimes structural as one aspect of their designs; the structural discipline when practiced as a specialty works closely with architects and other engineering specialists.

Mechanical, electrical, and plumbing (MEP)

Mechanical engineering and electrical engineering engineers are specialists, commonly referred to as (mechanical, electrical, and plumbing) when engaged in the building design fields. Also known as "building services engineering" in the United Kingdom, Canada, and Australia.[1] Mechanical engineers often design and oversee the heating, ventilation and air conditioning (HVAC), plumbing, and rain gutter systems. Plumbing designers often include design specifications for simple active fire protection systems, but for more complicated projects, fire protection engineers are often separately retained. Electrical engineers are responsible for the building's power distribution, telecommunication, fire alarm, signalization, lightning protection and control systems, as well as lighting systems.

The architectural engineer (PE) in the United States

In many jurisdictions of the United States, the architectural engineer is a licensed engineering professional.[2] Usually a graduate of an architectural engineering university program preparing students to perform whole-building design in competition with architect-engineer teams; or for practice in one of structural, mechanical or electrical fields of building design, but with an appreciation of integrated architectural requirements.

Formal architectural engineering education, following the engineering model of earlier disciplines, developed in the late 19th century, and became widespread in the United States by the mid-20th century. With the establishment of a specific "architectural engineering" NCEES Professional Engineering registration examination in the 1990s, and first offering in April 2003, architectural engineering became recognized as a distinct engineering discipline in the United States. Architectural engineers are not entitled to practice architecture unless they are also licensed as architects.

The architect as architectural engineer

In some countries, the practice of architecture includes planning, designing and overseeing the building's construction, and architecture, as a profession providing architectural services, is referred to as "architectural engineering". In Japan, a "first-class architect" plays the dual role of architect and building engineer, although the services of a licensed "structural design first-class architect" are required for buildings over a certain scale.[3]

In some languages, such as Korean and Arabic, "architect" is literally translated as "architectural engineer". In some countries, an "architectural engineer" (such as the ingegnere edile in Italy) is entitled to practice architecture and is often referred to as an architect.[4] These individuals are often also structural engineers. In other countries, such as Germany, Austria, Iran, and most of the Arab countries, architecture graduates receive an engineering degree (Dipl.-Ing. – Diplom-Ingenieur).[5]

In Spain, an "architect" has a technical university education and legal powers to carry out building structure and facility projects.[6]

In Brazil, architects and engineers used to share the same accreditation process (CONFEA – Federal Council of Engineering, Architecture and Agronomy). Now the Brazilian architects and urbanists have their own accreditation process (CAU – Architecture and Urbanism Council). Besides traditional architecture design training, Brazilian architecture courses also offer complementary training in engineering disciplines such as structural, electrical, hydraulic and mechanical engineering. After graduation, architects focus in architectural planning, yet they can be responsible to the whole building, when it concerns to small buildings (except in electric wiring, where the architect autonomy is limited to systems up to 30kVA, and it has to be done by an Electrical Engineer), applied to buildings, urban environment, built cultural heritage, landscape planning, interiorscape planning and regional planning.[7][8]

In Greece licensed architectural engineers are graduates from architecture faculties that belong to the Polytechnic University,[9] obtaining an "Engineering Diploma". They graduate after 5 years of studies and are fully entitled architects once they become members of the Technical Chamber of Greece (TEE – Τεχνικό Επιμελητήριο Ελλάδος).[10][11] The Engineering Diploma equals a master's degree in ECTS units (300) according to the Bologna Accords.[12]

Education

The architectural, structural, mechanical and electrical engineering branches each have well established educational requirements that are usually fulfilled by completion of a university program.

Architectural engineering as a single integrated field of study

What differentiates architectural engineering from architecture (architect) as a separate and single, integrated field of study, compared to other engineering disciplines, is its multi-disciplinary engineering approach. Through training in and appreciation of architecture, the field seeks integration of building systems within its overall building design. Architectural engineering includes the design of building systems including heating, ventilation and air conditioning (HVAC), plumbing, fire protection, electrical, lighting, architectural acoustics, and structural systems. In some university programs, students are required to concentrate on one of the systems; in others, they can receive a generalist architectural or building engineering degree.

See also



This article uses material from the Wikipedia article "", which is released under the Creative Commons Attribution-Share-Alike License 3.0. There is a list of all authors in Wikipedia

Architecure & BIM & MEP

Autodesk Revit, Nemetschek ArchiCAD, Nemetschek Allplan, Vectorworks, Bentley AECOMSIM, Bentley Microstation, Trimble Tekla, Trimble Sketchup, EliteCAD, Ascon Renga, BricsCAD, Hexagon, Rhinoceros CAD, Sweet Home 3D, BIM Object, BIM component, BIM library, BIM family, BIM catalog, GIS, Advanced Steel, AutoCAD MEP, linear, MagiCAD, Relux, TGA, VDI 3805, Lod100, Lod200, Lod300, Lod350, Lod400, Lod500, Loi, IFC, BuildingSmart, BIM family creation, 3D, Download, MEP BIM product library