powered by CADENAS

Social Share

Nickel titanium (16848 views - Material Database)

Nickel titanium, also known as Nitinol (part of shape memory alloy), is a metal alloy of nickel and titanium, where the two elements are present in roughly equal atomic percentages e.g. Nitinol 55, Nitinol 60. Nitinol alloys exhibit two closely related and unique properties: shape memory effect (SME) and superelasticity (SE; also called pseudoelasticity, PE). Shape memory is the ability of nitinol to undergo deformation at one temperature, then recover its original, undeformed shape upon heating above its "transformation temperature". Superelasticity occurs at a narrow temperature range just above its transformation temperature; in this case, no heating is necessary to cause the undeformed shape to recover, and the material exhibits enormous elasticity, some 10-30 times that of ordinary metal.
Go to Article

Nickel titanium

Nickel titanium

Nickel titanium, also known as Nitinol (part of shape memory alloy), is a metal alloy of nickel and titanium, where the two elements are present in roughly equal atomic percentages e.g. Nitinol 55, Nitinol 60.

Nickel Titanium
Material properties
Density 6.45 g/cm3 (0.233 lb/cu in)
Electrical resistivity (austenite) 82×106 Ω·cm
(martensite) 76×106 Ω·cm
Thermal conductivity (austenite) 0.18 W/cm·K
(martensite) 0.086 W/cm·K
Coefficient of thermal expansion (austenite) 11×106/°C
(martensite) 6.6×106/°C
Magnetic permeability < 1.002
Magnetic susceptibility (austenite) 3.7×106 emu/g
(martensite) 2.4×106 emu/g
Elastic modulus (austenite) 75–83 GPa
(martensite) 28–40 GPa
Yield strength (austenite) 195–690 MPa
(martensite) 70–140 MPa
Poisson's ratio 0.33
Nitinol properties are particular to the precise composition of the alloy and its processing. These specifications are typical for commercially available shape memory nitinol alloys.

Nitinol alloys exhibit two closely related and unique properties: shape memory effect (SME) and superelasticity (SE; also called pseudoelasticity, PE). Shape memory is the ability of nitinol to undergo deformation at one temperature, then recover its original, undeformed shape upon heating above its "transformation temperature". Superelasticity occurs at a narrow temperature range just above its transformation temperature; in this case, no heating is necessary to cause the undeformed shape to recover, and the material exhibits enormous elasticity, some 10-30 times that of ordinary metal.

History

The word Nitinol is derived from its composition and its place of discovery: (Nickel Titanium-Naval Ordnance Laboratory). William J. Buehler[1] along with Frederick Wang,[2] discovered its properties during research at the Naval Ordnance Laboratory in 1959.[3][4] Buehler was attempting to make a better missile nose cone, which could resist fatigue, heat and the force of impact. Having found that a 1:1 alloy of nickel and titanium could do the job, in 1961 he presented a sample at a laboratory management meeting. The sample, folded up like an accordion, was passed around and flexed by the participants. One of them applied heat from his pipe lighter to the sample and, to everyone's surprise, the accordion-shaped strip stretched and took its previous shape.[5]

While the potential applications for nitinol were realized immediately, practical efforts to commercialize the alloy did not take place until a decade later. This delay was largely because of the extraordinary difficulty of melting, processing and machining the alloy. Even these efforts encountered financial challenges that were not readily overcome until the 1980s, when these practical difficulties finally began to be resolved.

The discovery of the shape-memory effect in general dates back to 1932, when Swedish chemist Arne Ölander[6] first observed the property in gold-cadmium alloys. The same effect was observed in Cu-Zn (brass) in the early 1950s.[7]

Mechanism

Nitinol's unusual properties are derived from a reversible solid-state phase transformation known as a martensitic transformation, between two different martensite crystal phases, requiring 10,000–20,000 psi (69–138 MPa) of mechanical stress.

At high temperatures, nitinol assumes an interpenetrating simple cubic structure referred to as austenite (also known as the parent phase). At low temperatures, nitinol spontaneously transforms to a more complicated monoclinic crystal structure known as martensite (daughter phase).[8] There are four transition temperatures associated to the austenite-to-martensite and martensite-to-austenite transformations. Starting from full austenite, martensite begins to form as the alloy is cooled to the so-called martensite start temperature, or Ms, and the temperature at which the transformation is complete is called the martensite finish temperature, or Mf. When the alloy is fully martensite and is subjected to heating, austenite starts to form at the austenite start temperature, As, and finishes at the austenite finish temperature, Af.[9]

Thermal hysteresis of nitinol's phase transformation
The cooling/heating cycle shows thermal hysteresis. The hysteresis width depends on the precise nitinol composition and processing. Its typical value is a temperature range spanning about 20-50 K (20-50 °C; 36-90 °F) but it can be reduced or amplified by alloying[10] and processing.[11]

Crucial to nitinol properties are two key aspects of this phase transformation. First is that the transformation is "reversible", meaning that heating above the transformation temperature will revert the crystal structure to the simpler austenite phase. The second key point is that the transformation in both directions is instantaneous.

Martensite's crystal structure (known as a monoclinic, or B19' structure) has the unique ability to undergo limited deformation in some ways without breaking atomic bonds. This type of deformation is known as twinning, which consists of the rearrangement of atomic planes without causing slip, or permanent deformation. It is able to undergo about 6–8% strain in this manner. When martensite is reverted to austenite by heating, the original austenitic structure is restored, regardless of whether the martensite phase was deformed. Thus the name "shape memory" refers to the fact that the shape of the high temperature austenite phase is "remembered," even though the alloy is severely deformed at a lower temperature.[12]

A great deal of pressure can be produced by preventing the reversion of deformed martensite to austenite — from 35,000 psi to, in many cases, more than 100,000 psi (689 MPa). One of the reasons that nitinol works so hard to return to its original shape is that it is not just an ordinary metal alloy, but what is known as an intermetallic compound. In an ordinary alloy, the constituents are randomly positioned in the crystal lattice; in an ordered intermetallic compound, the atoms (in this case, nickel and titanium) have very specific locations in the lattice.[13] The fact that nitinol is an intermetallic is largely responsible for the complexity in fabricating devices made from the alloy.[why?]

The effect of nitinol composition on the Ms temperature.

The scenario described above (cooling austenite to form martensite, deforming the martensite, then heating to revert to austenite, thus returning the original, undeformed shape) is known as the thermal shape memory effect. To fix the original "parent shape," the alloy must be held in position and heated to about 500 °C (932 °F). This process is usually called shape setting.[14] A second effect, called superelasticity or pseudoelasticity, is also observed in nitinol. This effect is the direct result of the fact that martensite can be formed by applying a stress as well as by cooling. Thus in a certain temperature range, one can apply a stress to austenite, causing martensite to form while at the same time changing shape. In this case, as soon as the stress is removed, the nitinol will spontaneously return to its original shape. In this mode of use, nitinol behaves like a super spring, possessing an elastic range 10–30 times greater than that of a normal spring material. There are, however, constraints: the effect is only observed about 0-40 K (0-40 °C; 0-72 °F) above the Af temperature. This upper limit is referred to as Md,[15] which corresponds to the highest temperature in which it is still possible to stress-induce the formation of martensite. Below Md, martensite formation under load allows superelasticity due to twinning. Above Md, since martensite is no longer formed, the only response to stress is slip of the austenitic microstructure, and thus permanent deformation.

Nitinol is typically composed of approximately 50 to 51% nickel by atomic percent (55 to 56% weight percent).[13][16] Making small changes in the composition can change the transition temperature of the alloy significantly. Transformation temperatures in nitinol can be controlled to some extent, where Af temperature ranges from about −20 °C to +110 °C. Thus, it is common practice to refer to a nitinol formulation as "superelastic" or "austenitic" if Af is lower than a reference temperature, while as "shape memory" or "martensitic" if higher. The reference temperature is usually defined as the room temperature or the human body temperature (37 °C; 98 °F).

One often-encountered effect regarding nitinol is the so-called R-phase. The R-phase is another martensitic phase that competes with the martensite phase mentioned above. Because it does not offer the large memory effects of the martensite phase, it is usually of non practical use.

Manufacturing process

Nitinol is exceedingly difficult to make, due to the exceptionally tight compositional control required, and the tremendous reactivity of titanium. Every atom of titanium that combines with oxygen or carbon is an atom that is robbed from the NiTi lattice, thus shifting the composition and making the transformation temperature that much lower. There are two primary melting methods used today:

Vacuum arc remelting (VAR)
This is done by striking an electrical arc between the raw material and a water-cooled copper strike plate. Melting is done in a high vacuum, and the mold itself is water-cooled copper.
Vacuum induction melting (VIM)
This is done by using alternating magnetic fields to heat the raw materials in a crucible (generally carbon). This is also done in a high vacuum.

While both methods have advantages, it has been demonstrated that an industrial state-of-the-art VIM melted material has smaller inclusions than an industrial state-of-the-art VAR one, leading to a higher fatigue resistance.[17] Other research report that VAR employing extreme high-purity raw materials may lead to a reduced number of inclusions and thus to an improved fatigue behavior.[18] Other methods are also used on a boutique scale, including plasma arc melting, induction skull melting, and e-beam melting. Physical vapour deposition is also used on a laboratory scale.

Hot working of nitinol is relatively easy, but cold working is difficult because the enormous elasticity of the alloy increases die or roll contact, leading to tremendous frictional resistance and tool wear. For similar reasons, machining is extremely difficult—to make things worse, the thermal conductivity of nitinol is poor, so heat is difficult to be removed. Grinding (abrasive cutting), Electrical discharge machining (EDM) and laser cutting are all relatively easy.

Heat treating nitinol is delicate and critical. It is the knowledge intensive process to fine-tune the transformation temperatures. Aging time and temperature controls the precipitation of various Ni-rich phases, and thus controls how much nickel resides in the NiTi lattice; by depleting the matrix of nickel, aging increases the transformation temperature. The combination of heat treatment and cold working is essential in controlling the properties of nitinol products.[19]

Challenges

Fatigue failures of nitinol devices are a constant subject of discussion. Because it is the material of choice for applications requiring enormous flexibility and motion (e.g., peripheral stents, heart valves, smart thermomechanical actuators and electromechanical microactuators), it is necessarily exposed to much greater fatigue strains compared to other metals. While the strain-controlled fatigue performance of nitinol is superior to all other known metals, fatigue failures have been observed in the most demanding applications. There is a great deal of effort underway trying to better understand and define the durability limits of nitinol.

Nitinol is half nickel, and thus there has been a great deal of concern in the medical industry regarding the release of nickel, a known allergen and possible carcinogen.[19] (Nickel is also present in substantial amounts in stainless steel and cobalt-chrome alloys.) When properly treated (via electropolishing and/or passivation), nitinol forms a very stable protective TiO2 layer that acts as a very effective and self-healing barrier against ion exchange. It has been repeatedly shown that nitinol releases nickel at a slower pace than stainless steel, for example. With that said, very early medical devices were made without electropolishing, and corrosion was observed. Today's nitinol vascular self-expandable metallic stents, for example, show no evidence of corrosion or nickel release, and the outcomes in patients with and without nickel allergies are indistinguishable.

There are constant and long-running discussions regarding inclusions in nitinol, both TiC and Ti2NiOx. As in all other metals and alloys, inclusions can be found in Nitinol. The size, distribution and type of inclusions can be controlled to some extent. Theoretically, smaller, rounder and few inclusions should lead to increased fatigue durability. In literature, some early works report to have failed to show measurable differences,[20][21] while novel studies demonstrate a dependence of fatigue resistance on the typical inclusion size in an alloy.[17][18][22][23][24]

Nitinol is difficult to weld, both to itself and other materials. Laser welding nitinol to itself is a relatively routine process. More recently, strong joints between NiTi wires and stainless steel wires have been made using nickel filler.[25] Laser[26] and Tungsten Inert Gas (TIG)[27] welds have been made between NiTi tubes and stainless steel tubes . More research is ongoing into other processes and other metals to which nitinol can be welded.

Actuation frequency of nitinol is dependent on the heat management, especially during the cooling phase. Numerous methods are used to increase the cooling performance, such as forced air,[28] flowing liquids,[29] thermoelectric modules (i.e. Peltier or semiconductor heat pumps),[30] heat sinks,[31] conductive materials[32] and higher surface-to-volume ratio[33] (improvements up to 3.3 Hz with very thin wires[34] and up to 100 Hz with thinfilm nitinol[35]). The fastest nitinol actuation recorded was carried by a high voltage capacitor discharge which heated an SMA wire in a manner of microseconds, and resulted in a complete phase transformation (and high velocities) in a few milliseconds.[36]

Recent advances have shown that processing of nitinol can expand thermomechanical capabilities, allowing for multiple shape memories to be embedded within a monolithic structure.[37][38] Research on multi-memory technology is on-going and promises to deliver enhanced shape memory devices in the near future[39] ,[40] and the application of new materials and material structures, such hybrid shape memory materials (SMMs) and shape memory composites (SMCs).[41]

Applications

There are four commonly used types of applications for nitinol:

Free recovery

Nitinol is deformed at a low temperature, and heated to recover its original shape through the Shape Memory effect.

Constrained recovery

As for free recovery, except that recovery is rigidly prevented and thus a stress is generated.

Work production

Here the alloy is allowed to recover, but to do so it must act against a force (thus doing work).

Superelasticity

Nitinol acts as a super spring through the Superelastic effect.

In 1989 a survey was conducted in the United States and Canada that involved seven organizations. The survey focused on predicting the future technology, market, and applications of SMAs. The companies predicted the following uses of nitinol in a decreasing order of importance: (1) Couplings, (2) Biomedical and medical, (3) Toys, demonstration, novelty items, (4) Actuators, (5) Heat Engines, (6) Sensors, (7) Cryogenically activated die and bubble memory sockets, and finally (8) lifting devices.[42]

Today, nitinol finds application in the listed industrial applications:

Thermal and electrical actuators

  • Nitinol can be used to replace conventional actuators (solenoids, servo motors, etc.), such as in the Stiquito, a simple hexapod robot.
  • Nitinol springs are used in thermal valves for fluidics, where the material both acts as a temperature sensor and an actuator.
  • It is used as autofocus actuator in action cameras and as an Optical Image Stabilizer in mobile phones.[43]
  • It is used in pneumatic valves form comfort seating and has become an industry standard.
  • The 2014 Chevrolet Corvette incorporates nitinol actuators, which replaced heavier motorized actuators to open and close the hatch vent that releases air from the trunk, making it easier to close.

Biocompatible and biomedical applications

  • Nitinol is highly biocompatible and has properties suitable for use in orthopedic implants. Due to Nitinol's unique properties it has seen a large demand for use in less invasive medical devices. Nitinol tubing is commonly used in catheters, stents, and superelastic needles.
  • In colorectal surgery [1], the material is used in devices for reconnecting the intestine after removing the pathology.
  • Nitinol is used for devices developed by Franz Freudenthal to treat Patent ductus arteriosus, blocking a blood vessel that bypasses the lungs and has failed to close after birth in an infant.[44]
  • In dentistry, the material is used in orthodontics for brackets and wires connecting the teeth. Once the SMA wire is placed in the mouth its temperature rises to ambient body temperature. This causes the nitinol to contract back to its original shape, applying a constant force to move the teeth. These SMA wires do not need to be retightened as often as other wires because they can contract as the teeth move unlike conventional stainless steel wires. Additionally, nitinol can be used in endodontics, where nitinol files are used to clean and shape the root canals during the root canal procedure. Because of the high fatigue tolerance and flexibility of nitinol, it greatly decreases the possibility of an endodontic file breaking inside the tooth during root canal treatment, thus improving safety for the patient.
  • Another significant application of nitinol in medicine is in stents: a collapsed stent can be inserted into an artery or vein, where body temperature warms the stent and the stent returns to its original expanded shape following removal of a constraining sheath; the stent then helps support the artery or vein to improve blood flow. It is also used as a replacement for sutures - nitinol wire can be weaved through two structures then allowed to transform into its preformed shape, which should hold the structures in place.
  • Similarly, collapsible structures composed of braided, microscopically-thin nitinol filaments can be used in neurovascular interventions such as stroke thrombolysis, embolization, and intracranial angioplasty.[45]
  • A more recent application of nitinol wire is in female contraception, specifically in intrauterine devices.

Damping systems in structural engineering

  • Superelastic Nitinol finds a variety of applications in civil structures such as bridges and buildings. One such application is Intelligent Reinforced Concrete (IRC), which incorporates Ni-Ti wires embedded within the concrete. These wires can sense cracks and contract to heal macro-sized cracks.[46]
  • Another application is active tuning of structural natural frequency using Nitinol wires to dampen vibrations.

Other applications and prototypes

  • Demonstration model heat engines have been built which use nitinol wire to produce mechanical energy from hot and cold heat sources.[47] A prototype commercial engine developed in the 1970s by engineer Ridgway Banks at Lawrence Berkeley National Laboratory, was named the Banks Engine.[48][49][50][51][52]
  • Nitinol is also popular in extremely resilient glasses frames.[53] It is also used in some mechanical watch springs.
  • Boeing engineers successfully flight-tested SMA-actuated morphing chevrons on the Boeing 777-300ER Quiet Technology Demonstrator 2.[54]
  • It can be used as a temperature control system; as it changes shape, it can activate a switch or a variable resistor to control the temperature.
  • It is used in cell-phone technology as a retractable antenna, or microphone boom, due to its highly flexible and mechanical memory nature.
  • It is used in some novelty products, such as self-bending spoons which can be used by amateur and stage magicians to demonstrate "psychic" powers or as a practical joke, as the spoon will bend itself when used to stir tea, coffee, or any other warm liquid.
  • It can also be used as wires which are used to locate and mark breast tumours so that the following surgery can be more exact.
  • Due to the high damping capacity of Superelastic nitinol, it is also used as a golf club insert.[55]
  • Nickel titanium can be used to make the underwires for underwire bras.[56][57][58]
  • It is used in some actuation-bending devices, such as those developed by Finnish technology company Modti Inc.
  1. ^ Buehler, W. J.; Gilfrich, J. W.; Wiley, R. C. (1963). "Effects of Low-Temperature Phase Changes on the Mechanical Properties of Alloys Near Composition TiNi". Journal of Applied Physics. 34 (5): 1475–1477. doi:10.1063/1.1729603. 
  2. ^ Wang, F. E.; Buehler, W. J.; Pickart, S. J. (1965). "Crystal Structure and a Unique Martensitic Transition of TiNi". Journal of Applied Physics. 36 (10): 3232–3239. doi:10.1063/1.1702955. 
  3. ^ "The Alloy That Remembers", Time, 1968-09-13 
  4. ^ Kauffman, G. B.; Mayo, I. (1997). "The Story of Nitinol: The Serendipitous Discovery of the Memory Metal and Its Applications". The Chemical Educator. 2 (2): 1–21. doi:10.1007/s00897970111a. 
  5. ^ Withers, N. (2014). "Magnificent Molecules - Nitinol" (PDF). The Mole (RSC). 2014 (2): 4. 
  6. ^ Ölander, A. (1932). "An Electrochemical Investigation of Solid Cadmium-Gold Alloys". Journal of the American Chemical Society. 54 (10): 3819–3833. doi:10.1021/ja01349a004. 
  7. ^ Hornbogen, E.; Wassermann, G. (1956). "Über den Einfluβ von Spannungen und das Auftreten von Umwandlungsplastizität bei β1-β-Umwandlung des Messings". Zeitschrift für Metallkunde. 47: 427–433. 
  8. ^ Otsuka, K.; Ren, X. (2005). "Physical Metallurgy of Ti-Ni-based Shape Memory Alloys". Progress in Materials Science. 50 (5): 511–678. doi:10.1016/j.pmatsci.2004.10.001. 
  9. ^ "Nitinol facts". Nitinol.com. 2013. 
  10. ^ Chluba, Christoph; Ge, Wenwei; Miranda, Rodrigo Lima de; Strobel, Julian; Kienle, Lorenz; Quandt, Eckhard; Wuttig, Manfred (2015-05-29). "Ultralow-fatigue shape memory alloy films". Science. 348 (6238): 1004–1007. ISSN 0036-8075. PMID 26023135. doi:10.1126/science.1261164. 
  11. ^ Spini, Tatiana Sobottka; Valarelli, Fabrício Pinelli; Cançado, Rodrigo Hermont; Freitas, Karina Maria Salvatore de; Villarinho, Denis Jardim; Spini, Tatiana Sobottka; Valarelli, Fabrício Pinelli; Cançado, Rodrigo Hermont; Freitas, Karina Maria Salvatore de (2014-04-01). "Transition temperature range of thermally activated nickel-titanium archwires". Journal of Applied Oral Science. 22 (2): 109–117. ISSN 1678-7757. PMC 3956402. PMID 24676581. doi:10.1590/1678-775720130133. 
  12. ^ Funakubo, Hiroyasu (1984), Shape memory alloys, University of Tokyo, pp. 7, 176 .
  13. ^ a b "Nitinol SM495 Wire" (properties, PDF). 2013. 
  14. ^ "Fabrication & Heat Treatment of Nitinol". memry.com. 2011-01-26. Retrieved 2017-03-28. 
  15. ^ R Meling, Torstein; Ødegaard, Jan (August 1998). "The effect of temperature on the elastic responses to longitudinal torsion of rectangular nickel titanium archwires". The Angle Orthodontist. 68 (4): 357–368. PMID 9709837. 
  16. ^ "Nitinol SE508 Wire" (properties, PDF). 2013. 
  17. ^ a b Urbano, Marco; Coda, Alberto; Beretta, Stefano; Cadelli, Andrea; Sczerzenie, Frank (2013-09-01). "The Effect of Inclusions on Fatigue Properties for Nitinol". doi:10.1520/STP155920120189. 
  18. ^ a b Robertson, Scott W.; Launey, Maximilien; Shelley, Oren; Ong, Ich; Vien, Lot; Senthilnathan, Karthike; Saffari, Payman; Schlegel, Scott; Pelton, Alan R. (2015-11-01). "A statistical approach to understand the role of inclusions on the fatigue resistance of superelastic Nitinol wire and tubing". Journal of the Mechanical Behavior of Biomedical Materials. 51: 119–131. ISSN 1878-0180. PMID 26241890. doi:10.1016/j.jmbbm.2015.07.003. 
  19. ^ a b Pelton, A.; Russell, S.; DiCello, J. (2003). "The Physical Metallurgy of Nitinol for Medical Applications". JOM. 55 (5): 33–37. doi:10.1007/s11837-003-0243-3. 
  20. ^ Morgan, N.; Wick, A.; DiCello, J.; Graham, R. (2006). "Carbon and Oxygen Levels in Nitinol Alloys and the Implications for Medical Device Manufacture and Durability". SMST-2006 Proceedings of the International Conference on Shape Memory and Superelastic Technologies (PDF). ASM International. pp. 821–828. ISBN 978-0-87170-862-5. LCCN 2009499204. doi:10.1361/cp2006smst821. 
  21. ^ Miyazaki, S.; Sugaya, Y.; Otsuka, K. (1989). "Mechanism of Fatigue Crack Nucleation in Ti-Ni Alloys". Shape memory materials : May 31-June 3, 1988, Sunshine City, Ikebukuro, Tokyo, Japan. Proceedings of the MRS International Meeting on Advanced Materials. 9. Materials Research Society. pp. 257–262. ISBN 1-55899-038-0. LCCN 90174266. 
  22. ^ "The Influence of Microcleanliness on the Fatigue Performance of Nitinol - Conference Proceedings - ASM International". www.asminternational.org. Retrieved 2017-04-05. 
  23. ^ "Academic paper (PDF): Smartflex NiTi Wires for Shape Memory Actuators". ResearchGate. Retrieved 2017-04-05. 
  24. ^ Rahim, M.; Frenzel, J.; Frotscher, M.; Pfetzing-Micklich, J.; Steegmüller, R.; Wohlschlögel, M.; Mughrabi, H.; Eggeler, G. (2013-06-01). "Impurity levels and fatigue lives of pseudoelastic NiTi shape memory alloys". Acta Materialia. 61 (10): 3667–3686. doi:10.1016/j.actamat.2013.02.054. 
  25. ^ US patent 6875949, Hall, P. C., "Method of Welding Titanium and Titanium Based Alloys to Ferrous Metals" 
  26. ^ Hahnlen, Ryan; Fox, Gordon (October 29, 2012). "Fusion welding of nickel–titanium and 304 stainless steel tubes: Part I: laser welding". Journal of Intelligent Material Systems and Structures. 24 (8). 
  27. ^ Fox, Gordon; Hahnlen, Ryan (October 29, 2012). "Fusion welding of nickel–titanium and 304 stainless steel tubes: Part II: tungsten inert gas welding". Journal of Intelligent Material Systems and Structures. 24 (8). 
  28. ^ Tadesse Y, Thayer N, Priya S (2010). "Tailoring the response time of shape memory alloy wires through active cooling and pre-stress". Journal of Intelligent Material Systems and Structures. 21: 19–40. doi:10.1177/1045389x09352814. 
  29. ^ Wellman PS, Peine WJ, Favalora G, Howe RD (1997). "Mechanical Design and Control of a High-Bandwidth Shape Memory Alloy Tactile Display". International Symposium on Experimental Robotics. 
  30. ^ Romano R, Tannuri EA (2009). "Modeling, control and experimental validation of a novel actuator based on shape memory alloys". Mechatronics. 19: 1169–1177. doi:10.1016/j.mechatronics.2009.03.007. 
  31. ^ Russell RA, Gorbet RB (1995). "Improving the response of SMA actuators". Robotics and Automation. 3: 2299–304. 
  32. ^ Chee Siong L, Yokoi H, Arai T (2005). "Improving heat sinking in ambient environment for the shape memory alloy (SMA)". Intelligent Robots and Systems: 3560–3565. 
  33. ^ An L, Huang WM, Fu YQ, Guo NQ (2008). "A note on size effect in actuating NiTi shape memory alloys by electrical current". Materials & Design. 29: 1432–1437. doi:10.1016/j.matdes.2007.09.001. 
  34. ^ https://www.saesgetters.com/sites/default/files/SMARTFLEX%20Products%20DATASHEETS_Layout%201.pdf
  35. ^ Winzek B; Schmitz S; Rumpf H; Sterzl T; Ralf Hassdorf; Thienhaus S (2004). "Recent developments in shape memory thin film technology". Materials Science and Engineering: A. 378: 40–46. doi:10.1016/j.msea.2003.09.105. 
  36. ^ Vollach, Shahaf, and D. Shilo. "The mechanical response of shape memory alloys under a rapid heating pulse." Experimental Mechanics 50.6 (2010): 803-811.
  37. ^ Khan, M. I.; Zhou Y. N. (2011), Methods and Systems for Processing Materials, Including Shape Memory Materials, WO Patent WO/2011/014,962 
  38. ^ Daly, M.; Pequegnat, A.; Zhou, Y.; Khan, M. I. (2012), "Enhanced thermomechanical functionality of a laser processed hybrid NiTi–NiTiCu shape memory alloy", Smart Materials and Structures, 21 (4): 045018, doi:10.1088/0964-1726/21/4/045018 
  39. ^ Daly, M.; Pequegnat, A.; Zhou, Y. N.; Khan, M. I. (2012), "Fabrication of a novel laser-processed NiTi shape memory microgripper with enhanced thermomechanical functionality", Journal of Intelligent Material Systems and Structures, 24 (8): 984–990, doi:10.1177/1045389X12444492 
  40. ^ Pequegnat, A.; Daly, M.; Wang, J.; Zhou, Y.; Khan, M. I. (2012), "Dynamic actuation of a novel laser-processed NiTi linear actuator", Smart Materials and Structures, 21 (9): 094004, doi:10.1088/0964-1726/21/9/094004 
  41. ^ Tao T, Liang YC, Taya M (2006). "Bio-inspired actuating system for swimming using shape memory alloy composites". Int J Automat Comput. 3page=366-373. 
  42. ^ Miller, R. K.; Walker, T. (1989). Survey on Shape Memory Alloys. Survey Reports. 89. Future Technology Surveys. p. 17. ISBN 9781558651005. OCLC 38076438. 
  43. ^ Actuator Solutions (2015-12-18), SMA AF / OIS Mechanism, retrieved 2017-04-05 
  44. ^ Alejandra Martins (2014-10-02). "The inventions of the Bolivian doctor who saved thousands of children". BBC Mundo. Retrieved 2015-03-30. 
  45. ^ Smith, Keith. "Nitinol Micro-Braids for Neurovascular Interventions". US BioDesign. 
  46. ^ Shape Memory Alloy Engineering (PDF). 2014. pp. 369–401. ISBN 9781322158457. 
  47. ^ "Nitinol Heat Engine Kit". Images Scientific Instruments. 2007. Retrieved 2011.  Check date values in: |access-date= (help)
  48. ^ Banks, R. (1975). "The Banks Engine". Die Naturwissenschaften. 62 (7): 305–308. doi:10.1007/BF00608890. 
  49. ^ Vimeo posting of "The Individualist", documentary on Ridgway Banks
  50. ^ "Single wire nitinol engine", Ridgway M. Banks, US Patent
  51. ^ "Metals that Remember", Popular Science, January 1988
  52. ^ "Engine Uses No Fuel", Milwaukee Journal, December 5, 1973
  53. ^ Hero Khan (2013-11-01), Nitinol Glasses, retrieved 2017-04-05 
  54. ^ "Boeing Frontiers Online". www.boeing.com. Retrieved 2017-04-05. 
  55. ^ "Memory Golf Clubs". spinoff.nasa.gov. Retrieved 2017-04-05. 
  56. ^ Brady, G. S.; Clauser, H. R.; Vaccari, J. A. (2002). Materials Handbook (15th ed.). McGraw-Hill Professional. p. 633. ISBN 978-0-07-136076-0. Retrieved 2009-05-09. 
  57. ^ Sang, D.; Ellis, P.; Ryan, L.; Taylor, J.; McMonagle, D.; Petheram, L.; Godding, P. (2005). Scientifica. Nelson Thornes. p. 80. ISBN 0-7487-7996-5. Retrieved 2009-05-09. 
  58. ^ Jones, G.; Falvo, M. R.; Taylor, A. R.; Broadwell, B. P. (2007). "Nanomaterials: Memory Wire". Nanoscale Science. NSTA Press. p. 109. ISBN 1-933531-05-3. Retrieved 2009-05-09. 

Further reading

A process of making parts and forms of Type 60 Nitinol having a shape memory effect, comprising: selecting a Type 60 Nitinol. Inventor G,Julien CEO of Nitinol Technologies, Inc. (Washington State)

Science Digest articles - Miracle Metal 1982 - PDF


41xx steelAL-6XNAlGaAlloy 20AlnicoAlumelAluminijAluminium alloyAluminium bronzeAluminium-lithium alloyAmalgam (kemija)Arsenical bronzeArsenical copperBell metalBerilijBeryllium copperBillon (alloy)BirmabrightBismanolBizmutMjedBrightrayBroncaBulat steelCalamine brassLijevano željezoCelestriumChinese silverChromelKromChromium hydrideKobaltColored goldKonstantan (legura)Bakar (element)Copper hydrideCopper–tungstenCorinthian bronzeCrown goldČelični lijevCunifeKuproniklCymbal alloysDamascirani čelikDevarda's alloyDuraluminijDutch metalElectrical steelElektrumElektron (alloy)ElinvarFernicoFeroslitineFerroceriumFerrochromeFerromanganeseFerromolybdenumFerrosiliconFerrotitaniumFerrouraniumField's metalFlorentine bronzeGalfenolGalinstanGalijGilding metalStakloGlucydurZlatoGuanín (bronze)GunmetalHaynes InternationalCrna korintska broncaHiduminiumBrzorezni čelikMikrolegirani čelikHydronaliumInconelIndijInvarŽeljezoIron–hydrogen alloyItalmaKanthal (alloy)KovarOlovo (element)MagnalijMagnezijMagnox (alloy)MangalloyManganinMaraging čelikMarine grade stainlessMartensitic stainless steelMegalliumMelchior (alloy)MercuryMolybdochalkosMonelMuntz metalMushet steelNichromeNikalNovo srebroNicrosilNisilNordijsko zlatoOrmoluPhosphor bronzeSirovo željezoPinchbeck (alloy)PlastikaPlexiglasPlutonijKalijReynolds 531RhoditeRodijRose's metalSamarijSanicro 28SkandijShakudoSrebroSilver steelNatrijSolderSpeculum metalSpiegeleisenČelik za oprugeStaballoyNehrđajući čelikČelikStelliteKonstrukcijski čelikSurgical stainless steelTerneKositarTitanijTombacAlatni čelikTumbagaType metalUranijVitalliumCOR-TEN čelikWood's metalWootz steelY alloyZeron 100CinkCirkonijMu-metalPermalloySupermalloyNickel hydridePlutonium–gallium alloySodium-potassium alloyMischmetalLitijTerfenol-DPseudo palladiumScandium hydrideSamarium–cobalt magnetArgentium sterling silverBritannia silverDoré bullionGoloidPlatinum sterlingShibuichiSterling silverTibetan silverTitanium Beta CTitanijeve legureTitanium hydrideGum metalTitanium goldTitanijev nitridBabbitt (alloy)Britanija metalTvrdi kositarQueen's metalWhite metalUranium hydrideZamakZirconium hydrideVodikHelijBor (element)DušikKisikFluorMetanMezzanineAtom

This article uses material from the Wikipedia article "", which is released under the Creative Commons Attribution-Share-Alike License 3.0. There is a list of all authors in Wikipedia

Material Database

database,rohs,reach,compliancy,directory,listing,information,substance,material,restrictions,data sheet,specification