powered by CADENAS

Social Share

Amazon

Hook (6190 views - Tooling)

A hook is a tool consisting of a length of material, typically metal, that contains a portion that is curved or indented, such that it can be used to grab onto, connect, or otherwise attach itself onto another object. In a number of uses, one end of the hook is pointed, so that this end can pierce another material, which is then held by the curved or indented portion.
Go to Article

Explanation by Hotspot Model

Youtube


    

Hook

Hook

A hook is a tool consisting of a length of material, typically metal, that contains a portion that is curved or indented, such that it can be used to grab onto, connect, or otherwise attach itself onto another object. In a number of uses, one end of the hook is pointed, so that this end can pierce another material, which is then held by the curved or indented portion.

Variations

  1. ^ Unger-Hamilton, Romana (July 1985). "Microscopic Striations on Flint Sickle-Blades as an Indication of Plant Cultivation: Preliminary Results". World Archaeology. 17 (1): 121–6. doi:10.1080/00438243.1985.9979955.
  2. ^ Banning, E.B. (1998). "The Neolithic Period: Triumphs of Architecture, Agriculture, and Art". Near Eastern Archaeology. 61 (4): 188–237. doi:10.2307/3210656. JSTOR 3210656.
  3. ^ Beazley, Elisabeth (1990). Beazley's Design and Detail of the Space Between Buildings. Taylor & Francis. p. 230. ISBN 978-0-419-13620-0.
  4. ^ Porter, Brian; Christopher Tooke (2007). Carpentry and Joinery 3. Butterworth-Heinemann. p. 200. ISBN 978-0-7506-6505-6.


This article uses material from the Wikipedia article "", which is released under the Creative Commons Attribution-Share-Alike License 3.0. There is a list of all authors in Wikipedia

Tooling

tooling,tool,drill,cam,manufacturing