powered by CADENAS

Social Share

Amazon

Hex map (9036 views - Game & Play & Gamification)

A hex map, hex board, or hex grid is a game board design commonly used in wargames of all scales. The map is subdivided into a hexagonal tiling, small regular hexagons of identical size.
Go to Article

Explanation by Hotspot Model

Youtube


    

Hex map

Hex map

Hex map

Licensed under GNU General Public License (Wesnoth).

A hex map, hex board, or hex grid is a game board design commonly used in wargames of all scales. The map is subdivided into a hexagonal tiling, small regular hexagons of identical size.

Advantages and disadvantages

The primary advantage of a hex map over a traditional square grid map is that the distance between the center of each and every pair of adjacent hex cells (or hex) is the same. By comparison, in a square grid map, the distance from the center of each square cell to the center of the four diagonal adjacent cells it shares a corner with is greater than the distance to the center of the four adjacent cells it shares an edge with. This equidistant property of all adjacent hexes is desirable for games in which the measurement of movement is a factor. The other advantage is the fact that neighbouring cells always share edges; there are no two cells with contact at only a point.

One disadvantage of a hex map is that hexes have adjacent cells in only six directions instead of eight, as in a square grid map. Commonly, cells will form continuous straight lines "up" and "down", or "north" and "south", in which case the other four adjacent cells lie "north-west", "north-east", "south-west" and "south-east". As a result, no hex cell has an adjacent hex cell lying directly east or west of it, making movement in a straight line east or west impossible. Instead, paths in these directions, and any other path that does not bisect one of the six cell edges, will "zig-zag"; since no two directions are orthogonal, it is impossible to move forward in one direction without moving backwards slightly in the other.

A hexagonal chess board, showing the three-colour system and the diagonal moves of a bishop.
POV-Ray render mimicking Fallout's trimetric projection and hexagonal grid.

Games that traditionally use the four cardinal directions, or otherwise suit a square grid, may adapt to a hex grid in different ways. For example, hexagonal chess replaces the four directions of orthogonal movement (along ranks and files) with the six directions to adjacent cells, through cell edges. The four directions of diagonal movement are likewise replaced with the six directions that lie through vertices of the cell; these "diagonal" movements travel along the edge between a pair of adjacent cells before arriving at another cell. A three-colour grid aids in visualising this movement, since it preserves the traditional chessboard's property that pieces moving diagonally land only on cells of the same colour.

Uses

The hex map has been a favourite for game designers since 1961, when Charles S. Roberts of the Avalon Hill game company published the second edition of Gettysburg with a hex map. The hex grid is a distinguishing feature of the games from many wargame publishers, and a few other games (such as The Settlers of Catan).

The hex map has also been popular for role-playing game wilderness maps. They were used in the Dungeons & Dragons boxed sets of the 1980s and related TSR products. GDW also used a hex grid map in mapping space for their science-fiction RPG Traveller.

A few abstract games are played on a hex grid, such as the six games of the GIPF series as well as Hex and the television game show based on it, Blockbusters. Chinese Checkers is played on a hex grid and several variants of chess have also been invented for a hex board.

Early examples of strategy video games that use hex maps include 1983's Nobunaga's Ambition,[1] 1989's Military Madness (the first entry in the Nectaris series),[2] and 1991's Master of Monsters.[3] The first Civilization had a hex map version during development, but designers decided against it because "the world was not ready ... it was too freaky"[4]. While the first four iterations of the popular Civilization computer game franchise used square maps, Civilization V and Civilization VI use hexagonal maps. Other games that uses hex maps are The Battle for Wesnoth, Dragon Age Journeys, Heroes of Might and Magic III, and Forge of Empires.

See also


As (carte à jouer)Jeu d'actionScience-fiction post-apocalyptiqueBorne d'arcadeJeu d'arcadeRéalité augmentéeAvatar (informatique)Trotteur (marche)BackgammonBalance bicycleBaoding ballsBroadswordBattle royale (genre de jeu vidéo)BattleMechBattleTechFou (échecs)Card countingJeu de cartesCarrousel (loisir)Casino (lieu)Les Colons de CatanePendule d'échecsPuissance 4FléchettesMaison de poupéeDominos (jeu)Edge sortingFidget spinnerVue à la première personneJeu de tir à la première personneFortniteJeuGame boyContrôleur de jeuMoteur de jeuManette de jeuSystème de jeu de PokémonJoueur de jeu vidéoGaming houseGaming keypadGoogle CardboardHalo 3: ODSTPalais des glaces (attraction)Immersive technologyJob SimulatorJoystickRoi (échecs)Cavalier (échecs)Lego DuploMinifigFlash McQueenList of magical weaponsList of most-played video games by player countMagic : L'AssembléeJeu de rôle en ligne massivement multijoueurPoupée russeMétro 2033Metro 2033Mini 4WDMiniature model (gaming)Jeu de figurinesMonopolyMonopoly (série de jeux vidéo)MultijoueurOrigamiOriginal video animationPion (échecs)FlipperPersonnage joueurJoueur contre joueurPlayerUnknown's BattlegroundsTerrain de jeuxPokémonPokerPortal (jeu vidéo)Casse-têteDame (échecs)Modélisme ferroviaireCharadeCheval à basculeTour (échecs)Rubik's CubeJeu de tirMachine à sousSnookerCube SomaSpinning coneSquishiesBalle anti-stressSuper MarioSurvival horrorTabletop gameTangramOurs en pelucheTetrisTours de HanoïJouetBloc (jouet)Train jouetTransformers DecepticonsConsole de jeux vidéoMonde virtuelJeu de guerreWarhammer 40,000Wooden toy trainWorld of WarcraftYukikaze (anime)

This article uses material from the Wikipedia article "", which is released under the Creative Commons Attribution-Share-Alike License 3.0. There is a list of all authors in Wikipedia

Game & Play & Gamification

3d,model,playground,board games,computer,strategy,thinktank