powered by CADENAS

Social Share

Amazon

Tabletop game (8820 views - Game & Play & Gamification)

Tabletop games are games that are normally played on a table or other flat surface, such as board games, card games, dice games, miniatures wargames or tile-based games.
Go to Article

Explanation by Hotspot Model

Youtube


    

Tabletop game

Tabletop game

Tabletop game

Tabletop games are games that are normally played on a table or other flat surface, such as board games, card games, dice games, miniatures wargames or tile-based games.[1][2]

Classification according to equipment used

Tabletop games can be classified according to the general form, or equipment utilized:[3]

Game category Game examples
Adventure games Adventure board games, Adventure gamebooks
Board games Backgammon, Can't Stop, Chess, German-style board games, Go, Reversi
Card games Solitaire, Collectible card games, Hanafuda, Tarot card games
Dice games Bunco, Craps, Farkle, Generala, Poker dice, Sic bo, Yahtzee, Zombie Dice
Paper and pencil games Battleship, Connect 5, Dots and Boxes, Hangman, Sprouts, Sudoku
Role-playing games Call of Cthulhu, Dungeons & Dragons, Warhammer Fantasy Roleplay
Strategy games Wargames, Government simulation games, Miniatures games
Tile-based games 15 puzzle, Anagrams, Dominoes, Mahjong, Mahjong solitaire, Tangrams

Games like chess and draughts are examples of games belonging to the board game category. Other games, however, use various attributes and cannot be classified unambiguously (e.g. Monopoly utilises a board as well as dice and cards).

For several of these categories there are sub-categories and even sub-sub-categories or genres. For instance, German-style board games, board wargames, and Roll-and-move games are all types of board games that differ markedly in style and general interest.

Classification according to elements of chance

As an alternative to classifying games by equipment, they can also be classified according to the elements of chance involved. In game theory, two fundamentally different elements of chance can play a role:

  • Chance due to outcome uncertainty, e.g. due to dice rolls or due to unknown cards being dealt during the game. Games in which outcome uncertainty plays a role are referred to as stochastic games as opposed to deterministic games.
  • Chance due to state uncertainty, e.g. due to the opponent's position or cards not being visible, or due to the simultaneous move character of the game. Games in which state uncertainty plays a role are referred to as partial or imperfect information games as opposed to full or perfect information games.

Examples of the chance classification for some well-known tabletop games are given in the table below.

Full/perfect information Partial/imperfect information
Deterministic
Stochastic

Organizations

List of organizations that sponsor events featuring tabletop games:

Numerous independent, local groups run by gamers exist to play tabletop games. Additionally, many colleges have student run organizations pertaining solely to table top gaming. The Collegiate Association of Table Top Gamers is one such organization that has a few chapters at different schools.

In culture

  • TableTop is a web series about tabletop games. It was created by Wil Wheaton and Felicia Day and is hosted by Wheaton.[4] TableTop is published on Felicia Day's YouTube channel, Geek & Sundry. In each episode, following a brief explanation of one or more tabletop games, Wheaton plays the games with guests, usually web or TV personalities.[5] A wide range of hobby gaming titles have been played, from classic German-style board games and family games to RPGs and card games.[6]
  • International TableTop Day is celebrated every spring all over the world.[7] In 2014 it took place in 80 countries at over 3,000 events.

See also


As (carte à jouer)Jeu d'actionScience-fiction post-apocalyptiqueBorne d'arcadeJeu d'arcadeRéalité augmentéeAvatar (informatique)Trotteur (marche)BackgammonBalance bicycleBaoding ballsBroadswordBattle royale (genre de jeu vidéo)Fou (échecs)Card countingJeu de cartesCarrousel (loisir)Casino (lieu)Les Colons de CatanePendule d'échecsPuissance 4FléchettesMaison de poupéeDominos (jeu)Edge sortingFidget spinnerVue à la première personneJeu de tir à la première personneFortniteJeuGame boyContrôleur de jeuMoteur de jeuManette de jeuSystème de jeu de PokémonJoueur de jeu vidéoGaming houseGaming keypadGoogle CardboardHalo 3: ODSTPalais des glaces (attraction)Immersive technologyJob SimulatorJoystickRoi (échecs)Cavalier (échecs)Lego DuploMinifigFlash McQueenList of magical weaponsList of most-played video games by player countMagic : L'AssembléeJeu de rôle en ligne massivement multijoueurPoupée russeMétro 2033Metro 2033Mini 4WDMiniature model (gaming)Jeu de figurinesMonopolyMonopoly (série de jeux vidéo)MultijoueurOrigamiOriginal video animationPion (échecs)FlipperPersonnage joueurJoueur contre joueurPlayerUnknown's BattlegroundsTerrain de jeuxPokémonPokerPortal (jeu vidéo)Casse-têteDame (échecs)Modélisme ferroviaireCharadeCheval à basculeTour (échecs)Rubik's CubeJeu de tirMachine à sousSnookerCube SomaSpinning coneSquishiesBalle anti-stressSuper MarioSurvival horrorTangramOurs en pelucheTetrisTours de HanoïJouetBloc (jouet)Train jouetTransformers DecepticonsConsole de jeux vidéoMonde virtuelJeu de guerreWarhammer 40,000Wooden toy trainWorld of WarcraftYukikaze (anime)BattleMechBattleTechHex mapInternational Chess Day

This article uses material from the Wikipedia article "", which is released under the Creative Commons Attribution-Share-Alike License 3.0. There is a list of all authors in Wikipedia

Game & Play & Gamification

3d,model,playground,board games,computer,strategy,thinktank