powered by CADENAS

Social Share

Amazon

Easter traditions (2492 views - Day Of)

Since its origins, Easter has been a time of celebration and feasting and many traditional Easter games and customs developed, such as egg rolling, egg tapping, pace egging, cascarones or confetti eggs, and egg decorating. Today Easter is commercially important, seeing wide sales of greeting cards and confectionery such as chocolate Easter eggs as well as other Easter foods. Even many non-Christians celebrate these features of the holiday while ignoring the religious aspects.
Go to Article

Explanation by Hotspot Model

Youtube


    

Easter traditions

Easter traditions

Since its origins, Easter has been a time of celebration and feasting and many traditional Easter games and customs developed, such as egg rolling, egg tapping, pace egging, cascarones or confetti eggs, and egg decorating. Today Easter is commercially important, seeing wide sales of greeting cards and confectionery such as chocolate Easter eggs as well as other Easter foods. Even many non-Christians celebrate these features of the holiday while ignoring the religious aspects.

Asia

Malaysia

Despite Malaysia being a Muslim majority country, Easter is celebrated in the states of Sabah and Sarawak in East Malaysia as there is a significant Christian indigenous population in both states.[1]

Continental Europe

Central and Eastern Europe

Ritual whipping of girls in Moravia (1910)

Many central and eastern European ethnic groups, including the Albanians, Armenians, Belarusians, Bulgarians, Croats, Czechs, Estonians, Georgians, Germans, Hungarians, Latvians, Lithuanians, Macedonians, Poles, Romanians, Russians, Serbs, Slovaks, Slovenes, and Ukrainians, decorate eggs for Easter.

In Bulgaria, the Easter eggs are decorated on Thursday or Saturday before Easter. Widespread tradition is to fight with eggs by pair, and the one who's egg is the last surviving is called borak (Bulgarian: борак, fighter). The tradition is to display the decorated eggs on the Easter table together with the Easter dinner consisting of roasted lamb, a salad called Easter salad (lettuce with cucumbers), and a sweet bread called kozunak.

In the Czech Republic, Slovakia, and some parts of Hungary, a tradition of spanking or whipping is carried out on Easter Monday. In the morning, men spank women with a special handmade whip called a pomlázka (in Czech) or korbáč (in Slovak); in eastern regions of former Czechoslovakia Moravia and Slovakia they also throw cold water on them. The pomlázka/korbáč consists of eight, 12 or even 24 withies (willow rods), is usually from half a metre to two meters long and decorated with coloured ribbons at the end. The spanking may be painful, but it's not intended to cause suffering. A legend says that women should be spanked with a whip in order to keep their health, beauty, and fertility during the whole next year.[2]

An additional purpose can be for men to exhibit their attraction to women; unvisited women can even feel offended. Traditionally, the spanked woman gives a coloured egg (kraslice) they've prepared by themselves as invitations to eat and drink and as a sign of her thanks to the man. If the visitor is a small boy, he is usually provided with sweets and a small amount of money.

In some regions, the women can get revenge in the afternoon or the following day when they can pour a bucket of cold water on any man. The habit slightly varies across Slovakia and the Czech Republic. A similar tradition existed in Poland (where it is called Dyngus Day), but it is now little more than an all-day water fight.

In Germany, decorated eggs are hung on branches of bushes and trees to make them Easter egg trees. Eggs are also used to dress wells for Easter, the Osterbrunnen, most prominently in the Fränkische Schweiz (Franconian Switzerland).[3]

In Bosnia and Herzegovina, Croatia, and Slovenia, a basket of food is prepared, covered with a handmade cloth, and brought to the church to be blessed. A typical Easter basket includes bread, colored eggs, ham, horseradish, and a type of nut cake called "potica".[4]

Hungary

In Hungary, Transylvania, Southern Slovakia, Kárpátalja, Northern Serbia - Vojvodina, and other territories with Hungarian-speaking communities, the day following Easter is called Locsoló Hétfő, "Watering Monday". Men usually visit families with girls and women. Water, perfume or perfumed water is sprinkled on the women and girls of the house by the visiting men, who are given in exchange an Easter egg. Traditionally Easter ham, colored boiled eggs and horseradish sauce is consumed on Sunday morning.

Poland

In Poland, white sausage and mazurek are typical Easter breakfast dishes.

The butter lamb (Baranek wielkanocny) is a traditional addition to the Easter meal for many Polish Catholics. Butter is shaped into a lamb either by hand or in a lamb-shaped mold.

Ukraine

Preparations for Easter celebration in Ukraine begin weeks before the feast day, with Great Lent being part of it. The Ukrainian Easter eggs include pysanky,[5] krashanky (edible, one-colour dyed eggs), driapanky (a design is scratched on the eggshell) etc. During the Easter Vigil a priest also blesses the parishioners' Easter baskets, which include Easter eggs, paska,[6] butter, cheese, kovbasa, salt and a few other products. With this food, on their return home, people break their fast. The ritual is called 'rozhovyny'. People visit their relatives and neighbours exchanging Easter greetings. Celebration of Easter in Ukraine is filled with many other customs and rituals, most of which are centuries-old.[7]

Italy

Italian traditional Easter cake called the Colomba Pasquale

In Florence, Italy, the unique custom of the Scoppio del carro is observed in which a holy fire lit from stone shards from the Holy Sepulchre are used to light a fire during the singing of the Gloria of the Easter Sunday mass, which is used to ignite a rocket in the form of a dove, representing peace and the holy spirit, which following a wire in turn lights a cart containing pyrotechnics in the small square before the Cathedral.[citation needed]

The Netherlands, Belgium and France

Church bells are silent as a sign of mourning for one or more days before Easter in The Netherlands, Belgium and France. This has led to an Easter tradition that says the bells fly out of their steeples to go to Rome (explaining their silence), and return on Easter morning bringing both colored eggs and hollow chocolate shaped like eggs or rabbits.

In both The Netherlands and Dutch-speaking Belgium many of more modern traditions exist alongside the Easter Bell story. The bells ("de Paasklokken") leave for Rome on Holy Saturday, called "Stille Zaterdag" (literally "Silent Saturday") in Dutch. In the northern and eastern parts of the Netherlands (Twente and Achterhoek), Easter Fires (in Dutch: Paasvuur) are lit on Easter Day at sunset.

In French-speaking Belgium and France the same story of Easter Bells (« les cloches de Pâques ») bringing eggs from Rome is told, but church bells are silent beginning Maundy Thursday, the first day of the Paschal Triduum.

Northern Germany

Typical German Easter bread

In northern Germany, Easter Fires (in German: Osterfeuer, listen ) are lit around sunset on Holy Saturday. Each of the federal states have their own regulations for allowing and/or the way of staging Easter Fires: While in the city and state of Hamburg, private persons are allowed to have an Easter Fire of any size on their own premises, in Schleswig-Holstein, for example, only the wide-spread voluntary fire brigades are allowed to organize and stage them on open fields. Over the past years, Easter Fires themselves have become larger and developed to smaller versions of Volksfests with some snack stands selling Bratwurst, steak in bread rolls, beer, wine, and soft drinks as well as maybe one or two rides for the children. Usually, Easter Fires are kept burning over hours until dawn (roughly around 6 o'clock) and cause therefore a special atmosphere during the whole Easter Night with their bright lights in the dark and the omnipresent smell of smoke.

During the weeks before Easter, special Easter bread is sold (in German: Osterbrot). This is made with yeast dough, raisins, and almond splinters. Usually, it is cut in slices and spread with butter. People enjoy it either for breakfast or for tea time (in German: Kaffee und Kuchen, literally ″coffee and cake″).

Nordic countries

In Norway, in addition to staying at mountain cabins, cross-country skiing and painting eggs, a contemporary tradition is to read or watch murder mysteries at Easter. All the major television channels run crime and detective stories (such as Agatha Christie's Poirot), magazines print stories where the readers can try to figure out "Whodunnit", and new detective novels are scheduled for publishing before Easter. Even the milk cartons are altered for a couple of weeks. Each Easter a new short mystery story is printed on their sides. Stores and businesses close for five straight days at Easter, with the exception of grocery stores, which re-open for a single day on the Saturday before Easter Sunday.

In Finland and Sweden, traditions include egg painting and small children dressed as witches collecting candy door-to-door, in exchange for decorated pussy willows. This is a result of the mixing of an old Orthodox tradition (blessing houses with willow branches) and the Swedish Easter witch tradition.[8] Brightly coloured feathers and little decorations are also attached to birch branches in a vase. In Finland, it is common to plant ryegrass in a pot as a symbol of spring and new life. After the grass has grown, many people put chick decorations on it. Children busy themselves painting eggs and making paper bunnies.

Denmark has the gækkebrev tradition of sending relatives and friends artful paper cuttings, often with a snowdrop, and a rhyme with the letters of the sender's name replaced by dots. If the recipient guesses who sent it, the sender owes them a chocolate egg; and vice versa if they can't.[9] The decorated letter custom was originally a means of proposal or courtship, but is now considered mostly for children.

For lunch or dinner on Holy Saturday, families in Sweden and Denmark traditionally feast on a smörgåsbord of herring, salmon, potatoes, eggs, and other kinds of food. In Finland, it is common to eat roasted lamb with potatoes and other vegetables. In Finland, the Lutheran majority enjoys mämmi as another traditional Easter treat, while the Orthodox minority's traditions include eating pasha (also spelled paskha) instead.

In the western parts of Sweden and in Finnish Ostrobothnia, bonfires have at least since the 18th century been lit during Holy Saturday. This tradition is claimed to have its origin in Holland. During the last decades though, the bonfires have in many places been moved to Walpurgis Night, as this is the traditional date for bonfires in many other parts of the country.

Cyprus

As well as the common painted easter egg bump, in Cyprus it is customary for people to light great fires[10] (Greek: λαμπρατζια) in schools or church yards. The fires are made up of scrap wood, gathered usually by enthusiastic young boys which scour their neighbourhoods for them, in order to make their fire as great as it can be (and bigger than the neighbouring one). More than often this competition leads to fights happening over scraps of wood and the police or fire department being called to put out the fires that have gone out of control. It is customary for a small doll representing Judas Iscariot to be burnt. The same thing happens on Crete, but it is non-competitive, and the fire is called "founara" which means "big fire" in Cretan Greek. The founara burns coupled with the detonation of small dynamites called "plakatzikia" in plural, and with gunshots in the air.

English-speaking world

Throughout the English-speaking world, many Easter traditions are similar with only minor differences. For example, Saturday is traditionally spent decorating Easter eggs and hunting for them with children on Sunday morning, by which time they have been mysteriously hidden all over the house and garden. Other traditions involve parents telling their children that eggs and other treats, such as chocolate eggs or rabbits, and marshmallow chicks (Peeps), have been delivered by the Easter Bunny in an Easter basket, which children find waiting for them when they wake up. Many families observe the religious aspects of Easter by attending Sunday Mass or services in the morning and then participating in a feast or party in the afternoon.

Some families have a traditional Sunday roast, often of either roast lamb or ham. Easter breads such as Simnel cake, a fruit cake with eleven marzipan balls representing the eleven faithful apostles, or nut breads such as potica are traditionally served. Hot cross buns, spiced buns with a cross on top, are traditionally associated with Good Friday, but today are often eaten well before and after (and, indeed, are sold in many supermarkets and bakers' all year round).

In Europe

In Scotland, the north of England, and Northern Ireland, the traditions of rolling decorated eggs down steep hills and pace egging are still adhered to.

In the Republic of Ireland (officially) and in Northern Ireland (for some people), Easter is a day of remembrance for the men and women who died in the Easter Rising which began on Easter Monday 1916. Until 1966, there was a parade of veterans, past the headquarters of the Irish Volunteers at the General Post Office (GPO) on O'Connell Street, Dublin, and a reading of the Proclamation of the Irish Republic. It is usually celebrated on Easter Monday.

North America and the Caribbean

In Louisiana, USA, egg tapping is known as egg-knocking. Marksville, Louisiana claims to host the oldest egg-knocking competition in the US, dating back to the 1950s. Competitors pair up on the steps of the courthouse on Easter Sunday and knock the tips of two eggs together. If a participant's egg shell cracks they have to forfeit it, a process that continues until just one egg remains.[11]

In the British Overseas Territory of Bermuda, historically famous for growing and exporting the Easter lily, the most notable feature of the Easter celebration is the flying of kites to symbolize Christ's ascent.[12] Traditional Bermuda kites are constructed by Bermudians of all ages as Easter approaches, and are normally only flown at Easter. In addition to hot cross buns and Easter eggs, fish cakes are traditionally eaten in Bermuda at this time.

In Jamaica, eating bun and cheese is a highly anticipated custom by Jamaican nationals all over the world. The Jamaica Easter Buns are spiced and have raisins, and baked in a loaf tin. The buns are sliced and eaten with a slice of cheese. It is a common practice for employers to make gifts of bun and cheese or a single loaf of bun to staff members. According to the Jamaica Gleaner, "The basic Easter bun recipe requires wheat flour, brown sugar, molasses, baking powder or yeast and dried fruits."[13] Easter egg traditions and the Easter Bunny activities are not widespread in Jamaica. Also, Jamaican traditions include sometimes include throwing garlic onto the floor as a sign of good luck during Easter dinner.

Oceania

In New Zealand, the Auckland Easter Show is an annual tradition, also.

See also



This article uses material from the Wikipedia article "", which is released under the Creative Commons Attribution-Share-Alike License 3.0. There is a list of all authors in Wikipedia

Day Of

Day Of, celebration,holiday