powered by CADENAS

Social Share

Amazon

Baoding balls (10987 views - Game & Play & Gamification)

Baoding balls (Chinese: 保定健身球; pinyin: Bǎodìng Jiànshēn Qiú) are metal balls small enough to hold in one hand. They are also known as Chinese "balls for ball practice" exercise balls, Chinese health balls, Chinese meditation balls, Chinese medicine balls. Baoding balls are used by rotating two or more balls repeatedly in the hand. Intended to improve finger dexterity, relax the hand, or aid in the recovery of muscle strength and motor skills after surgery, Baoding balls work similarly to Western stress balls.
Go to Article

Explanation by Hotspot Model

Youtube


    

Baoding balls

Baoding balls

Baoding balls (Chinese: 保定健身球; pinyin: Bǎodìng Jiànshēn Qiú) are metal balls small enough to hold in one hand. They are also known as Chinese "balls for ball practice" exercise balls, Chinese health balls, Chinese meditation balls, Chinese medicine balls. Baoding balls are used by rotating two or more balls repeatedly in the hand. Intended to improve finger dexterity, relax the hand, or aid in the recovery of muscle strength and motor skills after surgery, Baoding balls work similarly to Western stress balls.

History

The first Baoding balls were likely created in Hebei, China, during the Ming Dynasty. Formerly, they were often called "iron balls" as they were originally made of iron. Meditation balls continue to be produced there.[1]

Composition

Inside Baoding balls: a wire and a marble

As metalworking advanced, "iron balls" became more popular. Construction methods varied. Most Baoding balls consist of a pair of hollow spheres, each containing a chime that rings when an inner ball strikes the outer sphere. Many modern examples are decorated with cloisonné and brass wire; these are essentially decorative since they easily chip when dropped or rubbed together. Baoding balls can also be made of solid jade, agate, marble, and other types of stone.

Hollow balls are generally more suitable for therapeutic use due to their lighter weight. Heavier balls of iron, steel or tungsten carbide require more effort for rotation. These are mainly used to build strength by resistance training.

Use

The basic exercise consists of holding a pair of Baoding balls in the palm of one hand, rotating them (switching the relative position of the two balls) while maintaining constant contact between them.

Once this technique has been mastered, the rotation speed can be gradually increased until the balls separate in the hand. Eventually one hand can learn to rotate them completely without the balls making contact with each other. Exercises have been developed involving more balls, where the main technique is to avoid contact with the other balls. This requires using a finger, usually the index finger, as a divider.

An average user should be able to start with a 45mm (1.8in) ball and move up to 60mm (2.4in) as their muscles get accustomed to the exercise. Larger Baoding balls between 70mm and 100mm (2.8in to 3.9in) can be used. Keeping larger balls separate while rotating them is an advanced skill.

The area of the hand exercised can be varied, altering the part of the hand they rotate over, or changing the orbit of the balls so that more force is exerted on a particular finger or finger joints.

Well-known strongmen such as John Brookfield used shot put balls as Baoding balls, rotating them to develop forearm muscles and improve their grip.

Health benefits

Though unsupported by scientific evidence, baoding balls are thought to exercise hand muscles, improve brain function and reduce stress when used as alternative medicine to stimulate the acupuncture points on the hand.[2][unreliable source?]

Baoding balls are often used in physical therapy to exercise the soft tissues of the hand, wrist, and arm.[medical citation needed]

  1. ^ "History and Types of Baoding Balls". baodingballs.com. Retrieved 26 August 2015.
  2. ^ "The Health Benefits of Chinese Baoding Balls". Retrieved 2015-09-23.

As (carte à jouer)Jeu d'actionScience-fiction post-apocalyptiqueBorne d'arcadeJeu d'arcadeRéalité augmentéeAvatar (informatique)BackgammonBalance bicycleBroadswordBattle royale (genre de jeu vidéo)Fou (échecs)Card countingJeu de cartesCarrousel (loisir)Casino (lieu)Les Colons de CatanePuissance 4FléchettesMaison de poupéeDominos (jeu)Edge sortingFidget spinnerVue à la première personneJeu de tir à la première personneFortniteJeuGame boyContrôleur de jeuMoteur de jeuManette de jeuSystème de jeu de PokémonJoueur de jeu vidéoGaming houseGaming keypadGoogle CardboardHalo 3: ODSTImmersive technologyJob SimulatorJoystickRoi (échecs)Cavalier (échecs)Lego DuploMinifigFlash McQueenList of magical weaponsList of most-played video games by player countMagic : L'AssembléeJeu de rôle en ligne massivement multijoueurPoupée russeMétro 2033Metro 2033Mini 4WDMonopolyMonopoly (série de jeux vidéo)MultijoueurOrigamiOriginal video animationPion (échecs)FlipperPersonnage joueurJoueur contre joueurPlayerUnknown's BattlegroundsTerrain de jeuxPokémonPokerPortal (jeu vidéo)Casse-têteDame (échecs)Modélisme ferroviaireCharadeCheval à basculeTour (échecs)Rubik's CubeJeu de tirMachine à sousSnookerCube SomaSpinning coneSquishiesBalle anti-stressSuper MarioSurvival horrorTangramOurs en pelucheTetrisTours de HanoïJouetBloc (jouet)Train jouetConsole de jeux vidéoMonde virtuelWooden toy trainWorld of WarcraftYukikaze (anime)Transformers DecepticonsWarhammer 40,000Jeu de figurinesMiniature model (gaming)Jeu de guerreTabletop gameBattleMechBattleTechHex mapBombe à eau

This article uses material from the Wikipedia article "", which is released under the Creative Commons Attribution-Share-Alike License 3.0. There is a list of all authors in Wikipedia

Game & Play & Gamification

3d,model,playground,board games,computer,strategy,thinktank