powered by CADENAS

Social Share

Amazon

Air superiority fighter (3735 views - Transportation - Air Water Earth)

An air superiority fighter, also spelled air-superiority fighter, is a type of fighter aircraft designed for entering and seizing control of enemy airspace as a means of establishing complete dominance over the enemy's air force (air supremacy). Air superiority fighters are designed primarily to effectively engage enemy fighters, more than other types of aircraft, although some may have a secondary role for air-to-ground strikes.
Go to Article

Explanation by Hotspot Model

Youtube


    

Air superiority fighter

Air superiority fighter

Air superiority fighter

An air superiority fighter, also spelled air-superiority fighter, is a type of fighter aircraft designed for entering and seizing control of enemy airspace as a means of establishing complete dominance over the enemy's air force (air supremacy). Air superiority fighters are designed primarily to effectively engage enemy fighters, more than other types of aircraft, although some may have a secondary role for air-to-ground strikes.

Evolution of the term

During World War II and through the Korean War, fighters were classified by their role: heavy fighter, interceptor, escort fighter, night fighter, and so forth. With the development of guided missiles in the 1950s, design diverged between fighters optimized to fight in the beyond visual range (BVR) regime (interceptors), and fighters optimized to fight in the within visual range (WVR) regime (air superiority fighters). In the United States, the influential proponents of BVR developed fighters with no forward-firing gun, such as the original F-4 Phantom II, as it was thought that they would never need to resort to WVR combat. These aircraft would sacrifice high maneuverability, and instead focus on other performance characteristics, as they presumably would never engage in a dogfight with enemy fighters.[citation needed]

Lessons in combat

Combat experiences during the Vietnam War proved BVR proponents wrong. Owing to restrictive rules of engagement and the failings of 1960s missile and radar technology, air combat often devolved into close-range dogfights. The lessons from this conflict spurred a rethinking of design priorities for fighter aircraft and development of the U.S. Navy's TOPGUN and the U.S. Air Force's Red Flag programs to teach pilots the lessons of dogfighting.[citation needed]

The first air superiority fighters

After lessons learned from combat experiences involving modern military air capacity, the U.S. Navy's VFAX/VFX and U.S. Air Force's F-X (Fighter Experimental) reassessed their tactical direction which resulted in the U.S. Navy's F-14 Tomcat and US Air Force's F-15 Eagle.[1] The two designs were built to achieve air superiority and significant consideration was given during the development of both aircraft to allow them to excel at the shorter ranges of fighter combat. Both aircraft also serve as interceptors due to their high maximum speed.[2][3]

By contrast, the Soviets (and the succeeding Russian Federation) developed and continue to operate separate types of air superiority (MiG-29, Su-27) and interceptor (MiG-25, MiG-31) fighters.[citation needed]

Evolution of secondary ground-attack capability

For the US Navy, the F-14 Tomcat was initially deployed solely as an air superiority fighter (plus fleet defense interceptor and tactical aerial reconnaissance). By contrast, the multirole F/A-18 Hornet was designed as strike fighter while having only enough of an edge to defend itself against enemy fighters if needed. While the F-14 had an undeveloped secondary ground attack capability (with a Stores Management System (SMS) that included air-to-ground options as well as rudimentary software in the AWG-9), the Navy did not want to risk it in the air-to-ground role at the time, due to its lack of proper defensive electronic countermeasures (DECM) and radar homing and warning (RHAW) for overland operations, as well as the fighter's high cost. In the 1990s, the US Navy added LANTIRN pods to its F-14s and deployed them on precision ground-attack missions.[4]

The F-15 Eagle was envisioned originally as an air superiority fighter and interceptor under the mantra "not a pound for air-to-ground".[5] However, the F-15C can carry "dumb" and GPS guided bombs, such capabilities which were first used by Israeli Air Force. In fact, the basic airframe proved versatile enough to produce a very capable strike fighter, the F-15E Strike Eagle. While designed for ground attack, it retains the air-to-air lethality of the original F-15.[6] Similarly, the F-16 Fighting Falcon was also originally designed as an air superiority fighter but has since evolved into a successful all-weather multirole aircraft.[7]

1990s to present

Since the 1990s, with air superiority fighters such as the F-14 and F-15 pressed into the strike role and/or having a strike derivative, the lines between air superiority fighters and multirole fighters has blurred somewhat.

With the retirement of the F-14 Tomcat, the US Navy has pressed its F/A-18 Hornet and its upsized derivative, the F/A-18E/F Super Hornet, into the air superiority role, despite the Hornets being originally designed as multirole strike fighters.

List

Country Manufacturer Aircraft Introduced
United States McDonnell Douglas F-15 Eagle 1976
Soviet Union/Russia Mikoyan MiG-29 1982
Soviet Union/Russia Sukhoi Su-27 1985
Russia/India Sukhoi Su-30MKI 2002
United States Lockheed Martin F-22 Raptor 2005
Russia Sukhoi Su-35S 2014

See also


PostcombustionAirbus Commercial AircraftAéronefCommandes de vol (avion)FuselageAvionAvion d'attaque au solBoeing 737Boeing 737 Next GenerationBoeing 787Boeing B-29 SuperfortressBoeing CH-47 ChinookBoeing F/A-18E/F Super HornetCarrier-based aircraftCessna O-2Cessna Skymasterde Havilland MosquitoAirbus Helicopters H225M CaracalEurofighter TyphoonPelle mécanique hydrauliqueAvion de chasseChasseur-bombardierRecord de vitesse aérienGeneral Dynamics F-16 Fighting FalconGrumman F6F HellcatHawker FuryHawker HurricaneHélicoptèreIAI KfirAvion à réactionJet engineLockheed Martin F-22 RaptorLockheed Martin F-35 Lightning IILockheed SR-71 BlackbirdMcDonnell Douglas F-4 Phantom IIMcDonnell Douglas MD-80McDonnell XF-85 GoblinMikoyan-Gourevitch MiG-27Military helicopterModel aircraftAvion multirôleNieuport 17Chasseur nocturneOlga E. CustodioAvion radiocommandéAvion de reconnaissanceVitesse du sonSoukhoï Su-27 FlankerSupersonic aircraftTranssoniqueAvion bipoutreBiréacteurThunderbirds (patrouille)Super-manœuvrabilitéGloster MeteorNorth American P-51 MustangNorth American P-51 Mustang variantsCourse aérienneMesserschmitt Bf 109Monocoque (structure)Verrière (aéronautique)Dassault Mirage F1Avion d'interceptionMcDonnell Douglas T-45 GoshawkMcDonnell Douglas AV-8B Harrier IIDassault Mirage 2000Eurocopter EC665 TigreHélicoptère d'attaqueAirbus HelicoptersBallon (aéronef)Ballon dirigeableGeneral Dynamics F-111 AardvarkAvion d'interdictionStrategic bomberElectronic-warfare aircraftTactique militaireGeneral Atomics MQ-1 PredatorIndustrie de l'armementAGM-114 HellfireMissileDirect Attack Guided RocketBoeing AH-64 ApacheArmed helicopterAircraft ordnanceAdvanced Attack HelicopterChasseur d'attaqueAir combat manoeuvringSupériorité aérienneUnited States Air ForceMcDonnell Douglas F/A-18 Hornet

This article uses material from the Wikipedia article "", which is released under the Creative Commons Attribution-Share-Alike License 3.0. There is a list of all authors in Wikipedia

Transportation - Air Water Earth

3D,CAD,Model,Libary,Railway, Train, Ship, Marine, Submarine, Automotive, Locomotive, Bike, Car, Formula 1, Space, Aircraft, Aerospace, Satelite, Automobile, Yacht