powered by CADENAS

Social Share

Amazon

Carrier-based aircraft (5435 views - Transportation - Air Water Earth)

Carrier-based aircraft, sometimes known as carrier-capable aircraft or carrier-borne aircraft, are naval aircraft designed for operations from aircraft carriers. They must be able to launch in a short distance and be sturdy enough to withstand the abrupt forces of launching from and recovering on a pitching deck. In addition, their wings are generally able to fold up, easing operations in tight quarters. Such aircraft are designed for many purposes including air-to-air combat, surface attack, anti-submarine warfare (ASW), search and rescue (SAR), transport (COD), weather observation, reconnaissance and airborne early warning and control (AEW&C) duties.The term is generally applied only to fixed-wing aircraft, as naval helicopters are able to operate from a wider variety of ships, including helicopter carriers and container ships.
Go to Article

Explanation by Hotspot Model

Youtube


    

Carrier-based aircraft

Carrier-based aircraft

Carrier-based aircraft

Carrier-based aircraft, sometimes known as carrier-capable aircraft or carrier-borne aircraft, are naval aircraft designed for operations from aircraft carriers. They must be able to launch in a short distance and be sturdy enough to withstand the abrupt forces of launching from and recovering on a pitching deck. In addition, their wings are generally able to fold up, easing operations in tight quarters.

Such aircraft are designed for many purposes including air-to-air combat, surface attack, anti-submarine warfare (ASW), search and rescue (SAR), transport (COD), weather observation, reconnaissance and airborne early warning and control (AEW&C) duties.[1]

The term is generally applied only to fixed-wing aircraft, as naval helicopters are able to operate from a wider variety of ships, including helicopter carriers and container ships.

History

The 1903 advent of fixed-wing aircraft was followed in 1910 by the first flight of an aircraft from the deck of an anchored warship (the United States Navy's USS Birmingham), and in 1912, by the first flight of an aircraft from the deck of a warship underway (the Royal Navy's HMS Hibernia). Seaplanes and seaplane tender support ships, such as HMS Engadine, followed. This evolution was well underway by the early 1920s, resulting in ships such as HMS Argus (1918), Hōshō (1922), USS Langley (1922), and Béarn (1927). With these developments, the need for specialized aircraft adapted for takeoffs and landings from the flight decks of those ships became recognized.

The significance of air power grew between the wars, driven by the increased range, carrying power, and effectiveness of carrier-launched aircraft, until it became impossible to disregard its importance during World War II, following the loss of many warships to aircraft, including the sinking of Prince of Wales and Repulse, the Battle of Taranto, the Attack on Pearl Harbor and numerous other incidents. Following the war, carrier operations continued to increase in size and importance.[2]

Types

Modern carrier-based aircraft are built in mainly three different versions to suit the needs of its various users. The following terms are those used currently by the U.S. Navy.

Catapult-Assisted Take-Off But Arrested Recovery

CATOBAR is a system used for the launch and recovery of aircraft from the deck of an aircraft carrier. Under this technique, aircraft are launched using a catapult-assisted take-off and landing on the ship using arresting wires. Although this system is more costly than alternative methods, it provides greater flexibility in carrier operations, since it allows the aircraft to operate with higher payloads. Ships with CATOBAR currently include the U.S. Nimitz class[2], and France's Charles de Gaulle.

The use of catapults allows an aircraft carrier to launch large fixed-wing aircraft. For example, the U.S. Navy launches its E-2 Hawkeye AEW aircraft and C-2A Greyhound cargo aircraft with catapults.

Short Take-Off and Vertical Landing

STOVL takeoffs are accomplished with "ski-jumps", instead of a catapult. STOVL use usually allows aircraft to carry a larger payload as compared to during VTOL use, while avoiding the complexity of a catapult. The best known example is the Hawker Siddeley Harrier Jump Jet,[3] despite being capable of VTOL takeoffs, is usually operated as a STOVL aircraft to increase its fuel and weapons load.

Short Take-Off But Arrested Recovery

STOBAR is a system used for the launch and recovery of aircraft from the deck of an aircraft carrier, combining elements of both STOVL and CATOBAR. Aircraft launch under their own power using a ski-jump to assist take-off (rather than using a catapult). These are conventional aircraft however and require arresting wires to land on the ship. The Russian Navy aircraft carrier Admiral Kuznetsov operated the Su-33, in this manner. Others include the Indian Vikramaditya and the future Vikrant-class aircraft carrier; both will operate MiG-29Ks.[4]

Unassisted takeoff

Prior to World War II, the weight of most aircraft allowed them to be launched from aircraft carriers under their own power, but required assistance in stopping. Catapults were installed but were used only when the ship was stationary or adequate wind over the deck could not be arranged by sailing into the wind. Even aircraft as large as the North American B-25 Mitchell were launched in this manner. This was possible because the ship's speed with even the lightest prevailing winds, combined with a low takeoff speed allowed early aircraft to gain flying speed in a very short distance. The most extreme version of this was the battleship platforms used during the 1920s when small, World War I-era biplane fighters such as the Sopwith Camel were launched from only a few dozen feet long mounted atop of a battleship's forward gun turret.

Conventional aircraft, such as the Curtiss P-40 Warhawk, Republic P-47 Thunderbolt, Supermarine Spitfire, and Hawker Hurricane, were often delivered to overseas air bases by aircraft carrier. They would be loaded onto an aircraft carrier in port by cranes, flown off the carrier at sea near their destination under their own power, and land on a friendly airfield ashore. These were not usually combat missions but in some cases the launched aircraft provided air cover for the ship, and the aircraft could not be recovered by the carrier.

Some STOL aircraft, such as the North American Rockwell OV-10 Bronco, have been operated from aircraft carriers and amphibious assault ships in this manner more recently, but this is not common practice.

Even very large aircraft such as the Lockheed C-130 Hercules have been successfully landed and launched from large aircraft carriers, but was done with no cargo and little fuel on board the aircraft.

Modern carrier-based aircraft in service

In service

Under development

See also


Airbus Commercial AircraftAéronefCommandes de vol (avion)FuselageAvionAltitudes et vitesses (aéronautique)Boeing 737Boeing 737 Next GenerationBoeing 787Boeing B-29 SuperfortressBoeing CH-47 ChinookBoeing F/A-18E/F Super HornetBoeing ScanEagleCessna O-2Cessna SkymasterAirbus Helicopters H225M CaracalEurofighter TyphoonAvion de chasseChasseur-bombardierRecord de vitesse aérienGeneral Dynamics F-16 Fighting FalconHawker FuryHawker HurricaneHélicoptèreLockheed Martin F-22 RaptorLockheed Martin F-35 Lightning IILockheed SR-71 BlackbirdMcDonnell Douglas F-4 Phantom IIMcDonnell Douglas MD-80McDonnell XF-85 GoblinMilitary helicopterAvion multirôleChasseur nocturneVitesse du sonSupersonic aircraftTranssoniqueAvion bipoutreBiréacteurThunderbirds (patrouille)Avion d'attaque au solGeneral Electric J79Compresseur axialAvioniqueMikoyan-Gourevitch MiG-27Soukhoï Su-27 FlankerAir superiority fighterSuper-manœuvrabilitéGloster MeteorNorth American P-51 Mustang variantsCourse aérienneMonocoque (structure)Verrière (aéronautique)Dassault Mirage F1Avion d'interceptionMcDonnell Douglas T-45 GoshawkMcDonnell Douglas AV-8B Harrier IIDassault Mirage 2000Eurocopter EC665 TigreHélicoptère d'attaqueAirbus HelicoptersBallon (aéronef)Ballon dirigeablePropulsion électrocinétiqueGeneral Dynamics F-111 AardvarkAvion d'interdictionStrategic bomberElectronic-warfare aircraftTactique militaireAvion militaireGeneral Atomics MQ-1 PredatorIndustrie de l'armementAGM-114 HellfireMissileDirect Attack Guided RocketBoeing AH-64 ApacheArmed helicopterAircraft ordnanceAdvanced Attack HelicopterTurbomoteurAvion à fuselage largeCargo aircraftAir cargoLockheed T-33 Silver StarFlight trainingCompagnie aérienneAviationAtterrissageDécollagePiste (aérodrome)AéronautiqueAircraft design processQuadrirotorMultirotorMcDonnell Douglas F/A-18 Hornet

This article uses material from the Wikipedia article "", which is released under the Creative Commons Attribution-Share-Alike License 3.0. There is a list of all authors in Wikipedia

Transportation - Air Water Earth

3D,CAD,Model,Libary,Railway, Train, Ship, Marine, Submarine, Automotive, Locomotive, Bike, Car, Formula 1, Space, Aircraft, Aerospace, Satelite, Automobile, Yacht