Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
Vickers Medium Mark I | |
---|---|
Vickers tanks on the move in England in the 1930s | |
Type | Medium tank |
Place of origin | United Kingdom |
Production history | |
Manufacturer | Vickers |
Specifications (Mk I) | |
Weight | 11.7 long tons |
Length | 17 ft 6 in (5.33 m) |
Width | 9 ft 1.5 in (2.781 m) |
Height | 9 ft 3 in (2.82 m) |
Crew | 5 |
Armour | 6.25 mm |
Main armament | QF 3 pounder gun (47 mm) |
Secondary armament | four 0.303 (7.7 mm) Hotchkiss M1909 Benét–Mercié machine guns two 0.303 Vickers machine guns |
Engine | Armstrong Siddeley V-8 air-cooled petrol engine 90 hp (67 kW) |
Transmission | 4-speed gearbox to a 2-speed epicyclic |
Suspension | helical spring |
Operational range | 120 mi (190 km) |
Speed | 15 mph (24 km/h) |
The Vickers Medium Mark I was a British tank of the Inter-war period built by Vickers.
After the First World War Britain disbanded most of its tank units leaving only five tank battalions equipped with the Mark V and the Medium Mark C. At first a large budget was made available for tank design but this was all spent on the failed development of the Medium Mark D.[1] When the government design bureau, the Tank Design Department, was closed in 1923 any direct official involvement in tank development was terminated. However private enterprise in the form of the Vickers-Armstrong company built two prototypes of a new tank in 1921.
In 1920 the Infantry had plans to acquire a Light Infantry Tank. Colonel Johnson of the Tank Design Department derived such a type from the Medium Mark D. In competition Vickers built the Vickers Light Tank.[2]
The Vickers design still was reminiscent of the Great War types. It had a high, lozenge-shaped, track frame with side doors but it also showed some improvements. There was a fully revolving turret and the suspension was provided by vertical helical springs, while the Medium Mark C still had a fixed turret and was unsprung. The Vickers was much smaller than the Medium C at just seven feet high and weighing only 8.5 short tons. It was driven by a separately compartmented 86 hp engine through an advanced hydraulic Williams-Jenney transmission, allowing infinitely variable turn cycles. The first prototype was a "Female" version with three Hotchkiss machine guns; the second prototype was a "Male" which had a 3-pounder gun in place of one of the machine guns and also a machine gun for anti-aircraft use. It looked far closer to a modern tank than its predecessors with the turret, the front of the fighting compartment and the hull front plate all strongly rounded. The advanced transmission proved to be utterly unreliable however and the project was abandoned in 1922 in favour of a generally more conventional design, the Vickers Light Tank Mark I. This would be renamed the Vickers Medium Tank Mark I in 1924 . The first prototypes were sent to Bovington for trial in 1923. The Vickers designation was A2E1.
Despite being in general more conventional, in one aspect the Medium Mark I looked rather modern: instead of a high track run it possessed a low and flat suspension system with five bogies, each having a pair of small double wheels. The axles of these were too weakly constructed; as Major-General N.W. Duncan put it in his Medium Marks I-III: "(...) a perpetual nuisance. The axles were continually breaking and the path of the Mark I tanks was littered with discarded wheels". This was cured by switching to a "box bogie" in 1931.[3] To ease repairs the suspension was not protected by an armoured covering. There were two vertical helical springs of unequal length in each of the five bogie casings attached to the hull. In front and behind the normal ten road wheel pairs, there was a tension wheel pair. Ground pressure was very high, even though at 11.7 long tons the vehicle was not very heavy for its size.
The engine was an air-cooled 90 hp Armstrong Siddeley engine derived from an aircraft type. Surprisingly the engine and transmission was distributed throughout the hull - with the engine to the left of the driver, the gearbox underneath the commander and final drive at the rear, which Duncan describes as "an unbelievable retrograde step in view of war-time experience". The Medium Mark B and the Mark VIII had introduced compartmentalisation to reduce the debilitating effects of engine noise and fumes on the crew. However, with the Medium Mark I considerations of ease of maintenance took precedence.
The engine drove, via a multiple dry-plate clutch, a four-speed gearbox. It had no synchromesh and switching between gears without excessive noise was a challenge to the driver.[4] A propeller shaft connected the gearbox to a bevel box at the end of the tank which divided the power to a separate epicyclic gear for each track. These gears automatically[citation needed] provided extra emergency torsion to the normal first and second gear if the vehicle suddenly slowed down due to an obstacle or soft ground.
The petrol tanks were at the very rear of the hull, so the fuel lines had to run along the whole length of the vehicle, pumping fuel to a secondary tank that fed the engine by gravity. The engine was lubricated and partially cooled by oil; leakage was common and the original four-gallon reservoir had to be replaced by a 13.5 one. The tank could be electrically started, but only if the motor was already warm, so the first start had to be done by hand from the inside of the vehicle. Maximum speed was about 15 mph and the range about 120 miles.
There was a cylindrical bevelled turret on top of the hull that carried a "Quick Firing" (shell and cartridge in one complete round) three-pounder gun (47 mm calibre) and four ball mountings for Hotchkiss machine guns. A novel, unique feature was a three-man turret. This meant that commander was not distracted with performing either the loader's or gunner's tasks and could fully concentrate on maintaining situational awareness.[5] This gave a huge potential combat advantage, but went largely unnoticed at the time.[citation needed] Except for the Lago prototype, a predecessor to the Stridsvagn m/42, produced by Landsverk in 1934[6] no other manufacturer constructed a tank with a three-man turret until the German Panzer III. The practical importance of this feature is signified by the fact that later into the Second World War, most of both sides tank designs either quickly switched to the three-man turret, or were abandoned as obsolete.[citation needed]
There was no co-axial machine gun. There was only room to operate one machine gun from the turret; normally one gun was switched between the respective mountings as the guns were removable. The turret machine gunner doubled as main gun loader. In each side of the hull was a Vickers machine gun. There was one gunner to operate these, he also functioned as a mechanic.
The shape of the Mark I Medium hull was very distinctive. The back was a simple armoured box; the front plate was high and perfectly vertical. Between them, from the armoured hood of the driver at the right of the vehicle six armour plates fanned out to the left, making for a complex hull geometry at that side. In all the tank made an ungainly squat impression. The crew of five was only poorly protected by 6.25 mm plating, rivetted to the chassis, barely enough to counter the threat posed by light machine guns. With its many shot traps the vehicle was unable to withstand even anti-tank rifle fire and it had a high-profile. The internal lay-out worsened this vulnerability as the petrol tanks were inside the main compartment.[7][not in citation given]
The Medium Mark I replaced some of the Mark V heavy tanks. Together with its successor, the slightly improved Vickers Medium Mark II, it served in the Royal Tank Regiments, being the first type of the in total 200 tanks to be phased out in 1938.[clarification needed]
The Medium Mark I was the first tank to see "mass" production since the last of the ten Char 2C's was finished in 1921. As only about thirty of the next most produced tank, the Renault NC27, were built, the British Mediums represented most of the world tank production during the 1920s. They never fired a shot in anger and their performance in a real battle can only be speculated upon but, as the only modern tanks in existence in the decade after the First World War, they provided the British with a unique opportunity to test the many new ideas about mechanised warfare using real operational units. The knowledge thus gained would prove invaluable in the Second World War.
On one Medium Mark I the engine was replaced by a Ricardo 90 hp diesel engine.
One Vickers Medium Mark 1 has survived at the Special Services Battalion Museum, Bloemfontein, South Africa.[11]
|website=
(help)
Wikimedia Commons has media related to Vickers Medium Mark I. |
Tankettes | |
---|---|
Light | |
Medium | |
Cavalry, Cruiser and Fast | |
Infantry | |
Heavy | |
Super-heavy | |
Armoured carriers | |
This article uses material from the Wikipedia article "", which is released under the Creative Commons Attribution-Share-Alike License 3.0. There is a list of all authors in Wikipedia
3D,CAD,Model,Libary,Railway, Train, Ship, Marine, Submarine, Automotive, Locomotive, Bike, Car, Formula 1, Space, Aircraft, Aerospace, Satelite, Automobile, Yacht