powered by CADENAS

Social Share

Amazon

Shaker scoop (4381 views - Mechanical Engineering)

A shaker scoop (sometimes called a shaker hood scoop or a shaker hood) is an automobile term for an air intake for combustion air that is mounted directly on top of the engine's air cleaner and protrudes through a hole in the hood. Since it is fastened directly to the engine, it moves with the engine's movement and vibration on its mountings, thus the 'shaker' name. Some official Chrysler literature referred to this popular hood style as the "Incredible Quivering Exposed Cold Air Grabber". This lengthy title has since been shortened by enthusiasts and collectors to the less tongue-twisting "shaker hood". Like all such scoops, its purpose is to increase performance at high speed by a 'ram air' effect, delivering high pressure air to the engine. However, engines draw air in hundreds of cubic feet per minute so scoops are not practical to raise intake pressures significantly. Other benefits of a shaker hood include elevation to prevent water from being drawn on flooded terrain, a cooler source of air, and a more direct path to the engine's throttle plate. Such scoops were fitted to a variety of cars, including: 1969 Ford Mustang Cobra Jet 1969/1970 Boss 302 Mustang 1970 Plymouth Barracuda Dodge Challenger Ford Torino Pontiac GTO Pontiac Firebird Trans Am Pontiac Can Am Grand Am Ford Falcon XY GT Phase III 2004 Ford Mustang Mach 1
Go to Article

Explanation by Hotspot Model

Youtube


    

Shaker scoop

Shaker scoop

Shaker scoop

Licensed under Creative Commons Attribution-Share Alike 3.0 (The original uploader was Icedtrueno at English Wikipedia.).

A shaker scoop (sometimes called a shaker hood scoop or a shaker hood) is an automobile term for an air intake for combustion air that is mounted directly on top of the engine's air cleaner and protrudes through a hole in the hood. Since it is fastened directly to the engine, it moves with the engine's movement and vibration on its mountings, thus the 'shaker' name.

Some official Chrysler literature referred to this popular hood style as the "Incredible Quivering Exposed Cold Air Grabber".[1] This lengthy title has since been shortened by enthusiasts and collectors to the less tongue-twisting "shaker hood".

Like all such scoops, its purpose is to increase performance at high speed by a 'ram air' effect, delivering high pressure air to the engine. However, engines draw air in hundreds of cubic feet per minute so scoops are not practical to raise intake pressures significantly. Other benefits of a shaker hood include elevation to prevent water from being drawn on flooded terrain, a cooler source of air, and a more direct path to the engine's throttle plate.

Such scoops were fitted to a variety of cars, including:



This article uses material from the Wikipedia article "", which is released under the Creative Commons Attribution-Share-Alike License 3.0. There is a list of all authors in Wikipedia

Mechanical Engineering

AutoCAD, SolidWorks, Autodesk Inventor, FreeCAD, Catia, Siemens NX, PTC Creo, Siemens Solid Edge, Microstation, TurboCAD, Draftsight, IronCAD, Spaceclaim, VariCAD, OnShape, IntelliCAD,T-FLEX, VariCAD, TenadoCAD, ProgeCAD, Cadra, ME10, Medusa, Designspark, KeyCreator, Caddy, GstarCAD, Varimetrix, ASCON Kompas-3D, Free Download, Autocad, 2D Library, DXF, DWG, 2D drawing, 3D digital library, STEP, IGES, 3D CAD Models, 3D files, CAD library, 3D CAD files, BeckerCAD, MegaCAD, Topsolid Missler, Vero VisiCAD, Acis SAT, Cimatron, Cadceus, Solidthinking, Unigraphics, Cadkey, ZWCAD, Alibre, Cocreate, MasterCAM, QCAD.org, QCAD, NanoCAD