powered by CADENAS

Social Share

Amazon

Video door-phone (3067 views - Electronics & PCB Engineering)

Video door-phone (also known as video door entry or video intercom) is a stand-alone intercom system used to manage calls made at the entrance to a building (residential complex, detached family home, workplace, etc.) with access controlled by audiovisual communication between the inside and outside. The main feature of video door entry is that it enables the person indoors to identify the visitor and, if (and only if) they wish, engage in conversation and/or open the door to allow access to the person calling.
Go to Article

Explanation by Hotspot Model

Video door-phone

Video door-phone

Video door-phone (also known as video door entry or video intercom) is a stand-alone intercom system used to manage calls made at the entrance to a building (residential complex, detached family home, workplace, etc.) with access controlled by audiovisual communication between the inside and outside. The main feature of video door entry is that it enables the person indoors to identify the visitor and, if (and only if) they wish, engage in conversation and/or open the door to allow access to the person calling.

Equipment

Video door entry consists of both outside and indoor elements: an outdoor panel on the outside, an electronic lock release and an indoor monitor. The outdoor panel or street panel is installed beside the entrance door or gateway and incorporates different elements ready for use in any climate conditions: one or several pushbuttons to make the call (usually one per home or apartment), a micro camera adapted for night vision to capture the image of the caller, a microphone to pick up their voice and a speaker to reproduce the voice of the occupant indoors. A video door entry panel may include push buttons to call the homes or offices and a camera to capture the street scene. The video entry monitor allows the occupant to see who has called, talk to the visitor and open the door. Installed indoors, the monitor consists of a screen showing the image of the person calling, a microphone and earpiece for conversation and a pushbutton to trigger the door lock release. The communication set up is full duplex. The electric door release is a device installed in the door lock and operated from inside the building to lift the latch and clear the way for the visitor.

Common equipment types

There are several variations on this basic format. In addition to outdoor panels with one pushbutton per apartment, it is possible to find others with a numeric keypad: in this case, designed for large residential installations, the homes are identified by codes. Others have built-in cardholders panels or even small screens to guide the user or facilitate entry for people with disabilities. Some video entry monitors have an earpiece similar to a telephone handset, while others are "hands-free". Other examples are monitors with memories which store an image every time someone calls at the door or touchscreen video entry systems.

Classification of Video door phone(VDP)

Video door phone can be classified two possible classification :

1. Security Layers :

a. Level 1 security - This is security layer added by VDP system at the community entrance. This layer is given to the guard who will directly verify the entry of a visitor to the community. Such systems are only at a community level.

b. Level 2 Security : This is also known as the lobby security - This is to get access to your lobby of the apartment in such a case the visitor will have to dial the number of the flat and then the flat owner allows the access to a visitor from the lobby entrance itself.

c. Level 3 security : In this case the visitor communicates with the outdoor camera in front of house door or villa gate.


2. Technologies & classification :

a. Standalone - A standalone VDP is a device used in villas or by individual home owners.

Types of technology of standalone VDP -

i. Analog VDP - It is analog display and camera.

ii.Connected digital VDP - This is a digital LCD display with Digital camera usually with image capture and video capturing ability when the bell is pressed. In this case normally some additional camera integration is also allowed.

iii. Wireless video door bell(VDB) : A camera units which gets connected to interned or router and allows communication with ones mobile or tablet top communicate with the visitor.


b. Multi-apartment- This is a solution where there is an mass housing scenario.

i. Analog Multi-apartment systems - This is a Analog VDP providing 3 tier security.

ii. IP VDP Multi-apartment system - This is IP VDP which is 3 tier security and integration with BMS (Building management system ), Security systems like intrusion , CCTV building security and in most cases even Home Automation.

Automatic operation

When a visitor presses one of the outdoor panel pushbuttons, the built-in camera is connected and the image captured outdoors appears on the monitor screen. Connection takes place automatically with no need to activate the equipment, which is one of the essential elements of video door entry. As of this point, the person inside the building can open the door if they wish or begin a conversation, which is usually secret (cannot be heard by other users of the same facility). The equipment also disconnects automatically after a set time has elapsed. The video entry system as a whole runs on low voltage energy from the building’s trunk

Extra functions

Many terminals currently on the market are ready to accept extensions, making the monitor into a small automatic function control centre. From here, the user can view one or several additional cameras installed at other access points, trigger light switches or open a second door, etc.

Video door entry systems with access control

Video door entry systems are commonly found integrated with different access control systems. This means that elements are installed in the same outdoor panel to allow certain previously authorised users to access the premises. The most common means are proximity cards, fingerprint readers, a keypad for secret numbers or even Bluetooth triggered by mobile phone.

Adaptive equipment

Different equipment sets are currently found on the market which make use more accessible for people with different disabilities. So, thinking of the visually impaired, the outdoor panel may include information in Braille alongside the pushbuttons, or a voice synthesiser can also be added which indicates when the door is opened. For people with hearing impairment, the outdoor panel may include a screen with icons signalling the communication status: if the user is calling, if someone is speaking from indoors or opening the door. Also with this type of user in mind, the monitor may be fitted with an inductive loop, an element which interacts with conventional hearing aids to facilitate conversation with the outside without their presence being noticed by other users. The kit also includes visual or audio call alerts.

See also



This article uses material from the Wikipedia article "", which is released under the Creative Commons Attribution-Share-Alike License 3.0. There is a list of all authors in Wikipedia

Electronics & PCB Engineering

Cadence, Mentor Graphics, Eagle CAD, Altium Designer, AUTODESK EAGLE, Cadence Allegro, DesignSpark PCB , Mentor PADS, Mentor Xpedition, Novarm DipTrace, Pulsonix, TARGET 3001!, Xpedition xDX Designer, Zuken CADSTAR, Altium P-CAD, Agnisys, Altera Quartus, OrCAD, kiCAD, Solido Design Automation, ELectronics, PCB, Curcuit Board, 3D drawings, 3D library, 3D content, PCB Design, 2D symbols, 2D drawings, 2D icons, 2D schematics