powered by CADENAS

Social Share

Amazon

Fire pit (9418 views - Architecure & BIM & MEP)

A fire pit or a fire hole can vary from a pit dug in the ground to an elaborate gas burning structure of stone, brick, and metal. The common feature of fire pits is that they are designed to contain fire and prevent it from spreading.
Go to Article

Explanation by Hotspot Model

Youtube


    

Fire pit

Fire pit

A fire pit or a fire hole can vary from a pit dug in the ground to an elaborate gas burning structure of stone, brick, and metal. The common feature of fire pits is that they are designed to contain fire and prevent it from spreading.

Contemporary types

Pre-made fire pits are the most common form of fire pits and can be purchased from a store.[1] These are commonly made of pre cast concrete or metal and/or a combination of metal table and stone. They are usually natural gas, propane (LP) or bio ethanol. Wood burning fire pits made of metal are also quite common but under increasing scrutiny due to fire bans and air particulate emissions. Natural gas and propane burners in these sort of pre fabricated vessels are certified under ANSI (American), CSA (Canadian) and CE (European) standards. Unregulated and uncertified fire pit burners are increasingly being scrutinized by regulatory authorities and being denied permits. Fire pits have recommended clearance to combustibles and require at least 5 feet above the flame and 16" circumference from the exterior perimeter of the vessel.

Essentially, to make a fire pit only a hole is required in order to safely contain a fire. This can be as simple as digging a hole in the ground, or as complex as hollowing out a brick or rock pillar. A wood-burning fire pit should be located at least ten feet (three metres) away from structures for safety. Use of a fire pit in adverse conditions should be avoided, and basic fire safety precautions apply.

The Dakota smokeless fire pit

The Dakota fire pit is an efficient, simple fire design that produces little to no smoke.[2] As depicted in the illustration, two small holes are dug in the ground: one for the firewood and the other to provide a draft of air. Small twigs are packed into the fire hole and readily combustible material is set on top and lit. The fire burns from the top downward, drawing a steady, laminar stream of fresh air from the air hole as it burns. Because the air passes freely around the fuel, near complete combustion is achieved, the result being a fire that burns strongly and brightly and with little or no seen smoke. The Dakota fire pit is a tactical fire used by the United States military as the flame produces a low light signature, reduced smoke, and is easier to ignite under strong wind conditions.[3]

Fire pits in history

Many cultures, particularly nomadic ones would cut the turf above the fire-pit in a turf cutting ceremony, replacing the turf afterwards to hide any evidence of the fire.[4] Elements of this ceremony remain in traditional youth organizations such as the Woodcraft Folk.

Modern fire pits

Many homeowners are using fire pits for warmth, entertainment and cooking or as focal points for an outdoor living space.[5] Some recent trends have included the modification of compression tank ends to create a fire bowl that can be placed in the ground or on legs. See Indian Fire Bowls [6]

Archaeological significance

The remains of fire pits preserve information about past cultures. Radiocarbon dating from charcoal found in old fire pits can estimate when regions were first populated or when civilizations died out. Bones and seeds found in fire pits indicate the diet of that area.

In archaeological terms fire pits are referred to as features because they can be seen and recorded as part of the site but cannot be moved without being destroyed.

See also



This article uses material from the Wikipedia article "", which is released under the Creative Commons Attribution-Share-Alike License 3.0. There is a list of all authors in Wikipedia

Architecure & BIM & MEP

Autodesk Revit, Nemetschek ArchiCAD, Nemetschek Allplan, Vectorworks, Bentley AECOMSIM, Bentley Microstation, Trimble Tekla, Trimble Sketchup, EliteCAD, Ascon Renga, BricsCAD, Hexagon, Rhinoceros CAD, Sweet Home 3D, objet BIM, composant BIM, bibliothèque BIM, famille BIM, catalogue BIM, GIS, Advanced Steel, AutoCAD MEP, linéaire, MagiCAD, Relux, TGA, VDI 3805, Lod100, Lod200, Lod300, Lod350, Lod400, Lod500, Loi, IFC, BuildingSmart, création de famille BIM, 3D, téléchargement, bibliothèque de produits MEP BIM