powered by CADENAS

Social Share

Gate (7438 views - Architecure & BIM & MEP)

A gate or gateway is a point of entry to a space which is enclosed by walls. Gates may prevent or control the entry or exit of individuals, or they may be merely decorative. Other terms for gate include yett and port. The word derives from the old Norse "gata", meaning road or path, and originally referred to the gap in the wall or fence, rather than the barrier which closed it. The moving part or parts of a gateway may be called "doors", but used for the whole point of entry door usually refers to the entry to a building, or an internal opening between different rooms. A gate may have a latch to keep it from swinging and a lock for security. Larger gates can be used for a whole building, such as a castle or fortified town, or the actual doors that block entry through the gatehouse. Today, many gate doors are opened by an automated gate operator.
Go to Article

Explanation by Hotspot Model

Gate

Gate

Gate

Licensed under Creative Commons Zero, Public Domain Dedication (Mike Sándor).

A gate or gateway is a point of entry to a space which is enclosed by walls. Gates may prevent or control the entry or exit of individuals, or they may be merely decorative. Other terms for gate include yett and port. The word derives from the old Norse "gata", meaning road or path, and originally referred to the gap in the wall or fence, rather than the barrier which closed it. The moving part or parts of a gateway may be called "doors", but used for the whole point of entry door usually refers to the entry to a building, or an internal opening between different rooms.

A gate may have a latch to keep it from swinging and a lock for security. Larger gates can be used for a whole building, such as a castle or fortified town, or the actual doors that block entry through the gatehouse. Today, many gate doors are opened by an automated gate operator.

Types

Types of gates include:

Image gallery

See also



This article uses material from the Wikipedia article "", which is released under the Creative Commons Attribution-Share-Alike License 3.0. There is a list of all authors in Wikipedia

Architecure & BIM & MEP

Autodesk Revit, Nemetschek ArchiCAD, Nemetschek Allplan, Vectorworks, Bentley AECOMSIM, Bentley Microstation, Trimble Tekla, Trimble Sketchup, EliteCAD, Ascon Renga, BricsCAD, Hexagon, Rhinoceros CAD, Sweet Home 3D, objet BIM, composant BIM, bibliothèque BIM, famille BIM, catalogue BIM, GIS, Advanced Steel, AutoCAD MEP, linéaire, MagiCAD, Relux, TGA, VDI 3805, Lod100, Lod200, Lod300, Lod350, Lod400, Lod500, Loi, IFC, BuildingSmart, création de famille BIM, 3D, téléchargement, bibliothèque de produits MEP BIM