Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
Licensed under Creative Commons Attribution-Share Alike 3.0 (User:Tshrinivasan).
The examples and perspective in this article may not represent a worldwide view of the subject. You may improve this article, discuss the issue on the talk page, or create a new article, as appropriate. (April 2016) (Learn how and when to remove this template message) |
A disposable cup is a type of disposable tableware and disposable food packaging. Disposable cup types include paper cups, plastic cups and foam cups.[1][2] Expanded polystyrene is used to manufacture foam cups,[3] and polypropylene is used to manufacture plastic cups.[4]
As they are produced for single use, disposable cups and other similar disposable products constitute a major source of consumer and household waste,[5] such as paper waste and plastic waste. It has been estimated that the average household discards around 70 disposable cups every year.[5]
US consumption is some 108 billion cups per year,[6] the UK uses an estimated 2.5 billion paper cups every year.[7]
The disposable cone-shaped paper cup was invented in 1908 by Lawrence Luellen, and in 1912 Luellen and Hugh Moore began marketing the Health Kup, another paper disposable cup.[8] The Health Kup was designed to create a means for people to drink water from public water barrels without spreading germs, which occurred when people would use a common (shared) cup or a dipper to hold the water.[8] The Health Kup was later renamed to Dixie Cup, and was named after a brand of dolls.[8] Luellen and Moore later developed a disposable paper ice cream cup, which included lids with images of sportspeople, movie stars and animals.[8]
Some companies, such as coffee retailers[9] and doughnut shops,[10] sell their products in disposable cups. A 2011 book estimated that a chain of doughnut shops used one billion disposable coffee cups in a year, enough to circle the Earth twice.[10] A 2012 article in OnEarth said that Starbucks used over four billion disposable coffee cups in 2011.[11] The Cup Noodles brand of instant noodles uses expanded polystyrene foam cups to contain the product.[12] Hot or boiling water is added to the dried noodles in the container, which cooks the product in a few minutes.[12] Nissin Foods began marketing the product in foam cups in the early 1970s.[13]
The manufacturing of paper cups contributes to water pollution when chemicals such as chlorine, chlorine dioxide and reduced sulfides enter waterways.[2] The manufacturing of foam cups contributes to air pollution when pentane is released into the air.[2]
The curbside recycling of polypropylene containers has slowly increased in some developed countries, but is still rather limited.[4]
McDonald's switched from foam cups to paper cups in 2014,[6] and is moving to recycle paper cups in the UK, as of 2016, in partnership with Simply Cups and James Cropper.[7]
Several coffee chains offer a discount if the customer brings along their own cup.[14]
At festivals such as the Bavarian Oktoberfest, costs due to theft or breakage are avoided without using disposables: The customer pays an upfront fee for a drinking glass or mug and receives a rebate at its return.
This article uses material from the Wikipedia article "", which is released under the Creative Commons Attribution-Share-Alike License 3.0. There is a list of all authors in Wikipedia
3d,CAO, modèles, bibloiothèque, téléchargement, dessin,step, blocs CAO, université, lycée, BTS, BEP, CAP, collège, école, statistiques, impression 3D