powered by CADENAS

Social Share

Amazon

Place of worship (2806 views - Monuments - Famous Buildings)

A place of worship is a specially designed structure or consecrated space where individuals or a group of people such as a congregation come to perform acts of devotion, veneration, or religious study. A building constructed or used for this purpose is sometimes called a house of worship. Temples, churches, synagogues and mosques are examples of structures created for worship. A monastery, particularly for Buddhists, may serve both to house those belonging to religious orders and as a place of worship for visitors. Natural or topographical features may also serve as places of worship, and are considered holy or sacrosanct in some religions; the rituals associated with the Ganges river are an example in Hinduism. Under International Humanitarian Law and the Geneva Conventions, religious buildings are offered special protection, similar to the protection guaranteed hospitals displaying the Red Cross or Red Crescent. These international laws of war bar firing upon or from a religious building. Religious architecture expresses the religious beliefs, aesthetic choices, and economic and technological capacity of those who create or adapt it, and thus places of worship show great variety depending on time and place.
Go to Article

Explanation by Hotspot Model

Youtube


    

Place of worship

Place of worship

The Parthenon in Athens, Greece, was built for the goddess Athena in 447–432 BC and remained devoted to her cult for nearly a thousand years, later serving as a Christian church and then as an Islamic mosque under the Ottoman Empire.

A place of worship is a specially designed structure or consecrated space where individuals or a group of people such as a congregation come to perform acts of devotion, veneration, or religious study. A building constructed or used for this purpose is sometimes called a house of worship. Temples, churches, synagogues and mosques are examples of structures created for worship. A monastery, particularly for Buddhists, may serve both to house those belonging to religious orders and as a place of worship for visitors. Natural or topographical features may also serve as places of worship, and are considered holy or sacrosanct in some religions; the rituals associated with the Ganges river are an example in Hinduism.

Under International Humanitarian Law and the Geneva Conventions, religious buildings are offered special protection, similar to the protection guaranteed hospitals displaying the Red Cross or Red Crescent. These international laws of war bar firing upon or from a religious building.

Religious architecture expresses the religious beliefs, aesthetic choices, and economic and technological capacity of those who create or adapt it, and thus places of worship show great variety depending on time and place.

Buddhism

Christianity

The word church derives from the Greek ekklesia, meaning the called-out ones. Its original meaning is to refer to the body of believers, or the body of Christ.[1] The word church is used to refer to a Christian place of worship by some Christian denominations, including Anglicans and Catholics. Other Christian denominations, including the Religious Society of Friends, Mennonites, Christadelphians, and some unitarians, object to the use of the word "church" to refer to a building, as they argue that this word should be reserved for the body of believers who worship there.[2] Instead, these groups use words such as "Hall" to identify their places of worship or any building in use by them for the purpose of assembly.

Classical antiquity

Ancient Greece

Ancient Rome

The main place of worship is called a "Mandir"

Some people call it Hindu temple. Tha name Mandir comes from Sanskrit and means house, temple or palace. Hinduism has no set day of worship each week, there in no rules about when Hindus go to the Mandit. They visit the Mandir when ever they feel the need to. Shoes are removed before entering.



The symbolism and structure of a Hindu temple are rooted in Vedic traditions, deploying circles and squares.[3] A temple incorporates all elements of Hindu cosmos—presenting the good, the evil and the human, as well as the elements of Hindu sense of cyclic time and the essence of life—symbolically presenting dharma, kama, artha, moksa, and karma.[4][5][6]

Islam

A Mosque (/mɒsk/; from Arabic: المسجد Al-masjid‎) is a place of worship for followers of Islam. There are strict and detailed requirements in Sunni jurisprudence (fiqh) for a place of worship to be considered a masjid, with places that do not meet these requirements regarded as musallas. There are stringent restrictions on the uses of the area formally demarcated as the mosque (which is often a small portion of the larger complex), and, in the Islamic Sharia law, after an area is formally designated as a mosque, it remains so until the Last Day.

Many mosques have elaborate domes, minarets, and prayer halls, in varying styles of architecture. Mosques originated on the Arabian Peninsula, but are now found in all inhabited continents. The mosque serves as a place where Muslims can come together for salat (صلاة ṣalāt, meaning "prayer") as well as a center for information, education, social welfare, and dispute settlement. The imam leads the congregation in prayer.

Jainism

Derasar is a word used for a Jain temple in Gujarat and southern Rajasthan. Basadi is a Jain shrine or temple in Karnataka[7] There are some guidelines to follow when one is visiting a Jain temple:[8]

  • Before entering the temple, one should bathe and wear fresh washed clothes
  • One should not be chewing any edibles
  • One should try to keep as silent as possible inside temple.
  • Mobile phones should not be used in the temple.

Judaism

  • SynagogueJudaism
    • Some synagogues, especially Reform synagogues, are called temples, but Orthodox and Conservative Judaism consider this inappropriate as they do not consider synagogues a replacement for the Temple in Jerusalem. Some Jewish congregations use the Yiddish term 'shul' to describe their place of worship or Beyt Knesset ( Hebrew בית כנסת ) meaning house of assembly.

Norse Paganism

Shinto

Sikhism

Taoism

Zoroastrianism

Vietnamese ancestral worship

See also



This article uses material from the Wikipedia article "", which is released under the Creative Commons Attribution-Share-Alike License 3.0. There is a list of all authors in Wikipedia

Monuments - Famous Buildings

3D - 3D Model - 3D CAD - 3D Building - 3D monument - 3D Map - 3D City - 3D GIS - LIDAR - CityGML - Paris London Berlin Rome Sydney Barcelona Vienna Wien Budapest Madrid London