powered by CADENAS

Social Share

Amazon

Stress ball (8390 views - Game & Play & Gamification)

A stress ball or hand exercise ball is a malleable toy, usually not more than 7 cm in diameter, which is squeezed in the hand and manipulated by the fingers, ostensibly to relieve stress and muscle tension or to exercise the muscles of the hand. Despite the name, many stress balls are not spherical. Some are molded in amusing shapes, and pad- or transfer-printed with corporate logos. They are presented to employees and clients of companies as promotional gifts. Stress balls are the third most popular promotional gift in the United Kingdom. Because of the many non-spherical shapes now available, stress balls are generically known as stress relievers.
Go to Article

Explanation by Hotspot Model

Youtube


    

Stress ball

Stress ball

A stress ball or hand exercise ball is a malleable toy, usually not more than 7 cm in diameter, which is squeezed in the hand and manipulated by the fingers, ostensibly to relieve stress and muscle tension or to exercise the muscles of the hand.

Despite the name, many stress balls are not spherical. Some are molded in amusing shapes, and pad- or transfer-printed with corporate logos. They are presented to employees and clients of companies as promotional gifts. Stress balls are the third most popular promotional gift in the United Kingdom.[when?] Because of the many non-spherical shapes now available, stress balls are generically known as stress relievers.[1]

Types

A selection of foam-rubber stress relievers

There are several different types of stress balls that originate from many different countries. The most common type of stress ball in America is the “bean bag” type, commonly known as a “Hacky Sack”. The stress ball that is most common in Australia is the foam type, this type prevents stress through resistance from squeezing the ball. The third type of stress ball is the Chinese form known as the Baoding ball. These are not like the others as these are not squeezable, they are solid, they usually come in pairs so you can roll them together to make a soothing sound and a smooth sensation feeling in your hands.[2]

Some stress relievers are made from closed-cell polyurethane foam rubber. These are made by injecting the liquid components of the foam into a mold. The resulting chemical reaction creates carbon dioxide bubbles as a byproduct, which in turn creates the foam.[3]

Stress balls, especially those used in physical therapy, can also contain gel of different densities inside a rubber or cloth skin. Another type uses a thin rubber membrane surrounding a fine powder. The latter type can be made at home by filling a balloon with baking soda. Some balls similar to a footbag are marketed and used as stress balls.

See also


AceVideojuego de acciónApocalyptic and post-apocalyptic fictionArcade cabinetArcadeRealidad aumentadaAvatar (Internet)BackgammonBicicleta de entrenamiento sin pedalesBasket-hilted swordBattle royale (videojuegos)AlfilConteo de cartasJuego de naipesCarruselCasinoLos Colonos de CatánConecta 4DardosDadoCasa de muñecas (juguete)DominóEdge sortingFidget spinnerFirst-person (gaming)Videojuego de disparos en primera personaFortniteJuegoGame boyControlador de videojuegoMotor de videojuegoMando (videojuegos)Gameplay of PokémonJugador de videojuegosGaming houseGaming keypadGoogle CardboardHalo 3: ODSTTecnología inmersivaJob SimulatorPalanca de mandoRey (ajedrez)Caballo (ajedrez)Lego DuploMinifiguraRayo McQueenList of magical weaponsAnexo:Videojuegos más jugados por número de jugadoresMagic: el encuentroVideojuego de rol multijugador masivo en líneaMatrioshkaMetro 2033 (novela)Metro 2033 (videojuego)Mini 4WDMonopolyMonopoly video gamesVideojuego multijugadorOrigamiOVAPeón (ajedrez)PinballPersonaje jugadorJugador contra jugadorPlayerUnknown's BattlegroundsEspacio de recreaciónPokémonPóquerPortal (videojuego)Rompecabezas (juego)Dama (ajedrez)Modelismo ferroviarioAdivinanzaCaballo balancínTorre (ajedrez)Cubo de RubikVideojuego de disparosMáquinas tragamonedasSnookerCubo SomaSpinning coneSquishiesSuper Mario (serie)Horror de supervivenciaTangramOsito de pelucheTetrisTorres de HanóiJugueteToy blockToy trainVideoconsolaMundo virtualWooden toy trainWorld of WarcraftYukikaze (anime)Esferas chinasTransformers DecepticonsWarhammer 40 000Miniature wargamingMiniatura (juegos)Juego de guerraJuego de mesaBattleMechBattleTechHex map

This article uses material from the Wikipedia article "", which is released under the Creative Commons Attribution-Share-Alike License 3.0. There is a list of all authors in Wikipedia

Game & Play & Gamification

3d,model,playground,board games,computer,strategy,thinktank