powered by CADENAS

Social Share

Amazon

Airspeed (4957 views - Transportation - Air Water Earth)

Airspeed is the speed of an aircraft relative to the air. Among the common conventions for qualifying airspeed are indicated airspeed ("IAS"), calibrated airspeed ("CAS"), equivalent airspeed ("EAS"), true airspeed ("TAS"), and density airspeed. Indicated airspeed is simply what is read off of an airspeed gauge connected to a pitot static system, calibrated airspeed is indicated airspeed adjusted for pitot system position and installation error, and equivalent airspeed is calibrated airspeed adjusted for compressibility effects. True airspeed is equivalent airspeed adjusted for air density, and is also the speed of the aircraft through the air in which it is flying. Calibrated airspeed is typically within a few knots of indicated airspeed, while equivalent airspeed decreases slightly from CAS as aircraft altitude increases or at high speeds. With EAS constant, true airspeed increases as aircraft altitude increases. This is because air density decreases with higher altitude, but an aircraft's wing requires the same amount of air particles (i.e., mass of air) flowing around it to produce the same amount of lift for a given AOA; thus, a wing must move faster through thinner air than thicker air to obtain the same amount of lift. The measurement and indication of airspeed is ordinarily accomplished on board an aircraft by an airspeed indicator ("ASI") connected to a pitot-static system. The pitot-static system comprises one or more pitot probes (or tubes) facing the on-coming air flow to measure pitot pressure (also called stagnation, total or ram pressure) and one or more static ports to measure the static pressure in the air flow. These two pressures are compared by the ASI to give an IAS reading.
Go to Article

Explanation by Hotspot Model

Youtube


    

Airspeed

Airspeed

Airspeed

Airspeed is the speed of an aircraft relative to the air. Among the common conventions for qualifying airspeed are indicated airspeed ("IAS"), calibrated airspeed ("CAS"), equivalent airspeed ("EAS"), true airspeed ("TAS"), and density airspeed.

Indicated airspeed is simply what is read off of an airspeed gauge connected to a pitot static system, calibrated airspeed is indicated airspeed adjusted for pitot system position and installation error, and equivalent airspeed is calibrated airspeed adjusted for compressibility effects. True airspeed is equivalent airspeed adjusted for air density, and is also the speed of the aircraft through the air in which it is flying.[1] Calibrated airspeed is typically within a few knots of indicated airspeed, while equivalent airspeed decreases slightly from CAS as aircraft altitude increases or at high speeds.

With EAS constant, true airspeed increases as aircraft altitude increases. This is because air density decreases with higher altitude, but an aircraft's wing requires the same amount of air particles (i.e., mass of air) flowing around it to produce the same amount of lift for a given AOA; thus, a wing must move faster through thinner air than thicker air to obtain the same amount of lift.

The measurement and indication of airspeed is ordinarily accomplished on board an aircraft by an airspeed indicator ("ASI") connected to a pitot-static system. The pitot-static system comprises one or more pitot probes (or tubes) facing the on-coming air flow to measure pitot pressure (also called stagnation, total or ram pressure) and one or more static ports to measure the static pressure in the air flow. These two pressures are compared by the ASI to give an IAS reading.

Indicated airspeed

Indicated airspeed (IAS) is the airspeed indicator reading (ASIR) uncorrected for instrument, position, and other errors. From current EASA definitions: Indicated airspeed means the speed of an aircraft as shown on its pitot static airspeed indicator calibrated to reflect standard atmosphere adiabatic compressible flow at sea level uncorrected for airspeed system errors.[2]

Outside the former Soviet bloc, most airspeed indicators show the speed in knots (nautical miles per hour). Some light aircraft have airspeed indicators showing speed in statute miles per hour or kilometers per hour.

An airspeed indicator is a differential pressure gauge with the pressure reading expressed in units of speed, rather than pressure. The airspeed is derived from the difference between the ram air pressure from the pitot tube, or stagnation pressure, and the static pressure. The pitot tube is mounted facing forward; the static pressure is frequently detected at static ports on one or both sides of the aircraft. Sometimes both pressure sources are combined in a single probe, a pitot-static tube. The static pressure measurement is subject to error due to inability to place the static ports at positions where the pressure is true static pressure at all airspeeds and attitudes. The correction for this error is the position error correction (PEC) and varies for different aircraft and airspeeds. Further errors of 10% or more are common if the airplane is flown in “uncoordinated” flight.

Calibrated airspeed

Calibrated airspeed (CAS) is indicated airspeed corrected for instrument errors, position error (due to incorrect pressure at the static port) and installation errors.

Calibrated airspeed values less than the speed of sound at standard sea level (661.4788 knots) are calculated as follows:

minus position and installation error correction.

where
is the calibrated airspeed,
is the impact pressure (inches Hg): the difference between total pressure and static pressure,
is 29.92126 inches Hg; static air pressure at standard sea level,
is 661.4788 knots;, speed of sound at standard sea level.

Units other than knots and inches of mercury can be used, if used consistently.

This expression is based on the form of Bernoulli's equation applicable to isentropic compressible flow. The values for and are consistent with the ISA i.e. the conditions under which airspeed indicators are calibrated.

Equivalent airspeed

Equivalent airspeed (EAS) is defined as the airspeed at sea level in the International Standard Atmosphere at which the (incompressible) dynamic pressure is the same as the dynamic pressure at the true airspeed (TAS) and altitude at which the aircraft is flying. That is, it is defined by the equation

where

is the density of air at the altitude at which the aircraft is currently flying;
is the density of air at sea level in the International Standard Atmosphere (1.225 kg/m3 or 0.00237 slug/ft3).

EAS is a measure of airspeed that is a function of incompressible dynamic pressure. Structural analysis is often in terms of incompressible dynamic pressure, so equivalent airspeed is a useful speed for structural testing. The significance of equivalent airspeed is that, at Mach numbers below the onset of wave drag, all of the aerodynamic forces and moments on an aircraft are proportional to the square of the equivalent airspeed. Thus, the handling and 'feel' of an aircraft, and the aerodynamic loads upon it, at a given equivalent airspeed, are very nearly constant and equal to those at standard sea level irrespective of the actual flight conditions.

At standard sea level pressure, CAS and EAS are equal. Up to about 200 knots CAS and 10,000 ft (3,000 m) the difference is negligible, but at higher speeds and altitudes CAS diverges from EAS due to compressibility.

True airspeed

The true airspeed (TAS; also KTAS, for knots true airspeed) of an aircraft is the speed of the aircraft relative to the airmass in which it is flying. The true airspeed and heading of an aircraft constitute its velocity relative to the atmosphere.

Uses of true airspeed

The true airspeed is important information for accurate navigation of an aircraft. To maintain a desired ground track whilst flying in a moving airmass, the pilot of an aircraft must use knowledge of wind speed, wind direction, and true air speed to determine the required heading. See wind triangle.

TAS is the true measure of aircraft performance in cruise, thus it is the speed listed in aircraft specifications, manuals, performance comparisons, pilot reports, and every situation when cruise or endurance performance needs to be measured. It is the speed normally listed on the flight plan, also used in flight planning, before considering the effects of wind.

Since indicated airspeed is a better indicator of power used and lift available, true airspeed is not used for controlling the aircraft during taxiing, takeoff, climb, descent, approach or landing; for these purposes the Indicated airspeed – IAS or KIAS (knots indicated airspeed) – is used.

Measurement of true airspeed

True airspeed is related to the Mach number and speed of sound by

Both the Mach number and the speed of sound can be computed using measurements of impact pressure, static pressure and outside air temperature.

At sea level in the International Standard Atmosphere (ISA) and at low speeds where air compressibility is negligible (and so a constant air density may be assumed), TAS equals CAS. Above approximately 100 knots (190 km/h), the compressibility error rises significantly.

In flight, it can be calculated using an E6B flight calculator or equivalent.

Since temperature variations are of a smaller influence, the ASI error can be roughly estimated as indicating about 2% less than TAS per 1,000 feet (300 m) of altitude above sea level. For example, an aircraft flying at 15,000 feet (4,600 m) in the international standard atmosphere with an IAS of 100 knots (190 km/h), is actually flying at 126 knots (233 km/h) TAS.

See also


AirbusAeronaveAFCSEstructura de aeronaveAviónBoeing 737Boeing 737 Next GenerationBoeing 787Boeing B-29 SuperfortressBoeing CH-47 ChinookBoeing Insitu ScanEagleCessna O-2 SkymasterCessna 336 / 337 SkymasterEurocopter EC725 Super CougarEurofighter TyphoonAvión de cazaCazabombarderoFlight airspeed recordFlying Scotsman (train)Lockheed Martin F-16 Fighting FalconGrumman F6F HellcatHawker FuryHawker HurricaneHelicópteroAvión de reacciónJet engineLockheed Martin F-22 RaptorLockheed Martin F-35 Lightning IILockheed SR-71McDonnell Douglas F-4 Phantom IIMcDonnell Douglas MD-80Caza polivalenteTwin-boom aircraftTwinjetUSAF ThunderbirdsVelocidad transónicaVelocidad del sonidoMcDonnell XF-85 Goblinde Havilland MosquitoCaza nocturnoBoeing F/A-18 Super HornetAvión embarcadoAvión de ataque a tierraPostcombustiónMikoyan MiG-27Sukhoi Su-27Gloster MeteorNorth American P-51 Mustang variantsAir racingMesserschmitt Bf 109MonocascoAircraft canopyDassault Mirage F1InterceptorMcDonnell Douglas T-45 GoshawkMcDonnell Douglas AV-8B Harrier IIDassault Mirage 2000Eurocopter EC665 TigreHelicóptero de ataqueAirbus HelicoptersGlobo aerostáticoDirigibleGeneral Dynamics F-111 AardvarkInterdictorBombardero estratégicoElectronic-warfare aircraftGeneral Atomics MQ-1 PredatorIndustria armamentísticaAGM-114 HellfireMisilCohete guiado de ataque directoBoeing AH-64 ApacheHelicóptero armadoAircraft ordnanceAdvanced Attack HelicopterFuerza Aérea de los Estados UnidosAviaciónAterrizajePista de aterrizajeAcrobacia aérea

This article uses material from the Wikipedia article "", which is released under the Creative Commons Attribution-Share-Alike License 3.0. There is a list of all authors in Wikipedia

Transportation - Air Water Earth

3D,CAD,Model,Libary,Railway, Train, Ship, Marine, Submarine, Automotive, Locomotive, Bike, Car, Formula 1, Space, Aircraft, Aerospace, Satelite, Automobile, Yacht