powered by CADENAS

Social Share

Amazon

Insert nut (2573 views - Tooling)

An insert nut provides a threaded socket for a wooden workpiece, similar to a wall anchor. Insert nuts are inserted into a pre-drilled hole by one of two means: screw in and hammer in. In both cases, the external protrusions bite into the wood, preventing the nut from either turning or pulling out. Insert nuts are advantageous over barrel nuts and T-nuts, because they can be installed from one side of the workpiece.
Go to Article

Explanation by Hotspot Model

Youtube


    

Insert nut

Insert nut

An insert nut provides a threaded socket for a wooden workpiece, similar to a wall anchor. Insert nuts are inserted into a pre-drilled hole by one of two means: screw in and hammer in. In both cases, the external protrusions bite into the wood, preventing the nut from either turning or pulling out.

Insert nuts are advantageous over barrel nuts and T-nuts, because they can be installed from one side of the workpiece.

Screw-in type

Screw-in insert nuts have an external thread and hex head and are screwed in with a Flat Blade Screwdriver or an Allen wrench. The screw-in insert nuts come in various sizes and take different screw sizes. For example, a "1/4-20" insert nut will take a 1/4-20 inch bolt. The pre-drilled hole must be as deep as the length of the insert nut plus any portion of the bolt that may be screwed past the end of the nut in the work piece.

Hammer-in type

Hammer-in insert nuts, also known as knock-in nuts,[citation needed] are lined with barbs and are hammered in. They are often made of steel, brass or nylon. They are designed to work in wood and particle board.[1]

Notes

  1. ^ Willacy, p. 39.

See also



This article uses material from the Wikipedia article "", which is released under the Creative Commons Attribution-Share-Alike License 3.0. There is a list of all authors in Wikipedia

Tooling

tooling,tool,drill,cam,manufacturing