powered by CADENAS

Social Share

Amazon

Cocktail (12557 views - Food Drinks Beverages)

When used to refer to any generic alcoholic mixed drink, cocktail may mean any beverage that contains three or more ingredients if at least one of those ingredients contains alcohol.
Go to Article

Explanation by Hotspot Model

Cocktail

Cocktail

Cocktail

When used to refer to any generic alcoholic mixed drink, cocktail may mean any beverage that contains three or more ingredients if at least one of those ingredients contains alcohol.

Usage and related terms

A cocktail more specifically may mean a beverage with at least three flavors, one of which is alcohol. More specifically still, it must contain alcohol, a sugar, and a bitter/citrus. When a mixed drink contains only a distilled spirit and a mixer, such as soda or fruit juice, it is a highball; many of the International Bartenders Association Official Cocktails are highballs. When a mixed drink contains only a distilled spirit and a liqueur, it is a duo and when it adds a mixer, it is a trio. Additional ingredients may be sugar, honey, milk, cream, and various herbs.[1]

Etymology

The origin of the word cocktail is disputed. The first recorded use of cocktail not referring to a horse is found in The Morning Post and Gazetteer in London, England, March 20, 1798:[2]

Mr. Pitt,
two petit vers of "L'huile de Venus"
Ditto, one of "perfeit amour"
Ditto, "cock-tail" (vulgarly called ginger)

The Oxford English Dictionary cites the word as originating in the U.S.[3] The first recorded use of cocktail as a beverage (possibly non-alcoholic) in the United States appears in The Farmer's Cabinet, April 28, 1803:[4]

Drank a glass of cocktail—excellent for the head...Call'd at the Doct's. found Burnham—he looked very wise—drank another glass of cocktail.

The first definition of cocktail known to be an alcoholic beverage appeared in The Balance and Columbian Repository (Hudson, New York) May 13, 1806; editor Harry Croswell answered the question, "What is a cocktail?":

Cock-tail is a stimulating liquor, composed of spirits of any kind, sugar, water, and bitters—it is vulgarly called bittered sling, and is supposed to be an excellent electioneering potion, in as much as it renders the heart stout and bold, at the same time that it fuddles the head. It is said, also to be of great use to a democratic candidate: because a person, having swallowed a glass of it, is ready to swallow any thing else.[5]

Etymologist Anatoly Liberman endorses as "highly probable" the theory advanced by Låftman (1946), which Liberman summarizes as follows:[6]

It was customary to dock the tails of horses that were not thoroughbred ... They were called cocktailed horses, later simply cocktails. By extension, the word cocktail was applied to a vulgar, ill-bred person raised above his station, assuming the position of a gentleman but deficient in gentlemanly breeding. ... Of importance [in the 1806 citation above] is ... the mention of water as an ingredient. ... Låftman concluded that cocktail was an acceptable alcoholic drink, but diluted, not a "purebred", a thing "raised above its station". Hence the highly appropriate slang word used earlier about inferior horses and sham gentlemen.

In his book Imbibe! (2007) David Wondrich also speculates that cocktail is a reference to a practice for perking up an old horse by means of a ginger suppository so that the animal would "cock its tail up and be frisky."[7]

Several authors have theorized that cocktail may be a corruption of cock ale.[8][9][10]

Development

There is a lack of clarity on the origins of cocktails.[11] Traditionally cocktails were a mixture of spirits, sugar, water, and bitters.[12] But by the 1860s, a cocktail frequently included a liqueur.[13][12]

The first publication of a bartenders' guide which included cocktail recipes was in 1862 – How to Mix Drinks; or, The Bon Vivant's Companion, by "Professor" Jerry Thomas. In addition to recipes for punches, sours, slings, cobblers, shrubs, toddies, flips, and a variety of other mixed drinks were 10 recipes for "cocktails". A key ingredient differentiating cocktails from other drinks in this compendium was the use of bitters. Mixed drinks popular today that conform to this original meaning of "cocktail" include the Old Fashioned whiskey cocktail, the Sazerac cocktail, and the Manhattan cocktail.

The ingredients listed (spirits, sugar, water, and bitters) match the ingredients of an Old Fashioned,[14] which originated as a term used by late 19th century bar patrons to distinguish cocktails made the "old-fashioned" way from newer, more complex cocktails.[4]

The term highball appears during the 1890s to distinguish a drink composed only of a distilled spirit and a mixer.[15]

The first "cocktail party" ever thrown was allegedly by Mrs. Julius S. Walsh Jr. of St. Louis, Missouri, in May 1917. Mrs. Walsh invited 50 guests to her home at noon on a Sunday. The party lasted an hour, until lunch was served at 1 pm. The site of this first cocktail party still stands. In 1924, the Roman Catholic Archdiocese of St. Louis bought the Walsh mansion at 4510 Lindell Boulevard, and it has served as the local archbishop's residence ever since.[16]

During Prohibition in the United States (1919–1933), when alcoholic beverages were illegal, cocktails were still consumed illegally in establishments known as speakeasies. The quality of liquor available during Prohibition was much worse than previously.[17] There was a shift from whiskey to gin, which does not require aging and is therefore easier to produce illicitly.[18] Honey, fruit juices, and other flavorings served to mask the foul taste of the inferior liquors. Sweet cocktails were easier to drink quickly, an important consideration when the establishment might be raided at any moment.

Cocktails became less popular in the late 1960s and through the 1970s, until resurging in the 1980s with vodka often substituting the original gin in drinks such as the martini. Traditional cocktails began to make a comeback in the 2000s,[19] and by the mid-2000s there was a renaissance of cocktail culture in a style typically referred to as mixology that draws on traditional cocktails for inspiration but utilizes novel ingredients and often complex flavors.[20]

See also



This article uses material from the Wikipedia article "", which is released under the Creative Commons Attribution-Share-Alike License 3.0. There is a list of all authors in Wikipedia

Food Drinks Beverages

food,liquor,alcohol,drink,beverage,coke