powered by CADENAS

Social Share

Pinion (5755 views - Mechanical Engineering)

A pinion is a round gear used in several applications: usually the smaller gear in a gear drive train, although in the first commercially successful steam locomotive (the Salamanca), the pinion was rather large. In many cases, such as remote controlled toys, the pinion is also the drive gear. the smaller gear that drives in a 90-degree angle towards a crown gear in a differential drive. the small front sprocket on a chain driven motorcycle. the round gear that engages and drives a rack in a rack and pinion mechanism and against a rack in a rack railway. in the case of radio-controlled cars with an engine (e.g. nitro) this pinion gear can be referred to as a clutch bell when it is paired with a centrifugal clutch.
Go to Article

Explanation by Hotspot Model

Pinion

Pinion

Pinion

A pinion is a round gear used in several applications:

See also



This article uses material from the Wikipedia article "", which is released under the Creative Commons Attribution-Share-Alike License 3.0. There is a list of all authors in Wikipedia

Mechanical Engineering

AutoCAD, SolidWorks, Autodesk Inventor, FreeCAD, Catia, Siemens NX, PTC Creo, Siemens Solid Edge, Microstation, TurboCAD, Draftsight, IronCAD, Spaceclaim, VariCAD, OnShape, IntelliCAD,T-FLEX, VariCAD, TenadoCAD, ProgeCAD, Cadra, ME10, Medusa, Designspark, KeyCreator, Caddy, GstarCAD, Varimetrix, ASCON Kompas-3D, Free Download, Autocad, 2D Library, DXF, DWG, 2D drawing, 3D digital library, STEP, IGES, 3D CAD Models, 3D files, CAD library, 3D CAD files, BeckerCAD, MegaCAD, Topsolid Missler, Vero VisiCAD, Acis SAT, Cimatron, Cadceus, Solidthinking, Unigraphics, Cadkey, ZWCAD, Alibre, Cocreate, MasterCAM, QCAD.org, QCAD, NanoCAD