powered by CADENAS

Social Share

Condensate pump (5747 views - Transportation - Air Water Earth)

A condensate pump is a specific type of pump used to pump the condensate (water) produced in an HVAC (heating or cooling), refrigeration, condensing boiler furnace, or steam system.
Go to Article

Explanation by Hotspot Model

Condensate pump

Condensate pump

Condensate pump

A condensate pump is a specific type of pump used to pump the condensate (water) produced in an HVAC (heating or cooling), refrigeration, condensing boiler furnace, or steam system.

Applications

Condensate pumps may be used to pump the condensate produced from latent water vapor in any of the following gas mixtures:

  • Conditioned (cooled or heated) building air
  • Refrigerated air in cooling and freezing systems
  • Steam in heat exchangers and radiators
  • The exhaust stream of very-high-efficiency furnaces

Condensate recovery systems help reduce three tangible costs of producing steam:

  • Fuel/energy costs
  • Boiler water make-up and sewage treatment
  • Boiler water chemical treatment

Construction and operation

Condensate pumps as used in hydronic systems are usually electrically powered centrifugal pumps. As used in homes and individual heat exchangers, they are often small and rated at a fraction of a horsepower, but in commercial applications they range in size up to many horsepower and the electric motor is usually separated from the pump body by some form of mechanical coupling. Large industrial pumps may also serve as the feedwater pump for returning the condensate under pressure to a boiler.

Condensate pumps usually run intermittently and have a tank in which condensate can accumulate. Eventually, the accumulating liquid raises a float switch energizing the pump. The pump then runs until the level of liquid in the tank is substantially lowered. Some pumps contain a two-stage switch. As liquid rises to the trigger point of the first stage, the pump is activated. If the liquid continues to rise (perhaps because the pump has failed or its discharge is blocked), the second stage will be triggered. This stage may switch off the HVAC equipment (preventing the production of further condensate), trigger an alarm, or both.

Some systems may include two pumps to service the tank. In this case, the two pumps often alternate operation, and a two-stage switch serves to energize the on-duty pump at the first stage and then energize the remaining pump at the second stage. This second stage action is in addition to any triggering of other system changes as noted for a single pump installation. In this way pump runtime is shared between the two, and a backup pump is provided in case one pump fails to function as designed.

Small pumps have tanks that range from 2 to 4 liters (0.5 to 1 gallon) and are usually supported using the flanges on their tanks or simply placed upon the floor. A plastic impeller in a molded volute at the bottom of the pump provides the pumping action; this impeller is connected to the motor via a metal shaft that extends downwards from the motor mounted above the tank's top. Large pumps are usually pad-mounted drawing liquid from a tank (sump) below the floor. The smallest pumps may have no tank at all and are simply placed within a container such as the drip pan of a dehumidifier appliance.

Steam condensate

In industrial steam systems the condensate pump is used to collect and return condensate from remote areas of the plant. The steam produced in the boiler can heat equipment and processes a considerable distance away. Once steam is used it turns to hot water or condensate. This pump and possibly many more around the plant returns this hot water back to a make-up tank closer to the boiler, where it can be reclaimed, chemically treated, and reused, in the boiler, consequently it can sometimes be referred to as a condensate return pump.

In a steam power plant, particularly shipboard ones, the condensate pump is normally located adjacent to the main condenser hotwell often directly below it. This pump sends the water to a make-up tank closer to the steam generator or boiler. If the tank is also designed to remove dissolved oxygen from the condensate, it is known as a deaereating feed tank (DFT). The output of the DFT supplies the feed booster pump which, in turn, supplies the feedwater pump which returns the feedwater to the boiler so the cycle can start over. Two pumps in succession are used to provide sufficient net positive suction head to prevent cavitation and the subsequent damage associated with it.

This pump is usually associated with a much larger tank, float switch, and an electric motor than the example above. Some systems are so remote that steam power is used to return the condensate where electricity is impractical to provide.

Disposal

The output of small condensate pumps is usually routed to a sewer, plumbing drain, or the outside world via PVCl plastic tubing (condensate drain line).

If the outlet of the line is at a higher level than the tank of the pump, a check valve is often fitted at the outlet of the pump so that liquid cannot flow backwards into the pump's tank. If the outlet is below the tank level, siphonage usually naturally clears the output line of all liquid when the pump is deenergized. In cold regions of the world, it is important that condensate lines that are exhausted outside be carefully designed so that no water can remain in the line to freeze up; this would block the line from further operation.

Condensate is not pure water. If it is being condensed from an air stream, it may have dust, microbes, or other contaminants in it. If it is condensed from steam, it may have traces of the various boiler water treatment chemicals. And if it is condensed from furnace exhaust gases, it may be acidic, containing sulfuric acid or nitric acid as a result of sulfur and nitrogen dioxides in the exhaust gas stream. Steam and exhaust condensate is usually hot. These various factors may combine (along with local regulations) to require careful handling or even chemical treatment of the condensate, and condensate pumps used for these services must be appropriately designed.

See also



This article uses material from the Wikipedia article "", which is released under the Creative Commons Attribution-Share-Alike License 3.0. There is a list of all authors in Wikipedia

Transportation - Air Water Earth

3D,CAD,Model,Libary,Railway, Train, Ship, Marine, Submarine, Automotive, Locomotive, Bike, Car, Formula 1, Space, Aircraft, Aerospace, Satelite, Automobile, Yacht