Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
The following is a list of fictional starships, cruisers, battleships, and other spacecraft in the Star Wars films, books, and video games.
The Azure Angel II was a modified Jedi Delta-7 Aethersprite-class light interceptor piloted by Anakin Skywalker during the Clone Wars.
CR90 corvettes, were consular vessels manufactured by the Corellian Engineering Corporation. While the CR90 would see initial use within the late Galactic Republic and Imperial Senate, many vessels would be appropriated by the early rebellion and the Rebel Alliance against the First Galactic Empire, despite not being designed as combat-oriented blockade runners or fast attack crafts.
The Death Star is the Empire's mobile space station which can destroy planets. It appears throughout the Star Wars franchise.
The Ebon Hawk is Darth Revan's ship in Star Wars: The Old Republic: Revan, Star Wars: Knights of the Old Republic, and Star Wars: Knights of the Old Republic II: The Sith Lords. It is designed to be reminiscent of the Millennium Falcon.[1]
A Gauntlet Fighter, or Kom'rk class fighter, is a Mandalorian class of ship. Larger than most starfighters, it can carry a larger crew and accommodate passengers. They were introduced in Star Wars: The Clone Wars, with one known as the Nightbrother later serving as Darth Maul's personal craft in Star Wars: Rebels.
Count Dooku (Christopher Lee) reaches Coruscant aboard a Geonosian Solar Sailer in Star Wars: Episode II – Attack of the Clones. The ship's solar sail was originally part of the concept for the Naboo royal starship in Star Wars: Episode I – The Phantom Menace.[2] The insectoid ship resembles both a beetle and a butterfly.[2] Its forward cockpit bubble was added when it was determined there was a need for a shot of Dooku sitting next to his pilot. It is somewhat similar to the private Antonov An-2 plane in real life.[2]
The Ghost is a modified VCX-100 light freighter, manufactured by the Corellian Engineering Corporation. Owned and piloted by the gifted Twi'lek, Hera Syndulla, it serves as "home base" for a small band of Lothal rebels during the Age of the Empire. Named for its ability to travel past Imperial sensors without detection on numerous missions and skirmishes, the craft included many hidden surprises that aided the crew in their fight against the Empire. Among its many features were a 360-degree dorsal laser cannon turret, two forward laser cannons, and two rear laser cannons, as well as sleeping quarters. It also included the Phantom II, an auxiliary shuttle that doubled as a fully armed starfighter.[3]
The Ghost makes a cameo appearance in Rogue One during the Battle of Scarif. Its captain, Hera Syndulla, is briefly mentioned in the film, and its repair droid, Chopper, makes a brief appearance on Yavin IV in the film.[4]
Imperial landing craft were inserted into the Special Edition release of Star Wars Episode IV: A New Hope. The all-CGI ships were initially designed as part of the Star Wars: Shadows of the Empire multimedia campaign.[5]
Lambda-class Shuttles first appeared in Return of the Jedi, and were later added to the Special Edition release of The Empire Strikes Back. Joe Johnston, Ralph McQuarrie, and Nilo Rodis-Jamero borrowed elements from the skyhopper designed for A New Hope when refining the shuttle's appearance.[6] Earlier versions were boxy, boat-like, or had TIE fighter-like components.[6] Industrial Light and Magic's modelmakers made two shooting models, although CGI versions were used for the craft's Special Edition appearance in The Empire Strikes Back.[6] The Theta-class shuttle in Revenge of the Sith was designed to appear like a predecessor to the Lambda class.[7] A Lambda-class shuttle makes a cameo appearance during the docking sequence of Inara Serra's shuttle in "Serenity", the pilot episode of Joss Whedon's Firefly.[8]
The Millennium Falcon is a highly modified YT-1300 light freighter. It is captained by smuggler Han Solo (Harrison Ford) and his Wookiee first mate, Chewbacca (Peter Mayhew).
A modified Corellian HWK-290 used by Kyle Katarn and Jan Ors in the Star Wars: Dark Forces and Star Wars: Dark Forces II: Jedi Knight video games.[9]
A Naboo Royal Cruiser is destroyed in a failed attempt to assassinate Padmé Amidala (Natalie Portman) at the beginning of Attack of the Clones. The ship's design was inspired by the B-2 Spirit stealth bomber.[10]
Padmé Amidala escapes from and returns to Naboo aboard a Naboo royal starship in The Phantom Menace. An early design depicted the ship powered by a solar sail; when Lucas called for a sleeker look, designer Doug Chiang drew inspiration from 1950s hood ornaments.[11]
Padmé Amidala travels to Mustafar aboard a Naboo star skiff in Star Wars: Episode III – Revenge of the Sith. Design Ryan Church sketched the ship to appear "supercharged".[12] Only the ship's boarding ramp was built full scale; some footage was altered from material used in Attack of the Clones.[12] The ship is designed to be reminiscent of the "rocket ships" seen in pulp science-fiction.[13]
Luke Skywalker (Mark Hamill) receives a prosthetic hand aboard the medical frigate Redemption at the conclusion of The Empire Strikes Back.[14] A Nebulon-B medical frigate is part of the Rebel Alliance fleet at the Battle of Endor in Return of the Jedi. Expanded Universe material states that relatively affordable Nebulon-B frigates, which are effective at engaging starfighters, are used by both the Rebellion and the Galactic Empire.[14] The frigates appear in several LucasArts titles, including the X-Wing flight simulators series, Empire at War real-time strategy game, and Star Wars: Battlefront, as well as episodes 'Zero Hour' and 'Secret Cargo' of Star Wars Rebels.
Industrial Light & Magic's Nilo Rodis-Jamero and Joe Johnston created the frigate late during work on The Empire Strikes Back, with the design following a suggestion by George Lucas that it be based on an outboard motor.[15] The model was produced in a short time with limited financial access; it was primarily built from components left over from previous kitbashing exercises, including battleship hulls and artillery pieces.[15] The resulting model was 247 centimetres (97 in) long, 99 centimetres (39 in) tall, and included a "window" where a still from the scene in the medical bay could be inserted for filming.[15][16]
Following the completion of filming, Lucas decided to revisit the end of the movie to better establish the characters' final locations, requiring a section of the frigate to be built that corresponded to the scale of the 2-foot (0.61 m) Millennium Falcon model.[15] The model was originally referred to as the Rebel starcruiser or Rebel cruiser, but during filming of Return of the Jedi, it was renamed Rebel Medical Frigate after the cruiser name was used for the Mon Calamari cruisers.[15][16]
Neimoidian shuttles appear throughout the prequel trilogy and Star Wars: The Clone Wars. Their design is based on a Trade Federation landing ship, turned vertically and altered to be more insectoid and less symmaetrical. They are also used by the other CIS leaders, such as Nuvo Vindi and Wat Tambor.[17]
The Outrider was digitally inserted into the Special Edition of A New Hope.[18]
Within Star Wars Legends, The Outrider is Dash Rendar's CEC YT-2400 class freighter in the Shadows of the Empire multimedia campaign. It is a playable ship in the Shadows of the Empire video game, and Kenner released an Outrider toy.[18] While Steve Perry outlined the ship's story and role, Doug Chiang designed the ship itself.[18]
A YT-2400 light freighter also appeared within the Star Wars Rebels Season 3 episode Iron Squadron. It was piloted by Mart Mattin, who was a nephew of Rebel Commander, Jun Sato.[19] It is unknown if the ship is meant to be same as the one in A New Hope. According to Gary Whitta, who served as writer of Rogue One, Dash Rendar is a controversial character among Lucasfilm Story Group, which decreases the chances of the character becoming part of Canon.[20]
The Radiant VII is the first vessel shown in The Phantom Menace. Jedi knights Qui-Gon Jinn (Liam Neeson) and Obi-Wan Kenobi (Ewan McGregor) travel aboard the Radiant VII on their mission to end the Trade Federation's blockade of the planet Naboo. After docking with the Federation's Droid Control Ship, the Radiant VII is destroyed to prevent the Jedi from escaping.[21] Originally, the Radiant VII was going to be sleek like most Old Republic ships depicted in the Star Wars prequel trilogy. However, Lucas suggested a design similar to the ships in the original trilogy; Doug Chiang and the Lucasfilm art department responded with a design similar to the Tantive IV model created for Star Wars Episode IV: A New Hope. Several antennae were added to focus attention to the cockpit during the opening sequence of The Phantom Menace.[22]
A ship used by Kyle Katarn and Jan Ors in Star Wars Jedi Knight II: Jedi Outcast after Kyle's first ship, the Moldy Crow, was destroyed.
Corellian CR90 and CR70 corvettes, often identified as "the Rebel blockade runners", such as Leia Organa's Tantive IV and Bail Organa's Sunderhead Heart, are small starships, usually used by Alderaanian people.
Republic assault ships of the Acclamator-class appear in Attack of the Clones. These ships, originally called "Jedi troop transports", demonstrate a connection to the original trilogy's star destroyers through their triangular hulls.[23]
Republic attack cruisers, also known as Venator-class star destroyers, or the most known term Jedi Cruisers, appear throughout the Star Wars franchise.
Consular-class Republic Cruisers like the Radiant VII are "instantly recognizable throughout the galaxy".[21] Republic cruisers are generally unarmed and feature a red color scheme as a symbol of neutrality and "diplomatic immunity".[24]
The ship used by Starkiller and Juno Eclipse in Star Wars: The Force Unleashed. It was first used by Starkiller to hunt down and kill any surviving Jedi Knights who somehow lived through "Order 66", but it soon after became a part of the Rebel Fleet around 0 BBY after Starkiller was betrayed by his master, "Darth Vader", and became a Jedi Padawan to Rahm Kota.
Darth Maul (Ray Park) pilots a Sith infiltrator, named Scimitar, in The Phantom Menace. Its design includes elements of the TIE interceptor and Lambda-class shuttle.[25] The vehicle has been made into toys by Hasbro and Galoob and models kits by Lego[26] and Ertl.
Slave I is the starship used by bounty hunter Boba Fett (Jeremy Bulloch) in The Empire Strikes Back and by his father Jango Fett (Temuera Morrison) in Attack of the Clones. The ship's design is said to resemble the shape of a street lamp.[27] However, the actual inspiration for the shape of the ship was a radar dish, according to Nilo Rodis-Jamero, the assistant art director and visual effects creator on The Empire Strikes Back. Rodis-Jamero created the initial design after seeing Joe Johnston's ideas for Boba Fett, and states that "the original design I had was round, but when you looked at it from the side, it became elliptical...George [Lucas] thought it was elliptical, so that's what it became." He goes on to say that "[w]hen building the ship at ILM, someone looked at the street lamps and pointed out that they looked like Boba's ship. So everyone began to think that was where I got the idea for the design."[28] Its appearance in the original release of The Empire Strikes Back was realized by a combination of matte paintings and a 69-centimeter (27 in) model.[29]
The Star Destroyers are the Galactic Empire's assault ships. Much like the Republic assault ships, the two have similar hulls, bridges, engines, and many other parts. They appear in a variety of forms throughout the Star Wars franchise.
Padmé Amidala and Anakin Skywalker travel to Naboo aboard a starfreighter in Attack of the Clones. The transport's design is partly based on an ocean liner.[30]
The Corellian corvette Tantive IV is the first ship to appear in Star Wars. It is used by Princess Leia (Carrie Fisher) in A New Hope, and a similar vehicle (the Sundered Heart) is used by her adoptive father, Bail Organa (Jimmy Smits), in Revenge of the Sith.
The Techno Union Starship is a capital ship used by both the Techno Union and the Intergalactic Banking Clan. It first appeared during the Battle of Geonosis (in Star Wars: Episode II – Attack of the Clones) where many of its kind had their fuel-cells taken out by Republic LAAT gunships, thus preventing them from escaping. Before the Battle of Geonosis, there were 286 of the starships on Geonosis, but only 169 escaped to space. It was designated as a "Hardcell-class transport starship", was 220 metres long, and was shaped like a rocket. It was used to deploy hailfire droids and later the Intergalactic Banking Clan's own battle droids, the IG lancers. The ship had a conical nose housing quarters for the organic crew, command decks and medical decks. It had six primary thruster units around its base that were capable of providing a fast take-off speed of 4,000 km/h.
Emperor Palpatine (Ian McDiarmid) travels aboard a Theta-class shuttle in Revenge of the Sith. The ship was designed to appear like a predecessor to the Lambda-class shuttle.[7] Only the shuttle's boarding ramp was built for filming.[7]
Trade Federation Lucrehulk-class battleships (or their enormous Lucrehulk-class LH-3210 cargo freighter alter-egos) appear in all three of the prequel films. Lucas called for these ships to have a "saucer" look with a distinct front and rear, achieved by placing the engines on one side of the ship and the antennae and docking bays on the other.[31]
The most famous Lucrehulk-class ship is the Trade Federation flagship cargo freighter Saak'ak.
General Grievous's flagship in Revenge of the Sith is the Trade Federation Cruiser Invisible Hand.[32] The raised spire helped differentiate the command ship from the other capital ships over Coruscant and to help map out the ship's various locations. More sets aboard the ship were built than seen in the film; several "serial-type escapades" were cut from the final release. Other sets, built inside a mount that could rotate them, were used to depict the vessel's collapse.[33]
Trade Federation Landing Ships transport the Trade Federation's invasion forces to Naboo's surface in The Phantom Menace. Although initial designs were reminiscent of dirigibles, the final design is based on a dragonfly.[34] Lucas liked the ship's similarity to a biplane.[34]
The Virago is Xizor's ship in Shadows of the Empire. Its clamshell design, styled after a stealth fighter, is inspired by pulley castings.[35]
The TIE Fighter is one of the most commonly used spacecraft in the galaxy. It is one of the many ships the Empire uses.
The YT-1300 Corellian light freighter, was a type of light freighter manufactured by the Corellian Engineering Corporation that saw commercial operation in the galaxy during the final days of the Galactic Republic and the reign of the Galactic Empire.[5] The Millennium Falcon, a smuggling vessel that became part of the Rebel Alliance fleet, was a YT-1300 of the YT-1300f-variety.
This article uses material from the Wikipedia article "", which is released under the Creative Commons Attribution-Share-Alike License 3.0. There is a list of all authors in Wikipedia
Movie, Animation, Cartoon