powered by CADENAS

Social Share

Ferromolybdenum (9900 views - Material Database)

Ferro molybdenum is an important iron-molybdenum alloy, with a molybdenum content of 60-75% It is the main source for molybdenum alloying of HSLA steel.
Go to Article

Ferromolybdenum

Ferromolybdenum

Ferro molybdenum is an important iron-molybdenum alloy, with a molybdenum content of 60-75%[1] It is the main source for molybdenum alloying of HSLA steel.

Production

The alloy is produced by heating a mixture of molybdenum(VI) oxide MoO3, aluminium, and iron.[2] The oxide and the aluminium combine via an aluminothermic reaction to give molybdenum in situ. The ferromolybdenum can be purified by electron beam melting or used as it is. For alloying with steel the ferromolybdenum is added to molten steel before casting. Among the biggest suppliers of ferromolybdenum in Europe are the English trading house Derek Raphael and Co Ltd and the German trading house Grondmet in Düsseldorf, Germany. A large ferromolybdenum producer in the US is Langeloth Metallurgical Company in Langeloth, Pennsylvania.[3]

  1. ^ C. K. Gupta (1992). Extractive Metallurgy of Molybdenum. CRC Press. ISBN 978-0-8493-4758-0. Retrieved 2008-11-03. 
  2. ^ Rudolf Fichte (2005), "Ferroalloys", Ullmann's Encyclopedia of Industrial Chemistry, Weinheim: Wiley-VCH, doi:10.1002/14356007.a10_305 
  3. ^ http://www.langeloth.com/

AlGaAlnicoAluminioAleaciones de aluminioBronce de aluminioAluminium-lithium alloyArsenical bronzeArsenical copperMetal de campanaBerilioBeryllium copperVellón (aleación)BirmabrightBismanolBismutoLatónBronceCalamine brassChinese silverCromoChromium hydrideCobaltoColored goldConstantánCobreCopper hydrideCopper–tungstenCorinthian bronzeCrown goldCunifeCuproníquelCymbal alloysDevarda's alloyDuraluminioDutch metalElectro (aleación)ElinvarFernicoFerroalloyFerrocerioFerrocromoFerromanganeseMetal de FieldFlorentine bronzeGalfenolGalinstanoGalioGilding metalVidrioGlucydurOroGuanín (bronze)GunmetalHepatizonHiduminiumHydronaliumIndio (elemento)HierroItalmaPlomoMagnalioMagnesioManganinaMegalliumMelchior (alloy)MercuryMolybdochalkosMetal MuntzNicromoNíquelAlpaca (aleación)Oro nórdicoOrmoluPhosphor bronzePinchbeck (alloy)PlásticoPlexiglasPlutonioPotasioRhoditaRodioMetal de RoseSamarioEscandioShakudōPlataSodioMetal de espejosAcero inoxidableAceroEsteliteAcero laminadoEstañoTitanioTombacTumbagaUranioVitalioMetal de WoodY alloyZincCirconioFerrosiliconFerrotitaniumFerrouraniumInvarFundición de hierroIron–hydrogen alloyArrabioKanthalKovarStaballoySpiegeleisenAcero bulatAcero de crisolAcero 41xxAcero de DamascoMangalloyAcero rápidoMushet steelMaraging steelAcero microaleadoReynolds 531Acero eléctricoAcero elásticoAL-6XNCelestriumAlloy 20Marine grade stainlessAcero inoxidable martensíticoSanicro 28Acero quirúrgicoZeron 100Silver steelAcero para herramientasAcero cortenAcero wootzSolderTerneType metalElektron (alloy)Amalgama (química)Magnox (alloy)AlumelBrightrayCromelHaynes InternationalInconelMonelNicrosilNisilNitinolMu-metalPermalloySupermalloyNickel hydridePlutonium–gallium alloyNaKMetal de MischLitioTerfenol-DPseudo palladiumScandium hydrideImán de samario-cobaltoArgentium sterling silverPlata de BritaniaDoré bullionGoloidPlatinum sterlingShibuichiSterling silverTibetan silverTitanium Beta CTitanium alloyTitanium hydrideGum metalTitanium goldNitruro de titanioBabbitt (metal)Metal de BritaniaPeltreQueen's metalWhite metalUranium hydrideZamakZirconium hydrideHidrógenoHelioBoroNitrógenoOxígenoFlúorMetanoEntresueloÁtomo

This article uses material from the Wikipedia article "", which is released under the Creative Commons Attribution-Share-Alike License 3.0. There is a list of all authors in Wikipedia

Material Database

database,rohs,reach,compliancy,directory,listing,information,substance,material,restrictions,data sheet,specification