Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
Licensed under GNU General Public License (The original uploader was SilentC at English Wikipedia).
This article does not cite any sources. Please help improve this article by adding citations to reliable sources. Unsourced material may be challenged and removed. (December 2009) (Learn how and when to remove this template message) |
A sharpening jig is often used when sharpening woodworking tools. Many of the tools used in woodworking have steel blades which are sharpened to a fine edge. A cutting edge is created on the blade at the point at which two surfaces of the blade meet. To create this cutting edge a bevel is formed on the blade, usually by grinding. This bevel is subsequently refined by honing until a satisfactorily sharp edge is created.
The purpose of the sharpening jig is to hold the blade or tool at the desired angle while grinding or honing the bevel. In some cases, the angle of the bevel is critical to the performance of the cutting edge—a jig allows for repeatability of this angle over a number of sharpening sessions.
There are many styles of jig available commercially. Fundamentally, all jigs are similar in that they allow the user to clamp the blade or tool in some way. The jig then has some means of referencing the clamped blade to the grinding or honing apparatus so that the bevel angle is maintained. One of the more common approaches is to have the jig ride on a roller. These types of jigs are usually used with a sharpening stone or plate, such as a waterstone, oilstone or diamond abrasive surface. Other types of jigs are used to present the blade to the wheel of a grinder. There are generally two types of hand sharpening jigs, push jigs and side to side jigs. Push jigs run perpendicular to the length of the stone and a side to side jig runs with the blade parallel to the length of the stone.
Many woodworkers prefer to learn the technique of sharpening by hand. This method does not require a jig, but requires a lot of practice to achieve satisfactory results - especially in situations where the bevel angle is critical.
This article uses material from the Wikipedia article "", which is released under the Creative Commons Attribution-Share-Alike License 3.0. There is a list of all authors in Wikipedia
AutoCAD, SolidWorks, Autodesk Inventor, FreeCAD, Catia, Siemens NX, PTC Creo, Siemens Solid Edge, Microstation, TurboCAD, Draftsight, IronCAD, Spaceclaim, VariCAD, OnShape, IntelliCAD,T-FLEX, VariCAD, TenadoCAD, ProgeCAD, Cadra, ME10, Medusa, Designspark, KeyCreator, Caddy, GstarCAD, Varimetrix, ASCON Kompas-3D, Free Download, Autocad, 2D Library, DXF, DWG, 2D drawing, 3D digital library, STEP, IGES, 3D CAD Models, 3D files, CAD library, 3D CAD files, BeckerCAD, MegaCAD, Topsolid Missler, Vero VisiCAD, Acis SAT, Cimatron, Cadceus, Solidthinking, Unigraphics, Cadkey, ZWCAD, Alibre, Cocreate, MasterCAM, QCAD.org, QCAD, NanoCAD