powered by CADENAS

Social Share

Villa (7416 views - Architecure & BIM & MEP)

A villa was originally an ancient Roman upper-class country house. Since its origins in the Roman villa, the idea and function of a villa have evolved considerably. After the fall of the Roman Republic, villas became small farming compounds, which were increasingly fortified in Late Antiquity, sometimes transferred to the Church for reuse as a monastery. Then they gradually re-evolved through the Middle Ages into elegant upper-class country homes. In modern parlance, 'villa' can refer to various types and sizes of residences, ranging from the suburban "semi-detached" double villa to residences in the wildland–urban interface.
Go to Article

Explanation by Hotspot Model

Villa

Villa

A villa was originally an ancient Roman upper-class country house. Since its origins in the Roman villa, the idea and function of a villa have evolved considerably. After the fall of the Roman Republic, villas became small farming compounds, which were increasingly fortified in Late Antiquity, sometimes transferred to the Church for reuse as a monastery. Then they gradually re-evolved through the Middle Ages into elegant upper-class country homes. In modern parlance, 'villa' can refer to various types and sizes of residences, ranging from the suburban "semi-detached" double villa to residences in the wildland–urban interface.

Roman

In ancient Roman architecture a villa was originally a country house built for the élite. Pliny the Elder, writing in the first century CE, identified several kinds of villas:

  • the villa urbana, a country seat that could easily be reached from Rome or another city for a night or two
  • the villa rustica, the farm-house estate that was permanently occupied by the servants who had charge generally of the estate, which would centre on the villa itself, perhaps only seasonally occupied. The Roman villae rusticae at the heart of latifundia were the earliest versions of what later and elsewhere became called plantations.

Not included as villae were the domus, a city house for the élite and privileged classes; and insulae, blocks of apartment buildings for the rest of the population. In Satyricon (1st century CE), Petronius described the wide range of Roman dwellings. Another type of villae is the "villa marittima", a seaside villa, located on the coast.

A concentration of Imperial villas existed on the Gulf of Naples, on the Isle of Capri, at Monte Circeo and at Antium (Anzio). Examples include the Villa of the Papyri in Herculaneum; and the "Villa of the Mysteries" and "Villa of the Vettii" in Pompeii.

Wealthy Romans also escaped the summer heat in the hills round Rome, especially around Tibur (Tivoand Frascati, such as at Hadrian's Villa. Cicero allegedly possessed no fewer than seven villas, the oldest of which was near Arpinum, which he inherited. Pliny the Younger had three or four, of which the example near Laurentium is the best known from his descriptions.

Roman writers refer with satisfaction to the self-sufficiency of their latifundium villas, where they drank their own wine and pressed their own oil. This was an affectation of urban aristocrats playing at being old-fashioned virtuous Roman farmers, it has been said that the economic independence of later rural villas was a symptom of the increasing economic fragmentation of the Roman Empire.

In Roman Britannia

Archaeologists have meticulously examined numerous Roman villas in England.[1] Like their Italian counterparts, they were complete working agrarian societies of fields and vineyards, perhaps even tileworks or quarries, ranged round a high-status power centre with its baths and gardens. The grand villa at Woodchester preserved its mosaic floors when the Anglo-Saxon parish church was built (not by chance) upon its site. Grave-diggers preparing for burials in the churchyard as late as the 18th century had to punch through the intact mosaic floors. The even more palatial villa rustica at Fishbourne near Winchester was built (uncharacteristically) as a large open rectangle, with porticos enclosing gardens entered through a portico. Towards the end of the 3rd century, Roman towns in Britain ceased to expand: like patricians near the centre of the empire, Roman Britons withdrew from the cities to their villas, which entered on a palatial building phase, a "golden age" of villa life. Villae rusticae are essential in the Empire's economy.

Model of Fishbourne Roman Palace, a governor's villa on the grandest scale

Two kinds of villa-plan in Roman Britain may be characteristic of Roman villas in general. The more usual plan extended wings of rooms all opening onto a linking portico, which might be extended at right angles, even to enclose a courtyard. The other kind featured an aisled central hall like a basilica, suggesting the villa owner's magisterial role. The villa buildings were often independent structures linked by their enclosed courtyards. Timber-framed construction, carefully fitted with mortises and tenons and dowelled together, set on stone footings, were the rule, replaced by stone buildings for the important ceremonial rooms. Traces of window glass have been found, as well as ironwork window grilles.

Monastery villas of Late Antiquity

With the decline and collapse of the Western Roman Empire in the fourth and fifth centuries, the villas were more and more isolated and came to be protected by walls. In England the villas were abandoned, looted, and burned by Anglo-Saxon invaders in the fifth century. But the concept of an isolated, self-sufficient agrarian working community, housed close together, survived into Anglo-Saxon culture as the vill, with its inhabitants - if formally bound to the land - as villeins.

In regions on the Continent, aristocrats and territorial magnates donated large working villas and overgrown abandoned ones to individual monks; these might become the nuclei of monasteries. In this way, the Italian villa system of late Antiquity survived into the early Medieval period in the form of monasteries that withstood the disruptions of the Gothic War (535–554) and the Lombards. About 529 Benedict of Nursia established his influential monastery of Monte Cassino in the ruins of a villa at Subiaco that had belonged to Nero.

From the sixth to the eighth century, Gallo-Roman villas in the Merovingian royal fisc were repeatedly donated as sites for monasteries under royal patronage in Gaul - Saint-Maur-des-Fossés and Fleury Abbey provide examples. In Germany a famous example is Echternach; as late as 698, Willibrord established an abbey at a Roman villa of Echternach near Trier, presented to him by Irmina, daughter of Dagobert II, king of the Franks. Kintzheim was Villa Regis, the "villa of the king". Around 590, Saint Eligius was born in a highly placed Gallo-Roman family at the 'villa' of Chaptelat near Limoges, in Aquitaine (now France). The abbey at Stavelot was founded ca 650 on the domain of a former villa near Liège and the abbey of Vézelay had a similar founding.

Post-Roman era

In post-Roman times a villa referred to a self-sufficient, usually fortified Italian or Gallo-Roman farmstead. It was economically as self-sufficient as a village and its inhabitants, who might be legally tied to it as serfs were villeins. The Merovingian Franks inherited the concept, followed by the Carolingian French but the later French term was basti or bastide.

Villa/Vila (or its cognates) is part of many Spanish and Portuguese placenames, like Vila Real and Villadiego: a villa/vila is a town with a charter (fuero or foral) of lesser importance than a ciudad/cidade ("city"). When it is associated with a personal name, villa was probably used in the original sense of a country estate rather than a chartered town. Later evolution has made the Hispanic distinction between villas and ciudades a purely honorific one. Madrid is the Villa y Corte, the villa considered to be separate from the formerly mobile royal court, but the much smaller Ciudad Real was declared ciudad by the Spanish crown.

Italian Renaissance

Tuscany

In 14th and 15th century Italy, a villa once more connoted a country house, like the first Medici villas, the Villa del Trebbio and that at Cafaggiolo, both strong fortified houses built in the 14th century in the Mugello region near Florence. In 1450 Giovanni de' Medici commenced on a hillside the Villa Medici in Fiesole, Tuscany, probably the first villa created under the instructions of Leon Battista Alberti, who theorized the features of the new idea of villa in his De Re Aedificatoria.

These first examples of Renaissance villa predate the age of Lorenzo de' Medici, who added the Villa di Poggio a Caiano by Giuliano da Sangallo, begun in 1470, in Poggio a Caiano, Province of Prato, Tuscany.

From Tuscany the idea of villa was spread again through Renaissance Italy and Europe.

Tuscan villa gardens

The Quattrocento villa gardens were treated as a fundamental and aesthetic link between a residential building and the outdoors, with views over a humanized agricultural landscape, at that time the only desirable aspect of nature. Later villas and gardens include the Palazzo Pitti and Boboli Gardens, Florence; the Villa di Pratolino, Province of Siena.

Rome

Rome had more than its share of villas with easy reach of the small sixteenth-century city: the progenitor, the first villa suburbana built since Antiquity, was the Belvedere or palazzetto, designed by Antonio Pollaiuolo and built on the slope above the Vatican Palace.

The Villa Madama, the design of which, attributed to Raphael and carried out by Giulio Romano in 1520, was one of the most influential private houses ever built; elements derived from Villa Madama appeared in villas through the 19th century. Villa Albani was built near the Porta Salaria. Other are the Villa Borghese; the Villa Doria Pamphili (1650); the Villa Giulia of Pope Julius III (1550), designed by Vignola. The Roman villas Villa Ludovisi and Villa Montalto, were destroyed during the late nineteenth century in the wake of the real estate bubble that took place in Rome after the seat of government of a united Italy was established at Rome.

The cool hills of Frascati gained the Villa Aldobrandini (1592); the Villa Falconieri and the Villa Mondragone. The Villa d'Este near Tivoli is famous for the water play in its terraced gardens. The Villa Medici was on the edge of Rome, on the Pincian Hill, when it was built in 1540. Besides these designed for seasonal pleasure, usually located within easy distance of a city, other Italian villas were remade from a rocca or castello, as the family seat of power, such as Villa Caprarola for the Farnese.

Near Siena in Tuscany, the Villa Cetinale was built by Cardinal Flavio Chigi. He employed Carlo Fontana, pupil of Gian Lorenzo Bernini to transform the villa and dramatic gardens in a Roman Baroque style by 1680. The Villa Lante garden is one of the most sublime creations of the Italian villa in the landscape, completed in the 17th century.

Venice

In the later 16th century in the northeastern Italian Peninsula the Palladian villas of the Veneto, designed by Andrea Palladio (1508–1580), were built in Vicenza in the Republic of Venice. Palladio always designed his villas with reference to their setting. He often unified all the farm buildings into the architecture of his extended villas. Examples are the Villa Emo, the Villa Godi, the Villa Forni Cerato, the Villa Capra "La Rotonda", and Villa Foscari.

The Villas are grouped into an association (Associazione Ville Venete) and offer touristic itineraries and accommodation possibilities.

Villas abroad

17th century

Soon after in Greenwich England, following his 1613–1615 Grand Tour, Inigo Jones designed and built the Queen's House between 1615–1617 in an early Palladian architecture style adaptation in another country. The Palladian villa style renewed its influence in different countries and eras and remained influential for over four hundred years, with the Neo-Palladian a part of the late 17th century and on Renaissance Revival architecture period.

18th and 19th centuries

In the early 18th century the English took up the term, and applied it to compact houses in the country,[2] especially those accessible from London: Chiswick House is an example of such a "party villa". Thanks to the revival of interest in Palladio and Inigo Jones, soon Neo-Palladian villas dotted the valley of the River Thames and English countryside. Marble Hill House in England was conceived originally as a "villa" in the 18th-century sense.[3]

In many ways the late 18th century Monticello, by Thomas Jefferson in Virginia, United States is a Palladian Revival villa. Other examples of the period and style are Hammond-Harwood House in Annapolis, Maryland; and many pre-American Civil War or Antebellum Plantations, such as Westover Plantation and many other James River plantations as well dozens of Antebellum era plantations in the rest of the Old South functioned as the Roman Latifundium villas had. A later revival, in the Gilded Age and early 20th century, produced The Breakers in Newport, Rhode Island, Filoli in Woodside, California, and Dumbarton Oaks in Georgetown, Washington, D.C.; by architects-landscape architects such as Richard Morris Hunt, Willis Polk, and Beatrix Farrand.

In the nineteenth century, villa was extended to describe any large suburban house that was free-standing in a landscaped plot of ground. By the time 'semi-detached villas' were being erected at the turn of the twentieth century, the term collapsed under its extension and overuse.

The second half of the nineteenth century saw the creation of large "Villenkolonien" in the German speaking countries, wealthy residential areas that were completely made up of large mansion houses and often built to an artfully created masterplan. Also many large mansions for the wealthy German industrialists were built, such as Villa Hügel in Essen. The Villenkolonie of Lichterfelde West in Berlin was conceived after an extended trip by the architect through the South of England. Representative historicist mansions in Germany include the Heiligendamm and other resort architecture mansions at the Baltic Sea, Rose Island and King's House on Schachen in the Bavarian Alps, Villa Dessauer in Bamberg, Villa Wahnfried in Bayreuth, Drachenburg near Bonn, Hammerschmidt Villa in Bonn, the Liebermann Villa and Britz House in Berlin, Albrechtsberg, Eckberg, Villa Stockhausen and Villa San Remo in Dresden, Villa Waldberta in Feldafing, Villa Kennedy in Frankfurt, Jenisch House and Budge-Palais in Hamburg, Villa Andreae and Villa Rothschild in Königstein, Villa Stuck and Pacelli-Palais in Munich, Schloss Klink at Lake Müritz, Villa Ludwigshöhe in Rhineland-Palatinate, Villa Haux in Stuttgart and Weinberg House in Waren.

In France the Château de Ferrières is an example of the Italian Neo-Renaissance style villa - and in Britain the Mentmore Towers by John Ruskin. A representative building of this style in Germany is Villa Haas (designed by Ludwig Hofmann) in Hesse.[4]

20th - 21st centuries

Europe

During the 19th and 20th century, the term "villa" became widespread for detached mansions in Europe. Special forms are for instance spa villas (Kurvillen in German) and seaside villas (Bädervillen in German), that became especially popular at the end of the 19th century. The tradition established back then continued throughout the 20th century and even until today.

Another trend was the erection of rather minimalist mansions in the Bauhaus style since the 1920s, that also continues until today.

In Denmark, Norway and Sweden "villa" denotes most forms of single-family detached homes, regardless or size and standard.

Americas

The villa concept lived and lives on in the haciendas of Latin America and the estancias of Brazil and Argentina. The oldest are original Portuguese and Spanish Colonial architecture; followed after independences in the Americas from Spain and Portugal, by the Spanish Colonial Revival style with regional variations. In the 20th century International Style villas were designed by Roberto Burle Marx, Oscar Niemeyer, Luis Barragán, and other architects developing a unique Euro-Latin synthesized aesthetic.

Villas are particularly well represented in California and the West Coast of the United States, where they were originally commissioned by well travelled "upper-class" patrons moving on from the Queen Anne style Victorian architecture and Beaux-Arts architecture. Communities such as Montecito, Pasadena, Bel Air, Beverly Hills, and San Marino in Southern California, and Atherton and Piedmont in the San Francisco Bay Area are a few examples of villa density.

The popularity of Mediterranean Revival architecture in its various iterations over the last century has been consistently used in that region and in Florida. Just a few of the notable early architects were Wallace Neff, Addison Mizner, Stanford White, and George Washington Smith. A few examples are the Harold Lloyd Estate in Beverly Hills, California, Medici scale Hearst Castle on the Central Coast of California, and Villa Montalvo in the Santa Cruz Mountains of Saratoga, California, Villa Vizcaya in Coconut Grove, Miami, American Craftsman versions are the Gamble House and the villas by Greene and Greene in Pasadena, California

Modern villas

Other

Today the term "villa" is often applied to vacation rental properties. In the United Kingdom the term is used of high quality detached homes in warm destinations, particularly Florida and the Mediterranean. The term is also used in Pakistan, and in some of the Caribbean islands such as Jamaica, Saint Barthélemy, Saint Martin, Guadeloupe, British Virgin Islands, and others. It is similar for the coastal resort areas of Baja California Sur and mainland Mexico, and for hospitality industry destination resort "luxury bungalows" in various worldwide locations.

In Indonesia, the term "villa" is applied to Dutch colonial country houses (landhuis). Nowadays, the term is more popularly applied to vacation rental usually located in countryside area.

In Australia "villas" or "villa units" are terms used to describe a type of townhouse complex which contains, possibly smaller attached or detached houses of up to 3-4 bedrooms that were built since the early 1980s.

In New Zealand the term "villa" is commonly used to describe a style of wooden weatherboard house constructed before WW1 characterised by high ceilings (often 12 ft), sash windows, and a long entrance hall.

In Cambodia "villa" is used as a loanword in the local language of Khmer, and is generally used to describe any type of detached townhouse that features yard space. The term doesn't apply to any particular architectural style or size, the only features that distinguish a Khmer villa from another building are the yard space and being fully detached. The terms "twin-villa" and "mini-villa" have been coined meaning semi-dettached and smaller versions respectively. Generally, these would be more luxurious and spacious houses than the more common row houses. The yard space would also typically feature some form of garden, trees or greenery. Generally, these would be properties in major cities, where there is more wealth and hence more luxurious houses.

See also



This article uses material from the Wikipedia article "", which is released under the Creative Commons Attribution-Share-Alike License 3.0. There is a list of all authors in Wikipedia

Architecure & BIM & MEP

Autodesk Revit, Nemetschek ArchiCAD, Nemetschek Allplan, Vectorworks, Bentley AECOMSIM, Bentley Microstation, Trimble Tekla, Trimble Sketchup, EliteCAD, Ascon Renga, BricsCAD, Hexagon, Rhinoceros CAD, Sweet Home 3D, BIM Object, BIM component, BIM library, BIM family, BIM catalog, GIS, Advanced Steel, AutoCAD MEP, linear, MagiCAD, Relux, TGA, VDI 3805, Lod100, Lod200, Lod300, Lod350, Lod400, Lod500, Loi, IFC, BuildingSmart, BIM family creation, 3D, Download, MEP BIM product library