powered by CADENAS

Social Share

Position sensor (7557 views - Mechanical Engineering)

A position sensor is any device that permits position measurement. It can either be an absolute position sensor or a relative one (displacement sensor). Position sensors can be linear, angular, or multi-axis. Some position sensors available today: Capacitive transducer Capacitive displacement sensor Eddy-current sensor Ultrasonic sensor Grating sensor Hall effect sensor Inductive non-contact position sensors Laser Doppler Vibrometer (optical) Linear variable differential transformer (LVDT) Multi-axis displacement transducer Photodiode array Piezo-electric transducer (piezo-electric) Potentiometer Proximity sensor (optical) Rotary encoder (angular) Seismic displacement pick-up String potentiometer (also known as string pot., string encoder, cable position transducer)
Go to Article

Position sensor

Position sensor

A position sensor is any device that permits position measurement. It can either be an absolute position sensor or a relative one (displacement sensor). Position sensors can be linear, angular, or multi-axis.

Some position sensors available today:

See also



This article uses material from the Wikipedia article "", which is released under the Creative Commons Attribution-Share-Alike License 3.0. There is a list of all authors in Wikipedia

Mechanical Engineering

AutoCAD, SolidWorks, Autodesk Inventor, FreeCAD, Catia, Siemens NX, PTC Creo, Siemens Solid Edge, Microstation, TurboCAD, Draftsight, IronCAD, Spaceclaim, VariCAD, OnShape, IntelliCAD,T-FLEX, VariCAD, TenadoCAD, ProgeCAD, Cadra, ME10, Medusa, Designspark, KeyCreator, Caddy, GstarCAD, Varimetrix, ASCON Kompas-3D, Free Download, Autocad, 2D Library, DXF, DWG, 2D drawing, 3D digital library, STEP, IGES, 3D CAD Models, 3D files, CAD library, 3D CAD files, BeckerCAD, MegaCAD, Topsolid Missler, Vero VisiCAD, Acis SAT, Cimatron, Cadceus, Solidthinking, Unigraphics, Cadkey, ZWCAD, Alibre, Cocreate, MasterCAM, QCAD.org, QCAD, NanoCAD