powered by CADENAS

Autodesk Revit (36 views - BIM Dictionary)

Autodesk Revit is building information modeling software for architects, structural engineers, MEP engineers, designers and contractors developed by Autodesk. It allows users to design a building and structure and its components in 3D, annotate the model with 2D drafting elements, and access building information from the building model's database. Revit is 4D BIM capable with tools to plan and track various stages in the building's lifecycle, from concept to construction and later maintenance and/or demolition.
Go to Article

Autodesk Revit

Autodesk Revit

Revit
Developer(s) Autodesk
Initial release 5 April 2000
Stable release
2017 / April 2016
Operating system 64-bit Windows
Type CAD Building information modeling
License Proprietary
Website Autodesk Revit site

Autodesk Revit is building information modeling software for architects, structural engineers, MEP engineers, designers and contractors developed by Autodesk. It allows users to design a building and structure and its components in 3D, annotate the model with 2D drafting elements, and access building information from the building model's database. Revit is 4D BIM capable with tools to plan and track various stages in the building's lifecycle, from concept to construction and later maintenance and/or demolition.

History

Charles River Software was founded in Newton, Massachusetts, on October 31, 1997, by Leonid Raiz and Irwin Jungreis, key developers of PTC's Pro/Engineer software for mechanical design, with the intent of bringing the power of parametric modeling to the building industry (PTC had previously tried and failed to market its recently acquired Reflex software to the construction sector).[1] With funding from venture capitalists Atlas Venture and North Bridge Venture Partners, Raiz and Jungreis hired several software developers and architects and began developing Revit in C++ on the Microsoft Windows platform. In 1999 they hired Dave Lemont as CEO and recruited board members Jon Hirschtick, founder of SolidWorks, and Arol Wolford, founder of CMD Group.

From the outset, Revit was intended to allow architects and other building professionals to design and document a building by creating a parametric three-dimensional model that included both the geometry and non-geometric design and construction information, which is also known as Building Information Modeling or BIM (1975 Eastman C.). At the time, several other software packages such as ArchiCAD and Reflex allowed working with a three-dimensional virtual building model, and allowed individual components to be controlled by parameters (parametric components). Two key differences in Revit were that its parametric components were created using a graphical "family editor" rather than a programming language, and all relationships between components, views, and annotations were captured by the model so that a change to any element would automatically propagate to keep the model consistent.[2] For example, moving a wall would update the neighboring walls, floors, and roofs, correct the placement and values of dimensions and notes, adjust the floor areas reported in schedules, redraw section views, etc., so that the model would remain connected and all documentation would be coordinated. The concept of bi-directional associativity[3] between components, views, and annotations was a distinguishing feature of Revit for many releases. The ease of making changes inspired the name Revit, a contraction of Revise-It. At the heart of Revit is a parametric change propagation engine that relied on a new technology, context-driven parametrics, that was more scalable than the variational and history-driven parametrics used in mechanical CAD software.[4] The term Parametric Building Model was adopted to reflect the fact that changes to parameters drove the whole building model and associated documentation, not just individual components.

The company was renamed Revit Technology Corporation in January 2000, and Revit version 1.0 was released on April 5, 2000. The software progressed rapidly, with version 2.0, 3.0, 3.1, 4.0, and 4.1 released in August 2000; October 2000; February 2001; June 2001; November 2001; and January 2002, respectively.[5]

The software was initially offered only as a monthly rental, with no option to purchase. Licensing was controlled by an entirely automatic process, an innovation at a time when human intervention and manual transmission of authorization codes was required to buy other types of design software.[6]

Autodesk, best known for its AutoCAD line of products, purchased the Massachusetts-based Revit Technology Corporation for US$133 million in 2002.[7] The purchase allowed more research, development and improvement of the software. Autodesk has released several versions of Revit since 2004. In 2005 Revit Structure was introduced, then in 2006 Revit MEP. After the 2006 release Revit Building was renamed Revit Architecture.[8]

Since Revit 2013 the different disciplines have been rolled into one product, simply called Revit.

In 2012[9] Revit LT[10] became the newest version of Revit on the market. It is a light version of Revit with a number of features such as rendering and multi user environments removed.[11]

With their Revit platform, Autodesk is a significant player in the BIM market together with Nemetschek (makers of ArchiCAD, AllPlan and Vectorworks), and Gehry Technologies with CATIA based Digital Project.[12]

Products

Since Revit 2013 all Revit functionality is available in one product.

In 2013, Autodesk released the feature limited Revit LT for the entry level market alongside the full featured Revit 2013.[13][11] That same year, Autodesk began introducing rental licensing for some of their products, including Revit.[14]

Autodesk sells Building Design Suites which each include a different selection of software packages. Revit is included in the Premium and Ultimate suites.[15]

With the release of Revit 2015 Autodesk dropped support for 32-bit Windows.

Use and Implementation

Revit can be used as a very powerful collaboration tool between different disciplines in the building design sphere. The different disciplines that use Revit approach the program from unique perspectives. Each of these perspectives is focused on completing that discipline's task. Companies that adopt the software first examine the existing work flow process to determine if such an elaborate collaboration tool is required.

Modeling

The Revit work environment allows users to manipulate whole buildings or assemblies (in the project environment) or individual 3D shapes (in the family editor environment). Modeling tools can be used with pre-made solid objects or imported geometric models. However, Revit is not a NURBS modeller and also lacks the ability to manipulate an object's individual polygons except on some specific object types such as roofs, slabs and terrain or in the massing environment.

There are many categories of objects ('families' in Revit terminology), which divide into three groups:

  • System Families, such as walls, floors, roofs and ceilings which are built inside a project
  • Loadable Families / Components, which are built with primitives (extrusions, sweeps, etc.) separately from the project and loaded into a project for use
  • In-Place Families, which are built in-situ within a project with the same toolset as loadable components

An experienced user can create realistic and accurate families ranging from furniture[16] to lighting fixtures,[17] as well as import existing models from other programs. Revit families can be created as parametric models with dimensions and properties. This lets users modify a given component by changing predefined parameters such as height, width or number in the case of an array. In this way a family defines a geometry which is controlled by parameters, each combination of parameters can be saved as a type, and each occurrence (instance in Revit) of a type can also contain further variations. For example, a swing door may be a Family. It may have types describing different sizes, and the actual building model will have instances of those types placed in walls where instance-based parameters could specify the door hardware uniquely for each occurrence of the door.

Due to the copyright nature of project work, it is rare and impractical to be able to buy fully 3D modelled Revit project models. Indeed as most projects are site specific and bespoke, obtaining an existing model is in many instances unsuitable. However, there are cicumstances where new practices or students that are training to learn Revit, do have a need to refer to completed models. Sources for these are limited, however they can be purchased at websites like BIMGallery and downloaded from websites like GrabCad. Revit model files have also been located using google search string "index of" + rvt" + "central" -html -htm -php .

Although Revit software comes with a range of families out of the box (OOTB), they are limited, so users can find a need to build their own families or buy them from online stores such as Plansort, Bimbandit or Andekan. A number of websites offer families for free including Revitcity, Augi and NationalBimlibrary.

In 2011 Dynamo[18] was released in beta form allowing first glimpses of directly programming the behavior of hosted components through a drag and drop node interface. This is similar to the way the visual programming language Grasshopper 3d works on objects in Rhinoceros 3D.[19]

Rendering

When a user makes a building, model, or any other kind of object in Revit, they may use Revit's rendering engine to make a more realistic image of what is otherwise a very diagrammatic model. This is accomplished by either using the premade model, wall, floor, etc., tools, or making her or his own models, walls, materials, etc. Revit 2010 comes with a plethora of predefined materials, each of which can be modified to the user's desires. The user can also begin with a "Generic" material. With this, the user can set the rotation, size, brightness, and intensity of textures, gloss maps (also known as shinemaps), transparency maps, reflection maps, oblique reflection maps, hole maps, and bump maps, as well as leaving the map part out and just using the sliders for any one (or all or none) of the aforementioned features of textures.

Cloud-based rendering with the experimental plug-in dubbed Project Neon, located on Autodesk Labs is in the beta phases and allows for the user to render their images through their Autodesk account instead of locally through their own computers. Revit models may also be linked directly into Autodesk 3ds Max (release 2013 and later) for more advanced rendering and animation projects with much of their material and object information maintained.

An addin available for Revit called Enscape3D allows live 3D rendering walkthroughs and flyarounds. It permits live updates and also allows for sound sources to be added so that acoustics may be tested.

See also



This article uses material from the Wikipedia article "Autodesk Revit", which is released under the Creative Commons Attribution-Share-Alike License 3.0. There is a list of all authors in Wikipedia

BIM (Architecture) Dictionary

BIM,catalogs,library,family,object,component, Architecture, AEC,  Building Smart, IFC, FCSI, IFSE DD, Lod 100, Lod 200, Lod 300, Lod 350, Lod 400, Lod 450, Lod 500, Loi, RFA, Revit,(.rfa)