This article does not cite any sources. Please help improve this article by adding citations to reliable sources. Unsourced material may be challenged and removed. (December 2009) (Learn how and when to remove this template message) |
Six-wheel drive (6WD or 6×6) is an all-wheel drive drivetrain configuration of three axles with at least two wheels on each axle capable of being driven simultaneously by the vehicle's engine. Unlike four-wheel drive drivetrains, the configuration is largely confined to heavy-duty off-road and military vehicles, such as all-terrain vehicles, armored vehicles, and prime movers.
When such a vehicle only has six wheels by definition all are driven. When it has ten – with two pairs of ganged "dual" wheels on each rear axle as on a GMC CCKW – all are also driven but the 6×6 designation remains. For most military applications where traction/mobility are considered more important than payload capability, single wheels on each axle (often referred to as super singles) are the norm.
Heavy hauler and ballast tractor 6×6s have had a long history as prime movers both in the military (as tank transports and artillery tractors), and commercially in logging and heavy equipment hauling both on- and off-road.
Most six-wheel drive vehicles have a forward axle and two at the rear (with only the front pair steering), or three evenly spaced in varying steering configurations. Depending on the vehicle's role, the number of wheels varies between six (in three pairs) and ten (with two in the front and two dual axles with four wheels apiece in the rear). Drive may be limited to the rear two axles for on-road use.
Military
Military/commercial
Commercial
Conversions
Recreational ATV/UTV
Concept car, testbed, and limited production commercial examples include:
Twin front axle
Twin rear axle
(Twin axle) drive in the rear, and an integrated "roll steer" function built into the suspension design. All 6x6 Australia Pty Ltd vehicles are ADR-compliant with IPA for both "heavy" and "light" vehicles.
10-wheel U.S. Army 6×6 Pacific Car & Foundry Co.-built M26 armored tank transporter tractor unit
10-wheel U.S. Army 6×6 M35 2½ ton cargo truck, with one front and two rear axles
6-wheel U.S. Marines 6×6 MTVR, with one front and two rear axles
Unusual two forward and one rear axle configuration of the Czech TATRAPAN
This article uses material from the Wikipedia article "Six-wheel drive", which is released under the Creative Commons Attribution-Share-Alike License 3.0. There is a list of all authors in Wikipedia
Car, Truck,MotorBike, Bicycle, Engine, Racer