Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
Licensed under Creative Commons Attribution-Share Alike 3.0 (Qwerty242).
A semi-trailer truck (more commonly semi truck or simply "semi") is the combination of a tractor unit and one or more semi-trailers to carry freight. A semi-trailer attaches to the tractor with a fifth-wheel coupling (hitch), with much of its weight borne by the tractor. The result is that both the tractor and semi-trailer will have a design distinctly different from that of a rigid truck and trailer.
It is variously known as a transport in Canada; semi or single in Australia and New Zealand; semi, tractor-trailer, big rig, or eighteen-wheeler in the United States; and articulated lorry, abbreviated artic, in the United Kingdom, Ireland and New Zealand.
In North America, the combination vehicles made up of a powered truck and one or more semitrailers are known as "semis", "semitrailers",[1] "tractor-trailers", "big rigs", "semi trucks", "eighteen-wheelers", or "semi-tractor trailers".
The tractor unit typically has two or three axles; those built for hauling heavy-duty commercial-construction machinery may have as many as five, some often being lift axles.
The most common tractor-cab layout has a forward engine, one steering axle, and two drive axles. The fifth-wheel trailer coupling on most tractor trucks is movable fore and aft, to allow adjustment in the weight distribution over its rear axle(s).
Ubiquitous in Europe, but less common in North America since the 1990s, is the cabover engine configuration, where the driver sits next to, or over the engine. With changes in the US to the maximum length of the combined vehicle, the cabover was largely phased out of North American over-the-road (long-haul) service by 2007. Cabovers were difficult to service; for a long time the cab could not be lifted on its hinges to a full 90-degree forward tilt, severely limiting access to the front part of the engine.
As of 2016[update], a truck could cost US$100,000, while the diesel fuel cost could be $70,000 per year.[2] Trucks average from 4 to 8 miles per US gallon (59 to 29 L/100 km), with fuel economy standards requiring better than 7 miles per US gallon (34 L/100 km) efficiency by 2014.[3] Power requirements in standard conditions are 170 hp at 55 mph (89 km/h) or 280 hp at 70 mph (113 km/h), and somewhat different power usage in other conditions.[4]
The cargo trailer usually has tandem axles at the rear, each of which has dual wheels, or eight tires on the trailer, four per axle. In the US it is common to refer to the number of wheel hubs, rather than the number of tires; an axle can have either single or dual tires with no legal difference.[5][6] The combination of eight tires on the trailer and ten tires on the tractor is what led to the moniker eighteen wheeler, although this term is considered by some truckers to be a misnomer (the term "eighteen-wheeler" is a nickname for a five-axle over-the-road combination). Many trailers are equipped with movable tandem axles to allow adjusting the weight distribution.
To connect the second of a set of doubles to the first trailer, and to support the front half of the second trailer, a converter gear known as a "dolly" is used. This has one or two axles, a fifth-wheel coupling for the rear trailer, and a tongue with a ring-hitch coupling for the forward trailer. Individual states may further allow longer vehicles, known as "longer combination vehicles" (or LCVs), and may allow them to operate on roads other than Interstates.
Long combination vehicle types include:
Future long combination vehicles under consideration and study for the U.S. MAP-21 transportation bill are container doubles. These combinations are under study for potential recommendation in November 2014:
The US federal government, which only regulates the Interstate Highway System, does not set maximum length requirements (except on auto and boat transporters), only minimums. Tractors can pull two or three trailers if the combination is legal in that state. Weight maximums are 20,000 lb (9,100 kg) on a single axle, 34,000 lb (15,000 kg) on a tandem, and 80,000 lb (36,000 kg) total for any vehicle or combination. There is a maximum width of 8.5 ft (2.6 m) and no maximum height.[7][8]
Roads other than the Interstates are regulated by the individual states, and laws vary widely. Maximum weight varies between 80,000 lb (36,000 kg) to 171,000 lb (78,000 kg), depending on the combination.[9] Most states restrict operation of larger tandem trailer setups such as triple units, turnpike doubles and Rocky-Mountain doubles. Reasons for limiting the legal trailer configurations include both safety concerns and the impracticality of designing and constructing roads that can accommodate the larger wheelbase of these vehicles and the larger minimum turning radii associated with them. In general, these configurations are restricted to the Interstates. Except for these units, double setups are not restricted to certain roads any more than a single setup. They are also not restricted by weather conditions or "difficulty of operation". The Canadian province of Ontario, however, does have weather-related operating restrictions for larger tandem trailer setups.[10]
The noticeable difference between tractor units in Europe and North America is that almost all European models are cab over engine (called "forward control" in England[11]), while the majority of North American trucks are "conventional" (called "normal control" or "bonneted" in England[12]).[13] European trucks, whether straight trucks or fully articulated, have a sheer face on the front. This allows shorter trucks with longer trailers (with larger freight capacity) within the legal maximum total length. Furthermore, it offers greater maneuverability in confined areas, a more balanced weight-distribution and better overall view for the driver. The major disadvantage is that for repairs on COE trucks, the entire cab has to hinge forward to allow maintenance access. Conversely, "conventional" cab tractors offer the driver a more comfortable driving environment, easier access getting in or out and better protection in a collision.[citation needed]
In Europe usually both rear tractor axles have dual wheels, while single or dual wheels are used for the cargo trailer. The most common combination used in Europe is a semi tractor with three axles, one a lift axle, and a cargo trailer with three axles, one also a lift axle, giving six axles and 22 wheels in total. This format is now common across Europe, due to reduced road-loading requirements, especially for bridges. The lift axles used on both tractors and trailers allow the trucks to remain legal, but increases maneuverability while at the same time reducing fuel consumption and tyre wear when carrying lighter loads, by raising one or multiple axle set(s) off the roadway. Although lift axles usually operate automatically, they can be lowered manually even while carrying light loads, in order to remain within legal (safe) limits when, for example, navigating back-road bridges with severely restricted axle loads. For greater detail, see the United Kingdom section, below.
When using a dolly, which generally has to be equipped with lights and a license plate, rigid trucks can be used to pull semi-trailers. The dolly is equipped with a fifth wheel to which the trailer is coupled. Because the dolly attaches to a pintle hitch on the truck, maneuvering a trailer hooked to a dolly is different from maneuvering a fifth wheel trailer. Backing the vehicle requires same technique as backing an ordinary truck/full trailer combination, though the dolly/semi setup is probably longer, thus requiring more space for maneuvering. The tractor/semi-trailer configuration is rarely used on timber trucks, since these will use the two big advantages of having the weight of the load on the drive wheels, and the loader crane used to lift the logs from the ground can be mounted on the rear of the truck behind the load, allowing a short (lightweight) crane to reach both ends of the vehicle without uncoupling. Also, construction trucks are more often seen in a rigid + midaxle trailer configuration instead of the tractor/semi-trailer setup.
In the United Kingdom the maximum permitted gross weight of a semi-trailer truck without the use of a Special Type General Order (STGO) is 97,000 lb (44 t). In order for a 97,000 lb semi-trailer truck to be permitted on UK roads the tractor and semi-trailer must have three or more axles each. Lower weight semi-trailer trucks can mean some tractors and trailer having fewer axles.[14] In practice, as with double decker buses and coaches in the UK, there is no legal height limit for semi-trailer trucks; however, bridges over 16.5 ft (5.03 m) do not have the height marked on them. Semi-trailer trucks in continental Europe have a height limit of 13.1 ft (4.0 m). Vehicles heavier than 97,000 lb are permitted on UK roads but are indivisible loads, which would be classed as abnormal (or oversize). Such vehicles are required to display an STGO (Special Types General Order) plate on the front of the tractor unit and, under certain circumstances, are required to travel by an authorized route and have an escort.
Most UK trailers are 45 ft (13.7 m) long and, dependent on the position of the fifth wheel and kingpin, a coupled tractor unit and trailer will have a combined length of between 50 and 55 ft (15.25 and 16.75 m). Although the Construction and Use Regulations allow a maximum rigid length of 60 ft (18.2 m), this, combined with a shallow kingpin and fifth wheel set close to the rear of the tractor unit, can give an overall length of around 75 ft (22.75 m).[15]
Starting in January 2012 the Department for Transport is conducting a trial of longer semi-trailers. The trial involves 900 semi-trailers of 48 ft (14.6 m) in length (i.e. 3 ft (1 m) longer than the current maximum), and a further 900 semi-trailers of 51 ft (15.65 m) in length (i.e. 7 ft (2.05 m) longer). This will result in the total maximum length of the semi-trailer truck being 57 ft (17.5 m) for trailers 48 ft in length, and 61 ft (18.55 m) for trailers 51 ft long. The increase in length will not result in the 97,000 lb weight limit being exceeded and will allow some operators to approach the weight limit which may not have been previously possible due to the previous length of trailers. The trial will run for a maximum of 10 years. Providing certain requirements are fulfilled, a Special Types General Order (STGO) allows for vehicles of any size or weight to travel on UK roads. However, in practice any such vehicle has to travel by a route authorized by the Department of Transport and move under escort. The escort of abnormal loads in the UK is now predominantly carried out by private companies, but extremely large or heavy loads that require road closures must still be escorted by the police.
In the UK, some semi-trailer trucks have eight tires on three axles on the tractor; these are known as six-wheelers or "six leggers", with either the center or rear axle having single wheels which normally steer as well as the front axle and can be raised when not needed (i.e. when unloaded or only a light load is being carried; an arrangement known as a TAG axle when it is the rear axle, or mid-lift when it is the center axle). Some trailers have two axles which have twin tires on each axle; other trailers have three axles, of which one axle can be a lift axle which has super-single wheels. In the UK, two wheels bolted to the same hub are classed as a single wheel, therefore a standard six-axle articulated truck is considered to have twelve wheels, even though it has twenty tires. The UK also allows semi-trailer truck which have six tires on two axles; these are known as four-wheelers.
This section does not cite any sources. Please help improve this section by adding citations to reliable sources. Unsourced material may be challenged and removed. (June 2014) (Learn how and when to remove this template message) |
In 2009, the operator Denby Transport designed and built a 83 ft long (25.25 m) B-Train (or B-Double) semi-trailer truck called the Denby Eco-Link to show the benefits of such a vehicle, which were a reduction in road accidents and result in less road deaths, a reduction in emissions due to the one tractor unit still being used and no further highway investment being required. Furthermore, Denby Transport asserted that two Eco-Links would replace three standard semi-trailer trucks while, if limited to the current UK weight limit of 97,000 lb, it was claimed the Eco-Link would reduce carbon emissions by 16% and could still halve the number of trips needed for the same amount of cargo carried in conventional semi-trailer trucks. This is based on the fact that for light but bulky goods such as toilet paper, plastic bottles, cereals and aluminum cans, conventional semi-trailer trucks run out of cargo space before they reach the weight limit. At 97,000 lb, as opposed to 132,000 lb usually associated with B-Trains, the Eco-Link also exerts less weight per axle on the road compared to the standard six-axle 97,000 lb semi-trailer truck.
The vehicle was built after Denby Transport believed they had found a legal-loophole in the present UK law to allow the Eco-Link to be used on the public roads. The relevant legislation concerned the 1986 Road Vehicles Construction and Use Regulations. The 1986 regulations state that "certain vehicles" may be permitted to draw more than one trailer and can be up to 85 ft (25.9 m).[citation needed] The point of law reportedly hinged on the definition of a "towing implement", with Denby prepared to argue that the second trailer on the Eco-Link was one. The Department for Transport were of the opinion that this refers to recovering a vehicle after an accident or breakdown, but the regulation does not explicitly state this.
During BTAC performance testing the Eco-Link was given an "excellent" rating for its performance in maneuverability, productivity, safety and emissions tests, superseding ordinary semi-trailer trucks in many respects. Reportedly, private trials had also shown the Denby vehicle had a 20% shorter stopping distance than conventional semi-trailer trucks of the same weight, due to having extra axles. The active steer system meant that the Eco-Link had a turning circle of 41 ft (12.5 m), the same as a conventional semi-trailer truck.
Although the Department for Transport advised that the Eco-Link was not permissible on public roads, Denby Transport gave the Police prior warning of the timing and route of the test drive on the public highway, as well as outlining their position in writing to the Eastern Traffic Area Office. On 1 December 2009 Denby Transport were preparing to drive the Eco-Link on public roads, but this was cut short because the Police pulled the semi-trailer truck over as it left the gates in order to test it for its legality "to investigate any... offenses which may be found". The Police said the vehicle was unlawful due to its length and Denby Transport was served with a notice by the Vehicle and Operator Services Agency (VOSA) inspector to remove the vehicle from the road for inspection. Having returned to the yard, Denby Transport was formally notified by Police and VOSA that the semi-trailer truck could not be used. Neither the Eco-Link, nor any other B-Train, have since been permitted on UK roads. However, this prompted the Department for Transport to undertake a desk study into semi-trailer trucks, which has resulted in the longer semi-trailer trial which commenced in 2012.
The maximum overall length in the EU and EEA member states was 18.75 m (61.5 ft) with a maximum weight of 40 tonnes, or 44 tonnes if carrying an ISO container.[16] However, rules limiting the semi-trailers to 16.5 m (54 ft) and 18.75 m are met with trucks carrying a standardized 7.82 m (26 ft) body with one additional 7.82 m body on tow as a trailer.[17] 25.25 metre truck combinations were developed under the branding of EcoCombi which influenced the name of EuroCombi for an ongoing standardization effort where such truck combinations shall be legal to operate in all jurisdictions of the European Economic Area. With the 50% increase in cargo weight, the fuel efficiency increases with an average of 20% with a corresponding relative decrease in carbon emissions and with the added benefit of one third fewer trucks on the road.[16] The 1996 EU regulation defines a Europe Module System (EMS) as it was implemented in Sweden. The wording of EMS combinations and EuroCombi are now used interchangeably to point to truck combinations as specified in the EU document; however, apart from Sweden and Finland, the EuroCombi is only allowed to operate on specific tracks in other EU member states. Since 1996, when Sweden and Finland formally won a final exemption from the European Economic Area rules with 60 tonne and 25.25 m (83 ft) combinations, all other From 2006, 25.25 m truck trailer combinations are to be allowed on restricted routes within Germany, following a similar (on-going) trial in The Netherlands. Similarly, Denmark has allowed 25.25 m combinations on select routes. These vehicles will run a 60 tonne weight limit. Two types are to be used: 1) a 26-tonne truck pulling a dolly and semi-trailer, or 2) an articulated tractor unit pulling a B-double, member states gained the ability to adopt the same rules. In Italy the maximum permitted weight (unless exceptional transport is authorized) is 44 tonnes for any kind of combination with five axles or more. Czechia has allowed 25.25 m combinations with a permission for a selected route.
The tractor/semi-trailer configuration is rarely used on timber trucks, since these will use the two big advantages of having the weight of the load on the drive wheels, and the loader crane used to lift the logs from the ground can be mounted on the rear of the truck behind the load, allowing a short (lightweight) crane to reach both ends of the vehicle without uncoupling. Also construction trucks are more often seen in a rigid + midaxle trailer configuration instead of the tractor/semi-trailer setup.
Denmark and Norway allow 25.25 m (83 ft) trucks (Denmark from 2008, and Norway from 2008 on selected routes). In Sweden the allowed length has been 24 m (79 ft) since 1967. Before that, the maximum length was unlimited; the only limitations were on axle load. What stopped Sweden from adopting the same rules as the rest of Europe, when securing road safety, was the national importance of a competitive forestry industry.[16][18] Finland, with the same road safety issues and equally important forestry industry, followed suit. The change made trucks able to carry three stacks of cut-to-length logs instead of two, as it would be in a short combination. They have one on stack together with a crane on the 6×4 truck, and two additional stacks on a four axle trailer. The allowed gross weight in both countries is up to 60 tonnes depending on the distance between the first and last axle.
In the negotiations starting in the late 1980s preceding Sweden and Finland's entries to the European Economic Area and later the European Union, they insisted on exemptions from the EU rules citing environmental concerns and the transportation needs of the logging industry. In 1995, after their entry to the union, the rules changed again, this time to allow trucks carrying a standard CEN unit of 7.82 m (26 ft) to draw a 13.6 m (45 ft) standard semi-trailer on a dolly, a total overall length of 25.25 m. Later, B-double combinations came into use, often with one 6 m (20 ft) container on the B-link and a 12 m (40 ft) container (or two 6 m containers) on a semi-trailer bed. In allowing the longer truck combinations, what would take two 16.5 m (54 ft) semi-trailer trucks and one 18.75 m (62 ft) truck and trailer to haul on the continent now could be handled by just two 25.25 m trucks – greatly reducing overall costs and emissions. Prepared since late 2012 and effective on January 2013, Finland has changed its regulations to allow total maximum legal weight of a combination to be 76 tonnes. At the same time the maximum allowed height would be increased by 20 cm (8 in); from current maximum of 4.2 m (13.8 ft) to 4.4 m (14.4 ft). The effect this major maximum weight increase would cause to the roads and bridges in Finland over time is strongly debated.
However, longer and heavier combinations are regularly seen on public roads; special permits are issued for special cargo. The mining company Boliden AB have a standing special permit for 80 tonne combinations on select routes between mines in the inland and the processing plant in Boliden, taking a 50 tonne load of ore. Volvo has a special permit for a 32 m (105 ft), steering B-trailer-trailer combination carrying two 12 m (40 ft) containers to and from Gothenburg harbour and the Volvo Trucks factory, all on the island of Hisingen.[19] Another example is the ongoing project En Trave Till (lit. One more pile/stack) started in December 2008. It will allow even longer vehicles to further rationalize the logging transports. As the name of the project points out, it will be able to carry four stacks of timber, instead of the usual three. The test is limited to Norrbotten county and the European route E4 between the timber terminal in Överkalix and the sawmill in Munksund (outside Piteå). The vehicle is a 30 m (98 ft) long truck trailer combination with a gross weight exceeding 90 tonnes. It is estimated that this will give a 20% lower cost and 20-25% CO2 emissions reduction compared to the regular 60 tonne truck combinations. As the combinations spreads its weight over more axles, braking distance, road wear and traffic safety is believed to be either the same or improved with the 90 tonne truck-trailer. In the same program two types of 74 tonne combinations will be tested in Dalsland and Bohuslän counties in western Sweden: an enhanced truck and trailer combination for use in the forest and a b-double for plain highway transportation to the mill in Skoghall. In 2012, the Northland Mining company received permission for 90 tonne combinations with normal axle load (an extra dolly) for use on the 150 km (93 mi) Kaunisvaara-Svappavaara route, carrying iron ore.[20][21][22]
As of 2015[update], the longest and heaviest truck in everyday use in Finland is operated by transport company Ketosen Kuljetus as part of a pilot project studying transport efficiency in the timber industry. The combined vehicle is 33-metre (108 ft) long, has 13 axles, and weighs a total of 104 tonnes (229,000 lb).[23][24]
Starting from Jan 21 2019 Finland Government change the maximum allowed length of truck from 25,25 meters to 34,50 meters. New types of vehicle combinations that differ from the current standards may also be used on the road. The requirements for combinations also include camera systems for side visibility, an advanced emergency braking and lane detector system, electronic driving stability system and electronically controlled brakes. [1] [2]
Australian road transport has a reputation for using very large trucks and road trains. This is reflected in the most popular configurations of trucks generally having dual drive axles and three axles on the trailers, with four tyres on each axle. This means that Australian single semi-trailer trucks will usually have 22 tyres, which is generally more than their counterparts in other countries. Super single tyres are sometimes used on tri-axle trailers. The suspension is designed with travel limiting, which will hold the rim off the road for one blown or deflated tyre for each side of the trailer, so a trailer can be driven at reduced speed to a safe place for repair. Super singles are also often used on the steer axle in Australia to allow greater loading over the steer axle. The increase in loading of steer tyres requires a permit.
Long haul transport usually operates as B-doubles with two trailers (each with three axles), for a total of nine axles (including steering). In some lighter duty applications only one of the rear axles of the truck is driven, and the trailer may have only two axles. From July 2007, the Australian Federal and State Governments allowed the introduction of B-triple trucks on a specified network of roads.[25] B-Triples are set up differently from conventional road trains. The front of their first trailer is supported by the turntable on the prime mover. The second and third trailers are supported by turntables on the trailers in front of them. As a result, B-Triples are much more stable than road trains and handle exceptionally well. True road trains only operate in remote areas, regulated by each state or territory government.
In total, the maximum length that any articulated vehicle may be (without a special permit and escort) is 53.5 m (176 ft), its maximum load may be up to 164 tonnes gross, and may have up to four trailers. However, heavy restrictions apply to the areas where such a vehicle may travel in most states. In remote areas such as the Northern Territory great care must be taken when sharing the road with longer articulated vehicles that often travel during the daytime, especially four-trailer road trains.
Articulated trucks towing a single trailer or two trailers (commonly known as "short doubles") with a maximum overall length of 19 m (62 ft) are referred to as "General access heavy vehicles" and are permitted in all areas, including metropolitan. B-doubles are limited to a maximum total weight of 62.5 tonnes and overall length of 25 m (82 ft), or 26 m (85 ft) if they are fitted with approved FUPS (Front Underrun Protection System) devices. B-doubles may only operate on designated roads, which includes most highways and some major metropolitan roads. B-doubles are very common in all parts of Australia including state capitals and on major routes they outnumber single trailer configurations.
Maximum width of any vehicle is 2.5 m (8.2 ft) and a height of 4.3 m (14 ft). In the past few years, allowance has been made by several states to allow certain designs of heavy vehicles up to 4.6 m (15 ft) high but they are also restricted to designated routes. In effect, a 4.6 meter high B-double will have to follow two sets of rules: they may access only those roads that are permitted for B-doubles and for 4.6 meter high vehicles.
In Australia, both conventional prime movers and cabovers are common, however, cabovers are most often seen on B-doubles on the eastern seaboard where the reduction in total length allows the vehicle to pull longer trailers and thus more cargo than it would otherwise.
An Australian prime mover Kenworth and B double trailer combination
A road train in Australia
B-double truck on the Sturt Highway
New Zealand's legislation governing truck dimensions falls under the Vehicle Dimensions and Mass Rules published by NZ Transport Agency.[26] New rules were introduced effective 1 February 2017.[27] which increased the maximum height, width and weight of loads and vehicles to simplify regulations, increase the amount of freight carried and to improve the range of vehicles and trailers available to transport operators.
Common combinations in New Zealand consist of a standard semi-trailer, a B-double or a rigid towing vehicle pulling a trailer with a drawbar. Standard maximum vehicle lengths for trailers with one axle set are:
Trailers with two axle sets can be 20 m (66 ft), including heavy rigid vehicles towing two trailers. Oversized loads require, at minimum, a permit, and may require a pilot vehicle.[28]
There are many types of semi-trailers in use, designed to haul a wide range of products.
The cargo trailer is, by means of a king pin, hooked to a horseshoe-shaped quick-release coupling device called a fifth wheel or a turntable hitch at the rear of the towing engine that allows easy hook up and release. The truck trailer cannot move by itself because it only has wheels at the rear end: it requires a forward axle, provided by the towing engine, to carry half the load weight. When braking hard at high speeds, the vehicle has a tendency to fold at the pivot point between the towing vehicle and the trailer. Such a truck accident is called a "trailer swing", although it is also commonly described as a "jackknife".[29] Jackknifing is a condition where the tractive unit swings round against the trailer, and not vice versa.
Semi trucks use air pressure, rather than hydraulic fluid, to actuate the brake. The use of air hoses allows for ease of coupling and uncoupling of trailers from the tractor unit. The most common failure is brake fade, usually caused when the drums or discs and the linings of the brakes overheat from excessive use.
The parking brake of the tractor unit and the emergency brake of the trailer are spring brakes that require air pressure in order to be released. They are applied when air pressure is released from the system, and disengaged when air pressure is supplied. This is a fail-safe design feature which ensures that if air pressure to either unit is lost, the vehicle will stop to a grinding halt, instead of continuing without brakes and becoming uncontrollable. The trailer controls are coupled to the tractor through two gladhand connectors, which provide air pressure, and an electrical cable, which provides power to the lights and any specialized features of the trailer.
Glad-hand connectors (also known as palm couplings) are air hose connectors, each of which has a flat engaging face and retaining tabs. The faces are placed together, and the units are rotated so that the tabs engage each other to hold the connectors together. This arrangement provides a secure connection but allows the couplers to break away without damaging the equipment if they are pulled, as may happen when the tractor and trailer are separated without first uncoupling the air lines. These connectors are similar in design to the ones used for a similar purpose between railroad cars. Two air lines typically connect to the trailer unit. An emergency or main air supply line pressurizes the trailer's air tank and disengages the emergency brake, and a second service line controls the brake application during normal operation.
In the UK, male/female quick release connectors (red line or emergency), have a female on the truck and male on the trailer, but a yellow line or service has a male on the truck and female on the trailer. This avoids coupling errors (causing no brakes) plus the connections will not come apart if pulled by accident. The three electrical lines will fit one way around a primary black, a secondary green, and an ABS lead, all of which are collectively known as suzies or suzie coils.
Another braking feature of semi-trucks is engine braking, which could be either a compression brake (usually shortened to Jake brake) or exhaust brake or combination of both. However, the use of compression brake alone produces a loud and distinctive noise, and to control noise pollution, some local municipalities have prohibited or restricted the use of engine brake systems inside their jurisdictions, particularly in residential areas. The advantage to using engine braking instead of conventional brakes is that a truck can descend a long grade without overheating its wheel brakes. Some vehicles can also be equipped with hydraulic or electric retarders which have an advantage of near silent operation.
Because of the wide variety of loads the semi may carry, they usually have a manual transmission to allow the driver to have as much control as possible. However, all truck manufacturers now offer semi-automatic transmissions (manual gearboxes with automated gear change), as well as automatic transmissions.
Semi-truck transmissions can have as few as three forward speeds or as many as 18 forward speeds (plus 2 reverse speeds). A large number of transmission ratios means the driver can operate the engine more efficiently. Modern on-highway diesel engines are designed to provide maximum torque in a narrow RPM range (usually 1200-1500 RPM); having more gear ratios means the driver can hold the engine in its optimum range regardless of road speed (drive axle ratio must also be considered).
A ten-speed manual transmission, for example is controlled via a six-slot H-box pattern, similar to that in five-speed cars — five forward and one reverse gear. Gears six to ten (and high speed reverse) are accessed by a Lo/High range splitter; gears one to five are Lo range; gears six to ten are High range using the same shift pattern. A Super-10 transmission, by contrast, has no range splitter; it uses alternating "stick and button" shifting (stick shifts 1-3-5-7-9, button shifts 2-4-6-8-10). The 13-, 15-, and 18-speed transmissions have the same basic shift pattern, but include a splitter button to enable additional ratios found in each range. Some transmissions may have 12 speeds.
Another difference between semi-trucks and cars is the way the clutch is set up. On an automobile, the clutch pedal is depressed full stroke to the floor for every gear shift, to ensure the gearbox is disengaged from the engine. On a semi-truck with constant mesh transmission (non synchronized), such as by the Eaton Roadranger series, not only is double clutching required, but a clutch brake is required as well. The clutch brake stops the rotation of the gears, and allows the truck to be put into gear without grinding when stationary. The clutch is pressed to the floor only to allow smooth engagement of low gears when starting from a full stop; when the truck is moving, the clutch pedal is pressed only far enough to break torque for gear changes.
An electrical connection is made between the tractor and the trailer through a cable often referred to as a pigtail. This cable is a bundle of wires in a single casing. Each wire controls one of the electrical circuits on the trailer, such as running lights, brake lights, turn signals, etc. A straight cable would break when the rig went around corners, so a coiled cable is used which retracts these coils when not under tension. It is these coils that cause the cable to look like a pigtail.
In most countries, a trailer or semi-trailer must have minimum
Although dual wheels are the most common, use of two single, wider tires, known as super singles, on each axle is becoming popular among bulk cargo carriers and other weight-sensitive operators. With increased efforts to reduce greenhouse gas emissions, the use of the super-single tire is gaining popularity. There are several advantages to this configuration. The first of these is that super singles reduce fuel consumption. In 1999, tests on an oval track showed a 10% fuel savings when super singles were used. These savings are realized because less energy is wasted flexing fewer tire sidewalls. Second, the lighter overall tire weight allows a truck to be loaded with more freight. The third advantage is that the single wheel encloses less of the brake unit, which allows faster cooling and reduces brake fade.
One of the major disadvantages of the super singles is that they are currently not as widely available as a standard tire. In addition, if a tire should become deflated or be destroyed, there is not another tire attached to the same hub to maintain the dynamic stability of the vehicle, as would be the case with dual wheels. With dual wheels, the remaining tire may be overloaded, but it will typically allow the vehicle to be safely stopped or driven to a repair facility.
In Europe, super singles became popular when the allowed weight of semitrailer rigs was increased from 38 to 40 tonnes.[30] In this reform the trailer industry replaced two 10-tonne (22,000 lb) axles with dual wheels, with three 8-tonne (18,000 lb) axles on wide-base single wheels. The significantly lower axle weight on super singles must be considered when comparing road wear from single versus dual wheels. The majority of super singles sold in Europe have a width of 385 mm (15.2 in). The standard 385 tires have a legal load limit of 4,500 kg (9,900 lb). (Note that expensive, specially reinforced 385 tires approved for 5,000 kg (11,000 lb) do exist. Their market share is tiny, except for mounting on the steer axle.)
An innovation rapidly growing in popularity is the skirted trailer. The space between the road and the bottom of the trailer frame was traditionally left open until it was realized that the turbulent air swirling under the trailer is a major source of aerodynamic drag. Three split skirt concepts were verified by the United States Environmental Protection Agency (EPA) to provide fuel savings greater than 5%, and four split skirt concepts had EPA-verified fuel savings between 4% and 5%.[31]
Skirted trailers are often combined with Underrun Protection Systems (underride guards), greatly improving safety for passenger vehicles sharing the road.
Technically called a Rear Underrun Protection System (RUPS), this is a rigid assembly hanging down from the bottom rear of the trailer, which is intended to provide some protection for passenger cars which collide with the rear of the trailer. Public awareness of this safeguard was increased in the aftermath of the accident that killed actress Jayne Mansfield on 29 June 1967, when the car she was in hit the rear of a tractor-trailer, causing fatal head trauma. After her death, the NHTSA recommended requiring a rear underride guard, also known as a Mansfield bar, an ICC bar, or a DOT bumper,[32][33]. In Europe, side and rear underrun protection are mandated on all lorries and trailers with a gross weight of 3,500 kg or more.[34]
The bottom rear of the trailer is near head level for an adult seated in a car, and without the underride guard, the only protection for such an adult's head in a rear-end collision would be the car's windshield. The front of the car goes under the platform of the trailer rather than making contact via the passenger car bumper, so the car's protective crush zone becomes irrelevant and air bags are ineffective in protecting the car passengers. The underride guard provides a rigid area for the car to contact at the height of its bumper.
In addition to rear underride guards, truck tractor cabs may be equipped with a Front Underrun Protection System (FUPS) at the front bumper of the truck, if the front end is not low enough for the bumper to provide the adequate protection on its own. The safest tractor-trailers are also equipped with side underride guards, also called Side Underrun Protection System (SUPS). These additional barriers prevent passenger cars from skidding underneath the trailer from the side, such as in an oblique or side collision, or if the trailer jackknifes across the road. In addition to safety benefits, these underride guards may improve fuel mileage by reducing air turbulence under the trailer at highway speeds.
Another benefit of having a sturdy underride guard is that it may be secured to a loading dock with a hook to prevent "trailer creep", a movement of the trailer away from the dock, which opens up a dangerous gap during loading or unloading operations.[35]
Current semi-truck manufacturers include:
A special driver's license is required to operate various commercial vehicles.
Regulations vary by province. A license to operate a vehicle with air brakes is required (i.e., normally a Class I, II, or III commercial license with an "A" or "S" endorsement in provinces other than Ontario). In Ontario, a "Z" endorsement[36] is required to drive any vehicle using air brakes; in provinces other than Ontario, the "A" endorsement is for air brake operation only, and an "S" endorsement is for both operation and adjustment of air brakes. Anyone holding a valid Ontario driver's license (i.e., excluding a motorcycle license) with a "Z" endorsement can legally drive any air-brake-equipped truck-trailer combination with a registered- or actual-gross-vehicle-weight (i.e., including towing- and towed-vehicle) up to 11 tonnes, that includes one trailer weighing no more than 4.6 tonnes if the license falls under the following three classes: Class E (school bus—maximum 24-passenger capacity or ambulance), F (regular bus—maximum 24-passenger capacity or ambulance) or G (car, van, or small-truck).
A Class B (any school bus), C (any urban-transit-vehicle or highway-coach), or D (heavy trucks other than tractor-trailers) license enables its holder to drive any truck-trailer combination with a registered- or actual-gross-vehicle-weight (i.e., including towing- and towed-vehicle) greater than 11 tonnes, that includes one trailer weighing no more than 4.6 tonnes.[37] Anyone holding an Ontario Class A license (or its equivalent) can drive any truck-trailer combination with a registered- or actual-gross-vehicle-weight (i.e., including towing- and towed-vehicles) greater than 11 tonnes, that includes one or more trailers weighing more than 4.6 tonnes.
Drivers of semi-trailer trucks generally require a Class A commercial driver's license (CDL) to operate any combination vehicles with a gross combination weight rating (or GCWR) in excess of 26,000 lb (11,800 kg) if the gross vehicle weight rating (GVWR) of the towed vehicle(s) is in excess of 10,000 lb (4,500 kg). Some states (such as North Dakota) provide exemptions for farmers, allowing non-commercial license holders to operate semis within a certain air-mile radius of their reporting location. State exemptions, however, are only applicable in intrastate commerce; stipulations of the Code of Federal Regulations (CFR) may be applied in interstate commerce. Also a person under the age of 21 cannot operate a commercial vehicle outside the state where the commercial license was issued. This restriction may also be mirrored by certain states in their intrastate regulations. A person must be at least 18 in order to be issued a commercial license.
In addition, endorsements are necessary for certain cargo and vehicle arrangements and types;
The Road Traffic Security Rules (道路交通安全規則) require a combination vehicle driver license (Chinese: 聯結車駕駛執照) to drive a combination vehicle (Chinese: 聯結車). These rules define a combination vehicle as a motor vehicle towing a heavy trailer, i.e., a trailer with a gross weight of more than 750 kilograms (1,653 lb).
A category CE driving licence is required to drive a tractor-trailer in Europe. Category C (Γ in Greece) is required for vehicles over 7,500 kg (16,500 lb), while category E is for heavy trailers, which in the case of trucks and buses means any trailer over 750 kg (1,650 lb). Vehicles over 3,500 kg (7,700 lb)—which is the maximum limit of B license—but under 7,500 kg can be driven with a C1 license. Buses require a D (Δ in Greece) license. A bus that is registered for no more than 16 passengers, excluding the driver, can be driven with a D1 license.
Truck drivers in Australia require an endorsed license. These endorsements are gained through training and experience. The minimum age to hold an endorsed license is 18 years, and/or must have held open (full) driver's license for minimum 12 months. The following are the heavy vehicle license classes in Australia:
In order to obtain an HC License the driver must have held an MR or HR license for at least 12 months. To upgrade to an MC License the driver must have held a HR or HC license for at least 12 months. From licenses MR and upward there is also a B Condition which may apply to the license if testing in a synchromesh or automatic transmission vehicle. The B Condition may be removed upon the driver proving the ability to drive a constant mesh transmission using the clutch. Constant mesh transmission refers to crash box transmissions, predominantly Road Ranger eighteen-speed transmissions in Australia.
In New Zealand, drivers of heavy vehicles require specific licenses, termed as classes. A Class 1 license (car license) will allow the driving of any vehicle with Gross Laden Weight (GLW) or Gross Combination Weight (GCW) of 6,000 kg (13,000 lb) or less. For other types of vehicles the classes are separately licensed as follows:
Further information on the New Zealand licensing system for heavy vehicles can be found at the New Zealand Transport Agency.
Modern day semi-trailer trucks often operate as a part of a domestic or international transport infrastructure to support containerized cargo shipment.
Various types of rail flat bed train cars are modified to hold the cargo trailer or container with wheels or without. This is called Intermodal or piggyback. The system allows the cargo to switch from highway to railway or vice versa with relative ease by using gantry cranes.
The large trailers pulled by a tractor unit come in many styles, lengths, and shapes. Some common types are: vans, reefers, flatbeds, sidelifts and tankers. These trailers may be refrigerated, heated, ventilated, or pressurized, depending on climate and cargo. Some trailers have movable wheel axles that can be adjusted by moving them on a track underneath the trailer body and securing them in place with large pins. The purpose of this is to help adjust weight distribution over the various axles, to comply with local laws.
This article uses material from the Wikipedia article "Semi-trailer truck", which is released under the Creative Commons Attribution-Share-Alike License 3.0. There is a list of all authors in Wikipedia
Car, Truck,MotorBike, Bicycle, Engine, Racer