Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
Intergraph Standard File Formats (ISFF) are the file formats common to MicroStation and Intergraph's Interactive Graphics Design System (IGDS). ISFF is made available to the public, so that third-party developers could create applications for MicroStation that read and write ISFF format without a license from Intergraph.
MicroStation versions 8 and newer support the V8 DGN file format, but which has a different internal data structure than the ISFF-based DGN. In cases where there is potential for confusion, ISFF-based DGN may be called Intergraph DGN, or V7 DGN.
Autodesk has chosen not to support DGN in AutoCAD 2006, although it does support the format in its Map3D, Land Desktop, and Civil3D products.
This computer-aided design software article is a stub. You can help Wikipedia by expanding it. |
This article uses material from the Wikipedia article "Intergraph Standard File Formats", which is released under the Creative Commons Attribution-Share-Alike License 3.0. There is a list of all authors in Wikipedia
3d,file,format,converter,import,export,translate,material,3dprinting,rendering,threejs,webgl,opengl,.ply,.stl,.obj,.mtl