World Day to Combat Desertification and Drought | |
---|---|
Also called | WDCDD |
Observed by | UN Members |
Celebrations | United Nations |
Date | 17 June |
Next time | 17 June 2019 (2019-06-17) |
Frequency | annual |
The World Day to Combat Desertification and Drought is a United Nations observance each June 17.[1] Its purpose is to raise awareness of the presence of desertification and drought, highlighting methods of preventing desertification and recovering from drought. Each year's global celebration has a unique, novel emphasis that had not been developed previously.
This day was proclaimed by the United Nations General Assembly resolution A/RES/49/115 on January 30, 1995, after the day when United Nations Convention to Combat Desertification is drafted.[2]
The 2030 Agenda for Sustainable Development declares that “we are determined to protect the planet from degradation, including through sustainable consumption and production, sustainably managing its natural resources and taking urgent action on climate change, so that it can support the needs of the present and future generations”. Specifically, SDG Goal 15: Life on Land states the resolve of the United Nations and the SDG signatory nations to halt and reverse land degradation.[3][circular reference][4]
This article uses material from the Wikipedia article "World Day to Combat Desertification and Drought", which is released under the Creative Commons Attribution-Share-Alike License 3.0. There is a list of all authors in Wikipedia
Day Of, celebration,holiday