Licensed under Creative Commons Attribution-Share Alike 3.0 (Papier K).
A bicycle-sharing system, public bicycle system, or bike-share scheme, is a service in which bicycles are made available for shared use to individuals on a short term basis for a price or free. Many bike share systems allow people to borrow a bike from a "dock" and return it at another dock belonging to the same system. Docks are special bike racks that lock the bike, and only release it by computer control. The user enters payment information, and the computer unlocks a bike. The user returns the bike by placing it in the dock, which locks it in place. Other systems are dockless. For many systems, smartphone mapping apps show nearby available bikes and open docks.
The first bike sharing projects were initiated by local community organisations, or as charitable projects intended for the disadvantaged, or to promote bicycles as a non-polluting form of transport, or they were business enterprises to rent out bicycles.
Ernest Callenbach's novel Ecotopia (1975) illustrated the idea. In the utopian novel of a society that does not use fossil fuels, Callenbach describes a bicycle sharing system which is available to inhabitants and is an integrated part of the public transportation system.[1]
The earliest well-known community bicycle program was started in the summer of 1965[2] by Luud Schimmelpennink in association with the group Provo in Amsterdam, the Netherlands.[3][4][2][5] the group Provo painted fifty bicycles white and placed them unlocked in Amsterdam for everyone to use freely.[6] This so-called White Bicycle Plan provided free bicycles that were supposed to be used for one trip and then left for someone else. Within a month, most of the bikes had been stolen and the rest were found in nearby canals.[7] The program is still active in some parts of the Netherlands (the Hoge Veluwe National Park; bikes have to stay inside the park). It originally existed as one in a series of White Plans proposed in the street magazine produced by the anarchist group PROVO. Years later, Schimmelpennink admitted that "the Sixties experiment never existed in the way people believe" and that "no more than about ten bikes" had been put out on the street "as a suggestion of the bigger idea". As the police had temporarily confiscated all of the White Bicycles within a day of their release to the public, the White Bicycle experiment had actually lasted less than one month.[8]
In an attempt to overcome losses from theft, the next innovation adopted by bike sharing programs was the use of so-called 'smart technology'. One of the first 'smart bike' programs was the Grippa™ bike storage rack system used in Portsmouth's Bikeabout scheme.[9][10][11] The Bikeabout scheme was launched in October 1995 by the University of Portsmouth, UK as part of its Green Transport Plan in an effort to cut car travel by staff and students between campus sites.[10] Funded in part by the EU's ENTRANCE[12] program, the Bikeabout scheme was a "smart card" fully automated system.[10][11][13] For a small fee, users were issued 'smart cards' with magnetic stripes to be swiped through an electronic card reader at a covered 'bike store' kiosk, unlocking the bike from its storage rack.[10] CCTV camera surveillance was installed at all bike stations in an effort to limit vandalism.[10] Upon arriving at the destination station, the smart card was used to open a cycle rack and record the bike's safe return.[10] A charge was automatically registered on the user's card if the bike was returned with damage or if the time exceeded the three hour maximum.[10] Implemented with an original budget of approximately £200,000, the Portsmouth Bikeabout scheme was never very successful in terms of rider usage,[14] in part due to the limited number of bike kiosks and hours of operation.[10][13] Seasonal weather restrictions and concerns over unjustified charges for bike damage also imposed barriers to usage.[10] The Bikeabout program was discontinued by the University in 1998 in favor of expanded minibus service; the total costs of the Bikeabout program were never disclosed.[15][16]
In 1995 a system of 300 bicycles using coins to unlock the bicycles in the style of shopping carts was introduced in Copenhagen. It was initiated by Morten Sadolin and Ole Wessung. The idea was developed by both Copenhageners after they were victims of bicycle theft one night in 1989.[17] Copenhagen's ByCylken program was the first large-scale urban bike share program to feature specially designed bikes with parts that could not be used on other bikes. To obtain a bicycle, riders pay a refundable deposit at one of 100 special locking bike stands, and have unlimited use of the bike within a specified 'city bike zone'.[18] The fine for not returning a bicycle or leaving the bike sharing zone exceeds US $150, and is strictly enforced by the Copenhagen police. Originally, the program's founders hoped to completely finance the program by selling advertising space on the bicycles, which was placed on the bike's frame and its solid disc-type wheels. This funding source quickly proved to be insufficient, and the city of Copenhagen took over the administration of the program, funding most of the program costs through appropriations from city revenues along with contributions from corporate donors. Since the City Bikes program is free to the user, there is no return on the capital invested by the municipality, and a considerable amount of public funds must constantly be re-invested to keep the system in service, to enforce regulations, and to replace missing bikes.
One of the first community bicycle projects in the United States was started in Portland, Oregon in 1994 by civic and environmental activists Tom O'Keefe, Joe Keating and Steve Gunther. It took the approach of simply releasing a number of bicycles to the streets for unrestricted use. While Portland's Yellow Bike Project was successful in terms of publicity, it proved unsustainable due to theft and vandalism of the bicycles. The Yellow Bike Project was eventually terminated, and replaced with the Create A Commuter (CAC) program, which provides free secondhand bicycles to certain preselected low-income and disadvantaged people who need a bicycle to get to work or attend job training courses.[19] Since 1994, many community projects around the country have attempted programs similar in nature to the Yellow Bike Project, most of which have since been abandoned.
Bike share technology has evolved over the course of decades, and development of programs in Asia has grown exponentially. Of the world's 15 biggest public bike share programs, 13 are in China. In 2012, the biggest are in Wuhan and Hangzhou, with around 90,000 and 60,000 bikes respectively.[20]
Bike-sharing systems have developed and evolved with society changes and technological improvements. The systems can be grouped into five categories or generations. Many bicycle programmes paint their bicycles in a strong solid colour, such as yellow or white. Painting the bicycles helps to advertise the programme, as well as deter theft (a painted-over bicycle frame is normally less desirable to a buyer). However, theft rates in many bike-sharing programmes remain high, as most shared-use bicycles have value only as basic transport, and may be resold to unsuspecting buyers after being cleaned and repainted. In response, some large-scale bike sharing programmes have designed their own bike using specialised frame designs and other parts to prevent disassembly and resale of stolen parts.
Also known as bicycle rental, bike hire or zero generation. In this system a bicycle can be rented or borrowed from a location and returned to that location. These bicycle renting systems often cater to day-trippers or tourists. This system is also used by cycling schools for potential cyclists who don't have a bicycle. The locations or stations are not automated but are run by employees or volunteers.
Regional programs have been implemented where numerous renting locations are set up at railway stations and at local businesses (usually restaurants, museums and hotels) creating a network of locations where bicycles can be borrowed from and returned (e.g. ZweiRad FreiRad with at times 50 locations [21]). In this kind of network for example a railway station master can allocate a bicycle to a user that then returns it at a different location, for example a hotel. Some such systems require paying a fee, and some do not. Usually the user will be registered or a deposit will be left by the renting facility. The EnCicla Bike Share System in Medellín on its inception in 2011 had 6 staffed locations. It later grew to 32 automatic and 19 staffed stations making it a hybrid between a zero generation and third generation system.
Sometimes known as bike library systems, these bicycles may be lent free of charge, for a refundable deposit, or for a small fee. A bicycle is checked out to one person who will typically keep it for several months, and is encouraged or obliged to lock it between uses. A disadvantage is a lower usage frequency, around three uses per day on average as compared to 2 to 15 uses per day typically experienced with other bike-sharing schemes. Advantages of long-term use include rider familiarity with the bicycle, and constant, instant readiness.
The bicycle can be checked out like a library book, a liability waiver can be collected at check-out, and the bike can be returned any time. For each trip, a Library Bike user can choose the bike instead of a car, thus lowering car usage. The long-term rental system generally results in fewer repair costs to the scheme administrator, as riders are incentivised to obtain minor maintenance in order to keep the bike in running order during the long rental period. Most of the long-term systems implemented to date are funded solely through charitable donations of second-hand bicycles, using unpaid volunteer labour to maintain and administer the bicycle fleet. While reducing or eliminating the need for public funding, such a scheme imposes an outer limit to program expansion. The Arcata Bike Library, in California, has loaned over 4000 bicycles using this system.
Also known as free bikes, unregulated or first generation. In this type of programme the bicycles are simply released into a city or given area for use by anyone. In some cases, such as a university campus, the bicycles are only designated for use within certain boundaries. Users are expected to leave the bike unlocked in a public area once they reach their destination. Depending on the quantity of bicycles in the system availability of such bicycles can suffer because the bikes are not required to be returned to a centralised station. Such a system can also suffer under distribution problems where many bicycles end up in a valley of a city but few are found on the hills of a city. Since parked and unlocked bikes may be taken by another user at any time, the original rider might have to find an alternative transport for the return trip. This system does away with the cost of having a person allocating a vehicle to a user and it is the system with the lowest hemmschwelle or psychological barrier for a potential user. However, bicycle sharing programs without locks, user identification, and security deposits have also historically suffered loss rates from theft and vandalism. Many initiatives have been abandoned after a few years (e.g. Portland's Yellow Bike Project was abandoned after 3 years[22]), while others have been successful for decades (e.g. Austin's Yellow Bike Project active since 1997[23]). Most of these systems are based around volunteer work and are supported by municipalities. Bicycle repair and maintenance are done by a volunteer project or from the municipality contracted operator but also can be, and sometimes is, completed by individual users who find a defect on a free bike.
Also known as Bycykel or as second generation, this system was developed by Morten Sadolin and Ole Wessung of Copenhagen after both were victims of bicycle theft one night in 1989.[24] They envisioned a freely available bicycle sharing system that would encourage spontaneous usage and also reduce bicycle theft. The bicycles, designed for intense utilitarian use with solid rubber tires and wheels with advertising plates, have a slot into which a shopping cart return key can be pushed. A coin (in most versions a 20 DKK or 2 EUR coin) needs to be pushed into the slot to unlock the bike from the station. The bicycle can thus be borrowed free of charge and for an unlimited time and the deposit coin can be retrieved by returning the bicycle to a station again. Since the deposit is a fraction of the bike's cost, and user is not registered this can be vulnerable to theft and vandalism. However, the distinct Bycykel design, well known to the public and to the law authorities does deter misuse to a degree. Implemented systems usually have a zone or area where it is allowed to drive in. The first coin deposit (small) systems were launched in 1991 in Farsø and Grenå, Denmark, and in 1993 in Nakskov, Denmark with 26 bikes and 4 stations. In 1995 the first large-scale 800 bike strong second generation bike-sharing program was launched in Copenhagen as Bycyklen.[25] The system was further introduced in Helsinki (2000-2010) and Vienna in (2002) and in Aarhus[26] 2003.
Also known as docking stations bicycle-sharing, or membership bicycles or third generation consist of bicycles that can be borrowed or rented from a automated station or "docking stations" or "docks" and can be returned at another station belonging to the same system. The docking stations are special bike racks that lock the bike, and only release it by computer control. Individuals registered with the program identify themselves with their membership card (or by a smart card, via cell phone, or other methods) at any of the hubs to check out a bicycle for a short period of time, usually three hours or less. In many schemes the first half-hour is free. In recent years, in an effort to reduce losses from theft and vandalism, many bike-sharing schemes now require a user to provide a monetary deposit or other security, or to become a paid subscriber. The individual is responsible for any damage or loss until the bike is returned to another hub and checked in.
This system was developed as Public Velo by Hellmut Slachta and Paul Brandstätter from 1990 to 1992, and first implemented by the University of Portsmouth and Portsmouth City Council as Bikeabout in 1996 and in Rennes as LE vélo STAR. Since then over 1000 bicycle sharing system of this generation have been launched.[27] The countries with the most dock based systems are Spain (132), Italy (104), and China (79).[6][4] As of June 2014[update], public bike share systems were available in 50 countries on five continents, including 712 cities, operating approximately 806,200 bicycles at 37,500 stations.[28][29] As of May 2011[update], the Wuhan and Hangzhou Public Bicycle bike-share systems in China were the largest in the world, with around 90,000 and 60,000 bicycles respectively.[6] By 2013, China had a combined fleet of 650,000 public bikes.[30]
This bicycle-sharing system saves the labour costs of staffed stations (zero generation), reduces vandalism and theft compared to first and second generation systems by registering users but requires a higher investment for docking stations compared to the fourth generation dockless bikes. The third generations hold an advantage over fourth generation systems by being able to adapted docking stations into E-bike recharging stations for E-bike sharing.[31][32]
Also known as Call a Bike, free floating bike or fourth generation, the dockless bike hire systems consist of a bicycle with a lock that is usually integrated onto the frame and does not require a docking station. The earliest versions of this system consisted of for-rent-bicycles that were locked with combination locks and that could be unlocked by a registered user by calling the vendor to receive the combination to unlock the bicycle. The user would then call the vendor a second time to communicate where the bicycle had been parked and locked. This system was further developed by Deutsche Bahn in 1998 to incorporate a digital authentication codes (that changes) to automatically lock and unlock bikes. Deutsche Bahn launched Call a Bike in 2000, enabling users to unlock via SMS or telephone call, and more recently with an app.[33] Recent technological and operational improvements by telephones and GPSs have paved the way for dramatic increase of this type of private app driven "dockless" bicycle-sharing system. In particular in China, Ofo and Mobike have become the world's largest bike share operators with millions of bikes spread over 100 cities.[34] Today dockless bike shares are designed whereby a user need not return the bike to a kiosk or station; rather, the next user can find it by GPS.[35][36][37] Over 30 private companies have started operating in China.[38][39] However, the rapid growth vastly outpaced immediate demand and overwhelmed Chinese cities, where infrastructure and regulations were not prepared to handle a sudden flood of millions of shared bicycles.[40]
Due to the fact that this system does not require docking stations and thus does not need built infrastructure that may require city planning and building permissions, the system has spread rapidly on a global scale,.[41] At times dockless bike-sharing systems have been criticized as rogue systems instituted without respect for local authorities.[42] In many cities were entrepreneurial companies have independently introduced this bicycle sharing system, adequate parking facilities for bikes are missing, city officials lack regulation experience for this mode of transportation and social habits have not developed either. In some jurisdictions, authorities have confiscated "rogue" dockless bicycles that are improperly parked for potentially blocking pedestrian traffic on sidewalks[43] and in other cases new laws have been introduced to regulate the shared bikes.
In some cities Deutsche Bahn's Call a Bike has Call a Bike fix system, which has fixed docking stations versus the flex dockless version, some systems are combined into a hybrid of third and fourth generation systems. Some Nextbike systems are also a 3rd and 4th generation hybrid. With the arrival of dockless bike shares, there are now over 70 private dockless bikeshares operating a combined fleet of 16 million sharebikes according to estimates of Ministry of Transport of China.[44][45] Beijing alone has 2.35 million sharebikes from 15 companies.[46]
In the United States, many major metropolitan areas are experimenting with dockless bikeshare systems, which have been popular with commuters but subject to complaints about illegal parking.[47]
The reasons and goals of Bike-sharing vary but can be grouped into the following Most large-scale urban bike sharing programmes utilise numerous bike check-out stations, and operate much like public transit systems, catering to tourists and visitors as well as local residents. Their central concept is to provide free or affordable access to bicycles for short-distance trips in an urban area as an alternative to motorised public transport or private vehicles, thereby reducing congestion, noise, and air pollution. Bicycle-sharing systems have also been cited as a way to solve the "last mile" problem and connect users to public transit networks.[48]
People use bike-share for various reasons. Some who would otherwise use their own bicycle have concerns about theft or vandalism, parking or storage, and maintenance.[49][50] However, dock systems, serving only stations, resemble public transit, and have therefore been criticized as less convenient than a privately owned bicycle used door-to-door.[51]
Bicycle-sharing systems are an economic good, and are generally classified as a private good due to their excludable and rivalrous nature. While some bicycle-sharing systems are free, most require some user fee or subscription, thus excluding the good to paying consumers. Bicycle-sharing systems also provide a discrete and limited number of bikes, whose distribution can vary throughout a city. One person's usage of the good diminishes the ability of others to use the same good. Nonetheless, the hope of many cities is to partner with bike-share companies to provide something close to a public good.[52] Public good status may be achieved if the service is free to consumers and there are a sufficient number of bicycles such that one person's usage does not encroach upon another's use of the good.
In a national-level programme that combines a typical rental system with several of the above system types, a passenger railway operator or infrastructure manager partners with a national cycling organisation and others to create a system closely connected with public transport. These programmes usually allow for a longer rental time of up to 24 or 48 hours, as well as tourists and round trips. In some German cities the national rail company offers a bike rental service called Call a Bike.
In Guangzhou, China, the privately operated Guangzhou Bus Rapid Transit system includes cycle lanes, and a public bicycle system.[53]
In some cases, like Santander Cycles in London, the bicycle sharing system is owned by the public transport authority itself.
In other cases, like EnCicla in the city of Medellin (Colombia, South America), the Bicycle Sharing System is connected to other modes of transportation, such as the Metro.[54]
Some car park operators such as Vinci Park in France lend bikes to their customers who park a car.[55]
City CarShare, a San Francisco-based non-profit, received a federal grant in 2012 to integrate electric bicycles within its existing car-sharing fleet. The program is set to launch before the end of 2012 with 45 bikes.[56] [needs update]
The financing of bicycle-sharing system have been maintained by a combination of fees, volunteer, charity, advertisements, business interest groups and government subsidies. The international expansion dockless bicycles in mid 2010s has been financed by investment capital.
User rent fees may range from the equivalent of US$0.50 to 30.00 per day, rent fees for 15- or 20-minute intervals can range from a few cents to 1.00. Many bike-share systems offer subscriptions that make the first 30–45 minutes of use either free or very inexpensive, encouraging use as transportation. This allows each bike to serve several users per day but reduces revenue. Monthly or yearly membership subscriptions and initial registration fees may apply. To reduce losses from theft often users are required to commit to temporary deposit via a credit card or debit card. If the bike is not returned within the subscription period, or returned with significant damage, the bike sharing operator keeps the deposit or withdraws money from the user's credit card account. operated by private companies as is the case in most cities in China.[57]
US
New York rental rates are among the highest in the world, as far as we know.[citation needed] The cost of annual membership in the US varies between $100 and $160.[citation needed]
Europe
Bike riders shared in Europe usually pay between € 0.50 to €1 per trip, and an average of € 10-12 for a full day cycling.
Many first and second generation bicycle sharing programs were and are community run organisations as "Community Bike programmes", as done in IIT Bombay. Often maintenance and repair is performed by unpaid volunteers that complete this work in their own free time.
Charity fundraising drives and charitable organisations have and do support bicycle sharing programs, including Rotary Clubs and Lions Clubs.
Second and third generation schemes in the 90s already prominently included advertising opportunities on the individual bikes in form of advertisement areas on the wheels or frame. Other schemes are completely branded according to a sponsor, notable example London's bike share which was originally branded and sponsored by Barclays Bank and subsequently by Santander UK Several European cities, including the French cities of Lyon and Paris as well as London, Barcelona, Stockholm and Oslo, have signed contracts with private advertising agencies (JCDecaux in Brussels, Lyon, Paris, Seville, Dublin and Oslo; Clear Channel in Stockholm, Barcelona, Antwerp, Perpignan and Zaragoza) which supply the city with thousands of bicycles free of charge (or for a minor fee). In return, the agencies are allowed to advertise both on the bikes themselves and in other select locations in the city. typically in the form of advertising on stations or the bicycles themselves.
Municipalities have operated and do operate bicycle share systems as a public service, paying for the initial investment, maintenance and operations if it is not covered by other revenue sources. Governments can also supported bicycle share programs in forms of one time grants (often to buy a set of bicycles), yearly of monthly subsidies, or by paying part of the employee wages (example in repair workshops that employee long-term unemployed persons). Many of the membership-based systems are operated through public-private partnerships. Some schemes may be financed as a part of the public transportation system (for example Smoove). In Melbourne the government subsidises the sale of bicycle helmets[58] to enable spontaneous cyclists comply with the mandatory helmet laws.
GPS traceable vehicle commute patterns and usage habits present valuable data for government agencies, marketing companies or researchers. Strong commuter patterns can be filtered out and potential transportation services (e.g. commuter bus) can be tailored to existing demand. Potential audiences can be better assessed and understood.
Another advantage of bike-sharing systems is that the smart-cards allow the bicycles to be returned to any station in the system, which facilitates one-way rides to work, education or shopping centres. Thus, one bike may take 10–15 rides a day with different users and can be ridden up to 10,000 km (6,200 mi) a year (citing Lyon, France). Each bike has at least one of these rides with one unique user per day which indicates that in 2014 there were a minimum of at least 294 million unique bike share cyclists worldwide (806,200 bicycles x 365) although common sense indicates that this figure may be a very small estimate of the true number of bike share users.[59]
It was found—in cities like Paris and Copenhagen—that to have a major impact there had to be a high density of available bikes. Copenhagen has 2500 bikes which cannot be used outside the 9 km2 (3.5 sq mi) zone of the city centre (a fine of DKr 1000 applies to any user taking bikes across the canal bridges around the periphery). Since Paris's Vélib' programme operates with an increasing fee past the free first half-hour, users have a strong disincentive to take the bicycles out of the city centre. The distance between stations is only 300–400 metres (1,000–1,300 ft) in inner city areas.
in US, bike sharing is still a male-dominated space where male users made up for more than 80% of total trips made in 2017.
A study published in 2015 in the journal Transportation concludes that bike sharing systems can be grouped into behaviourally similar categories based upon their size.[61] Cluster analysis shows that larger systems display greater behavioural heterogeneity amongst their stations, and smaller systems generally have stations which all behave similarly in terms of their daily utilisation patterns.
Bike-share programs generate a number of economic externalities, both positive and negative. The positive externalities include reduction of traffic congestion and pollution, while the negative externalities include degradation of urban aesthetic environment and reduction of parking. Furthermore, bike-share programs have pecuniary effects. Some of these economic externalities (e.g. reduced congestion) can be systematically evaluated using empirical data, and therefore may be internalized through government subsidy. On the other hand, "nuisance" externalities (e.g. street and sidewalk clutter) are more subjective and harder to quantify, and may not be able to be internalized.
A primary goal of bicycle-sharing systems has been to reduce traffic congestion, particularly in large urban areas. Some empirical evidence indicates that this goal has been achieved to varying degrees in different cities. A 2015 article in Transport Reviews examined bike-share systems in five cities, including Washington, D.C. and Minneapolis. The article found that in D.C., individuals substituted bike-share rides for automobile trips 8 percent of the time, and almost 20 percent of the time in Minneapolis.[62] A separate study on Washington, D.C.'s Capital Bikeshare found that the bike-share program contributed a 2 to 3 percent reduction in traffic congestion within the evaluated neighborhood.[63] 2017 studies in Beijing and Shanghai have linked the massive increase of dockless bike shares to the decrease in the number of private automobile trips that are less than five kilometres.[64] In Guangzhou, the arrival of dockless bike shares had a positive impact in the growth of cycling modeshare.[65]
Not only do bike-share systems intend to reduce traffic congestion, they also aim to reduce air pollution through decreased automobile usage, and indrectly through the reduction of congestion. The study on D.C.'s Capital Bikeshare estimated that the reduction in traffic congestion would be equivalent to roughly $1.28 million in annual benefits, accrued through the reduction in congestion-induced CO2 emissions.[63] A separate study of transportation in Australia estimated that 1.5 kilograms of CO2 equivalent emissions are avoided by an urban resident who travels 5 kilometers by cycling rather than by car during rush hour periods.[66]
Healthy Transport
Beside the people who ride without a helmet and injure their head, bicycle-sharing systems has a positive health effects to people overall.[67] Cycling is a good way for exercise and stress relief. It can increase recreation and improve sociability of a city, which make people live more happy and relax. The report from Centers for Disease Control and Prevention (CDC) point out that cycling also help preventing disease like obesity, heart disease (can reduce up to 82%) and diabetes (can reduce up to 58%). Therefore, bicycle-sharing systems has a positive effect on metal and physical health, which attract more people to use. (Demand increase)[68]
Bike-share programs, especially the earlier services that required docking areas along urban streets, may encroach upon the space available for on-street car parking. Reduced car parking is therefore a negative externality, which is off-set by six to eight bikes fitting into one car park. As bike-share companies have transitioned into dockless programs, this effect may have been reduced.
In some cities, the many dockless bike-share bicycles have cluttered streets and sidewalks, degrading the urban aesthetic environment and blocking pedestrian traffic. In particular, cycles on Chinese city streets have created sections of clogged sidewalks no longer walkable, and piles of illegally parked bicycles.[69]
Due to the vehicles being left in the public right of way, or abandoned obstructing pedestrians, the dockless vehicles have been called "litter bikes".[70]
As bicycle-sharing systems continue to grow and provide an affordable alternative for commuters, the relatively low price of these services may induce competitors to offer lower prices. For instance, municipal public transit organizations may lower prices for buses or subways to continue to compete with bike-share systems. Pecuniary effects may even extend to bicycle manufacturers and retailers, where these producers might reduce prices of bicycles and other complementary goods (e.g. helmets, lights). However, empirical research is needed to test these hypotheses.
Safety
As most of the dockless bikes system do not provide helmet for riders, the proportion of head injuries that related to bicycle increased.[71] Without providing a helmet with the bikes, it increases the risk of using the bicycle-sharing system, even the bicycle companies encourage rider to prepare one.[72] "Safety first." In order to transport from one place to the other, people will pick the fastest and safest way to travel. Therefore, the risk of injury might decrease the number of people who use the bicycle-sharing system, which cause a decrease in demand.
In public economics, there is a role for government intervention in a market if market failures exist, or in the case of redistribution. As several studies have found, bike-share programs appear to produce net positive externalities in reduced traffic congestion and pollution, for example.[73][63] The bike-sharing market does not produce at the social optimum, justifying the need for government intervention in the form of a subsidy for the provision of this good in order to internalize the positive externality. Many cities have adopted public-private partnerships to provide bike-shares, such as in Washington, D.C. with Capital Bikeshares.[74] These partially government-funded programs may serve to better provide the good of bike-shares.
Many bike-share companies and public-private partnerships aim to supply shared bicycles as a public good. In order for bike-shares to be a public good, they must be both non-excludable and non-rival. Numerous bike-share programs already offer their services partly for free or at least at very low prices, therefore nearing the non-excludable requirement.[18] However, in order to achieve the non-rival requirement, shared bicycles must be supplied at a certain density within an urban area. There are numerous challenges with attaining non-rivalry, for instance, redistribution of bicycles from low-demand regions to regions with high-demand.[75] Mobike, a China-based company, is attempting to solve this problem by paying their users to ride their bikes from low-demand areas to high-demand areas.[76] Other companies such as OBike have introduced a points system to penalize negative behavior, namely, illegal parking of shared bicycles.[77] Economists speculate that a combination of efficient pricing with well-designed regulatory policies could significantly mitigate problems of over-supply and clutter.[78]
The Chinese bicycle-sharing market demonstrated the danger of oversupply in 2018. Companies took advantage of unclear regulations in the preceding years to introduce millions of shared bikes to the country's cities. Users were not educated in how to use the systems properly and in many cases treated them as disposable, parking them anywhere. City governments were forced to impound the abandoned bikes when they blocked public thoroughfares, and millions of bikes went directly to junkyards after the companies that owned them went bankrupt.[79][80]
A study published in the American Journal of Public Health reports observing[73] an increase in cycling and health benefits where bicycle sharing systems are run. In the United States, bikesharing programs have proliferated in recent years, but collision and injury rates for bikesharing are lower than previously computed rates for personal bicycling; at least two people have been killed while using a bike share scheme.[81][82][83]
There is also considerable evidence that bike-share programs must be adopted in tandem with city infrastructure, namely, the creation of bike lanes. A 2012 study published in the American Journal of Public Health found that Toronto’s cyclists were 30-50% more likely to be involved in an accident on major roads without cycle lanes than on those with.[84]
Despite their theoretical and observed benefits, bike-share programs have come under attack as their presence has grown throughout the world. Much of this criticism has focused on the use of public funding - concerned critics posit that the use of tax dollars for bike-share programs should instead be diverted towards building or maintaining roads and other services that more residents use on a daily basis.[85] However, this argument relies on a faulty assumption that taxpayer money is a significant source of bike-share funding. An analysis by People for Bikes, an organization that advocates for new and safe bike infrastructure, found that public investment in Salt Lake City’s Greenbike and Denver's B-Cycle programs was significantly less than traditional public transit (e.g. bus or rail) in those same cities, on a per-trip basis. Both Greenbike and B-Cycle's publicly funded subsidies amount to 10 percent or less of the total cost of one trip.[86] In contrast, Salt Lake City's’s bus and rail system (UTA) relies on 80 percent public funding for a single trip.[86]
Other critics claim that bike-share programs fail to reach more low-income communities.[87] Some efforts have attempted to address this issue, such as New York City's Citi Bike's discounted membership program, which is aimed at increasing ridership among low-income residents. However, around 80 percent of study respondents reported that they had no knowledge of the program's discount.[87]
This article uses material from the Wikipedia article "Bicycle-sharing system", which is released under the Creative Commons Attribution-Share-Alike License 3.0. There is a list of all authors in Wikipedia
Car, Truck,MotorBike, Bicycle, Engine, Racer