powered by CADENAS

Social Share

MeshLab (3909 views - 3D Printing Dictionary)

MeshLab is an advanced 3D mesh processing software system that is oriented to the management and processing of unstructured large meshes and provides a set of tools for editing, cleaning, healing, inspecting, rendering, and converting these kinds of meshes. MeshLab is free and open-source software, subject to the requirements of the GNU General Public License (GPL), version 2 or later, and is used as both a complete package and a library powering other software. It is well known in the more technical fields of 3D development and data handling. MeshLab is developed by the ISTI - CNR research center; initially MeshLab was created as a course assignment at the University of Pisa in late 2005. It is a general-purpose system aimed at the processing of the typical not-so-small unstructured 3D models that arise in the 3D scanning pipeline. The automatic mesh cleaning filters includes removal of duplicated, unreferenced vertices, non-manifold edges, vertices, and null faces. Remeshing tools support high quality simplification based on quadric error measure, various kinds of subdivision surfaces, and two surface reconstruction algorithms from point clouds based on the ball-pivoting technique and on the Poisson surface reconstruction approach. For the removal of noise, usually present in acquired surfaces, MeshLab supports various kinds of smoothing filters and tools for curvature analysis and visualisation. It includes a tool for the registration of multiple range maps based on the iterative closest point algorithm. MeshLab also includes an interactive direct paint-on-mesh system that allows to interactively change the color of a mesh, to define selections and to directly smooth out noise and small features. MeshLab is available for most platforms, including Windows, Linux, Mac OS X, and, with reduced functionality, on iOS and Android and even as a pure client-side JavaScript application called MeshLabJS. The system supports input/output in the following formats: PLY, STL, OFF, OBJ, 3DS, VRML 2.0, U3D, X3D and COLLADA. MeshLab can also import point clouds reconstructed using Photosynth. MeshLab is used in various academic and research contexts, like microbiology, cultural heritage, surface reconstruction, paleontology, for rapid prototyping in orthopedic surgery, in orthodontics, and desktop manufacturing.
Go to Article

MeshLab

MeshLab

MeshLab

Licensed under GNU General Public License (The original uploader was ALoopingIcon at English Wikipedia).

MeshLab
MeshLab 1.2.1
Developer(s) ISTI - CNR
Stable release
2016.12 / December 23, 2016; 7 months ago (2016-12-23)[1]
Written in C++, JavaScript
Operating system Cross-platform
Type Graphics software
License GPL
Website www.meshlab.net
www.meshlabjs.net

MeshLab is an advanced 3D mesh processing software system that is oriented to the management and processing of unstructured large meshes and provides a set of tools for editing, cleaning, healing, inspecting, rendering, and converting these kinds of meshes. MeshLab is free and open-source software, subject to the requirements of the GNU General Public License (GPL), version 2 or later, and is used as both a complete package and a library powering other software. It is well known in the more technical fields of 3D development and data handling.

MeshLab is developed by the ISTI - CNR research center; initially MeshLab was created as a course assignment at the University of Pisa in late 2005. It is a general-purpose system aimed at the processing of the typical not-so-small unstructured 3D models that arise in the 3D scanning pipeline.

The automatic mesh cleaning filters includes removal of duplicated, unreferenced vertices, non-manifold edges, vertices, and null faces. Remeshing tools support high quality simplification based on quadric error measure, various kinds of subdivision surfaces, and two surface reconstruction algorithms from point clouds based on the ball-pivoting technique and on the Poisson surface reconstruction approach. For the removal of noise, usually present in acquired surfaces, MeshLab supports various kinds of smoothing filters and tools for curvature analysis and visualisation.

It includes a tool for the registration of multiple range maps based on the iterative closest point algorithm. MeshLab also includes an interactive direct paint-on-mesh system that allows to interactively change the color of a mesh, to define selections and to directly smooth out noise and small features.

MeshLab is available for most platforms, including Windows, Linux, Mac OS X, and, with reduced functionality, on iOS and Android and even as a pure client-side JavaScript application called MeshLabJS. The system supports input/output in the following formats: PLY, STL, OFF, OBJ, 3DS, VRML 2.0, U3D, X3D and COLLADA. MeshLab can also import point clouds reconstructed using Photosynth.

MeshLab is used in various academic and research contexts, like microbiology,[2] cultural heritage,[3] surface reconstruction,[4] paleontology,[5] for rapid prototyping in orthopedic surgery,[6] in orthodontics,[7] and desktop manufacturing.[8]

Additional images

See also



This article uses material from the Wikipedia article "MeshLab", which is released under the Creative Commons Attribution-Share-Alike License 3.0. There is a list of all authors in Wikipedia

3D Printing Dictionary

OpenLAB, Fablab, OpenSCAD, FreeCAD, BRL-CAD, RhinocerosCAD, LibreCAD, Vectary, 123D, TinkerCAD, Wings 3D, MOI3D, leapfrog 3D, Geomagic, Paint3D, STLfinder, Yeggi, Yobi3D, 3D Shape Search, PARTcloud, Thingiverse, GrabCAD, AMF, Additive Manufacturing, STL, Stereolitography, Mesh, MeshMixer, Free Download, lowpoly, 3D voxel,things, digital design, physical objects, rapid prototyping, 3D objects, 3D printing, reprap, fabrication, laser cutter,abs