powered by CADENAS

Social Share

Amazon

Harbor (3034 views - Transportation - Air Water Earth)

A harbor or harbour (see spelling differences; synonyms: wharves, haven) is a sheltered body of water where ships, boats, and barges can be docked. The term harbor is often used interchangeably with port, which is a man-made facility built for loading and unloading vessels and dropping off and picking up passengers. Ports usually include one or more harbors. Alexandria Port in Egypt is an example of a port with two harbors. Harbors may be natural or artificial. An artificial harbor can have deliberately constructed breakwaters, sea walls, or jettys or they can be constructed by dredging, which requires maintenance by further periodic dredging. An example of an artificial harbor is Long Beach Harbor, California, United States, which was an array of salt marshes and tidal flats too shallow for modern merchant ships before it was first dredged in the early 20th century. In contrast, a natural harbor is surrounded on several sides by prominences of land. Examples of natural harbors include Sydney Harbour, Australia and Trincomalee Harbour in Sri Lanka.
Go to Article

Explanation by Hotspot Model

Youtube


    

Harbor

Harbor

A harbor or harbour (see spelling differences; synonyms: wharves, haven) is a sheltered body of water where ships, boats, and barges can be docked. The term harbor is often used interchangeably with port, which is a man-made facility built for loading and unloading vessels and dropping off and picking up passengers. Ports usually include one or more harbors. Alexandria Port in Egypt is an example of a port with two harbors.

Harbors may be natural or artificial. An artificial harbor can have deliberately constructed breakwaters, sea walls, or jettys or they can be constructed by dredging, which requires maintenance by further periodic dredging. An example of an artificial harbor is Long Beach Harbor, California, United States, which was an array of salt marshes and tidal flats too shallow for modern merchant ships before it was first dredged in the early 20th century.[1] In contrast, a natural harbor is surrounded on several sides by prominences of land. Examples of natural harbors include Sydney Harbour, Australia and Trincomalee Harbour in Sri Lanka.

Artificial harbors

Artificial harbors are frequently built for use as ports. The oldest artificial harbor known is the Ancient Egyptian site at Wadi al-Jarf, on the Red Sea coast, which is at least 4500 years old (ca. 2600-2550 BC, reign of King Khufu). The largest artificially created harbor is Jebel Ali in Dubai.[2] Other large and busy artificial harbors include:

The Ancient Carthaginians constructed fortified, artificial harbors called cothons.

Natural harbors

A natural harbor is a landform where a part of a body of water is protected and deep enough to furnish anchorage. Many such harbors are rias. Natural harbors have long been of great strategic naval and economic importance, and many great cities of the world are located on them. Having a protected harbor reduces or eliminates the need for breakwaters as it will result in calmer waves inside the harbor. Some examples are:

Ice-free harbors

For harbors near the North and South Poles, being ice-free is an important advantage, especially when it is year-round. Examples of these include:

The world's southmost harbor, located at Antarctica's Winter Quarters Bay (77° 50′ South), is sometimes ice-free, depending on the summertime pack ice conditions.[3]

Important harbors

Although the world's busiest port is a hotly contested title, in 2006 the world's busiest harbor by cargo tonnage was the Port of Shanghai.[7][needs update]

The following are large natural harbors:

See also



This article uses material from the Wikipedia article "Harbor", which is released under the Creative Commons Attribution-Share-Alike License 3.0. There is a list of all authors in Wikipedia

Transportation - Air Water Earth

3D,CAD,Model,Libary,Railway, Train, Ship, Marine, Submarine, Automotive, Locomotive, Bike, Car, Formula 1, Space, Aircraft, Aerospace, Satelite, Automobile, Yacht