powered by CADENAS

Social Share

Amazon

Maritime pilot (4162 views - Transportation - Air Water Earth)

A maritime pilot, marine pilot, harbor pilot, bar pilot, or simply pilot, is a sailor who maneuvers ships through dangerous or congested waters, such as harbors or river mouths. They are navigational experts possessing knowledge of the particular waterway such as its depth, currents, and hazards.
Go to Article

Explanation by Hotspot Model

Youtube


    

Maritime pilot

Maritime pilot

Maritime pilot

A maritime pilot, marine pilot, harbor pilot, bar pilot, or simply pilot, is a sailor who maneuvers ships through dangerous or congested waters, such as harbors or river mouths. They are navigational experts possessing knowledge of the particular waterway such as its depth, currents, and hazards.

History

A pilot boarding a ship from a pilot boat while underway

The word pilot probably came from Middle French pilot, pillot, from Italian pilota, from Late Latin pillottus; perhaps ultimately from Ancient Greek πηδόν (pēdón, "blade of an oar, oar").[citation needed]

The work functions of the pilot go back to Ancient Greece and Roman times, when locally experienced harbour captains, mainly local fishermen, were employed by incoming ships' captains to bring their trading vessels into port safely.[citation needed] Eventually, because the act of pilotage needed to be regulated and to ensure that pilots had adequate insurance, the harbours licensed pilots.[citation needed] The California Board of Pilot Commissioners was the first government agency created by California's legislature, in 1850.[citation needed]

Before harbour boards were established, pilots known as hobblers would compete with one another. The first to reach an incoming ship would navigate it to the docks and receive payment.[1] In Dún Laoghaire, Ireland, there is a monument to the hobblers who lost their lives.[2] In Kent they were known as "hovellers" and worked alongside and in competition with the licensed pilots, but were sometimes blamed as wreckers.[3] George Byng Gattie defends the hovellers or "hobilers" as lifesavers in his 1890 book about the Goodwin Sands.[4]

Pilots had to have quick transport to get from the port to the incoming ships. They initially used their own fishing boats to reach the incoming vessels, but these were heavy working boats, which led to the development of the specialised pilot boat.

Joseph Henderson was an early American harbor pilot who was a Sandy Hook pilot for the New York Harbor and along the East Coast of the United States during the American Civil War.

In the inland brown water trade another type of pilots are known as trip pilots. Due to the shortage of qualified posted masters these independent contractors fill the holes in the manning schedule on inland push boats on various inland river routes.[citation needed]

Duties involved

In English law, Section 742 of the Merchant Shipping Act 1894 defines a pilot as "any person not belonging to a ship who has the conduct thereof." In other words, someone other than a member of the crew who has control over the speed, direction, and movement of the ship. The Pilotage Act 1987 governs the management of maritime pilots and pilotage in harbors in the United Kingdom.[citation needed]

Pilots may be required to have prior maritime experience prior to becoming a pilot. For example, the California Board of Pilot Commissioners requires that pilot trainees must have a master's license, two years command experience on tugs or deep draft vessels, and pass a written exam and simulator exercise, followed by a period of up to three years training gaining experience with different types of vessel and docking facilities. Following licensing, pilots are required to engage in continuing educational programs.[5]

Normally, the pilot joins an incoming ship prior to the ship's entry into the shallow water at the designated "pilot boarding area" via helicopter or pilot boat and climbs a pilot ladder sometimes up to 40 feet (~12 metres) to the deck of the largest container and tanker ships. Climbing the pilot ladder can be dangerous, even more so in rough seas considering that both the ship to be piloted and the pilot's own vessel are usually moving. With outgoing vessels, a pilot boat returns the pilot to land after the ship has successfully negotiated coastal waters.[6]

Pilots are required by law in most major sea ports of the world for large ships.[citation needed] Pilots specifically use pilotage techniques relying on nearby visual reference points and local knowledge of tides, swells, currents, depths and shoals that might not be readily identifiable on nautical charts without first hand experience in the waters in question.[citation needed]

Legally, the master has full responsibility for safe navigation of their vessel, even if a pilot is on board. If they have clear grounds that the pilot may jeopardize the safety of navigation, they can relieve the pilot from their duties and ask for another pilot or, if not compulsory to have a pilot on board, navigate the vessel without one. In every case, during the time passed aboard for operation, the pilot will remain under the master's authority, and always out of "ship's command chain". The pilot remains aboard as an important and indispensable consultant of the master.[citation needed] Only in transit of the Panama Canal and in Canada does the pilot have the full responsibility for the navigation of the vessel.[citation needed]

However, in some countries, deck officers of vessels who have strong local knowledge and experience of navigating in those ports, such as a ferry, may be issued with a pilotage exemption certificate, which relieves them of the need to take a pilot on board.[7][8]

Compensation

The Florida Alliance of Maritime Organizations reported that Florida pilots salaries range from US$100,000 to US$400,000 annually. This was similar to other US states with large ports.[9] Columbia Bar pilots earn about US$180,000 per year.[10] A 2008 review of pilot salary in the United States showed that pay ranged from about US$250,000 to over US$500,000 per year.[11]

Pilot compensation has been controversial in many ports, including Los Angeles and Long Beach, California, especially regarding pilots who are employed by public agencies instead of acting as independent contractors.[12][13]

Compensation varies in other nations. In New Zealand, according to the government career service, pilots earn NZ$90,000-120,000.[14]

In popular culture

See also



This article uses material from the Wikipedia article "Maritime pilot", which is released under the Creative Commons Attribution-Share-Alike License 3.0. There is a list of all authors in Wikipedia

Transportation - Air Water Earth

3D,CAD,Model,Libary,Railway, Train, Ship, Marine, Submarine, Automotive, Locomotive, Bike, Car, Formula 1, Space, Aircraft, Aerospace, Satelite, Automobile, Yacht