Highest governing body | Fédération Aéronautique Internationale |
---|---|
Characteristics | |
Contact | No |
Mixed gender | Yes |
Presence | |
Country or region | Worldwide |
Olympic | No |
World Games | 1997 – 2017 |
The term air sports covers a range of aerial activities such as:
The sports inserted above are governed internationally by Fédération Aéronautique Internationale and at the national level by aero clubs such as the National Aeronautics Association and the Royal Aero Club. The FAI web site contains lists of these national organizations. In some of the categories listed above are lightweight classes which can be alternatively grouped as Ultralight aviation.
Other aerial activities are not governed by the FAI rules
This article uses material from the Wikipedia article "Air sports", which is released under the Creative Commons Attribution-Share-Alike License 3.0. There is a list of all authors in Wikipedia
Entertainment