powered by CADENAS

Social Share

Amazon

Oboe (14239 views - Music)

Oboes ( OH-boh) belong to the classification of double reed woodwind instruments. Oboes are usually made of wood, but there are also oboes made of synthetic materials. The most common oboe plays in the treble or soprano range. A soprano oboe measures roughly 65 cm (25 1⁄2 in) long, with metal keys, a conical bore and a flared bell. Sound is produced by blowing into the reed at a sufficient air pressure, causing it to vibrate with the air column. The distinctive tone is versatile and has been described as "bright". When the word oboe is used alone, it is generally taken to mean the treble instrument rather than other instruments of the family, such as the bass oboe, the cor anglais (English horn), or oboe d'amore A musician who plays the oboe is called an oboist. Today, the oboe is commonly used in concert bands, orchestras, chamber music, film music, some genres of folk music, and as a solo instrument, and occasionally heard in jazz, rock, pop, and popular music.
Go to Article

Explanation by Hotspot Model

Youtube


    

Oboe

Oboe

Oboe
An oboe
Woodwind instrument
Classification
Hornbostel–Sachs classification422.112-71
(Double-reeded aerophone with keys)
DevelopedMid 17th century from the shawm
Playing range
Related instruments

Oboes (/ˈb/ OH-boh) belong to the classification of double reed woodwind instruments. Oboes are usually made of wood, but there are also oboes made of synthetic materials. The most common oboe plays in the treble or soprano range. A soprano oboe measures roughly 65 cm (25 12 in) long, with metal keys, a conical bore and a flared bell. Sound is produced by blowing into the reed at a sufficient air pressure, causing it to vibrate with the air column.[1] The distinctive tone is versatile and has been described as "bright".[2] When the word oboe is used alone, it is generally taken to mean the treble instrument rather than other instruments of the family, such as the bass oboe, the cor anglais (English horn), or oboe d'amore

A musician who plays the oboe is called an oboist.

Today, the oboe is commonly used in concert bands, orchestras, chamber music, film music, some genres of folk music, and as a solo instrument, and occasionally heard in jazz, rock, pop, and popular music.

Sound

An oboe reed

In comparison to other modern woodwind instruments, the treble oboe is sometimes referred to as having a clear and penetrating voice. The Sprightly Companion, an instruction book published by Henry Playford in 1695, describes the oboe as "Majestical and Stately, and not much Inferior to the Trumpet." In the play Angels in America the sound is described as like "that of a duck if the duck were a songbird".[3] The rich timbre is derived from its conical bore (as opposed to the generally cylindrical bore of flutes and clarinets). As a result, oboes are easier to hear over other instruments in large ensembles due to its penetrating sound.[4] The highest note is a semitone lower than the nominally highest note of the B clarinet. Since the clarinet has a wider range, the lowest note of the B clarinet is significantly deeper (a minor sixth) than the lowest note of the oboe.[5]

Music for the standard oboe is written in concert pitch (i.e., it is not a transposing instrument), and the instrument has a soprano range, usually from B3 to G6. Orchestras tune to a concert A played by the first oboe.[6] According to the League of American Orchestras, this is done because the pitch is secure and its penetrating sound makes it ideal for tuning.[7] The pitch of the oboe is affected by the way in which the reed is made. The reed has a significant effect on the sound. Variations in cane and other construction materials, the age of the reed, and differences in scrape and length all affect the pitch. German and French reeds, for instance, differ in many ways, causing the sound to vary accordingly. Weather conditions such as temperature and humidity also affect the pitch. Skilled oboists adjust their embouchure to compensate for these factors. Subtle manipulation of embouchure and air pressure allows the oboist to express timbre and dynamics.

Reeds

Most professional oboists make their reeds to suit their individual needs. By making their reeds, oboists can precisely control factors such as tone color, intonation, and responsiveness.

Occasionally, novice oboists may begin with a Fibrecane reed, which is made of a synthetic material. Commercially available cane reeds are available in several degrees of hardness; a medium reed is very popular, and most beginners use medium-soft reeds. These reeds, like clarinet, saxophone, and bassoon reeds, are made from Arundo donax. As oboists gain more experience, they may start making their own reeds after the model of their teacher or buying handmade reeds (usually from a professional oboist) and using special tools including gougers, pre-gougers, guillotines, knives, and other tools to make the reed to their liking. [8] According to the late John Mack, former principal oboist of the Cleveland Orchestra, an oboe student must fill a laundry basket with finished reeds in order to master the art.[9] "Making good reeds requires years of practice, and the amateur is often well advised not to embark on making his own reeds, ... Orchestral musicians sometimes do this [make reeds], and co-principals in particular often earn a bit on the side in this way. ... Many professional musicians import their reed cane ... directly from the growers in southern France and split it vertically into three parts themselves. Oboes require thicknesses of about 10 millimeters."[citation needed] This allows each oboist to adjust the reeds precisely for individual embouchure, oral cavity, oboe angle, and air support. The reed is considered the part of oboe playing that makes it so difficult because slight variations in temperature, altitude, weather, and climate will change a perfectly working reed into an unplayable collection of cane.

History

In English, prior to 1770, the standard instrument was called a "hautbois", "hoboy", or "French hoboy" (/ˈhbɔɪ/ HOH-boy; borrowed from the French name, a compound word made of haut ["high", "loud"] and bois ["wood", "woodwind"]).[10] The spelling of oboe was adopted into English c. 1770 from the Italian oboè, a transliteration of the 17th-century pronunciation of the French name.

The regular oboe first appeared in the mid-17th century, when it was called a hautbois. This name was also used for its predecessor, the shawm, from which the basic form of the hautbois was derived.[11] Major differences between the two instruments include the division of the hautbois into three sections, or joints (which allowed for more precise manufacture), and the elimination of the pirouette, the wooden ledge below the reed which allowed players to rest their lips.

The exact date and place of origin of the hautbois are obscure, as are the individuals who were responsible. Circumstantial evidence, such as the statement by the flautist composer Michel de la Barre in his Memoire, points to members of the Philidor (Filidor) and Hotteterre families. The instrument may in fact have had multiple inventors.[12] The hautbois quickly spread throughout Europe, including Great Britain, where it was called "hautboy", "hoboy", "hautboit", "howboye", and similar variants of the French name.[13] It was the main melody instrument in early military bands, until it was succeeded by the clarinet.[14]

The standard Baroque oboe is generally made of boxwood and has three keys: a "great" key and two side keys (the side key is often doubled to facilitate use of either the right or left hand on the bottom holes). In order to produce higher pitches, the player has to "overblow", or increase the air stream to reach the next harmonic. Notable oboe-makers of the period are the Germans Jacob Denner and J.H. Eichentopf, and the English Thomas Stanesby (died 1734) and his son Thomas Jr (died 1754). The range for the Baroque oboe comfortably extends from C4 to D6. With the resurgence of interest in early music in the mid 20th century, a few makers began producing copies to specifications taken from surviving historical instruments.

Classical oboe, copy by Sand Dalton of an original by Johann Friedrich Floth, c. 1805

Classical

The Classical period brought a regular oboe whose bore was gradually narrowed, and the instrument became outfitted with several keys, among them were those for the notes D, F, and G. A key similar to the modern octave key was also added called the "slur key," though it was at first used more like the "flick" keys on the modern German bassoon.[15] Only later did French instrument makers redesign the octave key to be used in the manner of the modern key (i.e. held open for the upper register, closed for the lower). The narrower bore allows the higher notes to be more easily played, and composers began to more often utilize the oboe's upper register in their works. Because of this, the oboe's tessitura in the Classical era was somewhat broader than that found in Baroque works. The range for the Classical oboe extends from C4 to F6 (using the scientific pitch notation system), though some German and Austrian oboes are capable of playing one half-step lower. Classical-era composers who wrote concertos for oboe include Mozart (both the solo concerto in C major K. 314/285d and the lost original of Sinfonia Concertante in E major K. 297b, as well as a fragment of F major concerto K. 417f), Haydn, (both the Sinfonia Concertante in B Hob. I:105 and the spurious concerto in C major Hob. VIIg:C1), Beethoven (the F major concerto, Hess 12, of which only sketches survive, though the second movement was reconstructed in the late 20th century), and numerous other composers including Johann Christian Bach, Johann Christian Fischer, Jan Antonín Koželuh, and Ludwig August Lebrun. Many solos exist for the regular oboe in chamber, symphonic, and operatic compositions from the Classical era.

Viennese or Wiener oboe

The Wiener oboe is a type of modern oboe that retains the essential bore and tonal characteristics of the historical oboe. The Akademiemodel Wiener Oboe, first developed in the late 19th century by Josef Hajek from earlier instruments by C. T. Golde of Dresden (1803–73), is now made by several makers such as André Constantinides, Karl Rado, Guntram Wolf, Christian Rauch and Yamaha. It has a wider internal bore, a shorter and broader reed and the fingering-system is very different than the conservatoire oboe.[16] In The Oboe, Geoffrey Burgess and Bruce Haynes write "The differences are most clearly marked in the middle register, which is reedier and more pungent, and the upper register, which is richer in harmonics on the Viennese oboe".[17] Guntram Wolf describes them: "From the concept of the bore, the Viennese oboe is the last representative of the historical oboes, adapted for the louder, larger orchestra, and fitted with an extensive mechanism. Its great advantage is the ease of speaking, even in the lowest register. It can be played very expressively and blends well with other instruments."[18] The Viennese oboe is, along with the Vienna horn, perhaps the most distinctive member of the Wiener Philharmoniker instrumentarium.

Conservatoire oboe

This oboe was developed further in the 19th century by the Triébert family of Paris. Using the Boehm flute as a source of ideas for key work, Guillaume Triébert and his sons, Charles and Frederic, devised a series of increasingly complex yet functional key systems. A variant form using large tone holes, the Boehm system oboe, was never in common use, though it was used in some military bands in Europe into the 20th century. F. Lorée of Paris made further developments to the modern instrument. Minor improvements to the bore and key work have continued through the 20th century, but there has been no fundamental change to the general characteristics of the instrument for several decades.[19]

Modern Oboe

The modern standard oboe is most commonly made from grenadilla, also known as African blackwood, though some manufacturers also make oboes out of other members of the genus Dalbergia, which includes cocobolo, rosewood, and violetwood (also known as kingwood). Ebony (genus Diospyros) has also been used. Student model oboes are often made from plastic resin, to avoid instrument cracking to which wood instruments are prone, but also to make the instrument more economical. The oboe has an extremely narrow conical bore. It is played with a double reed consisting of two thin blades of cane tied together on a small-diameter metal tube (staple) which is inserted into the reed socket at the top of the instrument. The commonly accepted range for the oboe extends from B3 to about G6, over two and a half octaves, though its common tessitura lies from C4 to E6. Some student oboes only extend down to B3 (the key for B is not present). However, this variant is becoming less common.

A modern oboe with the "full conservatoire" ("conservatory" in the US) or Gillet key system has 45 pieces of keywork, with the possible additions of a third-octave key and alternate (left little finger) F- or C-key. The keys are usually made of nickel silver, and are silver- or occasionally gold-plated. Besides the full conservatoire system, oboes are also made using the British thumbplate system. Most have "semi-automatic" octave keys, in which the second-octave action closes the first, and some have a fully automatic octave key system, as used on saxophones. Some full-conservatory oboes have finger holes covered with rings rather than plates ("open-holed"), and most of the professional models have at least the right-hand third key open-holed. Professional oboes used in the UK and Iceland frequently feature conservatoire system combined with a thumb plate. Releasing the thumb plate has the same effect as pressing down the right-hand index-finger key. This produces alternate options which eliminate the necessity for most of the common cross-intervals (intervals where two or more keys need to be released and pressed down simultaneously), but cross intervals are much more difficult to execute in such a way that the sound remains clear and continuous throughout the frequency change (a quality also called legato and often called-for in the oboe repertoire).

Other members of the oboe family

The standard oboe has several siblings of various sizes and playing ranges. The most widely known and used today is the cor anglais, or English horn, the tenor (or alto) member of the family. A transposing instrument; it is pitched in F, a perfect fifth lower than the oboe. The oboe d'amore, the alto (or mezzo-soprano) member of the family, is pitched in A, a minor third lower than the oboe. J.S. Bach made extensive use of both the oboe d'amore as well as the taille and oboe da caccia, Baroque antecedents of the cor anglais. Even less common is the bass oboe (also called baritone oboe), which sounds one octave lower than the oboe. Delius and Holst both scored for the instrument. Similar to the bass oboe is the more powerful heckelphone, which has a wider bore and larger tone than the baritone oboe. Only 165 heckelphones have ever been made. Not surprisingly, competent heckelphone players are difficult to find due to the extreme rarity of this particular instrument.[20] The least common of all are the musette (also called oboe musette or piccolo oboe), the sopranino member of the family (it is usually pitched in E or F above the oboe), and the contrabass oboe (typically pitched in C, two octaves deeper than the standard oboe).

Folk versions of the oboe, sometimes equipped with extensive keywork, are found throughout Europe. These include the musette (France) and the piston oboe and bombarde (Brittany), the piffero and ciaramella (Italy), and the xirimia (also spelled chirimia) (Spain). Many of these are played in tandem with local forms of bagpipe, particularly with the Italian müsa and zampogna or Breton biniou. Similar oboe-like instruments, most believed to derive from Middle Eastern models, are also found throughout Asia as well as in North Africa.[citation needed]


Notable classical works featuring the oboe

Unaccompanied pieces

Use in non-classical music

Traditional and folk music

Although folk oboes are still used in many European folk music traditions, the modern oboe has been little used in folk music. One exception was Derek Bell, harpist for the Irish group The Chieftains, who used the regular instrument in some performances and recordings. The United States contra dance band Wild Asparagus, based in western Massachusetts, also uses the oboe, played by David Cantieni. The folk musician Paul Sartin plays the oboe in several English folk bands including Faustus and Bellowhead. Welsh bagpipe player and bagpipe maker Jonathan Shorland plays a 'rustic oboe' similar to the Breton 'piston' with the bands Primeaval and Juice. He formerly played with Fernhill, who play traditional Welsh music. The popular traditional music of Brittany boasts a significant professional class of musicians playing increasingly sophisticated double reed instruments, supported by professional instrument makers, reed manufacturers and the educational system. The Breton 'piston' oboe and bombard have expanded from traditional roles into genres as diverse as jazz, rock, and classical music.[citation needed]

Jazz

The oboe remains uncommon in jazz music, but there have been notable uses of the instrument. Some early bands in the 1920s and '30s, most notably that of Paul Whiteman, included it for coloristic purposes. The multi-instrumentalist Garvin Bushell (1902–1991) played the oboe in jazz bands as early as 1924 and used the instrument throughout his career, eventually recording with John Coltrane in 1961.[22] Gil Evans featured oboe in sections of his famous Sketches of Spain collaboration with trumpeter Miles Davis. Though primarily a tenor saxophone and flute player, Yusef Lateef was among the first (in 1961) to use the oboe as a solo instrument in modern jazz performances and recordings. Composer and double bassist Charles Mingus gave the oboe a brief but prominent role (played by Dick Hafer) in his composition "I.X. Love" on the 1963 album Mingus Mingus Mingus Mingus Mingus. Marshall Allen occasionally played an oboe with Sun Ra.[citation needed]

With the birth of jazz fusion in the late 1960s, and its continuous development through the following decade, the oboe became somewhat more prominent, replacing on some occasions the saxophone as the focal point. The oboe was used with great success by the Welsh multi-instrumentalist Karl Jenkins in his work with the groups Nucleus and Soft Machine, and by the American woodwind player Paul McCandless, co-founder of the Paul Winter Consort and later Oregon. Romeo Penque also played the oboe on Roland Kirk's 1975 album Return of the 5000 Lb. Man, in the song "Theme for the Eulipions."[citation needed]

The 1980s saw an increasing number of oboists try their hand at non-classical work, and many players of note have recorded and performed alternative music on oboe. Some present-day jazz groups influenced by classical music, such as the Maria Schneider Orchestra, feature the oboe.[citation needed]

Rock and pop

The oboe has been used sporadically in rock/pop recordings (e.g., Frankie Valli and The Four Seasons "Big Man In Town" 1964; Dion "Abraham, Martin & John" 1968; The Carpenters' "For All We Know," 1970; Donovan's "Jennifer Juniper," 1968), generally by studio musicians on recordings of specific songs.[citation needed]

Peter Gabriel, during his period as lead singer in the progressive rock band Genesis, played oboe on some of the group's studio recordings. Andy Mackay played oboe for Roxy Music both in the studio and on stage.[citation needed]

In the 2000s, Robbie J. de Klerk, the vocalist of the Dutch melodic doom/death metal band Another Messiah[23] also played the oboe in most songs. In America, the band Hoboe defines itself as a rock band showcasing amplified oboe since 2000, fronted by oboist Zen Ben.[24] Indie singer-songwriter and composer Sufjan Stevens, having studied the instrument in school, often includes the instrument in his arrangements and compositions, most frequently in his geographic tone-poems Illinois, Michigan, and his orchestral suite The BQE.[25]

Film music

The oboe is frequently featured in film music, often to underscore a particularly poignant or sad scene, for example in the motion picture Born on the Fourth of July, where an oboe delicately takes the theme with a romantic and harmonic touch before the strings hand it over once again to the trumpet. One of the most prominent uses of the oboe in a film score is Ennio Morricone's "Gabriel's Oboe" theme from the 1986 film The Mission.

It is featured as a solo instrument in the theme "Across the Stars" from the John Williams score to Star Wars: Episode II – Attack of the Clones. The oboe is also used in "The Search" from the Basil Poledouris score to Conan the Barbarian.

Ilaiyaraja, a famous Indian film music composer, has also used the oboe in much of his film music. Examples include Dalapathi (1991); the title track of Aditya 369 (1991); Pazhassiraja (2009); and Nandalaala (2010). The oboe has also been used by more recent Indian music composers, such as A. R. Rahman, who has used it in the film Jodha Akbar (2008).

Notable oboists

Oboe manufacturers

Notes

  1. ^ Fletcher & Rossing 1998, 401–403.
  2. ^ "Sound Characteristics of the Oboe". Vienna Symphonic Library. Retrieved 9 September 2012.
  3. ^ Kushner 1993, 167: "The oboe: official instrument of the International Order of Travel Agents. If the duck was a songbird it would sing like this. Nasal, desolate, the call of migratory things."
  4. ^ American Symphony Orchestra League. Oxford Music Online. Oxford University Press. 2001.
  5. ^ http://www.ifcompare.com/clarinet-vs-oboe/ Archived 2016-03-04 at the Wayback Machine
  6. ^ Thomas, Julia. "Executive Director of the Rockford Symphony Orchestra". Rockford Symphony Orchestra. Rockford Symphony Orchestra. Retrieved October 20, 2014.
  7. ^ "About the Orchestra" American League of Orchestras, (accessed January 1, 2009).
  8. ^ Joppig 1988, 208–209.
  9. ^ Masterclass by John Mack, Aspen Music Festival and School, 2004
  10. ^ Marcuse 1975, 371.
  11. ^ Burgess & Haynes 2004, 27
  12. ^ Burgess & Haynes 2004, 28 ff
  13. ^ Carse 1965, 120.
  14. ^ Burgess & Haynes 2004, 102.
  15. ^ Haynes, Bruce; Burgess, Geoffrey (2016-05-01). The Pathetick Musician. Oxford University Press. ISBN 9780199373734.
  16. ^ Haynes, Bruce; Burgess, Geoffrey (2016-05-01). The Pathetick Musician. Oxford University Press. p. 176. ISBN 9780199373734.
  17. ^ Burgess & Haynes 2004, 212.
  18. ^ "Modern Woodwind Instruments". Guntram Wolf. Retrieved 27 November 2012.
  19. ^ Howe 2003.
  20. ^ Howe and Hurd 2004.
  21. ^ "Zelenka". www.jdzelenka.net.
  22. ^ Coltrane Discography Archived 2009-01-02 at the Wayback Machine Dave Wild
  23. ^ Another Messiah Encyclopaedia Metallum
  24. ^ Hoboe Hoboe.com
  25. ^ Album Credits for Sufjan Stevens Allmusic.com
  26. ^ "A. Laubin, Inc. – Oboes and English Horns". www.alaubin.com.
  27. ^ david. "Loree – Paris". www.loree-paris.com.
  28. ^ "Home - Oboe Marigaux". www.marigaux.com.
  • Baines, Anthony: 1967, Woodwind Instruments and Their History, third edition, with a foreword by Sir Adrian Boult. London: Faber and Faber.
  • Beckett, Morgan Hughes: 2008, "The Sensuous Oboe". Orange, CA: Scuffin University Press. ISBN 0-456-00432-7.
  • Burgess, Geoffrey, and Bruce Haynes: 2004, The Oboe. The Yale Musical Instrument Series. New Haven, Connecticut and London: Yale University Press. ISBN 0-300-09317-9.
  • Carse, Adam: 1965, Musical Wind Instruments: A History of the Wind Instruments Used in European Orchestras and Wind-Bands from the Later Middle Ages up to the Present Time New York: Da Capo Press. ISBN 0-306-80005-5.
  • Fletcher, Neville H., and Thomas D. Rossing: 1998, The Physics of Musical Instruments, second edition. New York, Berlin, Heidelberg: Springer-Verlag. ISBN 978-1441931207.
  • Gioielli, Mauro: 1999. "La 'calamaula' di Eutichiano". Utriculus 8, no. 4 (32) (October–December): 44–45.
  • Harris-Warrick, Rebecca: 1990, "A Few Thoughts on Lully's Hautbois" Early Music 18, no. 1 (February, "The Baroque Stage II"): 97-98+101-102+105-106.
  • Haynes, Bruce: 1985, Music for Oboe, 1650–1800: A Bibliography. Fallen Leaf Reference Books in Music, 8755-268X; no. 4. Berkeley, California: Fallen Leaf Press. ISBN 0-914913-03-4.
  • Haynes, Bruce: 1988, "Lully and the Rise of the Oboe as Seen in Works of Art". Early Music 16, no. 3 (August): 324–38.
  • Haynes, Bruce: 2001, The Eloquent Oboe: A History of the Hautboy 1640–1760. Oxford Early Music Series. Oxford and New York: Oxford University Press. ISBN 0-19-816646-X.
  • Howe, Robert: 2003, "The Boehm System Oboe and Its Role in the Development of the Modern Oboe". Galpin Society Journal 56:27–60 +plates on 190–92.
  • Howe, Robert, and Peter Hurd: 2004, "The Heckelphone at 100". Journal of the American Musical Instrument Society 30:98–165.
  • Joppig, Gunther: 1988. The Oboe and the Bassoon, translated by Alfred Clayton. Portland: Amadeus Press. ISBN 0-931340-12-8.
  • Kushner, Tony: 1993. Angels in America: A Gay Fantasia on National Themes, single-volume edition. New York: Theatre Communications Group. ISBN 1-55936-107-7.
  • Marcuse, Sybil: 1975, Musical Instruments: A Comprehensive Dictionary Revised edition, The Norton Library, New York: W. W. Norton. ISBN 0-393-00758-8

External links



This article uses material from the Wikipedia article "Oboe", which is released under the Creative Commons Attribution-Share-Alike License 3.0. There is a list of all authors in Wikipedia

Music

3d,printed,3dprinting,3dprint,music,song,dvd,dcrom,schellak,top hit