powered by CADENAS

Social Share

Amazon

Machete (musical instrument) (6256 views - Music)

The machete (Portuguese: machete de braga) is a small stringed instrument from Madeira, Portugal. The instrument has four metal strings, in contrast to its slightly larger cousin, the machete de rajão, which has five metal strings. Historians believe the machete was introduced in Madeira as Braguinha from Braga, and it is the immediate predecessor of the ukulele, being introduced to Hawaii by Portuguese immigrants in the late 19th century.
Go to Article

Explanation by Hotspot Model

Youtube


    

Machete (musical instrument)

Machete (musical instrument)

The machete (Portuguese: machete de braga) is a small stringed instrument from Madeira, Portugal. The instrument has four metal strings, in contrast to its slightly larger cousin, the machete de rajão, which has five metal strings. Historians believe the machete was introduced in Madeira as Braguinha from Braga, and it is the immediate predecessor of the ukulele, being introduced to Hawaii by Portuguese immigrants in the late 19th century.[1]

See also



This article uses material from the Wikipedia article "Machete (musical instrument)", which is released under the Creative Commons Attribution-Share-Alike License 3.0. There is a list of all authors in Wikipedia

Music

3d,printed,3dprinting,3dprint,music,song,dvd,dcrom,schellak,top hit