Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
This article needs additional citations for verification. Please help improve this article by adding citations to reliable sources. Unsourced material may be challenged and removed. Find sources: "Radio control" – news · newspapers · books · scholar · JSTOR (March 2010) (Learn how and when to remove this template message) |
Radio control (often abbreviated to R/C or simply RC) is the use of radio signals to remotely control a device. Radio control is used for control of model vehicles from a hand-held radio transmitter. Industrial, military, and scientific research organizations make use of radio-controlled vehicles as well.
In 1894, the first example of wirelessly controlling at a distance was during a demonstration by the British physicist Oliver Lodge, in which he made use of a Édouard Branly's coherer to make a mirror galvanometer move a beam of light when an electromagnetic wave was artificially generated. This was further refined by Guglielmo Marconi and William Preece, at a demonstration that took place on December 12, 1896, at Toynbee Hall in London, in which they made a bell ring by pushing a button in a box that was not connected by any wires.
In 1897 a British engineer Ernest Wilson had invented a torpedo that was controlled by "Hertzian" waves.[citation needed]
In 1898, at an exhibition at Madison Square Garden, Nikola Tesla demonstrated a small unmanned boat that used a coherer based radio control. In a bit of showmanship, Tesla entertained the audience to make it seem that the boat could apparently obey commands from the audience but it was, in fact, controlled by Tesla interpreting the verbal requests and sending appropriate frequencies to tuned circuits in the boat.[1] Tesla was granted a US patent on this invention on July 1, 1898.[2] In 1903, the Spanish engineer Leonardo Torres y Quevedo presented the "Telekino" at the Paris Academy of Science, and was granted a patent in France, Spain, Great Britain and the United States.[3] In 1904, Bat, a Windermere steam launch, was controlled using experimental radio control by its inventor, [Jack Kitchen].
In 1909 the French inventor Gabet demonstrated what he called his "Torpille Radio-Automatique", a radio-controlled torpedo.[4] In 1917, Archibald Low as head of the RFC Experimental Works, was the first person to use radio control successfully on an aircraft.
During World War I American inventor John Hays Hammond, Jr. developed many techniques used in subsequent radio control including developing remote controlled torpedoes, ships, anti-jamming system's and even a system allowing his remote-controlled ship targeting an enemy ship's searchlights.[5] In 1922 he installed radio control gear on the obsolete US Navy battleship USS Iowa so it could be used as a target ship[6] (sunk in gunnery exercise in March 1923).
The Soviet Red Army used remotely controlled teletanks during the 1930s in the Winter War against Finland and fielded at least two teletank battalions at the beginning of the Great Patriotic War. A teletank is controlled by radio from a control tank at a distance of 500–1,500 m, the two constituting a telemechanical group. There were also remotely controlled cutters and experimental remotely controlled planes in the Red Army. In the 1930s, the United Kingdom developed the radio-controlled Queen Bee, a remotely controlled unmanned Tiger Moth aircraft for a fleet's gunnery firing practice. The Queen Bee was superseded by the similarly named Queen Wasp, a purpose-built, target aircraft of higher performance.
Radio control was further developed during World War II, primarily by the Germans who used it in a number of missile projects. Their main effort was the development of radio-controlled missiles and glide bombs for use against shipping, a target otherwise both difficult and dangerous to attack. However, by the end of the war, the Luftwaffe was having similar problems attacking Allied bombers and developed a number of radio command guided anti-aircraft missiles, none of which saw service.
The effectiveness of the Luftwaffe's systems, primarily comprising the series of Telefunken Funk-Gerät (or FuG) 203 Kehl twin-axis, single joystick-equipped transmitters mounted in the deploying aircraft, and Telefunken's companion FuG 230 Straßburg receiver placed in the ordnance to be controlled during deployment and used by both the Fritz X unpowered, armored anti-ship bomb, and the powered Henschel Hs 293 guided bomb, was greatly reduced by British efforts to jam their radio signals, eventually with American assistance. After initial successes, the British launched a number of commando raids to collect the missile radio sets. Jammers were then installed on British ships, and the weapons basically "stopped working". The German development teams then turned to wire guidance once they realized what was going on, but the systems were not ready for deployment until the war had already moved to France.
The German Kriegsmarine operated FL-Boote (ferngelenkte Sprengboote) which were radio controlled motor boats filled with explosives to attack enemy shipping from 1944.
Both the British and US also developed radio control systems for similar tasks, to avoid the huge anti-aircraft batteries set up around German targets. However, no system proved usable in practice, and the one major US effort, Operation Aphrodite, proved to be far more dangerous to its users than to the target. The American Azon guided free-fall ordnance, however, proved useful in both the European and CBI Theaters of World War II.
Radio control systems of this era were generally electromechanical in nature, using small metal "fingers" or "reeds" with different resonant frequencies each of which would operate one of a number of different relays when a particular frequency was received. The relays would in turn then activate various actuators acting on the control surfaces of the missile. The controller's radio transmitter would transmit the different frequencies in response to the movements of a control stick; these were typically on/off signals. The radio gear used to control the rudder function on the American-developed Azon guided ordnance, however, was a fully proportional control, with the "ailerons", solely under the control of an on-board gyroscope, serving merely to keep the ordnance from rolling.
These systems were widely used until the 1960s, when the increasing use of solid state systems greatly simplified radio control. The electromechanical systems using reed relays were replaced by similar electronic ones, and the continued miniaturization of electronics allowed more signals, referred to as control channels, to be packed into the same package. While early control systems might have two or three channels using amplitude modulation, modern systems include 20 or more using frequency modulation.
The first general use of radio control systems in models started in the early 1950s with single-channel self-built equipment; commercial equipment came later. The advent of transistors greatly reduced the battery requirements, since the current requirements at low voltage were greatly reduced and the high voltage battery was eliminated. In both tube and early transistor sets the model's control surfaces were usually operated by an electromagnetic escapement controlling the stored energy in a rubber-band loop, allowing simple on/off rudder control (right, left, and neutral) and sometimes other functions such as motor speed.[7]
Crystal-controlled superheterodyne receivers with better selectivity and stability made control equipment more capable and at lower cost. Multi-channel developments were of particular use to aircraft, which really needed a minimum of three control dimensions (yaw, pitch and motor speed), as opposed to boats, which required only two or one.
As the electronics revolution took off, single-signal channel circuit design became redundant, and instead radios provided proportionally coded signal streams which a servomechanism could interpret, using Pulse-width modulation (PWM).
More recently, high-end hobby systems using Pulse-code modulation (PCM) features have come on the market that provide a computerized digital bit-stream signal to the receiving device, instead of the earlier PWM encoding type. However, even with this coding, loss of transmission during flight has become more common[citation needed], in part because of the ever more wireless society. Some more modern FM-signal receivers that still use "PWM" encoding instead can, thanks to the use of more advanced computer chips in them, be made to lock onto and use the individual signal characteristics of a particular PWM-type RC transmitter's emissions alone, without needing a special "code" transmitted along with the control information as PCM encoding has always required.
In the early 21st century, 2.4 gigahertz spread spectrum RC control systems have become increasingly utilized in control of model vehicles and aircraft. Now, these 2.4 GHz systems are being made by most radio manufacturers. These radio systems range in price from a couple thousand dollars, all the way down to under US$30 for some. Some manufacturers even offer conversion kits for older digital 72 MHz receivers and radios. As the emerging multitude of 2.4 GHz band spread spectrum RC systems usually use a "frequency-agile" mode of operations, like FHSS that do not stay on one set frequency any longer while in use, the older "exclusive use" provisions at model flying sites needed for VHF-band RC control systems's frequency control, for VHF-band RC systems that only used one set frequency unless serviced to change it, are not as mandatory as before.
Remote control military applications are typically not radio control in the direct sense, directly operating flight control surfaces and propulsion power settings, but instead take the form of instructions sent to a completely autonomous, computerized automatic pilot. Instead of a "turn left" signal that is applied until the aircraft is flying in the right direction, the system sends a single instruction that says "fly to this point".
Some of the most outstanding examples of remote radio control of a vehicle are the Mars Exploration Rovers such as Sojourner.
Today radio control is used in industry for such devices as overhead cranes and switchyard locomotives. Radio-controlled teleoperators are used for such purposes as inspections, and special vehicles for disarming of bombs. Some remotely controlled devices are loosely called robots, but are more properly categorized as teleoperators since they do not operate autonomously, but only under control of a human operator.
An industrial radio remote control can either be operated by a person, or by a computer control system in a machine to machine (M2M) mode. For example, an automated warehouse may use a radio-controlled crane that is operated by a computer to retrieve a particular item. Industrial radio controls for some applications, such as lifting machinery, are required to be of a fail-safe design in many jurisdictions.[8]
Industrial remote controls work differently from most consumer products. When the receiver receives the radio signal which the transmitter sent, it checks it so that it is the correct frequency and that any security codes match. Once the verification is complete, the receiver sends an instruction to a relay which is activated. The relay activates a function in the application corresponding to the transmitters button. This could be to engage an electrical directional motor in an overhead crane. In a receiver there are usually several relays, and in something as complex as an overhead crane, perhaps up to 12 or more relays are required to control all directions. In a receiver which opens a gate, two relays are often sufficient.[9]
Industrial remote controls are getting more and higher safety requirements. For example: a remote control may not lose the safety functionality in case of malfunction.[10] This can be avoided by using redundant relays with forced contacts.
This article uses material from the Wikipedia article "Radio control", which is released under the Creative Commons Attribution-Share-Alike License 3.0. There is a list of all authors in Wikipedia
3D,CAD,Model,Libary,Railway, Train, Ship, Marine, Submarine, Automotive, Locomotive, Bike, Car, Formula 1, Space, Aircraft, Aerospace, Satelite, Automobile, Yacht