powered by CADENAS

Social Share

Selective heat sintering (5276 views - 3D Printing Dictionary)

Selective heat sintering (SHS) is a type of additive manufacturing process. It works by using a thermal printhead to apply heat to layers of powdered thermoplastic. When a layer is finished, the powder bed moves down, and an automated roller adds a new layer of material which is sintered to form the next cross-section of the model. SHS is best for manufacturing inexpensive prototypes for concept evaluation, fit/form and functional testing. SHS is a Plastics additive manufacturing technique similar to selective laser sintering (SLS), the main difference being that SHS employs a less intense thermal printhead instead of a laser, thereby making it a cheaper solution, and able to be scaled down to desktop sizes.
Go to Article

Selective heat sintering

Selective heat sintering

Selective heat sintering (SHS) is a type of additive manufacturing process. It works by using a thermal printhead to apply heat to layers of powdered thermoplastic. When a layer is finished, the powder bed moves down, and an automated roller adds a new layer of material which is sintered to form the next cross-section of the model. SHS is best for manufacturing inexpensive prototypes for concept evaluation, fit/form and functional testing. SHS is a Plastics additive manufacturing technique similar to selective laser sintering (SLS), the main difference being that SHS employs a less intense thermal printhead instead of a laser, thereby making it a cheaper solution, and able to be scaled down to desktop sizes.[1]

  1. ^ "How Selective Heat Sintering Works". THRE3D.com. Retrieved 3 February 2014. 


This article uses material from the Wikipedia article "Selective heat sintering", which is released under the Creative Commons Attribution-Share-Alike License 3.0. There is a list of all authors in Wikipedia

3D Printing Dictionary

OpenLAB, Fablab, OpenSCAD, FreeCAD, BRL-CAD, RhinocerosCAD, LibreCAD, Vectary, 123D, TinkerCAD, Wings 3D, MOI3D, leapfrog 3D, Geomagic, Paint3D, STLfinder, Yeggi, Yobi3D, 3D Shape Search, PARTcloud, Thingiverse, GrabCAD, AMF, Additive Manufacturing, STL, Stereolitography, Mesh, MeshMixer, Free Download, lowpoly, 3D voxel,things, digital design, physical objects, rapid prototyping, 3D objects, 3D printing, reprap, fabrication, laser cutter,abs