Animation is a method in which pictures are manipulated to appear as moving images. In traditional animation, images are drawn or painted by hand on transparent celluloid sheets to be photographed and exhibited on film. Today, most animations are made with computer-generated imagery (CGI). Computer animation can be very detailed 3D animation, while 2D computer animation can be used for stylistic reasons, low bandwidth or faster real-time renderings. Other common animation methods apply a stop motion technique to two and three-dimensional objects like paper cutouts, puppets or clay figures.
Commonly the effect of animation is achieved by a rapid succession of sequential images that minimally differ from each other. The illusion—as in motion pictures in general—is thought to rely on the phi phenomenon and beta movement, but the exact causes are still uncertain. Analog mechanical animation media that rely on the rapid display of sequential images include the phénakisticope, zoetrope, flip book, praxinoscope and film. Television and video are popular electronic animation media that originally were analog and now operate digitally. For display on the computer, techniques like animated GIF and Flash animation were developed.
Animation is more pervasive than many people realise. Apart from short films, feature films, animated gifs and other media dedicated to the display of moving images, animation is also heavily used for video games, motion graphics and special effects. Animation is also prevalent in information technology interfaces.[1]
The physical movement of image parts through simple mechanics – in for instance the moving images in magic lantern shows – can also be considered animation. The mechanical manipulation of puppets and objects to emulate living beings has a very long history in automata. Automata were popularised by Disney as animatronics.
Animators are artists who specialize in creating animation.
The word "animation" stems from the Latin "animationem" (nominative "animatio"), noun of action from past participle stem of "animare", meaning "the action of imparting life". The primary meaning of the English word is "liveliness" and has been in use much longer than the meaning of "moving image medium".[2]
The history of animation started long before the development of cinematography. Humans have probably attempted to depict motion as far back as the Paleolithic period. Shadow play and the magic lantern offered popular shows with moving images as the result of manipulation by hand and/or some minor mechanics.
A 5,200-year old pottery bowl discovered in Shahr-e Sukhteh, Iran, has five sequential images painted around it that seem to show phases of a goat leaping up to nip at a tree.[3][4] In 1833, the phenakistiscope introduced the stroboscopic principle of modern animation, which would also provide the basis for the zoetrope (1866), the flip book (1868), the praxinoscope (1877) and cinematography.
Charles-Émile Reynaud further developed his projection praxinoscope into the Théâtre Optique with transparent hand-painted colorful pictures in a long perforated strip wound between two spools, patented in December 1888. From 28 October 1892 to March 1900 Reynaud gave over 12,800 shows to a total of over 500.000 visitors at the Musée Grévin in Paris. His Pantomimes Lumineuses series of animated films each contained 300 to 700 frames that were manipulated back and forth to last 10 to 15 minutes per film. Piano music, song, and some dialogue were performed live, while some sound effects were synchronized with an electromagnet.
After cinematography became a popular medium, some manufacturers of optical toys adapted small magic lanterns into toy film projectors for short loops of film. By 1902, they were producing many chromolithography film loops, usually by tracing live-action film footage (much like the later rotoscoping technique).
Some early filmmakers, including J. Stuart Blackton, Arthur Melbourne-Cooper, Segundo de Chomón and Edwin S. Porter experimented with stop-motion animation, possibly since around 1899. Blackton's The Haunted Hotel (1907) was the first huge success that baffled audiences with objects apparently moving by themselves and inspired other filmmakers to try the technique.
J. Stuart Blackton also experimented with animation drawn on blackboards and some cutout animation in Humorous Phases of Funny Faces (1906).
In 1908, Émile Cohl's Fantasmagorie was released with a white-on-black chalkline look created with negative prints from black ink drawings on white paper.[5] The film largely consists of a stick figure moving about and encountering all kinds of morphing objects, including a wine bottle that transforms into a flower.[6]
Inspired by Émile Cohl's stop-motion film Les allumettes animées [Animated Matches] (1908), Ladislas Starevich started making his influential puppet animations in 1910.
Winsor McCay's Little Nemo (1911) showcased very detailed drawings. His Gertie the Dinosaur (1914) was also an early example of character development in drawn animation.[7]
During the 1910s, the production of animated short films typically referred to as "cartoons", became an industry and cartoon shorts were produced for showing in cinemas.[8] The most successful producer at the time was John Randolph Bray, who, along with animator Earl Hurd, patented the cel animation process that dominated the animation industry for the rest of the decade.[9][10]
El Apóstol (Spanish: "The Apostle") was a 1917 Argentine animated film utilizing cutout animation, and the world's first animated feature film.[12][13] A fire that destroyed producer Federico Valle's film studio incinerated the only known copy of El Apóstol, and it is now considered a lost film.[14][15]
In 1919, the silent animated short Feline Follies was released, marking the debut of Felix the Cat, being the first animated character in the silent film era to gain significant popularity.
The earliest extant feature-length animated film is The Adventures of Prince Achmed (1926) made by director Lotte Reiniger and her collaborators Carl Koch and Berthold Bartosch.
The first animation with full sound synchronization (both music and dialogue) was a short by Walt Disney’s animation studio called Steamboat Willie, featuring Mickey Mouse in 1928.
In 1932, the first short animated film created entirely with Technicolor (using red/green/blue photographic filters and three strips of film in the camera) was Disney's Flowers and Trees, directed by Burt Gillett. The first full-color animated feature film was "Snow White and the Seven Dwarfs", also by Walt Disney.
Through the 1930s and 1950s, the golden age of American animation saw new animated characters emerge, including Goofy, Donald Duck, Daisy Duck, Bugs Bunny, Daffy Duck, Porky Pig, Betty Boop, Popeye, Sylvester the Cat, Woody Woodpecker, Tweety, Wile E. Coyote and Road Runner, Elmer Fudd, Foghorn Leghorn, Yosemite Sam, Tasmanian Devil, Hunky and Spunky, Droopy, Little Audrey, Tom and Jerry, Barney Bear, Mr. Magoo, Mighty Mouse, George and Junior, the Fox and the Crow and the animated adoption of Superman, Baby Huey, Casper the Friendly Ghost, Little Lulu, among others.
In 1958, Hanna-Barbera released The Huckleberry Hound Show, the first half hour television program to feature only in animation.[16] Terrytoons released Tom Terrific that same year.[17][18] Television significantly decreased public attention to the animated shorts being shown in theaters.[16]
Computer animation has become popular since Toy Story (1995), the first feature-length animated film completely made using this technique.[19]
In 2008, the animation market was worth US$68.4 billion.[20] Animation as an art and industry continues to thrive as of the mid-2010s because well-made animated projects can find audiences across borders and in all four quadrants. Animated feature-length films returned the highest gross margins (around 52%) of all film genres in 2004–2013.[21]
Traditional animation (also called cel animation or hand-drawn animation) was the process used for most animated films of the 20th century.[22] The individual frames of a traditionally animated film are photographs of drawings, first drawn on paper.[23] To create the illusion of movement, each drawing differs slightly from the one before it. The animators' drawings are traced or photocopied onto transparent acetate sheets called cels,[24] which are filled in with paints in assigned colors or tones on the side opposite the line drawings.[25] The completed character cels are photographed one-by-one against a painted background by a rostrum camera onto motion picture film.[26]
The traditional cel animation process became obsolete by the beginning of the 21st century. Today, animators' drawings and the backgrounds are either scanned into or drawn directly into a computer system.[27][28] Various software programs are used to color the drawings and simulate camera movement and effects.[29] The final animated piece is output to one of several delivery media, including traditional 35 mm film and newer media with digital video.[30][27] The "look" of traditional cel animation is still preserved, and the character animators' work has remained essentially the same over the past 70 years.[31] Some animation producers have used the term "tradigital" (a play on the words "traditional" and "digital") to describe cel animation that uses significant computer technology.
Examples of traditionally animated feature films include Pinocchio (United States, 1940),[32] Animal Farm (United Kingdom, 1954), Lucky and Zorba (Italy, 1998), and The Illusionist (British-French, 2010). Traditionally animated films produced with the aid of computer technology include The Lion King (US, 1994), The Prince of Egypt (US, 1998), Akira (Japan, 1988),[33] Spirited Away (Japan, 2001), The Triplets of Belleville (France, 2003), and The Secret of Kells (Irish-French-Belgian, 2009).
Full animation refers to the process of producing high-quality traditionally animated films that regularly use detailed drawings and plausible movement,[35] having a smooth animation.[36] Fully animated films can be made in a variety of styles, from more realistically animated works like those produced by the Walt Disney studio (The Little Mermaid, Beauty and the Beast, Aladdin, The Lion King) to the more 'cartoon' styles of the Warner Bros. animation studio. Many of the Disney animated features are examples of full animation, as are non-Disney works, The Secret of NIMH (US, 1982), The Iron Giant (US, 1999), and Nocturna (Spain, 2007). Fully animated films are animated at 24 frames per second, with a combination of animation on ones and twos, meaning that drawings can be held for one frame out of 24 or two frames out of 24.[37]
Limited animation involves the use of less detailed or more stylized drawings and methods of movement usually a choppy or "skippy" movement animation.[38] Limited animation uses fewer drawings per second, thereby limiting the fluidity of the animation. This is a more economic technique. Pioneered by the artists at the American studio United Productions of America,[39] limited animation can be used as a method of stylized artistic expression, as in Gerald McBoing-Boing (US, 1951), Yellow Submarine (UK, 1968), and certain anime produced in Japan.[40] Its primary use, however, has been in producing cost-effective animated content for media for television (the work of Hanna-Barbera,[41] Filmation,[42] and other TV animation studios[43]) and later the Internet (web cartoons).
Rotoscoping is a technique patented by Max Fleischer in 1917 where animators trace live-action movement, frame by frame.[44] The source film can be directly copied from actors' outlines into animated drawings,[45] as in The Lord of the Rings (US, 1978), or used in a stylized and expressive manner, as in Waking Life (US, 2001) and A Scanner Darkly (US, 2006). Some other examples are Fire and Ice (US, 1983), Heavy Metal (1981), and Aku no Hana (2013).
Live-action/animation is a technique combining hand-drawn characters into live action shots or live action actors into animated shots.[46] One of the earlier uses was in Koko the Clown when Koko was drawn over live action footage.[47] Other examples include Allegro Non Troppo (Italy, 1976), Who Framed Roger Rabbit (US, 1988), Space Jam (US, 1996) and Osmosis Jones (US, 2001).
Stop-motion animation is used to describe animation created by physically manipulating real-world objects and photographing them one frame of film at a time to create the illusion of movement.[48] There are many different types of stop-motion animation, usually named after the medium used to create the animation.[49] Computer software is widely available to create this type of animation; traditional stop motion animation is usually less expensive but more time-consuming to produce than current computer animation.[49]
Computer animation encompasses a variety of techniques, the unifying factor being that the animation is created digitally on a computer.[29][72] 2D animation techniques tend to focus on image manipulation while 3D techniques usually build virtual worlds in which characters and objects move and interact.[73] 3D animation can create images that seem real to the viewer.[74]
2D animation figures are created or edited on the computer using 2D bitmap graphics and 2D vector graphics.[75] This includes automated computerized versions of traditional animation techniques, interpolated morphing,[76] onion skinning[77] and interpolated rotoscoping.
2D animation has many applications, including analog computer animation, Flash animation, and PowerPoint animation. Cinemagraphs are still photographs in the form of an animated GIF file of which part is animated.[78]
Final line advection animation is a technique used in 2D animation,[79] to give artists and animators more influence and control over the final product as everything is done within the same department.[80] Speaking about using this approach in Paperman, John Kahrs said that "Our animators can change things, actually erase away the CG underlayer if they want, and change the profile of the arm."[81]
3D animation is digitally modeled and manipulated by an animator. The animator usually starts by creating a 3D polygon mesh to manipulate.[82] A mesh typically includes many vertices that are connected by edges and faces, which give the visual appearance of form to a 3D object or 3D environment.[82] Sometimes, the mesh is given an internal digital skeletal structure called an armature that can be used to control the mesh by weighting the vertices.[83][84] This process is called rigging and can be used in conjunction with keyframes to create movement.[85]
Other techniques can be applied, mathematical functions (e.g., gravity, particle simulations), simulated fur or hair, and effects, fire and water simulations.[86] These techniques fall under the category of 3D dynamics.[87]
An animator is an artist who creates a visual sequence (or audio-visual if added sound) of multiple sequential images that generate the illusion of movement, that is, an animation. Animations are currently in many areas of technology and video, such as cinema, television, video games or the internet. Generally, these works require the collaboration of several animators. The methods to create these images depend on the animator and style that one wants to achieve (with images generated by computer, manually ...).
Animators can be divided into animators of characters (artists who are specialized in the movements, dialogue and acting of the characters) and animators of special effects (for example vehicles, machinery or natural phenomena such as water, snow, rain).
The creation of non-trivial animation works (i.e., longer than a few seconds) has developed as a form of filmmaking, with certain unique aspects.[108] Traits common to both live-action and animated feature-length films are labor-intensity and high production costs.[109]
The most important difference is that once a film is in the production phase, the marginal cost of one more shot is higher for animated films than live-action films.[110] It is relatively easy for a director to ask for one more take during principal photography of a live-action film, but every take on an animated film must be manually rendered by animators (although the task of rendering slightly different takes has been made less tedious by modern computer animation).[111] It is pointless for a studio to pay the salaries of dozens of animators to spend weeks creating a visually dazzling five-minute scene if that scene fails to effectively advance the plot of the film.[112] Thus, animation studios starting with Disney began the practice in the 1930s of maintaining story departments where storyboard artists develop every single scene through storyboards, then handing the film over to the animators only after the production team is satisfied that all the scenes make sense as a whole. [113] While live-action films are now also storyboarded, they enjoy more latitude to depart from storyboards (i.e., real-time improvisation).[114]
Another problem unique to animation is the requirement to maintain a film's consistency from start to finish, even as films have grown longer and teams have grown larger. Animators, like all artists, necessarily have individual styles, but must subordinate their individuality in a consistent way to whatever style is employed on a particular film.[115] Since the early 1980s, teams of about 500 to 600 people, of whom 50 to 70 are animators, typically have created feature-length animated films. It is relatively easy for two or three artists to match their styles; synchronizing those of dozens of artists is more difficult.[116]
This problem is usually solved by having a separate group of visual development artists develop an overall look and palette for each film before animation begins. Character designers on the visual development team draw model sheets to show how each character should look like with different facial expressions, posed in different positions, and viewed from different angles.[117][118] On traditionally animated projects, maquettes were often sculpted to further help the animators see how characters would look from different angles.[31][117]
Unlike live-action films, animated films were traditionally developed beyond the synopsis stage through the storyboard format; the storyboard artists would then receive credit for writing the film.[119] In the early 1960s, animation studios began hiring professional screenwriters to write screenplays (while also continuing to use story departments) and screenplays had become commonplace for animated films by the late 1980s.
Criticism of animation has been common in media and cinema since its inception. With its popularity, a large amount of criticism has arisen, especially animated feature-length films.[120] Many concerns of cultural representation, psychological effects on children have been brought up around the animation industry, which has remained rather politically unchanged and stagnant since its inception into mainstream culture.[121]
As with any other form of media, animation too has instituted awards for excellence in the field. The original awards for animation were presented by the Academy of Motion Picture Arts and Sciences for animated shorts from the year 1932, during the 5th Academy Awards function. The first winner of the Academy Award was the short Flowers and Trees,[122] a production by Walt Disney Productions.[123][124] The Academy Award for a feature-length animated motion picture was only instituted for the year 2001, and awarded during the 74th Academy Awards in 2002. It was won by the film Shrek, produced by DreamWorks and Pacific Data Images.[125] Disney/Pixar have produced the most films either to win or be nominated for the award. The list of both awards can be obtained here:
Several other countries have instituted an award for best-animated feature film as part of their national film awards: Africa Movie Academy Award for Best Animation (since 2008), BAFTA Award for Best Animated Film (since 2006), César Award for Best Animated Film (since 2011), Golden Rooster Award for Best Animation (since 1981), Goya Award for Best Animated Film (since 1989), Japan Academy Prize for Animation of the Year (since 2007), National Film Award for Best Animated Film (since 2006). Also since 2007, the Asia Pacific Screen Award for Best Animated Feature Film has been awarded at the Asia Pacific Screen Awards. Since 2009, the European Film Awards have awarded the European Film Award for Best Animated Film.
The Annie Award is another award presented for excellence in the field of animation. Unlike the Academy Awards, the Annie Awards are only received for achievements in the field of animation and not for any other field of technical and artistic endeavor. They were re-organized in 1992 to create a new field for Best Animated Feature. The 1990s winners were dominated by Walt Disney, however, newer studios, led by Pixar & DreamWorks, have now begun to consistently vie for this award. The list of awardees is as follows:
This article uses material from the Wikipedia article "Animation", which is released under the Creative Commons Attribution-Share-Alike License 3.0. There is a list of all authors in Wikipedia
Blender, Autodesk Maya, 3D Studio MAX (.3DS, .MAX), Maxwell, Animation, 3D Model, Autodesk Softimage, Cinema 4D, Rendering, Animation, 3Dartist, c4d, maxon, lowpoly, 3Dart, blender3D