Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
A pallet inverter or pile turner is a machine that is used to turn over pallets whilst still loaded with products. The reasons for needing to turn over a pallet are varied, but one main reason is the need to replace a broken or inappropriate pallet without unstacking the whole load. Sometimes a manufacturer simply needs to turn their products to stop their contents settling. In some industries, it is necessary to transfer goods from one type of pallet to another – for example, when plastic pallets are used for on-site storage and wooden pallets are used for shipping. Pallet inverters can be built into production lines or be used as a stand-alone product. The term pallet inverter is also used to cover machines that turn the palletised load through 90 degrees only. [1]
This article uses material from the Wikipedia article "Pallet inverter", which is released under the Creative Commons Attribution-Share-Alike License 3.0. There is a list of all authors in Wikipedia
3D,Geneva double,mechanism,kinematics,rotation,translation