This article possibly contains original research. Please improve it by verifying the claims made and adding inline citations. Statements consisting only of original research should be removed. (April 2018) (Learn how and when to remove this template message) |
A chess clock consists of two adjacent clocks with buttons to stop one clock while starting the other, so that the two clocks never run simultaneously. Chess clocks are used in chess and other two-player games where the players move in turn. The purpose is to keep track of the total time each player takes for their own moves, and ensure that neither player overly delays the game.
Chess clocks were first used extensively in tournament chess, and are often called game clocks. The first time that game clocks were used in a chess tournament was in the London 1883 tournament.[1] Their use has since spread to tournament Scrabble, shogi, go, and nearly every competitive two-player board game, as well as other types of games. In a tournament, the arbiter typically places all clocks in the same orientation, so that they can easily assess games that need attention at later stages.
The simplest time control is "sudden death", in which players must make a predetermined number of moves in a certain amount of time or forfeit the game immediately. A particularly popular variant in informal play is blitz chess, in which each player is given a short time (e.g. five minutes) on the clock in which to play the entire game.
The players may take more or less time over any individual move. The opening moves in chess are often played quickly due to their familiarity, which leaves the players more time to consider more complex and unfamiliar positions later. It is not unusual in slow chess games for a player to leave the table, but the clock of the absent player continues to run if it is their turn, or starts to run if their opponent makes a move.
Analog clocks are equipped with a "flag" that falls to indicate the exact moment the player's time has expired. Analog clocks use mechanical buttons. Pressing the button on one player's side physically stops the movement of that player's clock and releases the hold on the opponent's.
The drawbacks of the mechanical clocks include accuracy and matching of the two clocks, and matching of the indicators (flags) of time expiration. Additional time cannot easily be added for more complex time controls, especially those that call for an increment or delay on every move, such as some forms of byoyomi. However, a malfunctioning analog clock is a less serious event than a malfunctioning digital clock.[2]
In 1973, to address the issues with analog clocks, Bruce Cheney, a Cornell University Electrical Engineering student and chess player, created the first digital chess clock as a project for an undergraduate EE course.[3] Typical of most inventions, it was crude compared to the products on the market many years later and was limited by the technology that existed at the time. For example, the display was done with red LEDs. LEDs require significant power, and as a result, the clock had to be plugged into a wall outlet. The high cost of LEDs at the time meant that only one set of digits could be displayed, that of the player whose turn it was to move. This meant that each player's time had to be multiplexed to the display when their time was running. In 1973, LSI chips were not readily or cheaply available, so all the multiplexing and logic were done using chips that consisted of four two-input TTL NAND gates, which resulted in excessive power consumption. Being plugged into the wall is obviously a major drawback, but had one advantage: the timebase for the clock was driven off of a rectified version of 60 cycle AC current. Each player had a separate counter, and, in a parallel to the original mechanical architecture, one player's counter was disabled while the other's was running. The clock only had one mode: time ran forward. It could be reset, but not set. It did not count the number of moves. But it successfully addressed the original goals of the project (accurate and matched timing).
The first commercially available digital chess clock was patented in 1975 by Joseph Meshi and Jeffrey R. Ponsor and sold as the Micromate-80.[4] Three years later a much-improved Micromate-180 was produced alongside Meshi's MBA Thesis, "Demand Analysis for a New Product (The Digital Chess Clock)", at San Diego State University, while Meshi and Ponsor continued to develop digital gaming.[5]
Digital clocks and Internet gaming have spurred a wave of experimentation with more varied and complex time controls than the traditional standards. Time control is commonly used in modern chess in many different methodologies. One particularly notable development, which has gained quite wide acceptance in chess, was proposed by former world champion Bobby Fischer, who in 1988 filed for U.S. Patent 4,884,255 (awarded in 1989) for a new type of digital chess clock. Fischer's digital clock gave each player a fixed period of time at the start of the game and then added a small amount after each move. Joseph Meshi called this "Accumulation" as it was a main feature of his patented Micromate-180 (US Patent 4,247,925 1978). This became the linchpin of Fischer's clock patented 10 years later. In this way, the players would never be desperately short of time.
The increment time control was first used in the privately organised 1992 Fischer–Spassky match, and quickly became popular in the wider chess world, and was used in the FIDE World Chess Championship 1998.[6] As of 2017 most top level tournaments use Fischer's system as well as an increasing number of lower level tournaments. Other aspects of Fischer's patent, such as a synthesized voice announcing how much time the players have, thus eliminating the need for them to keep looking at the clock, have not been adopted.
On March 10, 1994, a patent application was filed by inventors Frank A. Camaratta Jr. of Huntsville, Alabama, and William Goichberg of Salisbury Mills, New York, for a game timer especially suitable for playing the game of chess, which employed a "delay" feature. The game timer provides, among other features, a user-definable delay between the time the activation button is pressed and the time that the activated clock actually begins to count down. United States Patent 5,420,830 was issued on May 10, 1995, and subsequently assigned to the United States Chess Federation by the inventors. As with the Fischer clock, the benefit of the delay clock is to reduce the likelihood that a player with positional and/or material superiority will lose a match solely because of the expiration of time on that player's time clock. Delay is still popular in the U.S, although increment is becoming more popular in the US.
There are three main types of chess timing methods, two of which are mathematically equivalent: (1) Increment (invented by Bobby Fischer), (2) Bronstein delay (invented by David Bronstein), and (3) Simple delay.
This article uses material from the Wikipedia article "Chess clock", which is released under the Creative Commons Attribution-Share-Alike License 3.0. There is a list of all authors in Wikipedia
3d,model,playground,board games,computer,strategy,thinktank