Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
Licensed under Creative Commons Attribution-Share Alike 3.0 (Siemens).
Electricity generation is the process of generating electric power from sources of primary energy. For electric utilities in the electric power industry, it is the first stage in the delivery of electricity to end users, the other stages being transmission, distribution, energy storage and recovery, using the pumped-storage method.
A characteristic of electricity is that it is not a primary energy freely present in nature in remarkable amounts and it must be produced. Production is carried out in power stations (also called "power plants"). Electricity is most often generated at a power plant by electromechanical generators, primarily driven by heat engines fueled by combustion or nuclear fission but also by other means such as the kinetic energy of flowing water and wind. Other energy sources include solar photovoltaics and geothermal power.
The fundamental principles of electricity generation were discovered in the 1820s and early 1830s by British scientist Michael Faraday. His method, still used today, is for electricity to be generated by the movement of a loop of wire, or disc of copper between the poles of a magnet. Central power stations became economically practical with the development of alternating current (AC) power transmission, using power transformers to transmit power at high voltage and with low loss.
In 1870, commercial electricity production started with the coupling of the dynamo to the hydraulic turbine. In 1870, the mechanical production of electric power began the Second Industrial Revolution and created inventions using the energy, whose major contributors were Thomas Alva Edison and Nikola Tesla. Previously the only way to produce electricity was by chemical reactions or using battery cells, and the only practical use of electricity was for the telegraph.
Electricity generation at central power stations started in 1882, when a steam engine driving a dynamo at Pearl Street Station produced a DC current that powered public lighting on Pearl Street, New York. The new technology was quickly adopted by many cities around the world, which adapted their gas-fueled street lights to electric power, and soon after electric lights would be used in public buildings, in businesses, and to power public transport, such as trams and trains.
The first power plants used water power or coal;[1] and today a variety of energy sources are used, such as coal, nuclear, natural gas, hydroelectric, wind generators, and oil, as well as solar energy, tidal power, and geothermal sources. The use of power-lines and power-poles has been significantly important in the distribution of electricity.
Several fundamental methods exist to convert other forms of energy into electrical energy. The triboelectric effect, piezoelectric effect, and even direct capture of the energy of nuclear decay Betavoltaics are used in niche applications, as is direct conversion of heat to electric power in the thermoelectric effect. Utility-scale generation is done by rotating electric generators, or by photovoltaic systems. A very small proportion of electric power distributed by utilities is provided by batteries.
Electric generators transform kinetic energy into electricity. This is the most used form for generating electricity and is based on Faraday's law. It can be seen experimentally by rotating a magnet within closed loops of a conducting material (e.g. copper wire). Almost all commercial electrical generation is done using electromagnetic induction, in which mechanical energy forces a generator to rotate:
Electrochemistry is the direct transformation of chemical energy into electricity, as in a battery. Electrochemical electricity generation is important in portable and mobile applications. Currently, most electrochemical power comes from batteries.[5] Primary cells, such as the common zinc–carbon batteries, act as power sources directly, but secondary cells (i.e. rechargeable batteries) are used for storage systems rather than primary generation systems. Open electrochemical systems, known as fuel cells, can be used to extract power either from natural fuels or from synthesized fuels. Osmotic power is a possibility at places where salt and fresh water merge.
The photovoltaic effect is the transformation of light into electrical energy, as in solar cells. Photovoltaic panels convert sunlight directly to electricity. Although sunlight is free and abundant, solar power electricity is still usually more expensive to produce than large-scale mechanically generated power due to the cost of the panels. Low-efficiency silicon solar cells have been decreasing in cost and multijunction cells with close to 30% conversion efficiency are now commercially available. Over 40% efficiency has been demonstrated in experimental systems.[6] Until recently, photovoltaics were most commonly used in remote sites where there is no access to a commercial power grid, or as a supplemental electricity source for individual homes and businesses. Recent advances in manufacturing efficiency and photovoltaic technology, combined with subsidies driven by environmental concerns, have dramatically accelerated the deployment of solar panels. Installed capacity is growing by 40% per year led by increases in Germany, Japan, and the United States.
The selection of electricity production modes and their economic viability varies in accordance with demand and region. The economics vary considerably around the world, resulting in widespread selling prices, e.g. the price in Venezuela is 3 cents per kWh while in Denmark it is 40 cents per kWh. Hydroelectric plants, nuclear power plants, thermal power plants and renewable sources have their own pros and cons, and selection is based upon the local power requirement and the fluctuations in demand. All power grids have varying loads on them but the daily minimum is the base load, supplied by plants which run continuously. Nuclear, coal, oil and gas plants can supply base load.
Thermal energy is economical in areas of high industrial density, as the high demand cannot be met by renewable sources. The effect of localized pollution is also minimized as industries are usually located away from residential areas. These plants can also withstand variation in load and consumption by adding more units or temporarily decreasing the production of some units. Nuclear power plants can produce a huge amount of power from a single unit. However, recent disasters in Japan have raised concerns over the safety of nuclear power, and the capital cost of nuclear plants is very high. Hydroelectric power plants are located in areas where the potential energy from falling water can be harnessed for moving turbines and the generation of power. It is not an economically viable source of production where the load varies too much during the annual production cycle and the ability to store the flow of water is limited.
Due to advancements in technology, and with mass production, renewable sources other than hydroelectricity (solar power, wind energy, tidal power, etc.) experienced decreases in cost of production, and the energy is now in many cases cost-comparative with fossil fuels. Many governments around the world provide subsidies to offset the higher cost of any new power production, and to make the installation of renewable energy systems economically feasible. However, their use is frequently limited by their intermittent nature. If natural gas prices are below $3 per million British thermal units, generating electricity from natural gas is cheaper than generating power by burning coal.[7]
Almost all commercial electrical power on Earth is generated with a turbine, driven by wind, water, steam or burning gas. The turbine drives a generator, thus transforming its mechanical energy into electrical energy by electromagnetic induction. There are many different methods of developing mechanical energy, including heat engines, hydro, wind and tidal power. Most electric generation is driven by heat engines. The combustion of fossil fuels supplies most of the energy to these engines, with a significant fraction from nuclear fission and some from renewable sources. The modern steam turbine (invented by Sir Charles Parsons in 1884) currently generates about 80% of the electric power in the world using a variety of heat sources. Turbine types include:
Although turbines are most common in commercial power generation, smaller generators can be powered by gasoline or diesel engines. These may used for back up generation or isolated villages.
Electric generators were known in simple forms from the discovery of the magnetic induction of electric current in the 1830s. In general, some form of prime mover such as an engine or the turbines described above, drives a rotating magnetic field past stationary coils of wire thereby turning mechanical energy into electricity. A very large 2000 MW(2,682,000 horsepower) unit designed by Siemens was built for unit 3 at the Olkiluoto Nuclear Power Plant.[9] The only commercial scale electricity production that does not employ a generator is solar PV.
This section needs to be updated. Please update this article to reflect recent events or newly available information. (March 2015) |
Total worldwide gross production of electricity in 2016 was 25,082TWh. Sources of electricity were coal and peat 38.3%, natural gas 23.1%, hydroelectric 16.6%, nuclear power 10.4%, oil 3.7%, solar/wind/geothermal/tidal/other 5.6%, biomass and waste 2.3%.[10]
- | Coal | Oil | Natural Gas |
Nuclear | Renewables | other | Total |
---|---|---|---|---|---|---|---|
Average electric power (TWh/year) | 8,263 | 1,111 | 4,301 | 2,731 | 3,288 | 568 | 20,261 |
Average electric power (GW) | 942.6 | 126.7 | 490.7 | 311.6 | 375.1 | 64.8 | 2311.4 |
Proportion | 41% | 5% | 21% | 13% | 16% | 3% | 100% |
Total energy consumed at all power plants for the generation of electricity was 4,398,768 ktoe (kilo ton of oil equivalent) which was 36% of the total for primary energy sources (TPES) of 2008.
Electricity output (gross) was 1,735,579 ktoe (20,185 TWh), efficiency was 39%, and the balance of 61% was generated heat. A small part (145,141 ktoe, which was 3% of the input total) of the heat was utilized at co-generation heat and power plants. The in-house consumption of electricity and power transmission losses were 289,681 ktoe.
The amount supplied to the final consumer was 1,445,285 ktoe (16,430 TWh) which was 33% of the total energy consumed at power plants and heat and power co-generation (CHP) plants.[11]
The United States has long been the largest producer and consumer of electricity, with a global share in 2005 of at least 25%, followed by China, Japan, Russia, and India. As of Jan-2010, total electricity generation for the two largest generators was as follows: USA: 3,992 billion kWh (3,992 TWh); China: 3,715 billion kWh (3,715 TWh).
Data source of values (electric power generated) is IEA/OECD.[12] Listed countries are top 20 by population or top 20 by GDP (PPP) and Saudi Arabia based on CIA World Factbook 2009.[13]
Country's electricity sector | Fossil Fuel | Nuclear | rank | Renewable | Bio other* |
total | rank | |||||||||||
---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|
Coal | Oil | Gas | sub total |
rank | Hydro | Geo Thermal |
Solar PV* |
Solar Thermal |
Wind | Tide | sub total |
rank | ||||||
World total | 8,263 | 1,111 | 4,301 | 13,675 | - | 2,731 | - | 3,288 | 65 | 12 | 0.9 | 219 | 0.5 | 3,584 | - | 271 | 20,261 | - |
Proportion | 41% | 5.5% | 21% | 67% | - | 13% | - | 16% | 0.3% | 0.06% | 0.004% | 1.1% | 0.003% | 18% | - | 1.3% | 100% | - |
China | 2,733 | 23 | 31 | 2,788 | 2 | 68 | 8 | 585 | - | 0.2 | - | 13 | - | 598 | 1 | 2.4 | 3,457 | 2 |
India | 569 | 34 | 82 | 685 | 5 | 15 | 12 | 114 | - | 0.02 | - | 14 | - | 128.02 | 6 | 2.0 | 830 | 5 |
USA | 2,133 | 58 | 1011 | 3,101 | 1 | 838 | 1 | 282 | 17 | 1.6 | 0.88 | 56 | - | 357 | 4 | 73 | 4,369 | 1 |
Indonesia | 61 | 43 | 25 | 130 | 19 | - | - | 12 | 8.3 | - | - | - | - | 20 | 17 | - | 149 | 20 |
Brazil | 13 | 18 | 29 | 59 | 23 | 14 | 13 | 370 | - | - | - | 0.6 | - | 370 | 3 | 20 | 463 | 9 |
Pakistan | 0.1 | 32 | 30 | 62 | 22 | 1.6 | 16 | 28 | - | - | - | - | - | 28 | 14 | - | 92 | 24 |
Bangladesh | 0.6 | 1.7 | 31 | 33 | 27 | - | - | 1.5 | - | - | - | - | - | 1.5 | 29 | - | 35 | 27 |
Nigeria | - | 3.1 | 12 | 15 | 28 | - | - | 5.7 | - | - | - | - | - | 5.7 | 25 | - | 21 | 28 |
Russia | 197 | 16 | 495 | 708 | 4 | 163 | 4 | 167 | 0.5 | - | - | 0.01 | - | 167 | 5 | 2.5 | 1,040 | 4 |
Japan | 288 | 139 | 283 | 711 | 3 | 258 | 3 | 83 | 2.8 | 2.3 | - | 2.6 | - | 91 | 7 | 22 | 1,082 | 3 |
Mexico | 21 | 49 | 131 | 202 | 13 | 9.8 | 14 | 39 | 7.1 | 0.01 | - | 0.3 | - | 47 | 12 | 0.8 | 259 | 14 |
Philippines | 16 | 4.9 | 20 | 40 | 26 | - | - | 9.8 | 11 | 0.001 | - | 0.1 | - | 21 | 16 | - | 61 | 26 |
Vietnam | 15 | 1.6 | 30 | 47 | 25 | - | - | 26 | - | - | - | - | - | 26 | 15 | - | 73 | 25 |
Ethiopia | - | 0.5 | - | 0.5 | 29 | - | - | 3.3 | 0.01 | - | - | - | - | 3.3 | 28 | - | 3.8 | 30 |
Egypt | - | 26 | 90 | 115 | 20 | - | - | 15 | - | - | - | 0.9 | - | 16 | 20 | - | 131 | 22 |
Germany | 291 | 9.2 | 88 | 388 | 6 | 148 | 6 | 27 | 0.02 | 4.4 | - | 41 | - | 72 | 9 | 29 | 637 | 7 |
Turkey | 58 | 7.5 | 99 | 164 | 16 | - | - | 33 | 0.16 | - | - | 0.85 | - | 34 | 13 | 0.22 | 198 | 19 |
DR Congo | - | 0.02 | 0.03 | 0.05 | 30 | - | - | 7.5 | - | - | - | - | - | 7.5 | 22 | - | 7.5 | 29 |
Iran | 0.4 | 36 | 173 | 209 | 11 | - | - | 5.0 | - | - | - | 0.20 | - | 5.2 | 26 | - | 215 | 17 |
Thailand | 32 | 1.7 | 102 | 135 | 18 | - | - | 7.1 | 0.002 | 0.003 | - | - | - | 7.1 | 23 | 4.8 | 147 | 21 |
France | 27 | 5.8 | 22 | 55 | 24 | 439 | 2 | 68 | - | 0.04 | - | 5.7 | 0.51 | 75 | 8 | 5.9 | 575 | 8 |
UK | 127 | 6.1 | 177 | 310 | 7 | 52 | 10 | 9.3 | - | 0.02 | - | 7.1 | - | 16 | 18 | 11 | 389 | 11 |
Italy | 49 | 31 | 173 | 253 | 9 | - | - | 47 | 5.5 | 0.2 | - | 4.9 | - | 58 | 11 | 8.6 | 319 | 12 |
South Korea | 192 | 15 | 81 | 288 | 8 | 151 | 5 | 5.6 | - | 0.3 | - | 0.4 | - | 6.3 | 24 | 0.7 | 446 | 10 |
Spain | 50 | 18 | 122 | 190 | 14 | 59 | 9 | 26 | - | 2.6 | 0.02 | 32 | - | 61 | 10 | 4.3 | 314 | 13 |
Canada | 112 | 9.8 | 41 | 162 | 17 | 94 | 7 | 383 | - | 0.03 | - | 3.8 | 0.03 | 386 | 2 | 8.5 | 651 | 6 |
Saudi Arabia | - | 116 | 88 | 204 | 12 | - | - | - | - | - | - | - | - | - | - | - | 204 | 18 |
Taiwan | 125 | 14 | 46 | 186 | 15 | 41 | 11 | 7.8 | - | 0.004 | - | 0.6 | - | 8.4 | 21 | 3.5 | 238 | 16 |
Australia | 198 | 2.8 | 39 | 239 | 10 | - | - | 12 | - | 0.2 | 0.004 | 3.9 | - | 16 | 19 | 2.2 | 257 | 15 |
Netherlands | 27 | 2.1 | 63 | 92 | 21 | 4.2 | 15 | 0.1 | - | 0.04 | - | 4.3 | - | 4.4 | 27 | 6.8 | 108 | 23 |
Country | Coal | Oil | Gas | sub total |
rank | Nuclear | rank | Hydro | Geo Thermal |
Solar PV |
Solar Thermal |
Wind | Tide | sub total |
rank | Bio other |
Total | rank |
Solar PV* is Photovoltaics Bio other* = 198TWh (Biomass) + 69TWh (Waste) + 4TWh (other)
Variations between countries generating electrical power affect concerns about the environment. In France only 10% of electricity is generated from fossil fuels, the US is higher at 70% and China is at 80%.[12] The cleanliness of electricity depends on its source. Most scientists agree that emissions of pollutants and greenhouse gases from fossil fuel-based electricity generation account for a significant portion of world greenhouse gas emissions; in the United States, electricity generation accounts for nearly 40% of emissions, the largest of any source. Transportation emissions are close behind, contributing about one-third of U.S. production of carbon dioxide.[14] In the United States, fossil fuel combustion for electric power generation is responsible for 65% of all emissions of sulfur dioxide, the main component of acid rain.[15] Electricity generation is the fourth highest combined source of NOx, carbon monoxide, and particulate matter in the US.[16] In July 2011, the UK parliament tabled a motion that "levels of (carbon) emissions from nuclear power were approximately three times lower per kilowatt hour than those of solar, four times lower than clean coal and 36 times lower than conventional coal".[17]
Technology | Description | 50th percentile (g CO2/kWhe) |
---|---|---|
Hydroelectric | reservoir | 4 |
Wind | onshore | 12 |
Nuclear | various generation II reactor types | 16 |
Biomass | various | 18 |
Solar thermal | parabolic trough | 22 |
Geothermal | hot dry rock | 45 |
Solar PV | Polycrystalline silicon | 46 |
Natural gas | various combined cycle turbines without scrubbing | 469 |
Coal | various generator types without scrubbing | 1001 |
This article uses material from the Wikipedia article "Electricity generation", which is released under the Creative Commons Attribution-Share-Alike License 3.0. There is a list of all authors in Wikipedia
EPLAN, Aucotec, CAE, AutoCAD Electrical, IGE XAO, ElCAD, 2D drawings, 2D symbols, 3D content, 3D catalog, EPLAN Electric P8, Zuken E3, schematics, dataportal, data portal, wscad universe, electronic, ProPanel3D, .EDZ, eClass Advanced, eCl@ss Advanced