A monument is a type of—usually three-dimensional—structure that was explicitly created to commemorate a person or event, or which has become relevant to a social group as a part of their remembrance of historic times or cultural heritage, due to its artistic, historical, political, technical or architectural importance. Examples of monuments include statues, (war) memorials, historical buildings, archaeological sites, and cultural assets. If there is a public interest in its preservation, a monument can for example be listed as a UNESCO World Heritage Site. [1]
The origin of the word "monument" comes from the Greek mnemosynon and the Latin moneo, monere, which means 'to remind', 'to advise' or 'to warn',[2] suggesting a monument allows us to see the past thus helping us visualize what is to come in the future.[3] In English the word "monumental" is often used in reference to something of extraordinary size and power, as in monumental sculpture, but also to mean simply anything made to commemorate the dead, as a funerary monument or other example of funerary art.
Monuments have been created for thousands of years, and they are often the most durable and famous symbols of ancient civilizations. Prehistoric tumuli, dolmens, and similar structures have been created in a large number of prehistoric cultures across the world, and the many forms of monumental tombs of the more wealthy and powerful members of a society are often the source of much of our information and art from those cultures.[4] As societies became organized on a larger scale, so monuments so large as to be difficult to destroy like the Egyptian Pyramids, the Greek Parthenon, the Great Wall of China, Indian Taj Mahal or the Moai of Easter Island have become symbols of their civilizations. In more recent times, monumental structures such as the Statue of Liberty and Eiffel Tower have become iconic emblems of modern nation-states. The term monumentality relates to the symbolic status and physical presence of a monument. In this context, German art historian Helmut Scharf states that “A monument exists in the form of an object and also as symbol thereof. As a language symbol, a monument usually refers to something concrete, in some rare cases it is also used metaphorically [...]. A monument can be a language symbol for a unity of several monuments [...] or only for a single one, but in a broader sense it can also be used in nearly all knowable planes of being. [...] What is considered a monument always depends on the importance it attributes to the prevailing or traditional consciousness of a specific historical and social situation.”
Basically, the definition framework of the term monument depends on the current historical frame conditions. Aspects of the Culture of Remembrance and cultural memory are also linked to it, as well as questions about the concepts of public sphere and durability (of the one memorized) and the form and content of the monument (work-like monument). From an art historical point of view, the dichotomy of content and form opens up the problem of the “linguistic ability” of the monument. It becomes clear that language is an eminent part of a monument and it is often represented in “non-objective” or “architectural monuments”, at least with a plaque. In this connection, the debate touches on the social mechanisms that combine with Remembrance. These are acceptance of the monument as an object, the conveyed contents and the impact of these contents.
Monuments are frequently used to improve the appearance of a city or location. Planned cities such as Washington D.C., New Delhi and Brasília are often built around monuments. For example, the Washington Monument's location was conceived by L'Enfant to help organize public space in the city, before it was designed or constructed. Older cities have monuments placed at locations that are already important or are sometimes redesigned to focus on one. As Shelley suggested in his famous poem "Ozymandias" ("Look on my works, ye Mighty, and despair!"), the purpose of monuments is very often to impress or awe.
Structures created for others purposes that have been made notable by their age, size or historic significance may also be regarded as monuments. This can happen because of great age and size, as in the case of the Great Wall of China, or because an event of great importance occurred there such as the village of Oradour-sur-Glane in France. Many countries use Ancient monument or similar terms for the official designation of protected structures or archeological sites which may originally have been ordinary domestic houses or other buildings.
Monuments are also often designed to convey historical or political information, and they can thus develop an active socio-political potency. They can be used to reinforce the primacy of contemporary political power, such as the column of Trajan or the numerous statues of Lenin in the Soviet Union. They can be used to educate the populace about important events or figures from the past, such as in the renaming of the old General Post Office Building in New York City to the James A. Farley Building (James Farley Post Office), after former Postmaster General James Farley.[5] To fulfill its informative and educative functions a monument needs to be open to the public, which means that its spatial dimension as well as its content can be experienced by the public, and be sustainable. The former may be achieved either by situating the monument in public space or by a public discussion about the it and its meaning, the latter by the materiality of the monument or if its content immediately becomes part of the collective or cultural memory.
The social meanings of monuments are rarely fixed and certain and are frequently 'contested' by different social groups. As an example: whilst the former East German socialist state may have seen the Berlin Wall as a means of 'protection' from the ideological impurity of the west, dissidents and others would often argue that it was symbolic of the inherent repression and paranoia of that state. This contention of meaning is a central theme of modern 'post processual' archaeological discourse.
The term is often used to describe any structure that is a significant and legally protected historic work, and many countries have equivalents of what is called in United Kingdom legislation a Scheduled Monument, which often include relatively recent buildings constructed for residential or industrial purposes, with no thought at the time that they would come to be regarded as "monuments".
Until recently, it was customary for archaeologists to study large monuments and pay less attention to the everyday lives of the societies that created them. New ideas about what constitutes the archaeological record have revealed that certain legislative and theoretical approaches to the subject are too focused on earlier definitions of monuments. An example has been the United Kingdom's Scheduled Ancient Monument laws.
Other than municipal or national government that protecting the monuments in their jurisdiction, there are institutions dedicated on the efforts to protect and preserve monuments that considered to possess special natural or cultural significance for the world, such as UNESCO's World Heritage Site programme[6] and World Monuments Fund.[1]
Recently, more and more monuments are being preserved digitally (in 3D models) through organisations as CyArk.[7]
Victoria monument in London, a memorial to Queen Victoria of the British Empire
Independence Monument in Kyiv commemorate the Independence of Ukraine
The Statue of Liberty, the symbol of the United States' freedom
The Cristo Redentor, a modern religious monument in Brazil
The Maqam Echahid, in Algiers, iconic concrete monument commemorating the Algerian war for independence
The Eiffel Tower, in Paris, a monument commemorating the French Revolution for its centenary
Monas in Jakarta, commemorates the Indonesian struggle for independence
The Juche Tower, a symbol of North Korea's "self reliant" Juche political stance
Azadi tower in Tehran, commemorates the 2,500 years of the Persian Empire and the history of Iran
Brandenburg Gate in Berlin, national symbol of Germany and its unity
Lenin mausoleum in Moscow, an enduring symbol of Soviet Union Communism and Cold War
The Chiang Kai-shek Memorial in Taipei is a monument to honor Chiang Kai-shek
The Cathedral of Santiago de Compostela where Saint James is buried
Kościuszko Mound, Poland commemorates Tadeusz Kościuszko
The Bell Telephone Memorial, commemorates the invention of the telephone, Brantford, Ontario
The Hiroshima Cenotaph and Atomic Bomb Dome to remember the victims of August 6, 1945 atomic bombing
This article uses material from the Wikipedia article "Monument", which is released under the Creative Commons Attribution-Share-Alike License 3.0. There is a list of all authors in Wikipedia
3D,model,library,rendering,Inca,Maya,Egypt,Pyramids,Bible, Quoran,Gizeh,Greek,Ancient,Medival Times, Stone Age