powered by CADENAS

Social Share

Amazon

Refreshable braille display (8791 views - Basics)

A refreshable braille display or braille terminal is an electro-mechanical device for displaying braille characters, usually by means of round-tipped pins raised through holes in a flat surface. Visually impaired computer users who cannot use a computer monitor can use it to read text output. Speech synthesizers are also commonly used for the same task, and a blind user may switch between the two systems or use both at the same time depending on circumstances. Deafblind computer users may also use refreshable braille displays.
Go to Article

Explanation by Hotspot Model

Youtube


    

Refreshable braille display

Refreshable braille display

A refreshable braille display or braille terminal is an electro-mechanical device for displaying braille characters, usually by means of round-tipped pins raised through holes in a flat surface. Visually impaired computer users who cannot use a computer monitor can use it to read text output. Speech synthesizers are also commonly used for the same task, and a blind user may switch between the two systems or use both at the same time depending on circumstances. Deafblind computer users may also use refreshable braille displays.

Mechanical details

The base of a refreshable braille display often integrates a pure braille keyboard. Similar to the Perkins Brailler, the input is performed by two sets of four keys on each side, while output is via a refreshable braille display consisting of a row of electro-mechanical character cells, each of which can raise or lower a combination of eight round-tipped pins. Other variants exist that use a conventional QWERTY keyboard for input and braille pins for output, as well as input-only and output-only devices.

On some models the position of the cursor is represented by vibrating the dots, and some models have a switch associated with each cell to move the cursor to that cell directly.

The mechanism which raises the dots uses the piezo effect of some crystals, whereby they expand when a voltage is applied to them. Such a crystal is connected to a lever, which in turn raises the dot. There has to be a crystal for each dot of the display, i.e. eight per character.

Because of the complexity of producing a reliable display that will cope with daily wear and tear, these displays are expensive. Usually, only 40 or 80 braille cells are displayed. Models with between 18 and 40 cells exist in some notetaker devices.

Software

The software that controls the display is called a screen reader. It gathers the content of the screen from the operating system, converts it into braille characters and sends it to the display. Screen readers for graphical operating systems are especially complex, because graphical elements like windows or slidebars have to be interpreted and described in text form. Modern operating systems usually have an Application Programming Interface to help screen readers obtain this information, such as UI Automation (UIA) for Microsoft Windows, VoiceOver for macOS and iOS, and AT-SPI for GNOME.

Future designs

  • A rotating-wheel Braille display was developed in 2000 by the National Institute of Standards and Technology (NIST) and another at the Leuven University in Belgium.[1] Both wheels are still in the process of commercialization.[clarification needed] In these units, braille dots are put on the edge of a spinning wheel, which allows the user to read continuously with a stationary finger while the wheel spins at a selected speed. The braille dots are set in a simple scanning-style fashion as the dots on the wheel spin past a stationary actuator that sets the braille characters. As a result, manufacturing complexity is greatly reduced and rotating-wheel braille displays, when in actual production, should be less expensive than traditional braille displays.
  • Designs for a full braille computer monitor have been patented but not yet produced.[2]
  • A full-page braille display with 1,000 cells (25 lines of 40 cells) was developed in 2015 by the Tactisplay Corp.[3] With total 12,000 pixels configured in 120*100, it can show any BANA compatible braille graphic page in 8 seconds. This video shows operation of the device.
  • Tactile is a real-time text-to-braille translation device, currently under development at the Massachusetts Institute of Technology.[4]
  • A group of researchers from the University of Michigan is developing a refreshable braille tablet, similar to a Kindle, as seen in this video.

Braille e-book

See also



This article uses material from the Wikipedia article "Refreshable braille display", which is released under the Creative Commons Attribution-Share-Alike License 3.0. There is a list of all authors in Wikipedia

Basics

3d,cad,model,library,download,drawing,step,cad blocks,basics,university,highschool,college,grammer school,statistics,3dprinted