A Rickshaw originally denoted a two or three-wheeled passenger cart, now known as a pulled rickshaw, which is generally pulled by one man carrying one passenger. The first known use of the term was in 1879.[1] Over time, cycle rickshaws (also known as pedicabs or trishaws), auto rickshaws, and electric rickshaws were invented, and have replaced the original pulled rickshaws, with a few exceptions for their use in tourism.
Pulled rickshaws created a popular form of transportation, and a source of employment for male laborers, within Asian cities in the 19th century. Their appearance was related to newly acquired knowledge of ball-bearing systems. Their popularity declined as cars, trains and other forms of transportation became widely available.
Auto rickshaws are becoming more popular in some cities in the 21st century as an alternative to taxis because of their low cost.
Rickshaw originates from the Japanese word jinrikisha (人力車, 人 jin = human, 力 riki = power or force, 車 sha = vehicle), which literally means "human-powered vehicle".[2]
Rickshaws were invented in Japan circa 1869,[3][4] after the lifting of a ban on wheeled vehicles from the Tokugawa period (1603–1868),[5] and at the beginning of a rapid period of technical advancement in Japan.[4][6]
There are lots of theories about the inventor, with the most likely and widely accepted theory describing the Rickshaw as having been invented in Japan in 1869,[4] by Izumi Yosuke,[7][8] who formed a partnership with Suzuki Tokujiro and Takayama Kosuke to build the vehicles,[9] having been "inspired by the horse carriages that had been introduced to the streets of Tokyo a few years earlier".[10]
Other theories about the inventor of the Rickshaw include:
Japan historian Seidensticker wrote of the theories:
Though the origins of the rickshaw are not entirely clear, they seem to be Japanese, and of Tokyo specifically. The most widely accepted theory offers the name of three inventors, and gives 1869 as the date of invention.[3]
The vehicle had a wooden carriage that rode on "superior Western wheels" and was a dramatic improvement over earlier modes of transportation. Whereas the earlier sedan chairs required two people, the rickshaw generally only required one. More than one person was required for hilly or mountainous areas. It also provided a smoother ride for the passenger. Other forms of vehicles at the time were drawn by animals or were wheelbarrows.[4]
The Powerhouse Museum in Sydney, Australia, has had a rickshaw in its collection for over 120 years. It was made about 1880 and is described as:
A rickshaw, or Jinrikisha, is a light, two-wheeled cart consisting of a doorless, chairlike body, mounted on springs with a collapsible hood and two shafts. Finished in black lacquer-ware over timber, it was drawn by a single rickshaw runner.[15]
In the Late 19th century, hand-pulled Rickshaws became an inexpensive, popular mode of transportation across Asia.[4] Peasants who migrated to large Asian cities often worked first as a rickshaw runner.[16][17] It was "the deadliest occupation in the East, [and] the most degrading for human beings to pursue."[17][nb 1]
Starting in 1870, the Tokyo government issued a permit to build and sell 人力車 (jinrikisha : rickshaws in Japanese) to the trio that are believed in Asia to be the rickshaw's inventors: Izumi Yosuke, Takayama Kosuke, and Suzuki Tokujiro. In order to operate a rickshaw in Tokyo, a seal was required from these men.[10] By 1872, they replaced the kago and norimono, becoming the main mode of transportation in Japan, with about 40,000 rickshaws in service. At that time man-power was much cheaper than horse-power; horses were generally only used by the military. Some of the rickshaws were artistically decorated with paintings and rear elevations. In this time, the more exuberant styles of decorations were banned.[18] If the families were well-off financially they might have their own rickshaw runner. Generally, runners covered 32 to 48 kilometres (20 to 30 mi) in a day, at an average traveling speed of 8 kilometres (5.0 mi) per hour.[9][15]
Japanese rickshaw manufacturers produced and exported rickshaws to Asian countries and South Africa.[9]
Singapore received its first rickshaws in 1880 and soon after they were prolific, making a "noticeable change in the traffic on Singapore's streets."[4] Bullock carts and gharries were used before rickshaws were introduced.[17]
Many of the poorest individuals in Singapore in the late nineteenth century were poverty-stricken, unskilled people of Chinese ancestry. Sometimes called coolies, the hardworking men found that pulling a rickshaw was a new opportunity for employment.[19]
In 1897, martial law was declared to end a four-day rickshaw workers' strike.[20]
In China, the rickshaw was first seen in 1873 and was used for public transportation the following year. Within a year there were 10,000 rickshaws in operation.[21] Around 1880 rickshaws appeared in India, first introduced in Simla by Reverend J. Fordyce.[22] At the turn of the century they were introduced in Calcutta, India, and by 1914 were a conveyance for hire.[4] The rickshaw was also introduced to Korea in the late 19th century.[23]
After World War II, there was a major shift in the use of man-powered rickshaws:
Hand-pulled rickshaws became an embarrassment to modernizing urban elites in the Third World, and were widely banned, in part because they were symbolic, not of modernity, but of a feudal world of openly marked class distinctions. Perhaps the seated rickshaw passenger is too close to the back of the laboring driver, who, besides, is metaphorically a draught animal harnessed between shafts.[20]
The cycle rickshaw was built in the 1880s and was first used with regularity starting in 1929 in Singapore. They were found in every south and east Asian country by 1950. By the late 1980s there were estimated 4 million cycle rickshaws in the world.[24]
Rickshaws were introduced to Durban, South Africa, and by 1904 there were about 2,000 registered rickshaw pullers.[4][25] [26] Rickshaws operated in Nairobi in the beginning of the 20th century; pullers went on strike there in 1908.[27] In the 1920s, they were used in Bagamoyo, Tanga, Tanzania and other areas of East Africa for short distances.[28][29]
The rickshaw's popularity in Japan had declined by the 1930s with the advent of automated forms of transportation like automobiles and trains. After World War II, when gasoline and automobiles were scarce, they made a temporary come-back. The rickshaw tradition has stayed alive in Kyoto and Tokyo's geisha districts.[15][16] In the 1990s, German-made cycle rickshaws called "velotaxis" were introduced in Japanese cities, including Kobe.[16]
In post Hong Kong, Rickshaw was one of the main transportation either for transporting goods or for transporting people during the Japanese invasion, as known as the Battle of Hong Kong. Japanese military hired a bunch of rickshaw pullers to have them gathered and organize with other cooks and seamen for an underground armed team to enact the anti-British Colony clan. [30] However, after World War II, other forms of transport such as pedicabs and streetcar became strong competitors of rickshaws, leading the business of rickshaws might be in stagnation.[31]
In China, since 1874 that the new Communist government banned the vehicle in south China and replaced by the rickshaw[32] , the popularity of rickshaws has always been high. Chiuchow men formed a faction within the Canton rickshaw pullers union in the 1920s. In addition, the Chiuchow pullers could be identified by their hats which were rounded and flat at the top; while the rival Hoklo men had a cone-shaped headgear with sharp points at the top.[33] However, it began to decline in the 1920s[16] as the new Communist government introduced the streetcar system in 1924.[34] The number of rickshaw pullers had declined from 44,200 to 25,877 six months after the opening of the tramway.[34] It had also caused the Beijing tramway riot in October 1929.[34] A rough form of a rickshaw is sometimes used for hauling coal, building materials or other material. Both motorized and pedal-power cycle rickshaws, or pedicabs, were used for short distance passenger travel.[35] There are still many rickshaws in many cities for either touring purposes (in big cities such as Beijing and Shanghai, with traditional Chinese rickshaws) or short range transportation in some counties. However, the new Communist government banned rickshaws in Canton in the early 1950s, leading to another low tide of rickshaws.[33]
In Singapore, the rickshaw's popularity increased into the 20th century. There were approximately 50,000 rickshaws in 1920 and that number had doubled by 1930.[3] Cycle rickshaws were used in Singapore beginning in 1929. Within six years pulled rickshaws were outnumbered by cycle rickshaws,[24] which were also used by sightseeing tourists.[36][nb 2]
In the 1930s, cycle rickshaws were used in Kolkata, India; Jakarta, Indonesia; and Dhaka, Bangladesh. By 1950 they could be found in many South and East Asian countries.[24] By the end of the 20th century, there were 300,000 such vehicles in Dhaka.[37] By the end of 2013, there were about 100,000 electric rickshaws in Delhi.[38]
Pedicabs were introduced in North America in 1962, where they were a means of transportation at the Seattle World's Fair in the state of Washington.[39]
The 21st century has seen a resurgence in rickshaws, particularly in motorized rickshaws and cycle rickshaws. Auto rickshaws, also called velotaxis, have resurged as they are about 1/3 to 1/2 the cost of regular taxis. German velotaxis are three-wheeled, powered vehicles with a space for a driver and, behind the driver, space for two passengers.[40] Cycle rickshaws are used in many North American, European, and Asian cities.[12] They are increasingly being used as an eco-friendly way of short-range transportation, particularly in urban areas. Along with auto rickshaws, they are also used (particularly by Asian cities) for tourism, because of their "novelty value as an entertaining form of transportation". [12]
In Madagascar, pulled cycle and auto rickshaws are a common form of transportation in a number of cities, especially Antsirabe. They are known as pousse-pousse, meaning push-push.[41][42]
Macau - Still uses tri-wheels bicycle rickshaw, or Riquexó in Portuguese, as Macau was a Portuguese colony in the past, and this kind of transportation were very famous till late 20th century, due to the fact of being a small city and few cars, not so much motorcycle, very bad public transport and none other transport such as train or subway. You can go around Macau peninsula and the two island on rickshaw, and visit the Riquexó Museum and see the evolution of rickshaw since 18th till nowadays.
Automated cycle rickshaws, called velotaxis, are popular in Kyoto and Tokyo, Japan. Their use is growing at a rate of about 20-30% a year in Japanese cities. The traditional rickshaws are still alive for travelers in some tourist places in Japan. Rickshaws are found in Hong Kong.[40] In China, automated and pedal-power cycle rickshaws, or pedicabs, are used for short distance passenger travel in large cities and many medium-sized cities.[35] Most Indian cities offer auto rickshaw service; Hand-pulled rickshaws do exist in some areas, such as Kolkata (Calcutta) as a part of their transport system which also includes cycle rickshaws.[43]
In Australia, Cycle rickshaws or trishaws (3 wheels) are used in Melbourne and St Kilda. They are also seen in Cowaramup, Western Australia at Bakehouse '38.
Cycle rickshaws or trishaws (3 wheels) are used in most large continental European cities,[44] such as:
Within the United Kingdom, pedicabs operate in:
Wikimedia Commons has media related to Rickshaws. |
Look up rickshaw in Wiktionary, the free dictionary. |
Types of rickshaws include:
Pulled rickshaw, Madagascar
Cycle rickshaws, Nepal
Auto rickshaw, San Francisco, California
Pulled Rickshaw in Kolkata
FRP,GEM e-rickshaw Haryana, India
Cycle rickshaw in Jakarta, Indonesia known as "Bechak"
Designer
|
|
This article uses material from the Wikipedia article "Rickshaw", which is released under the Creative Commons Attribution-Share-Alike License 3.0. There is a list of all authors in Wikipedia
Car, Truck,MotorBike, Bicycle, Engine, Racer