Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
This article needs additional citations for verification. Please help improve this article by adding citations to reliable sources. Unsourced material may be challenged and removed. Find sources: "Three-wheeler" – news · newspapers · books · scholar · JSTOR (January 2012) (Learn how and when to remove this template message) |
A three-wheeler is a vehicle with three wheels. Some are motorized tricycles, which may be legally classed as motorcycles, while others are tricycles without a motor, some of which are human-powered vehicles and animal-powered vehicles.
Many three-wheelers which exist in the form of motorcycle-based machines are often called trikes and often have the front single wheel and mechanics similar to that of a motorcycle and the rear axle similar to that of a car. Often such vehicles are owner-constructed using a portion of a rear-engine, rear-drive Volkswagen Beetle in combination with a motorcycle front end. Other trikes include ATVs that are specially constructed for off-road use.
Three-wheelers can have either one wheel at the back and two at the front (2F1R), (for example: Morgan Motor Company) or one wheel at the front and two at the back (1F2R) (such as the Reliant Robin). Due to better safety when braking, an increasingly popular form is the front-steering "tadpole" or "reverse trike" sometimes with front drive but usually with rear drive. A variant on the 'one at the front' layout was the Scott Sociable, which resembled a four-wheeler with a front wheel missing.[1]
Three-wheelers, including some cyclecars, bubble cars and microcars, are built for economic and legal reasons: in the UK for tax advantages, or in the US to take advantage of lower safety regulations, being classed as motorcycles. As a result of their light construction and potential better streamlining, three-wheeled cars are usually less expensive to operate.[citation needed]
Three-wheeler transport vehicles known as auto rickshaws are a common means of public transportation in many countries in the world, and are an essential form of urban transport in many developing countries such as India and the Philippines.
Auto rickshaws are a form of novelty transport in many Eastern countries.[citation needed]
Early automotive pioneer Karl Benz developed a number of three-wheeled models.[2] One of these, the Benz Patent Motorwagen,[3] is regarded as the first purpose-built automobile. It was made in 1885.
In 1896, John Henry Knight showed a tri-car at The Great Exhibition.[2]
In 1897, Edward Butler (inventor) made the Butler Petrol Cycle, another three-wheeled car.
A Conti 6 hp Tri-car competed in (but did not complete) a 1907 Peking to Paris race sponsored by a French newspaper, Le Matin.[4]
Goliath pickup truck at a meeting for vintage cars in the Nineties
Davis D-2 Divan, at the National Automotive and Truck Museum, Auburn, Indiana, United States
Folding City Car: Zaschka Three-wheeled car, 1929. Engelbert Zaschka, German inventor, and his folding three-wheeler.
Velorex was a manufacturing cooperative in Solnice, Czechoslovakia, formed in 1936 to satisfy demand for small, inexpensive city cars.
An early Daihatsu Midget, which would serve as the basis for auto rickshaws that proliferate across South and Southeast Asia
A configuration of two wheels in the front and one wheel at the back presents two advantages: it has improved aerodynamics, and that it readily enables the use of a small lightweight motorcycle powerplant and rear wheel. This approach was used by the Messerschmitt KR200 and BMW Isetta. Alternatively, a more conventional front-engine, front wheel drive layout as is common in four-wheeled cars can be used, with subsequent advantages for transversal stability (the center of mass is further to the front) and traction (two driven wheels instead of one). Some vehicles have a front engine driving the single rear wheel, similar to the rear engine driving the rear wheel. The wheel must support acceleration loads as well as lateral forces when in a turn, and loss of traction can be a challenge.
A new tadpole configuration has been proposed with a rear engine driving the front wheels. This concept (Dragonfly Three Wheeler[5]) claims both stability and traction (two driven wheels), as well as a unique driving experience.
With two wheels in the front (the "tadpole" form or "reverse trike") the vehicle is far more stable in braking turns, but remains more prone to overturning in normal turns compared to an equivalent four-wheeled vehicle, unless the center of mass is lower and/or further forward. Motorcycle-derived designs suffer from most of the weight being towards the rear of the vehicle.[citation needed]
For lower wind resistance (which increases fuel efficiency), a teardrop shape is often used.[citation needed] A teardrop is wide and round at the front, tapering at the back. The three-wheel configuration allows the two front wheels to create the wide round surface of the vehicle. The single rear wheel allows the vehicle to taper at the back. Examples include the Aptera 2 Series and Myers Motors NmG.
Having one wheel in front and two in the rear for power reduces the cost of the steering mechanism but greatly decreases lateral stability when cornering while braking.
When the single wheel is in the front (the "delta" form, as in a child's pedal tricycle), the vehicle is inherently unstable in a braking turn, as the combined tipping forces at the center of mass from turning and braking can rapidly extend beyond the triangle formed by the contact patches of the wheels. This type, if not tipped, also has a greater tendency to spin out ("swap ends") when handled roughly.[citation needed]
The disadvantage of a three-wheel configuration is lateral instability—the car will tip over in a turn before it will slide. This can be prevented in three ways:
In the case of a three-wheeled ATV, tipping may be avoided by the rider leaning into turns.
To improve stability some three-wheelers are designed to tilt while cornering like a motorcyclist would do. The tilt may be controlled manually, mechanically or by computer.
A tilting three-wheeler's body or wheels, or both, tilt in the direction of the turn. Such vehicles can corner safely even with a narrow track.
Some tilting three-wheelers could be considered to be forms of feet forwards motorcycles or cabin motorcycles or both.
Three-wheeled battery powered designs include:
The world's fastest solar-powered vehicle, Ashiya University's Sky Ace TIGA, is a three-wheeler. It achieved 91.332 kilometres per hour (56.751 mph) at Shimojishima Airport, in Miyakojima, Okinawa, Japan, to win the Guinness World Record, on 20 August 2014.[6] It took the record from another three-wheeler, Sunswift IV, designed and built at the University of New South Wales in Australia,[7] by a margin of almost 3 km/h.
The world's first full-size self-propelled land vehicle was a three-wheeler. French Army Captain Nicolas-Joseph Cugnot's 1770 fardier à vapeur (steam dray), a steam tricycle with a top speed of around 3 km/h (2 mph), was intended for hauling artillery.[8]
Another of the earliest preserved examples is the Long steam tricycle, built by George A. Long around 1880 and patented in 1883,[9][10] now on display at the Smithsonian Institution.
The Whike is a recumbent tricycle with a sail, made in the Netherlands.
Due to the incidence of injuries related to their use, a 10-year ban, entirely voluntary for manufacturers, was placed on the sale of new three-wheeled all-terrain vehicles in the United States in January 1988.[citation needed] However, it should be noted that more injuries were sustained by riders by not applying a proper riding technique, and lack of wearing proper safety gear such as helmets and riding boots. In a search conducted by the Consumer Product Safety Commission, it was determined that "no inherent flaw was found in the three wheel design".[citation needed]
The examples and perspective in this section may not represent a worldwide view of the subject. You may improve this article, discuss the issue on the talk page, or create a new article, as appropriate. (October 2015) (Learn how and when to remove this template message) |
In the U.S, the National Highway Traffic Safety Administration defines and regulates three-wheeled vehicles as motorcycles.[11] However, in 2015 a bill was introduced in Congress that would prevent some three wheeled vehicles from being classified as motorcycles in the United States, instead creating a new classification for "autocycles".[12][13]
Driver's license and registration requirements vary on a state-by-state basis. Some states require drivers of three wheeled vehicles to have a motorcycle license and register the vehicle as a motorcycle. Some states, including Virginia, Kansas, and Indiana, classify some three wheeled vehicles as autocycles. Virginia defines an autocycle as "a three-wheeled motor vehicle that has a steering wheel and seating that does not require the operator to straddle or sit astride and is manufactured to comply with federal safety requirements for motorcycles."[14] Indiana defines it as "a three (3) wheeled motor vehicle in which the operator and passenger ride in a completely or partially enclosed seating area that is equipped with:(1) a rollcage or roll hoops; (2) safety belts for each occupant; and (3) antilock brakes;and is designed to be controlled with a steering wheel and pedals."[15] In other jurisdictions, such as British Columbia, Canada, and Connecticut, a three-wheeled vehicle with an enclosed passenger compartment or partially enclosed seat is considered an automobile.[citation needed]
Name | Country | Years manufactured | Comments |
---|---|---|---|
Léon Bollée Voiturette | France | 1895–? | |
TriPodCars[16] Tripod 1 | Australia | 2012–? | 400 kg Reverse Trike, Blackbird 1100 (150 hp), Bandit 1250, Hayabusa 1300, ZX14R (200+ hp) and EV |
Berkeley Cars Berkeley T60 | England | 1959 | |
Egg | Switzerland | 1896–99 | |
Advance 6 hp air-cooled Tri Car and 9 hp water-cooled Tri Car[17] | England | 1902–12 | |
Humber Tricar[18][19] | England | 1904 | |
Riley Olympia Tricar[20] | England | 1904 | [21] |
Lagonda Tricar[22] | England | 1904–07 | total production: 69 cars |
Anglian | England | 1905–07 | |
Armadale | England | 1906–07 | |
Morgan V-Twin and F-Series | England | 1911–39, 1932–52 | Morgan Super Sports 2-Seater 1937 |
American Tri-Car | United States | 1912 | |
Birmingham Small Arms Company Three Wheeler | England | 1929–36 | 1100cc engine[23] |
Zaschka | Germany | 1929 | Folding three-wheeler: Zaschka Three-wheeler 1929 |
Dymaxion car | United States | 1933 | Concept car designed by Buckminster Fuller |
Mathis VEL 333 | France | 1946 | 3 seats, flat-twin front engine, aluminium body, production less than 10 units |
1951 Hoffmann | Germany | 1951 | 2 seats, aluminium body, engine mounted on the rear wheel steering pivot |
Velorex Oskar and other models | Czechoslovakia | 1951–71 | Originally with leather bodies |
Isetta | UK | 1957–62 | Three-wheeled version of the Isetta built in the UK to take advantage of tax and licensing regulations |
Scootacar | UK | 1957–64 | |
Messerschmitt KR175 | Germany | 1953–55 | |
Messerschmitt KR200 | Germany | 1955–64 | |
Peel P50 | Isle of Man | 1963–64 | Smallest production car ever built |
HM Vehicles Free-way | United States | 1979–82 | |
Campagna T-Rex | Canada | 1996–present | |
Malone Car Company F1000|Skunk SS|TAZR | United Kingdom | 1999–present | High power internal combustion and pure electric versions released November 2010 |
Cree SAM | Switzerland | 2001 | Electric, only 80 produced |
Myers Motors NmG ("No more Gas") | United States | 2006–present | Single occupant all-electric plug-in |
BRP Can-Am Spyder RoadsterCan-Am Spyder Roadster | Canada | 2007–present | The Can-Am Spyder is a three-wheeled motorcycle manufactured by Bombardier Recreational Products |
Brudeli 645L | Norway | 2008– | |
Moonbeam | United States | 2008–present | 100 mpg DIY, fabric-covered car based on parts from two Honda 150cc motorscooters[24] |
Triac | United States | 2009–2011 | Electric, never entered production |
XR-3 Hybrid | United States | Plans–2008, Kit–2009 | Front 3 cylinder diesel (125 mpg), rear electric 40 mile range -(220 mpg when used as a hybrid)[25] |
Aptera 2e | United States | Electric or Plug-in hybrid, 300 mpg‑US (0.78 L/100 km) | |
Triton Trikes | United States | 2000–present | Gas power 42+ mpg - Parts lists, customize, Kits Available - call for info |
Polaris Slingshot | United States | 2015–present | |
Vanderhall Laguna Roadster | United States | 2016–present | Exotic Auto-cycle, mono-aluminum chassis, carbon fiber body, 200 HP, 1550 pounds dry weight, side-by-side seating, fwd. 1.4 liter turbo GM power plant. 6 speed Automatic with paddle shift option. Manufactured by Vanderhall Motor Works in Provo, Utah U.S.A |
Elio Motors | Shreveport, LA, United States | Begins 1H 2016[26] | Two passenger fully enclosed cockpit with car controls |
Girfalco Azkarra | Canada | 2017 | All-electric two-passenger three-wheeled vehicle, possibly the quickest three-wheeler |
Go3Wheeler | United States | 2014 | single person three wheeler |
Corbin Sparrow | |||
Piaggio MP3 | |||
Tri-Magnum | |||
Volkswagen GX3 | |||
Morgan 3-Wheeler | England | 2012–present | The power train is a 1983cc ‘V-twin’ fuel injected engine mated to a Mazda 5 speed (and reverse) gearbox |
Fuel Vapours Alé | Canada | 2005–present | Prototype. Gets 92 mpg. |
Name | Country | Years manufactured | Comments |
---|---|---|---|
Apino | Brazil | unknown | Mini Truck |
Benz Patent Motorwagen | Germany | 1886–93 | |
Eco-Fueler | USA | 2009–Present | |
La Va Bon Train | France | 1904–10 | 50–100 believed built |
Davis D-2 Divan | United States | 1947–48 | about 13–17 built, including the 494, a Jeep-like military vehicle[27] |
Scammell Scarab | England | 1948–67 | |
Autoette | United States | 1948–70 | |
Daihatsu Bee | Japan | 1951–1952 | |
Daihatsu Midget | Japan | 1957–72 | |
Mazda T-2000 | Japan | 1957–74 | |
Mazda K360 | Japan | 1959–69 | |
Mazda T600 | Japan | 1959–71 | |
Kia K-360 | Republic of Korea | 1962–1973 | Kia's first truck (OEM Mazda K-360) |
Kia T-1500 | Republic of Korea | 1963–? | 1484 cc, 60 hp, four cylinder and a maximum load of 1.5 tons. (OEM Mazda T-1500) |
Kia T-600 | Republic of Korea | 1969–1974 | 577cc, 20 HP and 500 kg load. Top speed of 75 km/h. 7726 produced (OEM Mazda T-600) |
Kia T-2000 | Republic of Korea | 1967–1981 | 1985 cc, 81 hp, four cylinder and a maximum load of 2 tons. 15952 produced (OEM Mazda T-2000) |
Electra-King | United States | 1964?–1980s? | Two-seater electric car[28] |
Bond 875 | England | 1965–70 | |
Bond Bug | England | 1970–74 | |
Reliant Robin | England | 1973–81, 1989–2002 | |
Reliant Regal | England | 1953–1973 | An example of this vehicle is the iconic van belonging to Del Boy and Rodney Trotter in the long-running BBC sitcom Only Fools and Horses, though it is often incorrectly referred to as a Reliant Robin. |
GM Lean Machine[29][30] | United States | 1980s | Tilt, concept car[31] |
Trivette | United States | 1974–1976 | |
Twike | Germany | 1995–present | Electric-human-power hybrid, developed in Switzerland |
ZAP Xebra | United States | 2006–2009 | electric power |
eTuk | United States | 2014– | re-designed tuk tuk for the US Market, including an all-electric motor[32] |
Snyder ST600-C | United States | 20??–20?? | |
Carver | Netherlands | 2007–2009 | Tilt |
CityEl | Denmark | Mini-El, City-El | |
CLEVER | |||
Harley-Davidson Servi-Car |
This article uses material from the Wikipedia article "Three-wheeler", which is released under the Creative Commons Attribution-Share-Alike License 3.0. There is a list of all authors in Wikipedia
Car, Truck,MotorBike, Bicycle, Engine, Racer